#include "inc/hw_types.h"
#include "driverlib/5xx_6xx/debug.h"
#include "driverlib/5xx_6xx/timer.h"
#include "deprecated/CCS/msp430xgeneric.h"
Functions | |
void | privateTimerProcessClockSourceDivider (unsigned int baseAddress, unsigned int clockSourceDivider) |
DEPRECATED FILE - Replaced by timera.c and timerb.c. | |
void | Timer_startContinuousMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int timerInterruptEnable_TAIE, unsigned int timerclear) |
void | Timer_startContinousMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int timerInterruptEnable_TAIE, unsigned int timerclear) |
void | Timer_startUpMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int timerPeriod, unsigned int timerInterruptEnable_TAIE, unsigned int captureCompareInterruptEnable_CCR0_CCIE, unsigned int timerclear) |
void | Timer_startUpDownMode (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int timerPeriod, unsigned int timerInterruptEnable_TAIE, unsigned int captureCompareInterruptEnable_CCR0_CCIE, unsigned int timerclear) |
void | Timer_initCapture (unsigned int baseAddress, unsigned int captureRegister, unsigned int captureMode, unsigned int captureInputSelect, unsigned short synchronizeCaptureSource, unsigned short captureInterruptEnable, unsigned int captureOutputMode) |
void | Timer_initCompare (unsigned int baseAddress, unsigned int compareRegister, unsigned short compareInterruptEnable, unsigned int compareOutputMode, unsigned int compareValue) |
void | Timer_enableInterrupt (unsigned int baseAddress) |
void | Timer_disableInterrupt (unsigned int baseAddress) |
unsigned long | Timer_getInterruptStatus (unsigned int baseAddress) |
void | Timer_enableCaptureCompareInterrupt (unsigned int baseAddress, unsigned int captureCompareRegister) |
void | Timer_disableCaptureCompareInterrupt (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned long | Timer_getCaptureCompareInterruptStatus (unsigned int baseAddress, unsigned int mask) |
void | Timer_clear (unsigned int baseAddress) |
unsigned short | Timer_getSynchronizedCaptureCompareInput (unsigned int baseAddress, unsigned int captureCompareRegister, unsigned short synchronized) |
unsigned char | Timer_getOutputForOutputModeOutBitValue (unsigned int baseAddress, unsigned int captureCompareRegister) |
unsigned int | Timer_getCaptureCompareCount (unsigned int baseAddress, unsigned int captureCompareRegister) |
void | Timer_setOutputForOutputModeOutBitValue (unsigned int baseAddress, unsigned int captureCompareRegister, unsigned char outputModeOutBitValue) |
void | Timer_generatePWM (unsigned int baseAddress, unsigned int clockSource, unsigned int clockSourceDivider, unsigned int timerPeriod, unsigned int compareRegister, unsigned int compareOutputMode, unsigned int dutyCycle) |
void | Timer_stop (unsigned int baseAddress) |
void | Timer_setCompareValue (unsigned int baseAddress, unsigned int compareRegister, unsigned int compareValue) |
void | Timer_clearTimerInterruptFlag (unsigned int baseAddress) |
void | Timer_clearCaptureCompareInterruptFlag (unsigned int baseAddress, unsigned int captureCompareRegister) |
void privateTimerProcessClockSourceDivider | ( | unsigned int | baseAddress, |
unsigned int | clockSourceDivider | ||
) |
DEPRECATED FILE - Replaced by timera.c and timerb.c.
Private clock source divider helper function
baseAddress | is the base address of the Timer module. |
clockSourceDivider | is the desired divider for the clock source |
Modified registers are TAxEX0, TAxCTL
References HWREG, TIMER_CLOCKSOURCE_DIVIDER_1, TIMER_CLOCKSOURCE_DIVIDER_10, TIMER_CLOCKSOURCE_DIVIDER_12, TIMER_CLOCKSOURCE_DIVIDER_14, TIMER_CLOCKSOURCE_DIVIDER_16, TIMER_CLOCKSOURCE_DIVIDER_2, TIMER_CLOCKSOURCE_DIVIDER_20, TIMER_CLOCKSOURCE_DIVIDER_24, TIMER_CLOCKSOURCE_DIVIDER_28, TIMER_CLOCKSOURCE_DIVIDER_3, TIMER_CLOCKSOURCE_DIVIDER_32, TIMER_CLOCKSOURCE_DIVIDER_4, TIMER_CLOCKSOURCE_DIVIDER_40, TIMER_CLOCKSOURCE_DIVIDER_48, TIMER_CLOCKSOURCE_DIVIDER_5, TIMER_CLOCKSOURCE_DIVIDER_56, TIMER_CLOCKSOURCE_DIVIDER_6, TIMER_CLOCKSOURCE_DIVIDER_64, TIMER_CLOCKSOURCE_DIVIDER_7, and TIMER_CLOCKSOURCE_DIVIDER_8.
Referenced by Timer_generatePWM(), Timer_startContinuousMode(), Timer_startUpDownMode(), and Timer_startUpMode().
void Timer_startContinuousMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | timerInterruptEnable_TAIE, | ||
unsigned int | timerclear | ||
) |
Starts timer in continuous mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMER_CLOCKSOURCE_EXTERNAL_TXCLK [Default value] TIMER_CLOCKSOURCE_ACLK TIMER_CLOCKSOURCE_SMCLK TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMER_CLOCKSOURCE_DIVIDER_1 [Default value] TIMER_CLOCKSOURCE_DIVIDER_2 TIMER_CLOCKSOURCE_DIVIDER_4 TIMER_CLOCKSOURCE_DIVIDER_8 TIMER_CLOCKSOURCE_DIVIDER_3 TIMER_CLOCKSOURCE_DIVIDER_5 TIMER_CLOCKSOURCE_DIVIDER_6 TIMER_CLOCKSOURCE_DIVIDER_7 TIMER_CLOCKSOURCE_DIVIDER_10 TIMER_CLOCKSOURCE_DIVIDER_12 TIMER_CLOCKSOURCE_DIVIDER_14 TIMER_CLOCKSOURCE_DIVIDER_16 TIMER_CLOCKSOURCE_DIVIDER_20 TIMER_CLOCKSOURCE_DIVIDER_24 TIMER_CLOCKSOURCE_DIVIDER_28 TIMER_CLOCKSOURCE_DIVIDER_32 TIMER_CLOCKSOURCE_DIVIDER_40 TIMER_CLOCKSOURCE_DIVIDER_48 TIMER_CLOCKSOURCE_DIVIDER_56 TIMER_CLOCKSOURCE_DIVIDER_64 |
timerInterruptEnable_TAIE | is to enable or disable timer interrupt Valid values are TIMER_TAIE_INTERRUPT_ENABLE TIMER_TAIE_INTERRUPT_DISABLE [Default value] |
timerclear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMER_DO_CLEAR TIMER_SKIP_CLEAR [Default value] |
Modified reister is TAxCTL
References ASSERT, HWREG, privateTimerProcessClockSourceDivider(), TIMER_CLOCKSOURCE_ACLK, TIMER_CLOCKSOURCE_DIVIDER_1, TIMER_CLOCKSOURCE_DIVIDER_10, TIMER_CLOCKSOURCE_DIVIDER_12, TIMER_CLOCKSOURCE_DIVIDER_14, TIMER_CLOCKSOURCE_DIVIDER_16, TIMER_CLOCKSOURCE_DIVIDER_2, TIMER_CLOCKSOURCE_DIVIDER_20, TIMER_CLOCKSOURCE_DIVIDER_24, TIMER_CLOCKSOURCE_DIVIDER_28, TIMER_CLOCKSOURCE_DIVIDER_3, TIMER_CLOCKSOURCE_DIVIDER_32, TIMER_CLOCKSOURCE_DIVIDER_4, TIMER_CLOCKSOURCE_DIVIDER_40, TIMER_CLOCKSOURCE_DIVIDER_48, TIMER_CLOCKSOURCE_DIVIDER_5, TIMER_CLOCKSOURCE_DIVIDER_56, TIMER_CLOCKSOURCE_DIVIDER_6, TIMER_CLOCKSOURCE_DIVIDER_64, TIMER_CLOCKSOURCE_DIVIDER_7, TIMER_CLOCKSOURCE_DIVIDER_8, TIMER_CLOCKSOURCE_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_SMCLK, TIMER_CONTINUOUS_MODE, TIMER_DO_CLEAR, TIMER_SKIP_CLEAR, TIMER_TAIE_INTERRUPT_DISABLE, TIMER_TAIE_INTERRUPT_ENABLE, and TIMER_UPDOWN_MODE.
Referenced by Timer_startContinousMode().
void Timer_startContinousMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | timerInterruptEnable_TAIE, | ||
unsigned int | timerclear | ||
) |
DEPRECATED- Spelling Error Fixed Starts timer in continuous mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMER_CLOCKSOURCE_EXTERNAL_TXCLK [Default value] TIMER_CLOCKSOURCE_ACLK TIMER_CLOCKSOURCE_SMCLK TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMER_CLOCKSOURCE_DIVIDER_1 [Default value] TIMER_CLOCKSOURCE_DIVIDER_2 TIMER_CLOCKSOURCE_DIVIDER_4 TIMER_CLOCKSOURCE_DIVIDER_8 TIMER_CLOCKSOURCE_DIVIDER_3 TIMER_CLOCKSOURCE_DIVIDER_5 TIMER_CLOCKSOURCE_DIVIDER_6 TIMER_CLOCKSOURCE_DIVIDER_7 TIMER_CLOCKSOURCE_DIVIDER_10 TIMER_CLOCKSOURCE_DIVIDER_12 TIMER_CLOCKSOURCE_DIVIDER_14 TIMER_CLOCKSOURCE_DIVIDER_16 TIMER_CLOCKSOURCE_DIVIDER_20 TIMER_CLOCKSOURCE_DIVIDER_24 TIMER_CLOCKSOURCE_DIVIDER_28 TIMER_CLOCKSOURCE_DIVIDER_32 TIMER_CLOCKSOURCE_DIVIDER_40 TIMER_CLOCKSOURCE_DIVIDER_48 TIMER_CLOCKSOURCE_DIVIDER_56 TIMER_CLOCKSOURCE_DIVIDER_64 |
timerInterruptEnable_TAIE | is to enable or disable timer interrupt Valid values are TIMER_TAIE_INTERRUPT_ENABLE TIMER_TAIE_INTERRUPT_DISABLE [Default value] |
timerclear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMER_DO_CLEAR TIMER_SKIP_CLEAR [Default value] |
Modified reister is TAxCTL
References Timer_startContinuousMode().
void Timer_startUpMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | timerPeriod, | ||
unsigned int | timerInterruptEnable_TAIE, | ||
unsigned int | captureCompareInterruptEnable_CCR0_CCIE, | ||
unsigned int | timerclear | ||
) |
Starts timer in up mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMER_CLOCKSOURCE_EXTERNAL_TXCLK [Default value] TIMER_CLOCKSOURCE_ACLK TIMER_CLOCKSOURCE_SMCLK TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMER_CLOCKSOURCE_DIVIDER_1 [Default value] TIMER_CLOCKSOURCE_DIVIDER_2 TIMER_CLOCKSOURCE_DIVIDER_4 TIMER_CLOCKSOURCE_DIVIDER_8 TIMER_CLOCKSOURCE_DIVIDER_3 TIMER_CLOCKSOURCE_DIVIDER_5 TIMER_CLOCKSOURCE_DIVIDER_6 TIMER_CLOCKSOURCE_DIVIDER_7 TIMER_CLOCKSOURCE_DIVIDER_10 TIMER_CLOCKSOURCE_DIVIDER_12 TIMER_CLOCKSOURCE_DIVIDER_14 TIMER_CLOCKSOURCE_DIVIDER_16 TIMER_CLOCKSOURCE_DIVIDER_20 TIMER_CLOCKSOURCE_DIVIDER_24 TIMER_CLOCKSOURCE_DIVIDER_28 TIMER_CLOCKSOURCE_DIVIDER_32 TIMER_CLOCKSOURCE_DIVIDER_40 TIMER_CLOCKSOURCE_DIVIDER_48 TIMER_CLOCKSOURCE_DIVIDER_56 TIMER_CLOCKSOURCE_DIVIDER_64 |
timerPeriod | is the specified timer period. This is the value that gets written into the CCR0. Limited to 16 bits[unsigned int] |
timerInterruptEnable_TAIE | is to enable or disable timer interrupt Valid values are TIMER_TAIE_INTERRUPT_ENABLE and TIMER_TAIE_INTERRUPT_DISABLE [Default value] |
captureCompareInterruptEnable_CCR0_CCIE | is to enable or disable timer CCR0 captureComapre interrupt. Valid values are TIMER_CCIE_CCR0_INTERRUPT_ENABLE and TIMER_CCIE_CCR0_INTERRUPT_DISABLE [Default value] |
timerclear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMER_DO_CLEAR TIMER_SKIP_CLEAR [Default value] |
Modified registers are TAxCTL, TAxCCR0, TAxCCTL0
References ASSERT, HWREG, privateTimerProcessClockSourceDivider(), TIMER_CCIE_CCR0_INTERRUPT_ENABLE, TIMER_CLOCKSOURCE_ACLK, TIMER_CLOCKSOURCE_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_SMCLK, TIMER_DO_CLEAR, TIMER_SKIP_CLEAR, TIMER_TAIE_INTERRUPT_ENABLE, TIMER_UP_MODE, and TIMER_UPDOWN_MODE.
void Timer_startUpDownMode | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | timerPeriod, | ||
unsigned int | timerInterruptEnable_TAIE, | ||
unsigned int | captureCompareInterruptEnable_CCR0_CCIE, | ||
unsigned int | timerclear | ||
) |
Starts timer in up down mode.
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMER_CLOCKSOURCE_EXTERNAL_TXCLK [Default value] TIMER_CLOCKSOURCE_ACLK TIMER_CLOCKSOURCE_SMCLK TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMER_CLOCKSOURCE_DIVIDER_1 [Default value] TIMER_CLOCKSOURCE_DIVIDER_2 TIMER_CLOCKSOURCE_DIVIDER_4 TIMER_CLOCKSOURCE_DIVIDER_8 TIMER_CLOCKSOURCE_DIVIDER_3 TIMER_CLOCKSOURCE_DIVIDER_5 TIMER_CLOCKSOURCE_DIVIDER_6 TIMER_CLOCKSOURCE_DIVIDER_7 TIMER_CLOCKSOURCE_DIVIDER_10 TIMER_CLOCKSOURCE_DIVIDER_12 TIMER_CLOCKSOURCE_DIVIDER_14 TIMER_CLOCKSOURCE_DIVIDER_16 TIMER_CLOCKSOURCE_DIVIDER_20 TIMER_CLOCKSOURCE_DIVIDER_24 TIMER_CLOCKSOURCE_DIVIDER_28 TIMER_CLOCKSOURCE_DIVIDER_32 TIMER_CLOCKSOURCE_DIVIDER_40 TIMER_CLOCKSOURCE_DIVIDER_48 TIMER_CLOCKSOURCE_DIVIDER_56 TIMER_CLOCKSOURCE_DIVIDER_64 |
timerPeriod | is the specified timer period |
timerInterruptEnable_TAIE | is to enable or disable timer interrupt Valid values are TIMER_TAIE_INTERRUPT_ENABLE TIMER_TAIE_INTERRUPT_DISABLE [Default value] |
captureCompareInterruptEnable_CCR0_CCIE | is to enable or disable timer CCR0 captureComapre interrupt. Valid values are TIMER_CCIE_CCR0_INTERRUPT_ENABLE and TIMER_CCIE_CCR0_INTERRUPT_DISABLE [Default value] |
timerclear | decides if timer clock divider, count direction, count need to be reset. Valid values are TIMER_DO_CLEAR TIMER_SKIP_CLEAR [Default value] |
Modified registers are TAxCTL, TAxCCR0, TAxCCTL0
References ASSERT, HWREG, privateTimerProcessClockSourceDivider(), TIMER_CCIE_CCR0_INTERRUPT_ENABLE, TIMER_CLOCKSOURCE_ACLK, TIMER_CLOCKSOURCE_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_SMCLK, TIMER_DO_CLEAR, TIMER_SKIP_CLEAR, TIMER_TAIE_INTERRUPT_ENABLE, and TIMER_UPDOWN_MODE.
void Timer_initCapture | ( | unsigned int | baseAddress, |
unsigned int | captureRegister, | ||
unsigned int | captureMode, | ||
unsigned int | captureInputSelect, | ||
unsigned short | synchronizeCaptureSource, | ||
unsigned short | captureInterruptEnable, | ||
unsigned int | captureOutputMode | ||
) |
Initializes Capture Mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
captureMode | is the capture mode selected. Valid values are TIMER_CAPTUREMODE_NO_CAPTURE [Default value] TIMER_CAPTUREMODE_RISING_EDGE TIMER_CAPTUREMODE_FALLING_EDGE TIMER_CAPTUREMODE_RISING_AND_FALLING_EDGE |
captureInputSelect | decides the Input Select TIMER_CAPTURE_INPUTSELECT_CCIxA [Default value] TIMER_CAPTURE_INPUTSELECT_CCIxB TIMER_CAPTURE_INPUTSELECT_GND TIMER_CAPTURE_INPUTSELECT_Vcc |
synchronizeCaptureSource | decides if capture source should be synchronized with timer clock Valid values are TIMER_CAPTURE_ASYNCHRONOUS [Default value] TIMER_CAPTURE_SYNCHRONOUS |
captureInterruptEnable | is to enable or disable timer captureComapre interrupt. Valid values are TIMER_CAPTURECOMPARE_INTERRUPT_DISABLE [Default value] TIMER_CAPTURECOMPARE_INTERRUPT_ENABLE |
captureOutputMode | specifies the ouput mode. Valid values are TIMER_OUTPUTMODE_OUTBITVALUE [Default value], TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_TOGGLE_RESET, TIMER_OUTPUTMODE_SET_RESET TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_TOGGLE_SET, TIMER_OUTPUTMODE_RESET_SET |
Modified register is TAxCCTLn
References ASSERT, HWREG, TIMER_CAPTURE_ASYNCHRONOUS, TIMER_CAPTURE_INPUTSELECT_CCIxA, TIMER_CAPTURE_INPUTSELECT_CCIxB, TIMER_CAPTURE_INPUTSELECT_GND, TIMER_CAPTURE_INPUTSELECT_Vcc, TIMER_CAPTURE_SYNCHRONOUS, TIMER_CAPTURECOMPARE_INTERRUPT_DISABLE, TIMER_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_CAPTUREMODE_FALLING_EDGE, TIMER_CAPTUREMODE_NO_CAPTURE, TIMER_CAPTUREMODE_RISING_AND_FALLING_EDGE, TIMER_CAPTUREMODE_RISING_EDGE, TIMER_DO_CLEAR, TIMER_OUTPUTMODE_OUTBITVALUE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_RESET_SET, TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_SET_RESET, TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_TOGGLE_RESET, TIMER_OUTPUTMODE_TOGGLE_SET, and TIMER_TAIE_INTERRUPT_ENABLE.
void Timer_initCompare | ( | unsigned int | baseAddress, |
unsigned int | compareRegister, | ||
unsigned short | compareInterruptEnable, | ||
unsigned int | compareOutputMode, | ||
unsigned int | compareValue | ||
) |
Initializes Compare Mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareInterruptEnable | is to enable or disable timer captureComapre interrupt. Valid values are TIMER_CAPTURECOMPARE_INTERRUPT_ENABLE and TIMER_CAPTURECOMPARE_INTERRUPT_DISABLE [Default value] |
compareOutputMode | specifies the ouput mode. Valid values are TIMER_OUTPUTMODE_OUTBITVALUE [Default value], TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_TOGGLE_RESET, TIMER_OUTPUTMODE_SET_RESET TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_TOGGLE_SET, TIMER_OUTPUTMODE_RESET_SET |
compareValue | is the count to be compared with in compare mode |
Modified register is TAxCCTLn and TAxCCRn
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_INTERRUPT_DISABLE, TIMER_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_OUTPUTMODE_OUTBITVALUE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_RESET_SET, TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_SET_RESET, TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_TOGGLE_RESET, and TIMER_OUTPUTMODE_TOGGLE_SET.
void Timer_enableInterrupt | ( | unsigned int | baseAddress | ) |
void Timer_disableInterrupt | ( | unsigned int | baseAddress | ) |
Disable timer interrupt
baseAddress | is the base address of the Timer module. |
Modified register is TAxCTL
References HWREG.
unsigned long Timer_getInterruptStatus | ( | unsigned int | baseAddress | ) |
Get timer interrupt status
baseAddress | is the base address of the Timer module. |
References HWREG.
void Timer_enableCaptureCompareInterrupt | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Enable capture compare interrupt
baseAddress | is the base address of the Timer module. |
captureCompareRegister | is the selected capture compare regsiter |
Modified register is TAxCCTLn
References ASSERT, HWREG, HWREGB, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, and TIMER_CAPTURECOMPARE_REGISTER_6.
void Timer_disableCaptureCompareInterrupt | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Disable capture compare interrupt
baseAddress | is the base address of the Timer module. |
captureCompareRegister | is the selected capture compare regsiter |
Modified register is TAxCCTLn
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, and TIMER_CAPTURECOMPARE_REGISTER_6.
unsigned long Timer_getCaptureCompareInterruptStatus | ( | unsigned int | baseAddress, |
unsigned int | mask | ||
) |
Return capture compare interrupt status
baseAddress | is the base address of the Timer module. |
mask | is the mask for the interrupt status Valid values is and OR of TIMER_CAPTURE_OVERFLOW, TIMER_CAPTURECOMPARE_INTERRUPT_FLAG |
Modified register is TAxCTL
References HWREG.
void Timer_clear | ( | unsigned int | baseAddress | ) |
Reset/Clear the timer clock divider, count direction, count
baseAddress | is the base address of the Timer module. |
Modified register is TAxCTL
References HWREG.
unsigned short Timer_getSynchronizedCaptureCompareInput | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister, | ||
unsigned short | synchronized | ||
) |
Get synchrnozied capturecompare input
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
synchronized | is to select type of capture compare input. Valid values are TIMER_READ_CAPTURE_COMPARE_INPUT TIMER_READ_SYNCHRONIZED_CAPTURECOMPAREINPUT |
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_INPUT_HIGH, TIMER_CAPTURECOMPARE_INPUT_LOW, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_READ_CAPTURE_COMPARE_INPUT, and TIMER_READ_SYNCHRONIZED_CAPTURECOMPAREINPUT.
unsigned char Timer_getOutputForOutputModeOutBitValue | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get ouput bit for output mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_OUTPUTMODE_OUTBITVALUE_HIGH, and TIMER_OUTPUTMODE_OUTBITVALUE_LOW.
unsigned int Timer_getCaptureCompareCount | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Get current capturecompare count
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, and TIMER_CAPTURECOMPARE_REGISTER_6.
void Timer_setOutputForOutputModeOutBitValue | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister, | ||
unsigned char | outputModeOutBitValue | ||
) |
Set ouput bit for output mode
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
outputModeOutBitValueis | the value to be set for out bit Valid values are TIMER_OUTPUTMODE_OUTBITVALUE_HIGH TIMER_OUTPUTMODE_OUTBITVALUE_LOW |
Modified register is TAxCCTLn
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_OUTPUTMODE_OUTBITVALUE_HIGH, and TIMER_OUTPUTMODE_OUTBITVALUE_LOW.
void Timer_generatePWM | ( | unsigned int | baseAddress, |
unsigned int | clockSource, | ||
unsigned int | clockSourceDivider, | ||
unsigned int | timerPeriod, | ||
unsigned int | compareRegister, | ||
unsigned int | compareOutputMode, | ||
unsigned int | dutyCycle | ||
) |
Generate a PWM with timer running in up down mode
baseAddress | is the base address of the Timer module. |
clockSource | selects Clock source. Valid values are TIMER_CLOCKSOURCE_EXTERNAL_TXCLK TIMER_CLOCKSOURCE_ACLK TIMER_CLOCKSOURCE_SMCLK TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK |
clockSourceDivider | is the divider for Clock source. Valid values are TIMER_CLOCKSOURCE_DIVIDER_1 TIMER_CLOCKSOURCE_DIVIDER_2 TIMER_CLOCKSOURCE_DIVIDER_4 TIMER_CLOCKSOURCE_DIVIDER_8 TIMER_CLOCKSOURCE_DIVIDER_3 TIMER_CLOCKSOURCE_DIVIDER_5 TIMER_CLOCKSOURCE_DIVIDER_6 TIMER_CLOCKSOURCE_DIVIDER_7 TIMER_CLOCKSOURCE_DIVIDER_10 TIMER_CLOCKSOURCE_DIVIDER_12 TIMER_CLOCKSOURCE_DIVIDER_14 TIMER_CLOCKSOURCE_DIVIDER_16 TIMER_CLOCKSOURCE_DIVIDER_20 TIMER_CLOCKSOURCE_DIVIDER_24 TIMER_CLOCKSOURCE_DIVIDER_28 TIMER_CLOCKSOURCE_DIVIDER_32 TIMER_CLOCKSOURCE_DIVIDER_40 TIMER_CLOCKSOURCE_DIVIDER_48 TIMER_CLOCKSOURCE_DIVIDER_56 TIMER_CLOCKSOURCE_DIVIDER_64 |
timerPeriod | selects the desired timer period |
compareRegister | selects the compare register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareOutputMode | specifies the ouput mode. Valid values are TIMER_OUTPUTMODE_OUTBITVALUE, TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_TOGGLE_RESET, TIMER_OUTPUTMODE_SET_RESET TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_TOGGLE_SET, TIMER_OUTPUTMODE_RESET_SET |
dutyCycle | specifies the dutycycle for the generated waveform |
Modified registers are TAxCTL, TAxCCR0, TAxCCTL0,TAxCCTLn
References ASSERT, HWREG, privateTimerProcessClockSourceDivider(), TIMER_CAPTURECOMPARE_INTERRUPT_ENABLE, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, TIMER_CAPTURECOMPARE_REGISTER_6, TIMER_CLOCKSOURCE_ACLK, TIMER_CLOCKSOURCE_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_INVERTED_EXTERNAL_TXCLK, TIMER_CLOCKSOURCE_SMCLK, TIMER_DO_CLEAR, TIMER_OUTPUTMODE_OUTBITVALUE, TIMER_OUTPUTMODE_RESET, TIMER_OUTPUTMODE_RESET_SET, TIMER_OUTPUTMODE_SET, TIMER_OUTPUTMODE_SET_RESET, TIMER_OUTPUTMODE_TOGGLE, TIMER_OUTPUTMODE_TOGGLE_RESET, TIMER_OUTPUTMODE_TOGGLE_SET, TIMER_TAIE_INTERRUPT_ENABLE, TIMER_UP_MODE, and TIMER_UPDOWN_MODE.
void Timer_stop | ( | unsigned int | baseAddress | ) |
Stops the timer
baseAddress | is the base address of the Timer module. |
Modified registers are TAxCTL
References HWREG.
void Timer_setCompareValue | ( | unsigned int | baseAddress, |
unsigned int | compareRegister, | ||
unsigned int | compareValue | ||
) |
Sets the value of the capture-compare register
baseAddress | is the base address of the Timer module. |
captureRegister | selects the Capture register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
compareValue | is the count to be compared with in compare mode |
Modified register is TAxCCRn
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, and TIMER_CAPTURECOMPARE_REGISTER_6.
void Timer_clearTimerInterruptFlag | ( | unsigned int | baseAddress | ) |
Clears the Timer TAIFG interrupt flag
baseAddress | is the base address of the Timer module. |
Modified bits are TAIFG og TAxCTL register
References HWREGB.
void Timer_clearCaptureCompareInterruptFlag | ( | unsigned int | baseAddress, |
unsigned int | captureCompareRegister | ||
) |
Clears the capture-compare interrupt flag
baseAddress | is the base address of the Timer module. |
captureCompareRegister | selects the Capture-compare register being used. Valid values are TIMER_CAPTURECOMPARE_REGISTER_0 TIMER_CAPTURECOMPARE_REGISTER_1 TIMER_CAPTURECOMPARE_REGISTER_2 TIMER_CAPTURECOMPARE_REGISTER_3 TIMER_CAPTURECOMPARE_REGISTER_4 TIMER_CAPTURECOMPARE_REGISTER_5 TIMER_CAPTURECOMPARE_REGISTER_6 Refer datasheet to ensure the device has the capture compare register being used |
Modified bits are CCIFG of TAxCCTLn register
References ASSERT, HWREG, TIMER_CAPTURECOMPARE_REGISTER_0, TIMER_CAPTURECOMPARE_REGISTER_1, TIMER_CAPTURECOMPARE_REGISTER_2, TIMER_CAPTURECOMPARE_REGISTER_3, TIMER_CAPTURECOMPARE_REGISTER_4, TIMER_CAPTURECOMPARE_REGISTER_5, and TIMER_CAPTURECOMPARE_REGISTER_6.