Go to the source code of this file.
Define Documentation
#define __MSP430_HAS_RC__ |
#define RAMCONTROL_SECTOR0 RCRS0OFF |
#define RAMCONTROL_SECTOR1 RCRS1OFF |
#define RAMCONTROL_SECTOR2 RCRS2OFF |
#define RAMCONTROL_SECTOR3 RCRS3OFF |
#define RAMCONTROL_SECTOR4 RCRS4OFF |
#define RAMCONTROL_SECTOR5 RCRS5OFF |
#define RAMCONTROL_SECTOR6 RCRS6OFF |
#define RAMCONTROL_SECTOR7 RCRS7OFF |
Function Documentation
void ramController_setSectorOff |
( |
unsigned int |
baseAddress, |
|
|
unsigned char |
sector |
|
) |
| |
Set specified RAM sector off
- Parameters:
-
baseAddress | is the base address of the Timer module. |
sector | is specified sector to be set off. Valid values are a logical OR of RAMCONTROL_SECTOR0 RAMCONTROL_SECTOR1 RAMCONTROL_SECTOR2 RAMCONTROL_SECTOR3 RAMCONTROL_SECTOR4 RAMCONTROL_SECTOR5 RAMCONTROL_SECTOR6 RAMCONTROL_SECTOR7 |
Modified register RCCTL0
- Returns:
- None
References ASSERT, HWREG, RAMCONTROL_SECTOR0, RAMCONTROL_SECTOR1, RAMCONTROL_SECTOR2, and RAMCONTROL_SECTOR3.
unsigned char ramController_getSectorState |
( |
unsigned int |
baseAddress, |
|
|
unsigned char |
sector |
|
) |
| |
Get RAM sector ON/OFF status
- Parameters:
-
baseAddress | is the base address of the Timer module. |
sector | is specified sector Valid values are a logical OR of RAMCONTROL_SECTOR0 RAMCONTROL_SECTOR1 RAMCONTROL_SECTOR2 RAMCONTROL_SECTOR3 RAMCONTROL_SECTOR4 RAMCONTROL_SECTOR5 RAMCONTROL_SECTOR6 RAMCONTROL_SECTOR7 |
Modified register RCCTL0
- Returns:
- Mask of the sector state that are ON
References ASSERT, HWREGB, RAMCONTROL_SECTOR0, RAMCONTROL_SECTOR1, RAMCONTROL_SECTOR2, and RAMCONTROL_SECTOR3.