Go to the source code of this file.
Defines |
#define | __MSP430_HAS_AES__ |
#define | AES_READY_INTERRUPT AESRDYIE |
#define | AES_ERROR_OCCURRED AESERRFG |
#define | AES_NO_ERROR 0x00 |
#define | AES_getEncryptedData AES_getDataOut |
#define | AES_getDecryptedData AES_getDataOut |
#define | AES_BUSY AESBUSY |
#define | AES_NOT_BUSY 0x00 |
#define | AES_INTERRUPT_ENABLE AESRDYI |
Functions |
unsigned char | AES_setCipherKey (unsigned int baseAddress, const unsigned char *CipherKey) |
unsigned char | AES_encryptData (unsigned int baseAddress, const unsigned char *Data, unsigned char *encryptedData) |
unsigned char | AES_decryptDataUsingEncryptionKey (unsigned int baseAddress, const unsigned char *Data, unsigned char *decryptedData) |
unsigned char | AES_decryptData (unsigned int baseAddress, const unsigned char *Data, unsigned char *decryptedData) |
unsigned char | AES_generateFirstRoundKey (unsigned int baseAddress, const unsigned char *CipherKey) |
void | AES_clearInterruptFlag (unsigned int baseAddress) |
unsigned long | AES_getInterruptFlagStatus (unsigned int baseAddress) |
void | AES_enableInterrupt (unsigned int baseAddress) |
void | AES_disableInterrupt (unsigned int baseAddress) |
void | AES_reset (unsigned int baseAddress) |
unsigned char | AES_startEncryptData (unsigned int baseAddress, const unsigned char *Data, unsigned char *encryptedData) |
unsigned char | AES_startDecryptDataUsingEncryptionKey (unsigned int baseAddress, const unsigned char *Data) |
unsigned char | AES_startDecryptData (unsigned int baseAddress, const unsigned char *Data) |
unsigned char | AES_startGenerateFirstRoundKey (unsigned int baseAddress, const unsigned char *CipherKey) |
unsigned char | AES_getDataOut (unsigned int baseAddress, unsigned char *OutputData) |
unsigned char | AES_isBusy (unsigned int baseAddress) |
void | AES_clearErrorFlag (unsigned int baseAddress) |
unsigned long | AES_getErrorFlagStatus (unsigned int baseAddress) |
Define Documentation
#define __MSP430_HAS_AES__ |
#define AES_READY_INTERRUPT AESRDYIE |
#define AES_ERROR_OCCURRED AESERRFG |
#define AES_NO_ERROR 0x00 |
#define AES_getEncryptedData AES_getDataOut |
#define AES_getDecryptedData AES_getDataOut |
#define AES_NOT_BUSY 0x00 |
#define AES_INTERRUPT_ENABLE AESRDYI |
Function Documentation
unsigned char AES_setCipherKey |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
CipherKey |
|
) |
| |
Loads a 128 bit cipher key to AES module.
- Parameters:
-
baseAddress | is the base address of the AES module. |
CipherKey | is a pointer to an unsigned char array with a length of 16 bytes that contains a 128 bit cipher key. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_encryptData |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data, |
|
|
unsigned char * |
encryptedData |
|
) |
| |
Encrypts a block of data using the AES module. The cipher key that is used for encryption should be loaded in advance by using function
- Parameters:
-
AES_setCipherKey(). | |
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains data to be encrypted. |
encryptedData | is a pointer to an unsigned char array with a length of 16 bytes in that the encrypted data will be written. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_decryptDataUsingEncryptionKey |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data, |
|
|
unsigned char * |
decryptedData |
|
) |
| |
Decryptes a block of data using the AES module. This function can be used to decrypt data by using the same key as used for a previous performed encryption. The decryption takes 214 MCLK.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains encrypted data to be decrypted. |
decryptedData | is a pointer to an unsigned char array with a length of 16 bytes in that the decrypted data will be written. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_decryptData |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data, |
|
|
unsigned char * |
decryptedData |
|
) |
| |
Decryptes a block of data using the AES module. This function requires a pregenerated decryption key. A key can be loaded and pregenerated by using function
- Parameters:
-
AES_generateFirstRoundKey() | . The decryption takes 167 MCLK. |
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains encrypted data to be decrypted. |
decryptedData | is a pointer to an unsigned char array with a length of 16 bytes in that the decrypted data will be written. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_generateFirstRoundKey |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
CipherKey |
|
) |
| |
Loads and generates first round key required for decryption
- Parameters:
-
baseAddress | is the base address of the AES module. |
CipherKey | is a pointer to an unsigned char array with a length of 16 bytes that contains the initial AES key. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
void AES_clearInterruptFlag |
( |
unsigned int |
baseAddress | ) |
|
Clears the AES ready interrupt flag.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Modified bit is AESRDYIFG of AESACTL0 register.
- Returns:
- None
References HWREGB.
unsigned long AES_getInterruptFlagStatus |
( |
unsigned int |
baseAddress | ) |
|
Gets the AES ready interrupt flag status.
- Parameters:
-
baseAddress | is the base address of the AES module. |
- Returns:
- unsigned long - AES_READY_INTERRUPT or 0x00.
References HWREGB.
void AES_enableInterrupt |
( |
unsigned int |
baseAddress | ) |
|
Enables AES ready interrupt.
- Parameters:
-
baseAddress | is the base address of the AES module. Modified bit is AESRDYIE of AESACTL0 register. |
- Returns:
- None.
References HWREGB.
void AES_disableInterrupt |
( |
unsigned int |
baseAddress | ) |
|
Disables AES ready interrupt.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Modified bit is AESRDYIE of AESACTL0 register.
- Returns:
- None.
References HWREGB.
void AES_reset |
( |
unsigned int |
baseAddress | ) |
|
Resets AES Module immediately.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Modified bit is AESSWRST of AESACTL0 register.
- Returns:
- None.
References HWREGB.
unsigned char AES_startEncryptData |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data, |
|
|
unsigned char * |
encryptedData |
|
) |
| |
Starts an encryption process on the AES module. This is the non-blocking equivalant of AES_encryptData. The cipher key that is used for decryption should be loaded in advance by using function
- Parameters:
-
AES_setCipherKey(). | |
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains data to be encrypted. |
encryptedData | is a pointer to an unsigned char array with a length of 16 bytes in that the encrypted data will be written. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_startDecryptDataUsingEncryptionKey |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data |
|
) |
| |
Starts an decryption process on the AES module. This is the non-blocking equivalant of AES_decryptDataUsingEncryptionKey. This function can be used to decrypt data by using the same key as used for a previous performed encryption. The decryption takes 214 MCLK.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains encrypted data to be decrypted. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_startDecryptData |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
Data |
|
) |
| |
Decryptes a block of data using the AES module. This is the non-blocking equivalant of AES_decryptData. This function requires a pregenerated decryption key. A key can be loaded and pregenerated by using function
- Parameters:
-
AES_generateFirstRoundKey() | . The decryption takes 167 MCLK. |
baseAddress | is the base address of the AES module. |
Data | is a pointer to an unsigned char array with a length of 16 bytes that contains encrypted data to be decrypted. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_startGenerateFirstRoundKey |
( |
unsigned int |
baseAddress, |
|
|
const unsigned char * |
CipherKey |
|
) |
| |
Loads and generates first round key required for decryption This is the non-blocking equivalant of AES_generateFirstRoundKey.
- Parameters:
-
baseAddress | is the base address of the AES module. |
CipherKey | is a pointer to an unsigned char array with a length of 16 bytes that contains the initial AES key. |
- Returns:
- STATUS_SUCCESS
References HWREG, and STATUS_SUCCESS.
unsigned char AES_getDataOut |
( |
unsigned int |
baseAddress, |
|
|
unsigned char * |
OutputData |
|
) |
| |
Reads back the output data from AES module. This function is meant to use after an encryption or decryption process that was started and finished by initiating an interrupt.
- Parameters:
-
baseAddress | is the base address of the AES module. |
- Returns:
- is a pointer to an unsigned char array with a length of 16 bytes in which the output data of the AES module is available. If AES module is busy returns NULL
References HWREG, STATUS_FAIL, and STATUS_SUCCESS.
unsigned char AES_isBusy |
( |
unsigned int |
baseAddress | ) |
|
Gets the AES module busy status.
- Parameters:
-
baseAddress | is the base address of the AES module. |
- Returns:
- unsigned char AES_BUSY or AES_NOT_BUSY
References HWREG.
void AES_clearErrorFlag |
( |
unsigned int |
baseAddress | ) |
|
Clears the AES error flag.
- Parameters:
-
baseAddress | is the base address of the AES module. |
Modified bit is AESERRFG of AESACTL0 register.
- Returns:
- None
References HWREGB.
unsigned long AES_getErrorFlagStatus |
( |
unsigned int |
baseAddress | ) |
|
Gets the AES error flag status.
- Parameters:
-
baseAddress | is the base address of the AES module. |
- Returns:
- unsigned long - AES_ERROR_OCCURRED or AES_NO_ERROR.
References HWREGB.