Contains EM SW Lib Result Handle. More...
#include <emSwLib.h>
Data Fields | |
EM_Total_Results * | emTotalResult |
Pointer to EM_Total_Results struct. More... | |
EM_Phase_Results * | phaseResults |
Pointer to EM_Phase_Result struct buffer. More... | |
EM_Phase_BG_Results * | phaseBGResults |
Pointer to the EM_Phase_BG_Results struct buffer. More... | |
EM_Metrology ** | phaseMetrologyPing |
Pointer to EM_Metrology struct Ping buffer. More... | |
EM_Metrology ** | phaseMetrologyPong |
Pointer to EM_Metrology struct Pong buffer. More... | |
uint8_t | phaseResultsSupportedLen |
Length of the phaseResultsSupportedPtr buffer. More... | |
Contains EM SW Lib Result Handle.
EM_Total_Results* _EM_SW_Lib_Result_Handle_::emTotalResult |
Pointer to EM_Total_Results struct.
EM_Phase_Results* _EM_SW_Lib_Result_Handle_::phaseResults |
Pointer to EM_Phase_Result struct buffer.
EM_Phase_BG_Results* _EM_SW_Lib_Result_Handle_::phaseBGResults |
Pointer to the EM_Phase_BG_Results struct buffer.
EM_Metrology** _EM_SW_Lib_Result_Handle_::phaseMetrologyPing |
Pointer to EM_Metrology struct Ping buffer.
EM_Metrology** _EM_SW_Lib_Result_Handle_::phaseMetrologyPong |
Pointer to EM_Metrology struct Pong buffer.
uint8_t _EM_SW_Lib_Result_Handle_::phaseResultsSupportedLen |
Length of the phaseResultsSupportedPtr buffer.