Contains EM SW Lib System Configuration. More...
#include <emSwLib.h>
Data Fields | |
int32_t * | currentSamplePtr |
Pointer to the current sample. More... | |
int16_t * | voltageSamplePtr |
Pointer to the voltage sample. More... | |
EM_Current_Sensor | currentSensor |
Sensor connected to the current (I) channel. More... | |
uint16_t | phaseResultsSupported |
EM_Phase_Calibration * | phaseCalibPtr |
Pointer to EM_Phase_Calibration struct. More... | |
Contains EM SW Lib System Configuration.
int32_t* _EM_Phase_Configuration_::currentSamplePtr |
Pointer to the current sample.
int16_t* _EM_Phase_Configuration_::voltageSamplePtr |
Pointer to the voltage sample.
EM_Current_Sensor _EM_Phase_Configuration_::currentSensor |
Sensor connected to the current (I) channel.
uint16_t _EM_Phase_Configuration_::phaseResultsSupported |
Register used to read what results will be calculated for this phase Note: This is a Read-Only register. Possible mask values are: - EM_PHASE_RESULT_CALC_VRMS
EM_Phase_Calibration* _EM_Phase_Configuration_::phaseCalibPtr |
Pointer to EM_Phase_Calibration struct.