Contains EM SW Lib Phase Calibration. More...
#include <emSwLib.h>
Data Fields | |
uint32_t | voltageSF |
Voltage Scaling Factor - used to calculate VRMS. More... | |
uint32_t | currentSF |
Current Scaling Factor - used to calculate IRMS. More... | |
uint32_t | activePowerSF |
Active Power Scaling Factor. More... | |
uint32_t | reactivePowerSF |
Active Power Scaling Factor. More... | |
int16_t | phaseCorrection |
Phase Correction between voltage and current (register units) More... | |
Contains EM SW Lib Phase Calibration.
uint32_t _EM_Phase_Calibration_::voltageSF |
Voltage Scaling Factor - used to calculate VRMS.
uint32_t _EM_Phase_Calibration_::currentSF |
Current Scaling Factor - used to calculate IRMS.
uint32_t _EM_Phase_Calibration_::activePowerSF |
Active Power Scaling Factor.
uint32_t _EM_Phase_Calibration_::reactivePowerSF |
Active Power Scaling Factor.
int16_t _EM_Phase_Calibration_::phaseCorrection |
Phase Correction between voltage and current (register units)