Data Fields
_EM_Phase_BG_Results_ Struct Reference

Contains EM Phase Background Results. More...

#include <emSwLib.h>

Data Fields

int32_t vDCEstimate
 DC Estimate for Voltage. More...
 
int16_t iDCEstimate [3]
 DC Estimate for Current. More...
 
int16_t reactPowPrevV90
 Previous V90 voltage used for the IIR filter in the reactive power calculation. More...
 
int16_t vPrevSample
 Previous Voltage sample used for the IIR filter in the reactive power calculation. More...
 
int32_t rogowskiPrevI90
 Previous I90 current used for the IIR filter in the Rogowski ADC current calculation. More...
 
int32_t iPrevSample
 Previous Current sample used for the IIR filter in the Rogowski ADC current calculation. More...
 

Detailed Description

Contains EM Phase Background Results.

Field Documentation

§ vDCEstimate

int32_t _EM_Phase_BG_Results_::vDCEstimate

DC Estimate for Voltage.

§ iDCEstimate

int16_t _EM_Phase_BG_Results_::iDCEstimate[3]

DC Estimate for Current.

§ reactPowPrevV90

int16_t _EM_Phase_BG_Results_::reactPowPrevV90

Previous V90 voltage used for the IIR filter in the reactive power calculation.

§ vPrevSample

int16_t _EM_Phase_BG_Results_::vPrevSample

Previous Voltage sample used for the IIR filter in the reactive power calculation.

§ rogowskiPrevI90

int32_t _EM_Phase_BG_Results_::rogowskiPrevI90

Previous I90 current used for the IIR filter in the Rogowski ADC current calculation.

§ iPrevSample

int32_t _EM_Phase_BG_Results_::iPrevSample

Previous Current sample used for the IIR filter in the Rogowski ADC current calculation.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale