Contains EM SW Lib Meter Configuration. More...
#include <emSwLib.h>
Data Fields | |
EM_Phase_Configuration * | phaseConfigPtr |
Pointer to the EM_Phase_Configuration struct buffer. More... | |
uint8_t | phaseLength |
Length of the emPhasePtr buffer. More... | |
uint8_t * | meterName |
Pointer to meter name string. More... | |
uint8_t * | libVersionNumber |
Pointer to library version number string. More... | |
uint8_t * | meterPW |
Contains EM SW Lib Meter Configuration.
EM_Phase_Configuration* _EM_Meter_Configuration_::phaseConfigPtr |
Pointer to the EM_Phase_Configuration struct buffer.
uint8_t _EM_Meter_Configuration_::phaseLength |
Length of the emPhasePtr buffer.
uint8_t* _EM_Meter_Configuration_::meterName |
Pointer to meter name string.
uint8_t* _EM_Meter_Configuration_::libVersionNumber |
Pointer to library version number string.
uint8_t* _EM_Meter_Configuration_::meterPW |