MSP430_DLL 3_02_01_009 Product Download Page
Build date: 11092011
The MSP debug stack (MSPDS) for all MSP430 devices consists of a dynamic link library as well as
embedded firmware that runs on flash emulation tools (FETs) such as the MSP-FET,
MSP-FET430UIF or eZ emulators.
It is the bridging element between all PC software and all MSP430 microcontroller derivatives and handles tasks such as
code download, stepping through code, break point handling and so forth. The MSP Debug Stack is used in IDEs such as Code Composer Studio (CCS),
IAR's Embedded Workbench for MSP430 or other tools like Smart RF Studio or Elprotronic's FlashPro430.
Included in
New Device Support
New Features
- The DLL version 3.2.1.9 is an all new DLL design compared to the last DLL version 2.4.9.1.
This new DLL includes also a new UIF-Firmware. Furthermore the USB driver has been changed to a certified CDC driver.
The DLL is implemented in C++ and follows an object based design, which is host operating system independent. The API
of the new DLL is the same as for the old one. DLL functionality keeps the same as in the old V2 DLL. The new DLL V3
also includes a compiled version of the DLLv2
Bug Fixes
Known Issues
- This MSP430.dll version might not be compatible with revision 1.3 of the MSP-FET430UIF if a capacitor is connected to the RST pin.
Older Releases
2_04_007_001
2_04_008_002
2_04_009_001
Related Links
|