![]() |
![]() |
MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include "rom_driverlib.h"
#include "rom_map_driverlib.h"
#include "driverlib.h"
#include "CAPT_CommConfig.h"
Go to the source code of this file.
Macros | |
#define | UART__EUSCI_A_PERIPHERAL (EUSCI_A0_BASE) |
CAPT_CommConfig is used to control UART__ENABLE. More... | |
#define | UART__LPMx_bits (LPM0_bits) |
#define | UART__SAMPLING_MODE (EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION) |
def UART__SAMPLING_MODE defines the eUSCI_A LF or HF mode. More... | |
#define | UART__PRESCALER (0x08) |
#define | UART__FIRST_STAGE_MOD (0x00) |
#define | UART__SECOND_STAGE_MOD (0x00) |