![]() |
![]() |
MSP430™CapTIvateSoftwareLibraryAPIGuide
1_83_00_05
|
#include <stdint.h>
#include <stdbool.h>
Go to the source code of this file.
Data Structures | |
struct | tByteQueue |
typedef tByteQueue More... | |
Enumerations | |
enum | tByteQueueError { eByteQueue_Success = 0, eByteQueue_QueueEmpty = -1, eByteQueue_QueueOverrun = -2 } |
tByteQueueError enumerates possible Byte Queue function errors. More... | |
Functions | |
bool | CAPT_initByteQueue (tByteQueue *pQueue, uint8_t *pBufferArray, uint16_t ui16BufferArraySize) |
int8_t | CAPT_pushOntoByteQueue (tByteQueue *pQueue, uint8_t ui8DataToAdd) |
int8_t | CAPT_pullFromByteQueue (tByteQueue *pQueue, uint8_t *pDestination) |
uint16_t | CAPT_getByteQueueSize (tByteQueue *pQueue) |
bool | CAPT_isByteQueueFull (tByteQueue *pQueue) |
bool | CAPT_isByteQueueEmpty (tByteQueue *pQueue) |