CapTIvate Design Center Release Notes
Table of Contents
Introduction
This is version 1.83.00.08 of CapTIvate Design Center.
CapTIvate™ is a capacitive user interface design ecosystem that takes the next big step in design process evolution. It brings together a capacitive measurement technology, a design GUI, a capacitive touch software library, and a hardware development platform.
Documentation
What’s New
Documentation
- CapTIvate Technology Guide:
- Add the Temperature Drift information in Design Guide section
- Update the Devices section with key sensing parameters and comparison between two generations
Software Library
- Add the support for new devices MSP430FR2672 and MSP430FR2673
Design Center
1.83.00.08
Please re-create the projects created from the previous version to get all the new features.
- Added support for TrackPad sensors
- Minor bug fixes
Upgrade and Compatibility Information
No special action is required to upgrade to this release.
Installation and Usage
- Download CapTIvate
- Run the appropriate platform specific installer: CapTIvateDesignCenter-
- -installer - Follow the installer directions
- To launch tool, use the desktop icon or execute the tool directly:
- Windows
- Start Menu -> All Programs -> Texas Instruments -> CapTIvateDesignCenter_<version> -> CapTIvateDesignCenter
- C:/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter.exe
- OS X
- /Applications/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Linux OS
- ~/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Windows
Host Support
Supported Operating Systems:
- Windows 7, 10
- Linux OS
- Apple OS X
Dependencies
Java JRE 1.7 or later must be installed on the host system. Click here to go to Java Download Page.
- Source code generated by this release requires:
- Code Composer Studio (CCS) v7.4
- IAR Embedded Workbench 7.11
Device Support
The following families of devices are supported in this release of CapTIvate Design Center:
- MSP430FR2512, MSP430FR2522
- MSP430FR2532, MSP430FR2533
- MSP430FR2632, MSP430FR2633
- MSP430FR2675, MSP430FR2676
- MSP430FR2672, MSP430FR2673
Validation Information
The CapTIvate Design Center was validated with the following IDEs:
Code Composer Studio 8.2 IAR Embedded Workbench 7.12
Known Issues
| ID | Summary |
|---|---|
| None | None |
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
- 1.82.00
- Add the support for new devices MSP430FR2672 and MSP430FR2673
- Added the Recommended Threshold Percentage calculation and warning feature to help the user to set a reliable proximity and touch threshold
- Add project version check function
- Documentation updates
- Minor bug fixes
- 1.81.00
- Added support for implementing custom slider/wheel position algorithm
- Added FR2676_CAPTIVATE-EMC example project
- Added Design Recommendation section in sensor properties window
- Documentation updates
- Minor bug fixes
- 1.80.00.30
- Added support for MSP430FR2676 and MSP430FR2675 devices
- Added Noise Immunity selection feature
- Added the CAPTIVATE-FR2676 MCU board example projects
- Updated SNR calculation tool with new rules and formulas
- Enhanced data logging feature
- Removed Maximum_Offset calibration algorithm
- Documentation updates
- Minor bug fixes
- 1.70.00.03
- Update SNR calculation tool with new rules and formulas
- Add Sensor Error Status Flags indication feature
- Add Low Power Mode Options selection feature
- Add Backchannel_UART example project
- Add EVM430-CAPMINI example project
- Enhance the data logging feature
- Documentation updates
- Minor bug fixes
- 1.60.00.00
| ID | Summary |
|---|---|
| MSPCAPLIB-176 | Add HID Bridge firmware Image to Design Center Download Package |
| MSPCAPLIB-175 | Streamline customer development in basic mode by updating default values and hiding additional parameters in basic mode (keep in advanced mode) |
| MSPCAPLIB-174 | Catch error when user opens a project in invalid workspace |
| MSPCAPLIB-168 | Fix broken links to API guide and SW change control document from the user's guide |
| MSPCAPLIB-167 | Add BOOSTXL-CAPKEYPAD chapter to CapTIvate Tech Guide |
| MSPCAPLIB-161 | Expand calibration algorithm options to include new Max-Offset calibration |
| MSPCAPLIB-155 | Add support for MSP430FR2522 and MSP430FR2512 devices |
| MSPCAPLIB-151 | Add section to the tech guide to describe pin selection methodology |
- 1.50.00.00
| ID | Summary |
|---|---|
| MSPCAPLIB-158 | Add Metal Touch examples and documentation updates |
| MSPCAPLIB-150 | Change “PARALLEL BLOCK” column heading to “PARALLEL GROUP” |
| MSPCAPLIB-138 | DesignCenter shall be modified to use the documentation tools from SimpleLink SDK SWTOOLS |
- 1.40.00.00
- Minimum Java requirement changed to 1.7.0_60
- Add “SetAll” button to element tuning parameter widgets (MSPCAPLIB-126)
- Add confirmation dialog when the target directory of code generation exists (MSPCAPLIB-129)
- Documentation updates
- Minor bug fixes
- v1.30.10.00
- Updated to CapTIvate Software Library v1.04.00.00
- Added support for using the VLO to clock the CapTIvate timer in LPM4 when in wake-on-proximity mode to the CAPT_App layer. This allows applications to achieve very low average power consumption when a crystal is not used for the low frequency clock (ACLK). Entering LPM4 disables ACLK (turning of XT1 or the REFO, whichever was used for ACLK). The CapTIvate peripheral may still be clocked from the VLO in LPM4, if the VLO is selected as the clock source. The trade-off with using this mode is reduced time-keeping accuracy in wake-on-proximity mode. To enable this feature, define CAPT_WOP_VLO_LPM4 in CAPT_App.c. For more details, see the Ultra Low Power section of the Design Guide chapter of the CapTIvate Technology Guide.
- Added the ProximityRangeSensor example project. This example project shows how to implement a basic range sensing application using the CAPTIVATE-PROXIMITY sensing panel.
- The MSP peripheral driver library is updated to include support for the DCO manual trim procedure.
- The CapTIvate Starter Project default stack size was reduced to 256B from 512B. Testing estimates the worst case stack usage for most applications to be <128B.
- Documentation updates
- Updated to CapTIvate Software Library v1.04.00.00
- v1.20.00.00
- Documentation updates
- Minor bug fixes
- v1.10.00.00
- Documentation updates
- Fix intermittent GUI startup issues
- Other minor bug fixes
- v1.00.20.00
- Initial public ES release
Technical Support and Product Updates
- Visit the MSP E2E Forum for support.