MSPM0 PMBus Library User’s Guide¶
1. Introduction¶
The MSPM0 PMBus Library is based on the MSPM0 SMBus library. The MSPM0 PMBus library provides a set of APIs to communicate over PMBus as a controller or a target.
2. PMBus Library Supported Features¶
This library was developed in compliance with the PMBus 1.3.1 specification.
2.1 PMBus Supported Features¶
Address, memory, communication and capability related commands
On, off, and margin testing related commands
Output voltage related commands
“Other commands” as detailed by the PMBus specification
Fault related commands
Power good signal limits
Output voltage sequencing commands
Unit status commands
Parametric information commands
Manufacturer’s information commands
2.3 PMBus Features Not Currently Implemented¶
The PMBus features listed below are supported in hardware but have not been implemented in this release:
ZONE_READ and ZONE_WRITE protocols
3. PMBus Example Usage¶
Three examples are given in the SDK demonstrating the PMBus controller , PMBus target and PMBus controller using group command.
To test the PMBus controller and target example connect the SDL and SDA pins of controller and target. Load the program to controller and target. The example services the following commands.
PMBus CMD |
CMD ID |
Write Type |
Read Type |
|---|---|---|---|
Device ID |
0xAD |
Block read |
|
Clear Faults |
0x03 |
Send Byte |
|
Vout Mode |
0x020 |
Write Byte |
Read Byte |
Vout OV warn Limit |
0x42 |
Write Word |
Read Word |
MRF ID |
0x99 |
Block Write |
Block Read |
Read Vout |
0x8B |
Read Word |
|
EXT_BYTE_CMD |
0x01FF |
Write Byte |
Read Byte |
EXT_WORD_CMD |
0x02FF |
Write Word |
Read Word |
Process call Byte |
0xD0 |
Write Word |
Read Word |
Process call Block |
0xD1 |
Block Write |
Block Read |
To test the group command, load the target examples to 2 launchpads with different slave addresses specified in the group commamnd examples. The group command example will communicate with both targets and service the PMBus comamnds.
3.1 PMBus Examples Supported Hardware¶
LP-MSPM0G3519 or LP-MSPM0G3507 LaunchPad evaluation boards
4. Library Versions¶
Version 2.00.00.00
SDK release: 2.04.00.xx
Updates:
Updated PMBus stack to support both as controller and target.
Added PMBus controller and target examples.
Added PMBus controller to support group commands.
Version 1.11.01.00
SDK Release: 2.03.00.xx
Updates:
Fix PMB_BLOCK_READ #define
Version 1.10.00.00
SDK Release: 1.30.00.xx
Updates:
Updates to use SMBus 1.30.00.xx.
Remove unimplemented PMBus_processTimeoutInt.
Update examples to use I2C boosterPack standard.
Version 1.00.00.01
SDK Release: 1.10.00.xx
Updates:
Initial release.