![]() |
![]() |
|
MSPM0L122X_L222X Driver Library
2.10.00.04
|
The Independent Watchdog Timer Driver Library allows full configuration of the MSPM0 iWDT module. The independent window watchdog timer (iWDT) in the LFSS IP is an SoC independent supervisor which monitors code execution and overall hang up scenarios of the SoC. Due to the nature of the LFSS IP, this iWDT has its own system independent power and clock source. If the application software does not successfully reset the watchdog within the programmed time, the watchdog generates a POR reset to the SoC