MSPM0L111X Driver Library  2.10.00.04
Data Structures | Macros | Enumerations | Functions
dl_uart.h File Reference

Detailed Description

UART Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_uart.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  DL_UART_Config
 Configuration struct for DL_UART_init. More...
 
struct  DL_UART_ClockConfig
 Configuration struct for DL_UART_setClockConfig. More...
 
struct  DL_UART_Main_backupConfig
 Configuration structure to backup UART Main peripheral state before going to STOP/STANDBY mode. Used by DL_UART_Main_saveConfiguration and DL_UART_Main_restoreConfiguration. More...
 
struct  DL_UART_Extend_backupConfig
 Configuration structure to backup UART Extend peripheral state before going to STOP/STANDBY mode. Used by DL_UART_Extend_saveConfiguration and DL_UART_Extend_restoreConfiguration. More...
 

Macros

#define DL_UART_INTERRUPT_DMA_DONE_TX   (UART_CPU_INT_IMASK_DMA_DONE_TX_SET)
 DMA done on transmit interrupt.
 
#define DL_UART_INTERRUPT_DMA_DONE_RX   (UART_CPU_INT_IMASK_DMA_DONE_RX_SET)
 DMA done on receive interrupt.
 
#define DL_UART_INTERRUPT_CTS_DONE   (UART_CPU_INT_IMASK_CTS_SET)
 Clear to send interrupt.
 
#define DL_UART_INTERRUPT_ADDRESS_MATCH   (UART_CPU_INT_IMASK_ADDR_MATCH_SET)
 9-bit mode address match interrupt
 
#define DL_UART_INTERRUPT_LINC0_MATCH   (UART_CPU_INT_IMASK_LINC0_SET)
 LINC0 match interrupt.
 
#define DL_UART_INTERRUPT_EOT_DONE   (UART_CPU_INT_IMASK_EOT_SET)
 End of transmission interrupt.
 
#define DL_UART_INTERRUPT_TX   (UART_CPU_INT_IMASK_TXINT_SET)
 UART transmit interrupt.
 
#define DL_UART_INTERRUPT_RX   (UART_CPU_INT_IMASK_RXINT_SET)
 UART receive interrupt.
 
#define DL_UART_INTERRUPT_LIN_COUNTER_OVERFLOW   (UART_CPU_INT_IMASK_LINOVF_SET)
 LIN hardware counter overflow interrupt.
 
#define DL_UART_INTERRUPT_LIN_RISING_EDGE   (UART_CPU_INT_IMASK_LINC1_SET)
 LIN rising edge LINC1 interrupt.
 
#define DL_UART_INTERRUPT_LIN_FALLING_EDGE   (UART_CPU_INT_IMASK_LINC0_SET)
 LIN falling edge LINC0 interrupt.
 
#define DL_UART_INTERRUPT_RXD_POS_EDGE   (UART_CPU_INT_IMASK_RXPE_SET)
 Positive Edge on UARTxRXD interrupt.
 
#define DL_UART_INTERRUPT_RXD_NEG_EDGE   (UART_CPU_INT_IMASK_RXNE_SET)
 Negative Edge on UARTxRXD interrupt.
 
#define DL_UART_INTERRUPT_OVERRUN_ERROR   (UART_CPU_INT_IMASK_OVRERR_SET)
 Overrun error interrupt.
 
#define DL_UART_INTERRUPT_BREAK_ERROR   (UART_CPU_INT_IMASK_BRKERR_SET)
 Break error interrupt.
 
#define DL_UART_INTERRUPT_PARITY_ERROR   (UART_CPU_INT_IMASK_PARERR_SET)
 Parity error interrupt.
 
#define DL_UART_INTERRUPT_FRAMING_ERROR   (UART_CPU_INT_IMASK_FRMERR_SET)
 Framing error interrupt.
 
#define DL_UART_INTERRUPT_RX_TIMEOUT_ERROR   (UART_CPU_INT_IMASK_RTOUT_SET)
 Receive timeout interrupt.
 
#define DL_UART_INTERRUPT_NOISE_ERROR   (UART_CPU_INT_IMASK_NERR_SET)
 Noise error interrupt.
 
#define DL_UART_DMA_INTERRUPT_RX   (UART_DMA_TRIG_RX_IMASK_RXINT_SET)
 UART interrupt for enabling UART receive as DMA trigger.
 
#define DL_UART_DMA_DONE_INTERRUPT_RX   (UART_CPU_INT_IMASK_DMA_DONE_RX_SET)
 UART interrupt indicating DMA is done with the RX.
 
#define DL_UART_DMA_INTERRUPT_RX_TIMEOUT   (UART_DMA_TRIG_RX_IMASK_RTOUT_SET)
 UART interrupt for enabling UART receive timeout as DMA trigger.
 
#define DL_UART_DMA_INTERRUPT_TX   (UART_DMA_TRIG_TX_IMASK_TXINT_SET)
 UART interrupt for enabling UART transmit as DMA trigger.
 
#define DL_UART_DMA_DONE_INTERRUPT_TX   (UART_CPU_INT_IMASK_DMA_DONE_TX_SET)
 UART interrupt indicating DMA is done with the TX.
 
#define DL_UART_ERROR_OVERRUN   (UART_RXDATA_OVRERR_SET)
 Overrun error ocurred.
 
#define DL_UART_ERROR_BREAK   (UART_RXDATA_BRKERR_SET)
 Break error ocurred.
 
#define DL_UART_ERROR_PARITY   (UART_RXDATA_PARERR_SET)
 Parity error ocurred.
 
#define DL_UART_ERROR_FRAMING   (UART_RXDATA_FRMERR_SET)
 Framing error ocurred.
 
#define DL_UART_PULSE_WIDTH_3_16_BIT_PERIOD   ((uint32_t) 0x00000000U)
 Sets the IrDA pulse width to 3/16 bit period when using the BITCLK16.
 

Enumerations

enum  DL_UART_IIDX {
  DL_UART_IIDX_DMA_DONE_TX = UART_CPU_INT_IIDX_STAT_DMA_DONE_TX,
  DL_UART_IIDX_DMA_DONE_RX = UART_CPU_INT_IIDX_STAT_DMA_DONE_RX,
  DL_UART_IIDX_CTS_DONE = UART_CPU_INT_IIDX_STAT_CTS,
  DL_UART_IIDX_ADDRESS_MATCH = UART_CPU_INT_IIDX_STAT_MODE_9B,
  DL_UART_IIDX_EOT_DONE = UART_CPU_INT_IIDX_STAT_EOT,
  DL_UART_IIDX_TX = UART_CPU_INT_IIDX_STAT_TXIFG,
  DL_UART_IIDX_RX = UART_CPU_INT_IIDX_STAT_RXIFG,
  DL_UART_IIDX_LIN_COUNTER_OVERFLOW = UART_CPU_INT_IIDX_STAT_LINOVF,
  DL_UART_IIDX_LIN_RISING_EDGE = UART_CPU_INT_IIDX_STAT_LINC1,
  DL_UART_IIDX_LIN_FALLING_EDGE = UART_CPU_INT_IIDX_STAT_LINC0,
  DL_UART_IIDX_RXD_POS_EDGE = UART_CPU_INT_IIDX_STAT_RXPE,
  DL_UART_IIDX_RXD_NEG_EDGE = UART_CPU_INT_IIDX_STAT_RXNE,
  DL_UART_IIDX_OVERRUN_ERROR = UART_CPU_INT_IIDX_STAT_OEFG,
  DL_UART_IIDX_BREAK_ERROR = UART_CPU_INT_IIDX_STAT_BEFG,
  DL_UART_IIDX_PARITY_ERROR = UART_CPU_INT_IIDX_STAT_PEFG,
  DL_UART_IIDX_FRAMING_ERROR = UART_CPU_INT_IIDX_STAT_FEFG,
  DL_UART_IIDX_RX_TIMEOUT_ERROR = UART_CPU_INT_IIDX_STAT_RTFG,
  DL_UART_IIDX_NOISE_ERROR = UART_CPU_INT_IIDX_STAT_NERR_EVT,
  DL_UART_IIDX_NO_INTERRUPT = UART_CPU_INT_IIDX_STAT_NO_INTR
}
 
enum  DL_UART_DMA_IIDX_RX {
  DL_UART_DMA_IIDX_RX_TRIGGER = UART_DMA_TRIG_RX_IIDX_STAT_RXIFG,
  DL_UART_DMA_IIDX_RX_TIMEOUT_TRIGGER = UART_DMA_TRIG_RX_IIDX_STAT_RTFG
}
 
enum  DL_UART_DMA_IIDX_TX { DL_UART_DMA_IIDX_TX_TRIGGER = UART_DMA_TRIG_TX_IIDX_STAT_TXIFG }
 
enum  DL_UART_PULSE_WIDTH {
  DL_UART_PULSE_WIDTH_5_NS = UART_GFCTL_AGFSEL_AGLIT_5,
  DL_UART_PULSE_WIDTH_10_NS = UART_GFCTL_AGFSEL_AGLIT_10,
  DL_UART_PULSE_WIDTH_25_NS = UART_GFCTL_AGFSEL_AGLIT_25,
  DL_UART_PULSE_WIDTH_50_NS = UART_GFCTL_AGFSEL_AGLIT_50
}
 
enum  DL_UART_OVERSAMPLING_RATE {
  DL_UART_OVERSAMPLING_RATE_16X = UART_CTL0_HSE_OVS16,
  DL_UART_OVERSAMPLING_RATE_8X = UART_CTL0_HSE_OVS8,
  DL_UART_OVERSAMPLING_RATE_3X = UART_CTL0_HSE_OVS3
}
 
enum  DL_UART_PARITY {
  DL_UART_PARITY_EVEN = (UART_LCRH_PEN_ENABLE | UART_LCRH_EPS_EVEN),
  DL_UART_PARITY_ODD = (UART_LCRH_PEN_ENABLE | UART_LCRH_EPS_ODD),
  DL_UART_PARITY_STICK_ONE = (UART_LCRH_PEN_ENABLE | UART_LCRH_SPS_ENABLE | UART_LCRH_EPS_ODD),
  DL_UART_PARITY_STICK_ZERO = (UART_LCRH_PEN_ENABLE | UART_LCRH_SPS_ENABLE | UART_LCRH_EPS_EVEN),
  DL_UART_PARITY_NONE = UART_LCRH_PEN_DISABLE
}
 
enum  DL_UART_WORD_LENGTH {
  DL_UART_WORD_LENGTH_5_BITS = UART_LCRH_WLEN_DATABIT5,
  DL_UART_WORD_LENGTH_6_BITS = UART_LCRH_WLEN_DATABIT6,
  DL_UART_WORD_LENGTH_7_BITS = UART_LCRH_WLEN_DATABIT7,
  DL_UART_WORD_LENGTH_8_BITS = UART_LCRH_WLEN_DATABIT8
}
 
enum  DL_UART_MODE {
  DL_UART_MODE_NORMAL = UART_CTL0_MODE_UART,
  DL_UART_MODE_RS485 = UART_CTL0_MODE_RS485,
  DL_UART_MODE_IDLE_LINE = UART_CTL0_MODE_IDLELINE,
  DL_UART_MODE_ADDR_9_BIT = UART_CTL0_MODE_ADDR9BIT,
  DL_UART_MODE_SMART_CARD = UART_CTL0_MODE_SMART,
  DL_UART_MODE_DALI = UART_CTL0_MODE_DALI
}
 
enum  DL_UART_DIRECTION {
  DL_UART_DIRECTION_TX = UART_CTL0_TXE_ENABLE,
  DL_UART_DIRECTION_RX = UART_CTL0_RXE_ENABLE,
  DL_UART_DIRECTION_TX_RX = (UART_CTL0_RXE_ENABLE | UART_CTL0_TXE_ENABLE),
  DL_UART_DIRECTION_NONE = (UART_CTL0_RXE_DISABLE | UART_CTL0_TXE_DISABLE)
}
 
enum  DL_UART_CLOCK {
  DL_UART_CLOCK_BUSCLK = UART_CLKSEL_BUSCLK_SEL_ENABLE,
  DL_UART_CLOCK_MFCLK = UART_CLKSEL_MFCLK_SEL_ENABLE,
  DL_UART_CLOCK_LFCLK = UART_CLKSEL_LFCLK_SEL_ENABLE
}
 
enum  DL_UART_FLOW_CONTROL {
  DL_UART_FLOW_CONTROL_RTS = UART_CTL0_RTSEN_ENABLE,
  DL_UART_FLOW_CONTROL_CTS = UART_CTL0_CTSEN_ENABLE,
  DL_UART_FLOW_CONTROL_RTS_CTS = (UART_CTL0_RTSEN_ENABLE | UART_CTL0_CTSEN_ENABLE),
  DL_UART_FLOW_CONTROL_NONE = (UART_CTL0_CTSEN_DISABLE | UART_CTL0_RTSEN_DISABLE)
}
 
enum  DL_UART_RTS {
  DL_UART_RTS_ASSERT = UART_CTL0_RTS_SET,
  DL_UART_RTS_DEASSERT = UART_CTL0_RTS_CLR
}
 
enum  DL_UART_STOP_BITS {
  DL_UART_STOP_BITS_ONE = UART_LCRH_STP2_DISABLE,
  DL_UART_STOP_BITS_TWO = UART_LCRH_STP2_ENABLE
}
 
enum  DL_UART_TXD_OUT {
  DL_UART_TXD_OUT_LOW = UART_CTL0_TXD_OUT_LOW,
  DL_UART_TXD_OUT_HIGH = UART_CTL0_TXD_OUT_HIGH
}
 
enum  DL_UART_TX_FIFO_LEVEL {
  DL_UART_TX_FIFO_LEVEL_3_4_EMPTY = UART_IFLS_TXIFLSEL_LVL_3_4,
  DL_UART_TX_FIFO_LEVEL_1_2_EMPTY = UART_IFLS_TXIFLSEL_LVL_1_2,
  DL_UART_TX_FIFO_LEVEL_1_4_EMPTY = UART_IFLS_TXIFLSEL_LVL_1_4,
  DL_UART_TX_FIFO_LEVEL_EMPTY = UART_IFLS_TXIFLSEL_LVL_EMPTY,
  DL_UART_TX_FIFO_LEVEL_ONE_ENTRY = UART_IFLS_TXIFLSEL_LVL_1
}
 
enum  DL_UART_RX_FIFO_LEVEL {
  DL_UART_RX_FIFO_LEVEL_ONE_ENTRY = UART_IFLS_RXIFLSEL_LVL_1,
  DL_UART_RX_FIFO_LEVEL_FULL = UART_IFLS_RXIFLSEL_LVL_FULL,
  DL_UART_RX_FIFO_LEVEL_3_4_FULL = UART_IFLS_RXIFLSEL_LVL_3_4,
  DL_UART_RX_FIFO_LEVEL_1_2_FULL = UART_IFLS_RXIFLSEL_LVL_1_2,
  DL_UART_RX_FIFO_LEVEL_1_4_FULL = UART_IFLS_RXIFLSEL_LVL_1_4
}
 
enum  DL_UART_IRDA_CLOCK {
  DL_UART_IRDA_CLOCK_BAUD_RATE = UART_IRCTL_IRTXCLK_BRCLK,
  DL_UART_IRDA_CLOCK_FUNCTIONAL = UART_IRCTL_IRTXCLK_BITCLK
}
 
enum  DL_UART_IRDA_POLARITY {
  DL_UART_IRDA_POLARITY_LOW = UART_IRCTL_IRRXPL_LOW,
  DL_UART_IRDA_POLARITY_HIGH = UART_IRCTL_IRRXPL_HIGH
}
 
enum  DL_UART_CLOCK_DIVIDE_RATIO {
  DL_UART_CLOCK_DIVIDE_RATIO_1 = UART_CLKDIV_RATIO_DIV_BY_1,
  DL_UART_CLOCK_DIVIDE_RATIO_2 = UART_CLKDIV_RATIO_DIV_BY_2,
  DL_UART_CLOCK_DIVIDE_RATIO_3 = UART_CLKDIV_RATIO_DIV_BY_3,
  DL_UART_CLOCK_DIVIDE_RATIO_4 = UART_CLKDIV_RATIO_DIV_BY_4,
  DL_UART_CLOCK_DIVIDE_RATIO_5 = UART_CLKDIV_RATIO_DIV_BY_5,
  DL_UART_CLOCK_DIVIDE_RATIO_6 = UART_CLKDIV_RATIO_DIV_BY_6,
  DL_UART_CLOCK_DIVIDE_RATIO_7 = UART_CLKDIV_RATIO_DIV_BY_7,
  DL_UART_CLOCK_DIVIDE_RATIO_8 = UART_CLKDIV_RATIO_DIV_BY_8
}
 
enum  DL_UART_CLOCK_DIVIDE2_RATIO {
  DL_UART_CLOCK_DIVIDE2_RATIO_1 = UART_CLKDIV2_RATIO_DIV_BY_1,
  DL_UART_CLOCK_DIVIDE2_RATIO_2 = UART_CLKDIV2_RATIO_DIV_BY_2,
  DL_UART_CLOCK_DIVIDE2_RATIO_3 = UART_CLKDIV2_RATIO_DIV_BY_3,
  DL_UART_CLOCK_DIVIDE2_RATIO_4 = UART_CLKDIV2_RATIO_DIV_BY_4,
  DL_UART_CLOCK_DIVIDE2_RATIO_5 = UART_CLKDIV2_RATIO_DIV_BY_5,
  DL_UART_CLOCK_DIVIDE2_RATIO_6 = UART_CLKDIV2_RATIO_DIV_BY_6,
  DL_UART_CLOCK_DIVIDE2_RATIO_7 = UART_CLKDIV2_RATIO_DIV_BY_7,
  DL_UART_CLOCK_DIVIDE2_RATIO_8 = UART_CLKDIV2_RATIO_DIV_BY_8
}
 

Functions

void DL_UART_init (UART_Regs *uart, const DL_UART_Config *config)
 Initialize the UART peripheral. More...
 
__STATIC_INLINE void DL_UART_enablePower (UART_Regs *uart)
 Enables the Peripheral Write Enable (PWREN) register for the UART. More...
 
__STATIC_INLINE void DL_UART_disablePower (UART_Regs *uart)
 Disables the Peripheral Write Enable (PWREN) register for the UART. More...
 
__STATIC_INLINE bool DL_UART_isPowerEnabled (const UART_Regs *uart)
 Returns if the Peripheral Write Enable (PWREN) register for the UART is enabled. More...
 
__STATIC_INLINE void DL_UART_reset (UART_Regs *uart)
 Resets uart peripheral. More...
 
__STATIC_INLINE bool DL_UART_isReset (const UART_Regs *uart)
 Returns if uart peripheral was reset. More...
 
__STATIC_INLINE void DL_UART_enable (UART_Regs *uart)
 Enable the UART peripheral. More...
 
__STATIC_INLINE bool DL_UART_isEnabled (const UART_Regs *uart)
 Checks if the UART peripheral is enabled. More...
 
__STATIC_INLINE void DL_UART_disable (UART_Regs *uart)
 Disable the UART peripheral. More...
 
void DL_UART_setClockConfig (UART_Regs *uart, const DL_UART_ClockConfig *config)
 Configure UART source clock. More...
 
void DL_UART_getClockConfig (const UART_Regs *uart, DL_UART_ClockConfig *config)
 Get UART source clock configuration. More...
 
void DL_UART_configBaudRate (UART_Regs *uart, uint32_t clockFreq, uint32_t baudRate)
 Configure the baud rate. More...
 
__STATIC_INLINE void DL_UART_setOversampling (UART_Regs *uart, DL_UART_OVERSAMPLING_RATE rate)
 Set the oversampling rate. More...
 
__STATIC_INLINE DL_UART_OVERSAMPLING_RATE DL_UART_getOversampling (const UART_Regs *uart)
 Get the oversampling rate. More...
 
__STATIC_INLINE void DL_UART_enableLoopbackMode (UART_Regs *uart)
 Enable loopback mode. More...
 
__STATIC_INLINE bool DL_UART_isLoopbackModeEnabled (const UART_Regs *uart)
 Check if loopback mode is enabled. More...
 
__STATIC_INLINE void DL_UART_disableLoopbackMode (UART_Regs *uart)
 Disable loopback mode. More...
 
__STATIC_INLINE void DL_UART_setDirection (UART_Regs *uart, DL_UART_DIRECTION direction)
 Set the direction of the UART communication. More...
 
__STATIC_INLINE DL_UART_DIRECTION DL_UART_getDirection (const UART_Regs *uart)
 Get the direction of the UART communication. More...
 
__STATIC_INLINE void DL_UART_enableMajorityVoting (UART_Regs *uart)
 Enable majority voting control. More...
 
__STATIC_INLINE bool DL_UART_isMajorityVotingEnabled (const UART_Regs *uart)
 Check if majority voting is enabled. More...
 
__STATIC_INLINE void DL_UART_disableMajorityVoting (UART_Regs *uart)
 Disable majority voting control. More...
 
__STATIC_INLINE void DL_UART_enableMSBFirst (UART_Regs *uart)
 Enable most significant bit (MSB) first. More...
 
__STATIC_INLINE bool DL_UART_isMSBFirstEnabled (const UART_Regs *uart)
 Check if most significant bit (MSB) first is enabled. More...
 
__STATIC_INLINE void DL_UART_disableMSBFirst (UART_Regs *uart)
 Disable most significant bit (MSB) first. More...
 
__STATIC_INLINE void DL_UART_enableTransmitPinManualControl (UART_Regs *uart)
 Enable control of the TXD pin. More...
 
__STATIC_INLINE bool DL_UART_isTransmitPinManualControlEnabled (const UART_Regs *uart)
 Check if control of the TXD pin is enabled. More...
 
__STATIC_INLINE void DL_UART_disableTransmitPinManualControl (UART_Regs *uart)
 Disable control of the TXD pin. More...
 
__STATIC_INLINE void DL_UART_setTransmitPinManualOutput (UART_Regs *uart, DL_UART_TXD_OUT txdOutVal)
 Set the output of the TXD pin. More...
 
__STATIC_INLINE DL_UART_TXD_OUT DL_UART_getTransmitPinManualOutput (const UART_Regs *uart)
 Get the output value of the TXD pin. More...
 
__STATIC_INLINE void DL_UART_enableManchesterEncoding (UART_Regs *uart)
 Enable Manchester encoding. More...
 
__STATIC_INLINE void DL_UART_disableManchesterEncoding (UART_Regs *uart)
 Disable Manchester encoding. More...
 
__STATIC_INLINE bool DL_UART_isManchesterEncodingEnabled (const UART_Regs *uart)
 Check if Manchester encoding is enabled. More...
 
__STATIC_INLINE void DL_UART_setCommunicationMode (UART_Regs *uart, DL_UART_MODE mode)
 Set the communication mode/protocol to use. More...
 
__STATIC_INLINE DL_UART_MODE DL_UART_getCommunicationMode (const UART_Regs *uart)
 Get the communication mode/protocol being used. More...
 
__STATIC_INLINE void DL_UART_setFlowControl (UART_Regs *uart, DL_UART_FLOW_CONTROL config)
 Set the flow control configuration. More...
 
__STATIC_INLINE DL_UART_FLOW_CONTROL DL_UART_getFlowControl (const UART_Regs *uart)
 Check the flow control configuration. More...
 
__STATIC_INLINE void DL_UART_setRTSOutput (UART_Regs *uart, DL_UART_RTS val)
 Set the request to send output signal. More...
 
__STATIC_INLINE DL_UART_RTS DL_UART_getRTSOutput (const UART_Regs *uart)
 Get the request to send output signal. More...
 
__STATIC_INLINE void DL_UART_enableFIFOs (UART_Regs *uart)
 Enable FIFOs. More...
 
__STATIC_INLINE void DL_UART_disableFIFOs (UART_Regs *uart)
 Disable FIFOs. More...
 
__STATIC_INLINE bool DL_UART_isFIFOsEnabled (const UART_Regs *uart)
 Check if FIFOs are enabled. More...
 
__STATIC_INLINE void DL_UART_enableLINSendBreak (UART_Regs *uart)
 Enable send break (for LIN protocol) More...
 
__STATIC_INLINE void DL_UART_disableLINSendBreak (UART_Regs *uart)
 Disable send break. More...
 
__STATIC_INLINE bool DL_UART_isLINSendBreakEnabled (const UART_Regs *uart)
 Check if send break is enabled. More...
 
__STATIC_INLINE bool DL_UART_isParityEnabled (const UART_Regs *uart)
 Check if parity is enabled. More...
 
__STATIC_INLINE void DL_UART_setParityMode (UART_Regs *uart, DL_UART_PARITY parity)
 Set the parity mode. More...
 
__STATIC_INLINE DL_UART_PARITY DL_UART_getParityMode (const UART_Regs *uart)
 Get parity mode. More...
 
__STATIC_INLINE void DL_UART_setStopBits (UART_Regs *uart, DL_UART_STOP_BITS numStopBits)
 Set the number of stop bits. More...
 
__STATIC_INLINE DL_UART_STOP_BITS DL_UART_getStopBits (const UART_Regs *uart)
 Get the number of stop bits. More...
 
__STATIC_INLINE void DL_UART_setWordLength (UART_Regs *uart, DL_UART_WORD_LENGTH wordLength)
 Set the word length. More...
 
__STATIC_INLINE DL_UART_WORD_LENGTH DL_UART_getWordLength (const UART_Regs *uart)
 Get the word length. More...
 
__STATIC_INLINE void DL_UART_enableSendIdlePattern (UART_Regs *uart)
 Send idle pattern. More...
 
__STATIC_INLINE void DL_UART_disableSendIdlePattern (UART_Regs *uart)
 Disable send idle pattern. More...
 
__STATIC_INLINE bool DL_UART_isSendIdlePatternEnabled (const UART_Regs *uart)
 Check if send idle pattern is enabled. More...
 
__STATIC_INLINE void DL_UART_setExternalDriverSetup (UART_Regs *uart, uint32_t val)
 Set external driver setup value. More...
 
__STATIC_INLINE uint32_t DL_UART_getExternalDriverSetup (const UART_Regs *uart)
 Get the external driver setup value. More...
 
__STATIC_INLINE void DL_UART_setExternalDriverHold (UART_Regs *uart, uint32_t val)
 Set external driver setup hold. More...
 
__STATIC_INLINE uint32_t DL_UART_getExternalDriverHold (const UART_Regs *uart)
 Get the external driver setup hold. More...
 
__STATIC_INLINE bool DL_UART_isBusy (const UART_Regs *uart)
 Checks if the UART is busy. More...
 
__STATIC_INLINE bool DL_UART_isRXFIFOEmpty (const UART_Regs *uart)
 Checks if the RX FIFO is empty. More...
 
__STATIC_INLINE bool DL_UART_isRXFIFOFull (const UART_Regs *uart)
 Checks if the RX FIFO is full. More...
 
__STATIC_INLINE bool DL_UART_isTXFIFOEmpty (const UART_Regs *uart)
 Checks if the TX FIFO is empty. More...
 
__STATIC_INLINE bool DL_UART_isTXFIFOFull (const UART_Regs *uart)
 Checks if the TX FIFO is full. More...
 
__STATIC_INLINE bool DL_UART_isClearToSend (const UART_Regs *uart)
 Checks if UART is clear to send. More...
 
__STATIC_INLINE bool DL_UART_isIdleModeDetected (const UART_Regs *uart)
 Checks if Idle mode has been detected. More...
 
__STATIC_INLINE void DL_UART_setTXFIFOThreshold (UART_Regs *uart, DL_UART_TX_FIFO_LEVEL threshold)
 Set the TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE DL_UART_TX_FIFO_LEVEL DL_UART_getTXFIFOThreshold (const UART_Regs *uart)
 Get the TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE void DL_UART_setRXFIFOThreshold (UART_Regs *uart, DL_UART_RX_FIFO_LEVEL threshold)
 Set the RX FIFO interrupt threshold level. The interrupts are generated based on a transition through a level rather than being based on the level. That is, the interrupts are generated when the fill level progresses through the trigger level. For example, if the receive trigger level is set to the half-way mark, the interrupt is triggered when the receive FIFO becomes half full. In other words, the interrupt is triggered after the receive FIFO is filled with two or more characters. More...
 
__STATIC_INLINE DL_UART_RX_FIFO_LEVEL DL_UART_getRXFIFOThreshold (const UART_Regs *uart)
 Get the RX FIFO interrupt threshold level. More...
 
__STATIC_INLINE void DL_UART_setRXInterruptTimeout (UART_Regs *uart, uint32_t timeout)
 Set the RX interrupt timeout. More...
 
__STATIC_INLINE uint32_t DL_UART_getRXInterruptTimeout (const UART_Regs *uart)
 Get the RX interrupt timeout. More...
 
__STATIC_INLINE uint32_t DL_UART_getIntegerBaudRateDivisor (const UART_Regs *uart)
 Get Integer Baud-Rate Divisor. More...
 
__STATIC_INLINE uint32_t DL_UART_getFractionalBaudRateDivisor (const UART_Regs *uart)
 Get Fractional Baud-Rate Divisor. More...
 
__STATIC_INLINE void DL_UART_setBaudRateDivisor (UART_Regs *uart, uint32_t integerDivisor, uint32_t fractionalDivisor)
 Set the baud rate divisor. More...
 
__STATIC_INLINE void DL_UART_setIrDABaudRateDivisor (UART_Regs *uart, uint32_t integerDivisor, uint32_t fractionalDivisor, DL_UART_CLOCK_DIVIDE2_RATIO clkDivisor2)
 Set the baud rate divisor for IrDA mode. More...
 
__STATIC_INLINE void DL_UART_setDigitalPulseWidth (UART_Regs *uart, uint32_t pulseWidth)
 Set the pulse width select for the digital glitch suppresion. More...
 
__STATIC_INLINE uint32_t DL_UART_getDigitalPulseWidth (const UART_Regs *uart)
 Get the pulse width select for the digital glitch suppresion. More...
 
__STATIC_INLINE void DL_UART_transmitData (UART_Regs *uart, uint8_t data)
 Writes data into the TX FIFO to transmit. More...
 
__STATIC_INLINE uint8_t DL_UART_receiveData (const UART_Regs *uart)
 Reads data from the RX FIFO. More...
 
__STATIC_INLINE uint32_t DL_UART_getErrorStatus (const UART_Regs *uart, uint32_t errorMask)
 Gets the status of the error flags of the received data. More...
 
__STATIC_INLINE void DL_UART_setLINCounterValue (UART_Regs *uart, uint16_t value)
 Set the LIN counter value. More...
 
__STATIC_INLINE uint16_t DL_UART_getLINCounterValue (const UART_Regs *uart)
 Get the LIN counter value. More...
 
__STATIC_INLINE void DL_UART_enableLINCounter (UART_Regs *uart)
 Enable the LIN counter. More...
 
__STATIC_INLINE bool DL_UART_isLINCounterEnabled (const UART_Regs *uart)
 Check if the LIN counter is enabled. More...
 
__STATIC_INLINE void DL_UART_disableLINCounter (UART_Regs *uart)
 Disable the LIN counter. More...
 
__STATIC_INLINE void DL_UART_enableLINCounterClearOnFallingEdge (UART_Regs *uart)
 Enable LIN counter clear and start counting on falling edge of RXD. More...
 
__STATIC_INLINE bool DL_UART_isLINCounterClearOnFallingEdge (const UART_Regs *uart)
 Check if LIN counting on falling edge of RXD is enabled. More...
 
__STATIC_INLINE void DL_UART_disableLINCounterClearOnFallingEdge (UART_Regs *uart)
 Disable LIN counting on falling edge of RXD. More...
 
__STATIC_INLINE void DL_UART_enableLINCountWhileLow (UART_Regs *uart)
 Enable LIN counter incrementing while RXD signal is low. More...
 
__STATIC_INLINE bool DL_UART_isLINCountWhileLowEnabled (const UART_Regs *uart)
 Check if LIN counter increments while RXD signal is low is enabled. More...
 
__STATIC_INLINE void DL_UART_disableLINCountWhileLow (UART_Regs *uart)
 Disable LIN counter increments while RXD signal is low. More...
 
__STATIC_INLINE void DL_UART_enableLINFallingEdgeCapture (UART_Regs *uart)
 Enable capture of the LIN counter on a falling edge. More...
 
__STATIC_INLINE bool DL_UART_isLINFallingEdgeCaptureEnabled (const UART_Regs *uart)
 Check status of capture of LIN counter on a falling edge. More...
 
__STATIC_INLINE void DL_UART_disableLINFallingEdgeCapture (UART_Regs *uart)
 Disable capture of LIN counter on a falling edge. More...
 
__STATIC_INLINE void DL_UART_enableLINRisingEdgeCapture (UART_Regs *uart)
 Enable capture of the LIN counter on a rising edge. More...
 
__STATIC_INLINE bool DL_UART_isLINRisingEdgeCaptureEnabled (const UART_Regs *uart)
 Check status of capture of LIN counter on a rising edge. More...
 
__STATIC_INLINE void DL_UART_disableLINRisingEdgeCapture (UART_Regs *uart)
 Disable capture of LIN counter on a rising edge. More...
 
__STATIC_INLINE void DL_UART_enableLINCounterCompareMatch (UART_Regs *uart)
 Enable LIN counter compare match mode. More...
 
__STATIC_INLINE void DL_UART_enableLINSyncFieldValidationCounterControl (UART_Regs *uart)
 Setup LIN counter control for sync field validation. More...
 
__STATIC_INLINE void DL_UART_enableLINReceptionCountControl (UART_Regs *uart)
 Setup LIN counter control for LIN reception. More...
 
__STATIC_INLINE bool DL_UART_isLINCounterCompareMatchEnabled (const UART_Regs *uart)
 Check if LIN counter compare match mode is enabled. More...
 
__STATIC_INLINE void DL_UART_disableLINCounterCompareMatch (UART_Regs *uart)
 Disable LIN counter compare match mode. More...
 
__STATIC_INLINE void DL_UART_setLINCounterCompareValue (UART_Regs *uart, uint16_t value)
 Set the value to be compared to the LIN counter. More...
 
__STATIC_INLINE uint16_t DL_UART_getLINFallingEdgeCaptureValue (const UART_Regs *uart)
 Get the LINC0 counter value. More...
 
__STATIC_INLINE uint16_t DL_UART_getLINRisingEdgeCaptureValue (const UART_Regs *uart)
 Get the LINC1 counter value. More...
 
__STATIC_INLINE void DL_UART_enableIrDAMode (UART_Regs *uart)
 Enable the IrDA encoder/decoder. More...
 
__STATIC_INLINE bool DL_UART_isIrDAModeEnabled (const UART_Regs *uart)
 Check if the IrDA encoder/decoder is enabled. More...
 
__STATIC_INLINE void DL_UART_disableIrDAMode (UART_Regs *uart)
 Disable the IrDA encoder/decoder. More...
 
__STATIC_INLINE void DL_UART_setIrDATXPulseClockSelect (UART_Regs *uart, DL_UART_IRDA_CLOCK uartClock)
 Set the IrDA transmit pulse clock select. More...
 
__STATIC_INLINE DL_UART_IRDA_CLOCK DL_UART_getIrDATXPulseClockSelect (const UART_Regs *uart)
 Get the IrDA transmit pulse clock select. More...
 
void DL_UART_configIrDAMode (UART_Regs *uart, DL_UART_IRDA_POLARITY polarity, uint32_t pulseLength, DL_UART_IRDA_CLOCK irdaClk)
 Set the IrDA configurations. More...
 
void DL_UART_setIrDAPulseLength (UART_Regs *uart, uint32_t pulseLength, DL_UART_IRDA_CLOCK irdaClk)
 Set the IrDA transmit pulse length. More...
 
__STATIC_INLINE uint32_t DL_UART_getIrDATXPulseLength (const UART_Regs *uart)
 Get the IrDA transmit pulse length. More...
 
__STATIC_INLINE void DL_UART_setIrDARXPulsePolarity (UART_Regs *uart, DL_UART_IRDA_POLARITY polarity)
 Set the IrDA receive input UCAxRXD polarity. More...
 
__STATIC_INLINE DL_UART_IRDA_POLARITY DL_UART_getIrDARXPulsePolarity (const UART_Regs *uart)
 Get the IrDA receive input UCAxRXD polarity. More...
 
__STATIC_INLINE void DL_UART_setAddressMask (UART_Regs *uart, uint32_t addressMask)
 Set the address mask for DALI, 9-bit, or Idle-Line mode. More...
 
__STATIC_INLINE uint32_t DL_UART_getAddressMask (const UART_Regs *uart)
 Get the address mask being used. More...
 
__STATIC_INLINE void DL_UART_setAddress (UART_Regs *uart, uint32_t address)
 Set the address. More...
 
__STATIC_INLINE uint32_t DL_UART_getAddress (const UART_Regs *uart)
 Get the address being used. More...
 
__STATIC_INLINE void DL_UART_enableInterrupt (UART_Regs *uart, uint32_t interruptMask)
 Enable UART interrupts. More...
 
__STATIC_INLINE void DL_UART_disableInterrupt (UART_Regs *uart, uint32_t interruptMask)
 Disable UART interrupts. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledInterrupts (const UART_Regs *uart, uint32_t interruptMask)
 Check which UART interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledInterruptStatus (const UART_Regs *uart, uint32_t interruptMask)
 Check interrupt flag of enabled UART interrupts. More...
 
__STATIC_INLINE uint32_t DL_UART_getRawInterruptStatus (const UART_Regs *uart, uint32_t interruptMask)
 Check interrupt flag of any UART interrupt. More...
 
__STATIC_INLINE DL_UART_IIDX DL_UART_getPendingInterrupt (const UART_Regs *uart)
 Get highest priority pending UART interrupt. More...
 
__STATIC_INLINE void DL_UART_clearInterruptStatus (UART_Regs *uart, uint32_t interruptMask)
 Clear pending UART interrupts. More...
 
__STATIC_INLINE void DL_UART_changeConfig (UART_Regs *uart)
 Prepares the UART to change the configuration. More...
 
__STATIC_INLINE void DL_UART_enableAnalogGlitchFilter (UART_Regs *uart)
 Enable the analog glitch filter on the RX input. More...
 
__STATIC_INLINE void DL_UART_disableAnalogGlitchFilter (UART_Regs *uart)
 Disable the analog glitch filter on the RX input. More...
 
__STATIC_INLINE bool DL_UART_isAnalogGlitchFilterEnabled (const UART_Regs *uart)
 Returns if analog glitch filter is enabled. More...
 
__STATIC_INLINE void DL_UART_enableGlitchFilterChaining (UART_Regs *uart)
 Enable analog and digital noise glitch filter chaining. More...
 
__STATIC_INLINE void DL_UART_disableGlitchFilterChaining (UART_Regs *uart)
 Disable analog and digital noise glitch filter chaining. More...
 
__STATIC_INLINE bool DL_UART_isGlitchFilterChainingEnabled (const UART_Regs *uart)
 Returns if glitch filter chaining enabled. More...
 
__STATIC_INLINE void DL_UART_setAnalogPulseWidth (UART_Regs *uart, DL_UART_PULSE_WIDTH pulseWidth)
 Set the pulse width select for the analog glitch suppresion. More...
 
__STATIC_INLINE DL_UART_PULSE_WIDTH DL_UART_getAnalogPulseWidth (const UART_Regs *uart)
 Get the pulse width select for the glitch suppresion. More...
 
void DL_UART_transmitDataBlocking (UART_Regs *uart, uint8_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
uint8_t DL_UART_receiveDataBlocking (const UART_Regs *uart)
 Blocks to ensure receive is ready before reading data. More...
 
bool DL_UART_transmitDataCheck (UART_Regs *uart, uint8_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_UART_receiveDataCheck (const UART_Regs *uart, uint8_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
uint32_t DL_UART_drainRXFIFO (const UART_Regs *uart, uint8_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 8 bit access. More...
 
uint32_t DL_UART_fillTXFIFO (UART_Regs *uart, const uint8_t *buffer, uint32_t count)
 Fill the TX FIFO until full using 8 bit access. More...
 
__STATIC_INLINE void DL_UART_enableDMAReceiveEvent (UART_Regs *uart, uint32_t interrupt)
 Enable UART interrupt for triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_UART_enableDMATransmitEvent (UART_Regs *uart)
 Enable UART interrupt for triggering the DMA transmit event. More...
 
__STATIC_INLINE void DL_UART_disableDMAReceiveEvent (UART_Regs *uart, uint32_t interrupt)
 Disables UART interrupt from triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_UART_disableDMATransmitEvent (UART_Regs *uart)
 Disables UART interrupt from triggering the DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledDMAReceiveEvent (const UART_Regs *uart, uint32_t interruptMask)
 Check which UART interrupt for DMA receive events is enabled. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledDMATransmitEvent (const UART_Regs *uart)
 Check if UART interrupt for DMA transmit event is enabled. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledDMAReceiveEventStatus (const UART_Regs *uart, uint32_t interruptMask)
 Check interrupt flag of enabled UART interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_UART_getEnabledDMATransmitEventStatus (const UART_Regs *uart)
 Check interrupt flag of enabled UART interrupt for DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_UART_getRawDMAReceiveEventStatus (const UART_Regs *uart, uint32_t interruptMask)
 Check interrupt flag of any UART interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_UART_getRawDMATransmitEventStatus (const UART_Regs *uart)
 Check interrupt flag of any UART interrupt for DMA transmit event. More...
 
__STATIC_INLINE DL_UART_DMA_IIDX_RX DL_UART_getPendingDMAReceiveEvent (const UART_Regs *uart)
 Get highest priority pending UART interrupt for DMA receive event. More...
 
__STATIC_INLINE DL_UART_DMA_IIDX_TX DL_UART_getPendingDMATransmitEvent (const UART_Regs *uart)
 Get highest priority pending UART interrupt for DMA transmit event. More...
 
__STATIC_INLINE void DL_UART_clearDMAReceiveEventStatus (UART_Regs *uart, uint32_t interruptMask)
 Clear pending UART interrupts for DMA receive event. More...
 
__STATIC_INLINE void DL_UART_clearDMATransmitEventStatus (UART_Regs *uart)
 Clear pending UART interrupt for DMA transmit event. More...
 
__STATIC_INLINE void DL_UART_setClockDivider2 (UART_Regs *uart, DL_UART_CLOCK_DIVIDE2_RATIO ratio)
 Sets the second clock divider ratio. More...
 
__STATIC_INLINE DL_UART_CLOCK_DIVIDE2_RATIO DL_UART_getClockDivider2 (const UART_Regs *uart)
 Gets the value of CLKDIV2. More...
 
bool DL_UART_Main_saveConfiguration (const UART_Regs *uart, DL_UART_Main_backupConfig *ptr)
 Save UART Main configuration before entering a power loss state. More...
 
bool DL_UART_Main_restoreConfiguration (UART_Regs *uart, DL_UART_Main_backupConfig *ptr)
 Restore UART Main configuration after leaving a power loss state. More...
 
bool DL_UART_Extend_saveConfiguration (const UART_Regs *uart, DL_UART_Extend_backupConfig *ptr)
 Save UART Extend configuration before entering a power loss state. More...
 
bool DL_UART_Extend_restoreConfiguration (UART_Regs *uart, DL_UART_Extend_backupConfig *ptr)
 Restore UART Extend configuration after leaving a power loss state. More...
 
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale