MSPM0L111X Driver Library  2.10.00.04
Data Structures | Macros | Enumerations | Functions
dl_trng.h File Reference

Detailed Description

True Random Number Generator (TRNG) Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_trng.h:

Go to the source code of this file.

Data Structures

struct  DL_TRNG_backupConfig
 Configuration structure to backup TRNG peripheral state before going to STOP/STANDBY mode. Used by DL_TRNG_saveConfiguration. More...
 

Macros

#define DL_TRNG_INTERRUPT_HEALTH_FAIL_EVENT   (TRNG_IMASK_IRQ_HEALTH_FAIL_MASK)
 TRNG interrupt definition for health test failed.
 
#define DL_TRNG_INTERRUPT_CMD_DONE_EVENT   (TRNG_IMASK_IRQ_CMD_DONE_MASK)
 TRNG interrupt definition for commafnd done.
 
#define DL_TRNG_INTERRUPT_CMD_FAIL_EVENT   (TRNG_IMASK_IRQ_CMD_FAIL_MASK)
 TRNG interrupt definition for command fail.
 
#define DL_TRNG_INTERRUPT_CAPTURE_RDY_EVENT   (TRNG_IMASK_IRQ_CAPTURED_RDY_MASK)
 TRNG interrupt definition for capture ready.
 
#define DL_TRNG_DIGITAL_HEALTH_TEST_SUCCESS   (0xFF)
 TRNG Digital health test success value.
 
#define DL_TRNG_ANALOG_HEALTH_TEST_SUCCESS   (0x1)
 TRNG Analog health test success value.
 

Enumerations

enum  DL_TRNG_IIDX {
  DL_TRNG_IIDX_HEALTH_FAIL = TRNG_IIDX_STAT_IRQ_HEALTH_FAIL,
  DL_TRNG_IIDX_CMD_DONE = TRNG_IIDX_STAT_IRQ_CMD_DONE,
  DL_TRNG_IIDX_CMD_FAIL = TRNG_IIDX_STAT_IRQ_CMD_FAIL,
  DL_TRNG_IIDX_CAPTURED_READY = TRNG_IIDX_STAT_IRQ_CAPTURED_RDY
}
 
enum  DL_TRNG_DECIMATION_RATE {
  DL_TRNG_DECIMATION_RATE_1 = 0x0,
  DL_TRNG_DECIMATION_RATE_2 = 0x1,
  DL_TRNG_DECIMATION_RATE_3 = 0x2,
  DL_TRNG_DECIMATION_RATE_4 = 0x3,
  DL_TRNG_DECIMATION_RATE_5 = 0x4,
  DL_TRNG_DECIMATION_RATE_6 = 0x5,
  DL_TRNG_DECIMATION_RATE_7 = 0x6,
  DL_TRNG_DECIMATION_RATE_8 = 0x7
}
 
enum  DL_TRNG_CMD {
  DL_TRNG_CMD_PWROFF = TRNG_CTL_CMD_PWR_OFF,
  DL_TRNG_CMD_TEST_DIG = TRNG_CTL_CMD_PWRUP_DIG,
  DL_TRNG_CMD_TEST_ANA = TRNG_CTL_CMD_PWRUP_ANA,
  DL_TRNG_CMD_NORM_FUNC = TRNG_CTL_CMD_NORM_FUNC
}
 
enum  DL_TRNG_CLOCK_DIVIDE {
  DL_TRNG_CLOCK_DIVIDE_1 = TRNG_CLKDIVIDE_RATIO_DIV_BY_1,
  DL_TRNG_CLOCK_DIVIDE_2 = TRNG_CLKDIVIDE_RATIO_DIV_BY_2,
  DL_TRNG_CLOCK_DIVIDE_4 = TRNG_CLKDIVIDE_RATIO_DIV_BY_4,
  DL_TRNG_CLOCK_DIVIDE_6 = TRNG_CLKDIVIDE_RATIO_DIV_BY_6,
  DL_TRNG_CLOCK_DIVIDE_8 = TRNG_CLKDIVIDE_RATIO_DIV_BY_8
}
 
enum  DL_TRNG_STATE {
  DL_TRNG_STATE_OFF = 0x0,
  DL_TRNG_STATE_PWRUP_ES = 0x1,
  DL_TRNG_STATE_NORM_FUNC = 0x3,
  DL_TRNG_STATE_TEST_DIG = 0x7,
  DL_TRNG_STATE_TEST_ANA = 0xB,
  DL_TRNG_STATE_ERROR = 0xA,
  DL_TRNG_STATE_PWRDOWN = 0x2
}
 

Functions

__STATIC_INLINE void DL_TRNG_enablePower (TRNG_Regs *trng)
 Enables the Peripheral Write Enable (PWREN) register for the TRNG. More...
 
__STATIC_INLINE void DL_TRNG_disablePower (TRNG_Regs *trng)
 Disables the Peripheral Write Enable (PWREN) register for the TRNG. More...
 
__STATIC_INLINE bool DL_TRNG_isPowerEnabled (TRNG_Regs *trng)
 Returns if the Peripheral Write Enable (PWREN) register for the TRNG is enabled. More...
 
__STATIC_INLINE DL_TRNG_CLOCK_DIVIDE DL_TRNG_getClockDivider (const TRNG_Regs *trng)
 Get the clock divider on the TRNG module. More...
 
__STATIC_INLINE void DL_TRNG_setClockDivider (TRNG_Regs *trng, DL_TRNG_CLOCK_DIVIDE clockDivider)
 Set the clock divider on the TRNG module. More...
 
__STATIC_INLINE void DL_TRNG_reset (TRNG_Regs *trng)
 Resets the TRNG module. More...
 
__STATIC_INLINE bool DL_TRNG_isReset (const TRNG_Regs *trng)
 Returns if TRNG peripheral was reset. More...
 
__STATIC_INLINE bool DL_TRNG_isCaptureReady (const TRNG_Regs *trng)
 Returns if the data capture is ready. More...
 
__STATIC_INLINE bool DL_TRNG_isCommandDone (const TRNG_Regs *trng)
 Returns if the issued TRNG command is done. More...
 
__STATIC_INLINE bool DL_TRNG_isCommandFail (const TRNG_Regs *trng)
 Returns if the issued TRNG command failed. More...
 
__STATIC_INLINE bool DL_TRNG_isHealthTestFail (const TRNG_Regs *trng)
 Returns if a health test failed. More...
 
__STATIC_INLINE void DL_TRNG_setDecimationRate (TRNG_Regs *trng, DL_TRNG_DECIMATION_RATE decimationRate)
 Set the decimation rate. More...
 
__STATIC_INLINE DL_TRNG_DECIMATION_RATE DL_TRNG_getDecimationRate (const TRNG_Regs *trng)
 Get the decimation rate. More...
 
__STATIC_INLINE uint8_t DL_TRNG_getDigitalHealthTestResults (const TRNG_Regs *trng)
 Get the digital health test results. More...
 
__STATIC_INLINE uint8_t DL_TRNG_getAnalogHealthTestResults (const TRNG_Regs *trng)
 Get the analog health test results. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getCurrentState (const TRNG_Regs *trng)
 Get the current state of the TRNG front end FSM. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getIssuedCommand (const TRNG_Regs *trng)
 Get the last accepted command that was issued to the TRNG. More...
 
__STATIC_INLINE bool DL_TRNG_isRepetitionTestFail (const TRNG_Regs *trng)
 Indicates if the repetition counter test caused the most recent failure. More...
 
__STATIC_INLINE bool DL_TRNG_isAdaptiveTestFail (const TRNG_Regs *trng)
 Indicates if the Adaptive Proportion Test (1,2,3, or 4-bit counters) caused the most recent failure. More...
 
__STATIC_INLINE void DL_TRNG_enableInterrupt (TRNG_Regs *trng, uint32_t interruptMask)
 Enable TRNG interrupt. More...
 
__STATIC_INLINE void DL_TRNG_disableInterrupt (TRNG_Regs *trng, uint32_t interruptMask)
 Disable TRNG interrupt. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getEnabledInterrupts (const TRNG_Regs *trng, uint32_t interruptMask)
 Check which TRNG interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getEnabledInterruptStatus (const TRNG_Regs *trng, uint32_t interruptMask)
 Check interrupt flag of enabled TRNG interrupt. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getRawInterruptStatus (const TRNG_Regs *trng, uint32_t interruptMask)
 Check interrupt flag of any TRNG interrupt. More...
 
__STATIC_INLINE DL_TRNG_IIDX DL_TRNG_getPendingInterrupt (const TRNG_Regs *trng)
 Get highest priority pending TRNG interrupt. More...
 
__STATIC_INLINE void DL_TRNG_clearInterruptStatus (TRNG_Regs *trng, uint32_t interruptMask)
 Clear pending TRNG interrupt. More...
 
__STATIC_INLINE void DL_TRNG_sendCommand (TRNG_Regs *trng, DL_TRNG_CMD cmd)
 Update control register's command bits to send a TRNG command. More...
 
__STATIC_INLINE uint32_t DL_TRNG_getCapture (const TRNG_Regs *trng)
 Get word capture from TRNG. More...
 
bool DL_TRNG_saveConfiguration (const TRNG_Regs *trng, DL_TRNG_backupConfig *ptr)
 Save TRNG configuration before entering a power loss state. More...
 
bool DL_TRNG_restoreConfiguration (TRNG_Regs *trng, DL_TRNG_backupConfig *ptr)
 Restore TRNG configuration after leaving a power loss state. Upon restoration, if the TRNG was not originally in OFF state, then the TRNG will be set to the normal operating mode. More...
 
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale