MSPM0C110X Driver Library  2.08.00.03
Data Structures | Macros | Enumerations | Functions
dl_vref.h File Reference

Detailed Description

Voltage Reference (VREF) Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_vref.h:

Go to the source code of this file.

Data Structures

struct  DL_VREF_ClockConfig
 Configuration struct for DL_VREF_setClockConfig. More...
 
struct  DL_VREF_Config
 Configuration struct for DL_VREF_Config. More...
 

Macros

#define DL_VREF_CTL1_READY_NOTRDY   (VREF_CTL1_READY_NOTRDY)
 VREF bit in CTL1 indicating the module is ready is not set.
 
#define DL_VREF_CTL1_READY_RDY   (VREF_CTL1_READY_RDY)
 VREF bit in CTL1 indicating the module is ready is set.
 
#define DL_VREF_SH_MIN   (VREF_CTL2_SHCYCLE_MINIMUM)
 Minimum value for VREF sample and hold, if enabled.
 
#define DL_VREF_SH_MAX   (VREF_CTL2_SHCYCLE_MAXIMUM)
 Maximum value for VREF sample and hold, if enabled.
 
#define DL_VREF_HOLD_MIN   (0x0000U)
 Minimum value for VREF hold, if enabled.
 
#define DL_VREF_HOLD_MAX   (0xFFFFU)
 Maximum value for VREF hold, if enabled.
 

Enumerations

enum  DL_VREF_CLOCK {
  DL_VREF_CLOCK_LFCLK = VREF_CLKSEL_LFCLK_SEL_MASK,
  DL_VREF_CLOCK_MFCLK = VREF_CLKSEL_MFCLK_SEL_MASK,
  DL_VREF_CLOCK_BUSCLK = VREF_CLKSEL_BUSCLK_SEL_MASK
}
 
enum  DL_VREF_CLOCK_DIVIDE {
  DL_VREF_CLOCK_DIVIDE_1 = 0,
  DL_VREF_CLOCK_DIVIDE_2 = 1,
  DL_VREF_CLOCK_DIVIDE_4 = 3,
  DL_VREF_CLOCK_DIVIDE_6 = 5,
  DL_VREF_CLOCK_DIVIDE_8 = 7
}
 
enum  DL_VREF_ENABLE {
  DL_VREF_ENABLE_DISABLE = VREF_CTL0_ENABLE_DISABLE,
  DL_VREF_ENABLE_ENABLE = VREF_CTL0_ENABLE_ENABLE
}
 
enum  DL_VREF_BUFCONFIG {
  DL_VREF_BUFCONFIG_OUTPUT_2_5V = VREF_CTL0_BUFCONFIG_OUTPUT2P5V,
  DL_VREF_BUFCONFIG_OUTPUT_1_4V = VREF_CTL0_BUFCONFIG_OUTPUT1P4V
}
 
enum  DL_VREF_SHMODE {
  DL_VREF_SHMODE_DISABLE = VREF_CTL0_SHMODE_DISABLE,
  DL_VREF_SHMODE_ENABLE = VREF_CTL0_SHMODE_ENABLE
}
 

Functions

__STATIC_INLINE void DL_VREF_enablePower (VREF_Regs *vref)
 Enables the Peripheral Write Enable (PWREN) register for the VREF. More...
 
__STATIC_INLINE void DL_VREF_disablePower (VREF_Regs *vref)
 Disables the Peripheral Write Enable (PWREN) register for the VREF. More...
 
__STATIC_INLINE bool DL_VREF_isPowerEnabled (VREF_Regs *vref)
 Returns if the Peripheral Write Enable (PWREN) register for the VREF is enabled. More...
 
__STATIC_INLINE void DL_VREF_enableInternalRef (VREF_Regs *vref)
 Enables Internal VREF. More...
 
__STATIC_INLINE void DL_VREF_disableInternalRef (VREF_Regs *vref)
 Disables Internal VREF, allows for External VREF. More...
 
__STATIC_INLINE bool DL_VREF_isEnabled (const VREF_Regs *vref)
 Checks if the internal VREF is enabled. More...
 
void DL_VREF_setClockConfig (VREF_Regs *vref, const DL_VREF_ClockConfig *config)
 Set the clock select and clock divide fields in VREF. More...
 
void DL_VREF_getClockConfig (const VREF_Regs *vref, DL_VREF_ClockConfig *config)
 Copy the clock select and clock divide fields in VREF to config. More...
 
__STATIC_INLINE void DL_VREF_reset (VREF_Regs *vref)
 Resets the VREF module. More...
 
__STATIC_INLINE bool DL_VREF_isReset (const VREF_Regs *vref)
 Returns if VREF peripheral was reset. More...
 
__STATIC_INLINE uint32_t DL_VREF_getStatus (const VREF_Regs *vref)
 Returns VREF register status. More...
 
void DL_VREF_configReference (VREF_Regs *vref, const DL_VREF_Config *config)
 Configure VREF enable, control registers. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale