MSPM0C110X Driver Library  2.08.00.03
Data Structures | Macros | Enumerations | Functions
dl_spi.h File Reference

Detailed Description

SPI Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_spi.h:

Go to the source code of this file.

Data Structures

struct  DL_SPI_Config
 Configuration struct for DL_SPI_init. More...
 
struct  DL_SPI_ClockConfig
 Configuration struct for DL_SPI_setClockConfig. More...
 
struct  DL_SPI_backupConfig
 Configuration structure to backup SPI peripheral state before going to STOP/STANDBY mode. Used by DL_SPI_saveConfiguration and DL_SPI_restoreConfiguration. More...
 

Macros

#define DL_SPI_CD_MODE_DATA   (SPI_CTL1_CDMODE_DATA >> SPI_CTL1_CDMODE_OFS)
 Data mode.
 
#define DL_SPI_CD_MODE_COMMAND   (SPI_CTL1_CDMODE_COMMAND >> SPI_CTL1_CDMODE_OFS)
 Command mode.
 
#define DL_SPI_INTERRUPT_DMA_DONE_TX   (SPI_CPU_INT_IMASK_DMA_DONE_TX_SET)
 DMA done 1 event for transmit interrupt.
 
#define DL_SPI_INTERRUPT_DMA_DONE_RX   (SPI_CPU_INT_IMASK_DMA_DONE_RX_SET)
 DMA done 1 event for receive interrupt.
 
#define DL_SPI_INTERRUPT_IDLE   (SPI_CPU_INT_IMASK_IDLE_SET)
 SPI has finished transfers and changed into idle mode interrupt.
 
#define DL_SPI_INTERRUPT_TX_EMPTY   (SPI_CPU_INT_IMASK_TXEMPTY_SET)
 Transmit FIFO empty interrupt.
 
#define DL_SPI_INTERRUPT_TX   (SPI_CPU_INT_IMASK_TX_SET)
 Transmit FIFO interrupt.
 
#define DL_SPI_INTERRUPT_RX   (SPI_CPU_INT_IMASK_RX_SET)
 Receive FIFO interrupt.
 
#define DL_SPI_INTERRUPT_RX_TIMEOUT   (SPI_CPU_INT_IMASK_RTOUT_SET)
 Receive timeout interrupt.
 
#define DL_SPI_INTERRUPT_RX_FULL   (SPI_CPU_INT_IMASK_RXFULL_SET)
 Receive FIFO full interrupt.
 
#define DL_SPI_INTERRUPT_TX_UNDERFLOW   (SPI_CPU_INT_IMASK_TXFIFO_UNF_SET)
 Transmit FIFO underflow interrupt.
 
#define DL_SPI_INTERRUPT_PARITY_ERROR   (SPI_CPU_INT_IMASK_PER_SET)
 Parity error.
 
#define DL_SPI_INTERRUPT_RX_OVERFLOW   (SPI_CPU_INT_IMASK_RXFIFO_OVF_SET)
 Receive FIFO overflow interrupt.
 
#define DL_SPI_DMA_INTERRUPT_RX   (SPI_DMA_TRIG_RX_IMASK_RX_SET)
 SPI interrupt for enabling SPI receive as DMA trigger.
 
#define DL_SPI_DMA_INTERRUPT_RX_TIMEOUT   (SPI_DMA_TRIG_RX_IMASK_RTOUT_SET)
 SPI interrupt for enabling SPI receive timeout as DMA trigger.
 
#define DL_SPI_DMA_INTERRUPT_TX   (SPI_DMA_TRIG_TX_IMASK_TX_SET)
 SPI interrupt for enabling SPI transmit as DMA trigger.
 

Enumerations

enum  DL_SPI_DMA_IIDX_RX {
  DL_SPI_DMA_IIDX_RX_TRIGGER = SPI_DMA_TRIG_RX_IIDX_STAT_RX_EVT,
  DL_SPI_DMA_IIDX_RX_TIMEOUT_TRIGGER = SPI_DMA_TRIG_RX_IIDX_STAT_RTOUT_EVT
}
 
enum  DL_SPI_DMA_IIDX_TX { DL_SPI_DMA_IIDX_TX_TRIGGER = SPI_DMA_TRIG_TX_IIDX_STAT_TX_EVT }
 
enum  DL_SPI_PARITY {
  DL_SPI_PARITY_EVEN,
  DL_SPI_PARITY_ODD,
  DL_SPI_PARITY_NONE = (SPI_CTL1_PREN_DISABLE | SPI_CTL1_PTEN_DISABLE)
}
 
enum  DL_SPI_FRAME_FORMAT {
  DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA1,
  DL_SPI_FRAME_FORMAT_TI_SYNC = (SPI_CTL0_FRF_TI_SYNC)
}
 
enum  DL_SPI_MODE {
  DL_SPI_MODE_CONTROLLER = (SPI_CTL1_CP_ENABLE),
  DL_SPI_MODE_PERIPHERAL = (SPI_CTL1_CP_DISABLE)
}
 
enum  DL_SPI_BIT_ORDER {
  DL_SPI_BIT_ORDER_MSB_FIRST = (SPI_CTL1_MSB_ENABLE),
  DL_SPI_BIT_ORDER_LSB_FIRST = (SPI_CTL1_MSB_DISABLE)
}
 
enum  DL_SPI_DATA_SIZE {
  DL_SPI_DATA_SIZE_4 = (SPI_CTL0_DSS_DSS_4),
  DL_SPI_DATA_SIZE_5 = (SPI_CTL0_DSS_DSS_5),
  DL_SPI_DATA_SIZE_6 = (SPI_CTL0_DSS_DSS_6),
  DL_SPI_DATA_SIZE_7 = (SPI_CTL0_DSS_DSS_7),
  DL_SPI_DATA_SIZE_8 = (SPI_CTL0_DSS_DSS_8),
  DL_SPI_DATA_SIZE_9 = (SPI_CTL0_DSS_DSS_9),
  DL_SPI_DATA_SIZE_10 = (SPI_CTL0_DSS_DSS_10),
  DL_SPI_DATA_SIZE_11 = (SPI_CTL0_DSS_DSS_11),
  DL_SPI_DATA_SIZE_12 = (SPI_CTL0_DSS_DSS_12),
  DL_SPI_DATA_SIZE_13 = (SPI_CTL0_DSS_DSS_13),
  DL_SPI_DATA_SIZE_14 = (SPI_CTL0_DSS_DSS_14),
  DL_SPI_DATA_SIZE_15 = (SPI_CTL0_DSS_DSS_15),
  DL_SPI_DATA_SIZE_16 = (SPI_CTL0_DSS_DSS_16)
}
 
enum  DL_SPI_CHIP_SELECT {
  DL_SPI_CHIP_SELECT_0 = (SPI_CTL0_CSSEL_CSSEL_0),
  DL_SPI_CHIP_SELECT_1 = (SPI_CTL0_CSSEL_CSSEL_1),
  DL_SPI_CHIP_SELECT_2 = (SPI_CTL0_CSSEL_CSSEL_2),
  DL_SPI_CHIP_SELECT_3 = (SPI_CTL0_CSSEL_CSSEL_3),
  DL_SPI_CHIP_SELECT_NONE = (0)
}
 
enum  DL_SPI_TX_FIFO_LEVEL {
  DL_SPI_TX_FIFO_LEVEL_3_4_EMPTY = SPI_IFLS_TXIFLSEL_LVL_3_4,
  DL_SPI_TX_FIFO_LEVEL_1_2_EMPTY = SPI_IFLS_TXIFLSEL_LVL_1_2,
  DL_SPI_TX_FIFO_LEVEL_1_4_EMPTY = SPI_IFLS_TXIFLSEL_LVL_1_4,
  DL_SPI_TX_FIFO_LEVEL_EMPTY = SPI_IFLS_TXIFLSEL_LVL_EMPTY,
  DL_SPI_TX_FIFO_LEVEL_ONE_FRAME = SPI_IFLS_TXIFLSEL_LEVEL_1
}
 
enum  DL_SPI_RX_FIFO_LEVEL {
  DL_SPI_RX_FIFO_LEVEL_ONE_FRAME = SPI_IFLS_RXIFLSEL_LEVEL_1,
  DL_SPI_RX_FIFO_LEVEL_FULL = SPI_IFLS_RXIFLSEL_LVL_FULL,
  DL_SPI_RX_FIFO_LEVEL_3_4_FULL = SPI_IFLS_RXIFLSEL_LVL_3_4,
  DL_SPI_RX_FIFO_LEVEL_1_2_FULL = SPI_IFLS_RXIFLSEL_LVL_1_2,
  DL_SPI_RX_FIFO_LEVEL_1_4_FULL = SPI_IFLS_RXIFLSEL_LVL_1_4
}
 
enum  DL_SPI_IIDX {
  DL_SPI_IIDX_DMA_DONE_TX = SPI_CPU_INT_IIDX_STAT_DMA_DONE_TX_EVT,
  DL_SPI_IIDX_DMA_DONE_RX = SPI_CPU_INT_IIDX_STAT_DMA_DONE_RX_EVT,
  DL_SPI_IIDX_IDLE = SPI_CPU_INT_IIDX_STAT_IDLE_EVT,
  DL_SPI_IIDX_TX_EMPTY = SPI_CPU_INT_IIDX_STAT_TX_EMPTY,
  DL_SPI_IIDX_TX = SPI_CPU_INT_IIDX_STAT_TX_EVT,
  DL_SPI_IIDX_RX = SPI_CPU_INT_IIDX_STAT_RX_EVT,
  DL_SPI_IIDX_RX_TIMEOUT = SPI_CPU_INT_IIDX_STAT_RTOUT_EVT,
  DL_SPI_IIDX_RX_FULL = SPI_CPU_INT_IIDX_STAT_RXFULL_EVT,
  DL_SPI_IIDX_TX_UNDERFLOW = SPI_CPU_INT_IIDX_STAT_TXFIFO_UNF_EVT,
  DL_SPI_IIDX_PARITY_ERROR = SPI_CPU_INT_IIDX_STAT_PER_EVT,
  DL_SPI_IIDX_RX_OVERFLOW = SPI_CPU_INT_IIDX_STAT_RXFIFO_OFV_EVT
}
 
enum  DL_SPI_CLOCK_DIVIDE_RATIO {
  DL_SPI_CLOCK_DIVIDE_RATIO_1 = SPI_CLKDIV_RATIO_DIV_BY_1,
  DL_SPI_CLOCK_DIVIDE_RATIO_2 = SPI_CLKDIV_RATIO_DIV_BY_2,
  DL_SPI_CLOCK_DIVIDE_RATIO_3 = SPI_CLKDIV_RATIO_DIV_BY_3,
  DL_SPI_CLOCK_DIVIDE_RATIO_4 = SPI_CLKDIV_RATIO_DIV_BY_4,
  DL_SPI_CLOCK_DIVIDE_RATIO_5 = SPI_CLKDIV_RATIO_DIV_BY_5,
  DL_SPI_CLOCK_DIVIDE_RATIO_6 = SPI_CLKDIV_RATIO_DIV_BY_6,
  DL_SPI_CLOCK_DIVIDE_RATIO_7 = SPI_CLKDIV_RATIO_DIV_BY_7,
  DL_SPI_CLOCK_DIVIDE_RATIO_8 = SPI_CLKDIV_RATIO_DIV_BY_8
}
 
enum  DL_SPI_CLOCK {
  DL_SPI_CLOCK_BUSCLK = SPI_CLKSEL_SYSCLK_SEL_ENABLE,
  DL_SPI_CLOCK_MFCLK = SPI_CLKSEL_MFCLK_SEL_ENABLE,
  DL_SPI_CLOCK_LFCLK = SPI_CLKSEL_LFCLK_SEL_ENABLE
}
 

Functions

void DL_SPI_init (SPI_Regs *spi, const DL_SPI_Config *config)
 Initialize the SPI peripheral. More...
 
__STATIC_INLINE void DL_SPI_enablePower (SPI_Regs *spi)
 Enables the Peripheral Write Enable (PWREN) register for the SPI. More...
 
__STATIC_INLINE void DL_SPI_disablePower (SPI_Regs *spi)
 Disables the Peripheral Write Enable (PWREN) register for the SPI. More...
 
__STATIC_INLINE bool DL_SPI_isPowerEnabled (const SPI_Regs *spi)
 Returns if the Peripheral Write Enable (PWREN) register for the SPI is enabled. More...
 
__STATIC_INLINE void DL_SPI_reset (SPI_Regs *spi)
 Resets spi peripheral. More...
 
__STATIC_INLINE bool DL_SPI_isReset (const SPI_Regs *spi)
 Returns if spi peripheral was reset. More...
 
__STATIC_INLINE void DL_SPI_enable (SPI_Regs *spi)
 Enable the SPI peripheral. More...
 
__STATIC_INLINE bool DL_SPI_isEnabled (const SPI_Regs *spi)
 Checks if the SPI peripheral is enabled. More...
 
__STATIC_INLINE void DL_SPI_disable (SPI_Regs *spi)
 Disable the SPI peripheral. More...
 
void DL_SPI_setClockConfig (SPI_Regs *spi, const DL_SPI_ClockConfig *config)
 Configure SPI source clock. More...
 
void DL_SPI_getClockConfig (const SPI_Regs *spi, DL_SPI_ClockConfig *config)
 Get SPI source clock configuration. More...
 
__STATIC_INLINE bool DL_SPI_isBusy (const SPI_Regs *spi)
 Checks if the SPI is busy transmitting. More...
 
__STATIC_INLINE bool DL_SPI_isTXFIFOEmpty (const SPI_Regs *spi)
 Checks if the TX FIFO is empty. More...
 
__STATIC_INLINE bool DL_SPI_isTXFIFOFull (const SPI_Regs *spi)
 Checks if the TX FIFO is full. More...
 
__STATIC_INLINE bool DL_SPI_isRXFIFOEmpty (const SPI_Regs *spi)
 Checks if the RX FIFO is empty. More...
 
__STATIC_INLINE bool DL_SPI_isRXFIFOFull (const SPI_Regs *spi)
 Checks if the RX FIFO is full. More...
 
__STATIC_INLINE void DL_SPI_setParity (SPI_Regs *spi, DL_SPI_PARITY parity)
 Sets the parity configuration used for transactions. More...
 
__STATIC_INLINE DL_SPI_PARITY DL_SPI_getParity (const SPI_Regs *spi)
 Get the current receive and transmit parity configuration. More...
 
__STATIC_INLINE void DL_SPI_enableReceiveParity (SPI_Regs *spi)
 Enables receive parity. More...
 
__STATIC_INLINE void DL_SPI_disableReceiveParity (SPI_Regs *spi)
 Disables receive parity. More...
 
__STATIC_INLINE bool DL_SPI_isReceiveParityEnabled (const SPI_Regs *spi)
 Checks if receive parity is enabled. More...
 
__STATIC_INLINE void DL_SPI_enableTransmitParity (SPI_Regs *spi)
 Enables transmit parity. More...
 
__STATIC_INLINE void DL_SPI_disableTransmitParity (SPI_Regs *spi)
 Disables transmit parity. More...
 
__STATIC_INLINE bool DL_SPI_isTransmitParityEnabled (const SPI_Regs *spi)
 Checks if transmit parity is enabled. More...
 
__STATIC_INLINE void DL_SPI_setFrameFormat (SPI_Regs *spi, DL_SPI_FRAME_FORMAT frameFormat)
 Set the frame format to use. More...
 
__STATIC_INLINE DL_SPI_FRAME_FORMAT DL_SPI_getFrameFormat (const SPI_Regs *spi)
 Get the frame format configuration. More...
 
__STATIC_INLINE void DL_SPI_setDataSize (SPI_Regs *spi, DL_SPI_DATA_SIZE dataSize)
 Set the size for transfers. More...
 
__STATIC_INLINE DL_SPI_DATA_SIZE DL_SPI_getDataSize (const SPI_Regs *spi)
 Get the configured size for transfers. More...
 
__STATIC_INLINE void DL_SPI_setMode (SPI_Regs *spi, DL_SPI_MODE mode)
 Set whether the device should be in controller/peripheral mode. More...
 
__STATIC_INLINE DL_SPI_MODE DL_SPI_getMode (const SPI_Regs *spi)
 Get the current mode for the SPI (controller/peripheral) More...
 
__STATIC_INLINE void DL_SPI_setBitOrder (SPI_Regs *spi, DL_SPI_BIT_ORDER bitOrder)
 Set the bit order used for transfers. More...
 
__STATIC_INLINE DL_SPI_BIT_ORDER DL_SPI_getBitOrder (const SPI_Regs *spi)
 Get the current bit order used for transfers. More...
 
__STATIC_INLINE void DL_SPI_enableLoopbackMode (SPI_Regs *spi)
 Enables loopback mode. More...
 
__STATIC_INLINE void DL_SPI_disableLoopbackMode (SPI_Regs *spi)
 Disables loopback mode. More...
 
__STATIC_INLINE bool DL_SPI_isLoopbackModeEnabled (const SPI_Regs *spi)
 Checks if the loopback mode is enabled. More...
 
__STATIC_INLINE void DL_SPI_setRepeatTransmit (SPI_Regs *spi, uint32_t numRepeats)
 Set counter for repeated transmit. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRepeatTransmit (const SPI_Regs *spi)
 Get counter for repeated transmit. More...
 
__STATIC_INLINE void DL_SPI_enablePeripheralAlignDataOnChipSelect (SPI_Regs *spi)
 Enables data alignment on chip select for peripherals. More...
 
__STATIC_INLINE void DL_SPI_disablePeripheralAlignDataOnChipSelect (SPI_Regs *spi)
 Disables data alignment on chip select for peripherals. More...
 
__STATIC_INLINE bool DL_SPI_isPeripheralAlignDataOnChipSelectEnabled (const SPI_Regs *spi)
 Checks if data alignment on chip select for peripherals is enabled. More...
 
__STATIC_INLINE void DL_SPI_enablePacking (SPI_Regs *spi)
 Enables packing feature. More...
 
__STATIC_INLINE void DL_SPI_disablePacking (SPI_Regs *spi)
 Disables packing feature. More...
 
__STATIC_INLINE bool DL_SPI_isPackingEnabled (const SPI_Regs *spi)
 Checks if packing feature is enabled. More...
 
__STATIC_INLINE void DL_SPI_setChipSelect (SPI_Regs *spi, DL_SPI_CHIP_SELECT chipSelect)
 Set chip select used for controller or peripheral mode. More...
 
__STATIC_INLINE DL_SPI_CHIP_SELECT DL_SPI_getChipSelect (const SPI_Regs *spi)
 Get chip select used for controller or peripheral mode. More...
 
__STATIC_INLINE void DL_SPI_setPeripheralReceiveTimeout (SPI_Regs *spi, uint32_t timeout)
 Set peripheral receive timeout. More...
 
__STATIC_INLINE uint32_t DL_SPI_getPeripheralReceiveTimeout (const SPI_Regs *spi)
 Get peripheral receive timeout. More...
 
__STATIC_INLINE void DL_SPI_setControllerCommandDataModeConfig (SPI_Regs *spi, uint32_t config)
 Configure the command/data mode. More...
 
__STATIC_INLINE uint32_t DL_SPI_getControllerCommandDataModeConfig (const SPI_Regs *spi)
 Get the command/data mode configuration. More...
 
__STATIC_INLINE void DL_SPI_enableControllerCommandDataMode (SPI_Regs *spi)
 Enables command/data mode. More...
 
__STATIC_INLINE void DL_SPI_disableControllerCommandDataMode (SPI_Regs *spi)
 Disables command/data mode. More...
 
__STATIC_INLINE bool DL_SPI_isControllerCommandDataModeEnabled (const SPI_Regs *spi)
 Checks if command/data mode is enabled. More...
 
__STATIC_INLINE void DL_SPI_enablePeripheralDataOutput (SPI_Regs *spi)
 Enables peripheral data output. More...
 
__STATIC_INLINE void DL_SPI_disablePeripheralDataOutput (SPI_Regs *spi)
 Disables peripheral data output. More...
 
__STATIC_INLINE bool DL_SPI_isPeripheralDataOutputEnabled (const SPI_Regs *spi)
 Checks if peripheral data output is enabled. More...
 
__STATIC_INLINE void DL_SPI_setDelayedSampling (SPI_Regs *spi, uint32_t delay)
 Set the delay sampling. More...
 
__STATIC_INLINE uint32_t DL_SPI_getDelayedSampling (const SPI_Regs *spi)
 Get the delay sampling. More...
 
__STATIC_INLINE void DL_SPI_setFIFOThreshold (SPI_Regs *spi, DL_SPI_RX_FIFO_LEVEL rxThreshold, DL_SPI_TX_FIFO_LEVEL txThreshold)
 Set the RX and TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE DL_SPI_TX_FIFO_LEVEL DL_SPI_getTXFIFOThreshold (const SPI_Regs *spi)
 Get the TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE DL_SPI_RX_FIFO_LEVEL DL_SPI_getRXFIFOThreshold (const SPI_Regs *spi)
 Get the RX FIFO interrupt threshold level. More...
 
__STATIC_INLINE void DL_SPI_setBitRateSerialClockDivider (SPI_Regs *spi, uint32_t SCR)
 Set the SPI bit rate serial clock divider (SCR) More...
 
__STATIC_INLINE uint32_t DL_SPI_getBitRateSerialClockDivider (const SPI_Regs *spi)
 Get the SPI bit rate serial clock divider (SCR) More...
 
__STATIC_INLINE void DL_SPI_transmitData8 (SPI_Regs *spi, uint8_t data)
 Writes 8-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE void DL_SPI_transmitData16 (SPI_Regs *spi, uint16_t data)
 Writes 16-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE void DL_SPI_transmitData32 (SPI_Regs *spi, uint32_t data)
 Writes 32-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE uint8_t DL_SPI_receiveData8 (const SPI_Regs *spi)
 Reads 8-bit data from the RX FIFO. More...
 
__STATIC_INLINE uint16_t DL_SPI_receiveData16 (const SPI_Regs *spi)
 Reads 16-bit data from the RX FIFO. More...
 
__STATIC_INLINE uint32_t DL_SPI_receiveData32 (const SPI_Regs *spi)
 Reads 32-bit data from the RX FIFO. More...
 
__STATIC_INLINE void DL_SPI_enableInterrupt (SPI_Regs *spi, uint32_t interruptMask)
 Enable SPI interrupts. More...
 
__STATIC_INLINE void DL_SPI_disableInterrupt (SPI_Regs *spi, uint32_t interruptMask)
 Disable SPI interrupts. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledInterrupts (const SPI_Regs *spi, uint32_t interruptMask)
 Check which SPI interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledInterruptStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of enabled SPI interrupts. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawInterruptStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of any SPI interrupt. More...
 
__STATIC_INLINE DL_SPI_IIDX DL_SPI_getPendingInterrupt (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt. More...
 
__STATIC_INLINE void DL_SPI_clearInterruptStatus (SPI_Regs *spi, uint32_t interruptMask)
 Clear pending SPI interrupts. More...
 
void DL_SPI_transmitDataBlocking8 (SPI_Regs *spi, uint8_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
void DL_SPI_transmitDataBlocking16 (SPI_Regs *spi, uint16_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
void DL_SPI_transmitDataBlocking32 (SPI_Regs *spi, uint32_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
uint8_t DL_SPI_receiveDataBlocking8 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
uint16_t DL_SPI_receiveDataBlocking16 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
uint32_t DL_SPI_receiveDataBlocking32 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
bool DL_SPI_transmitDataCheck8 (SPI_Regs *spi, uint8_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_transmitDataCheck16 (SPI_Regs *spi, uint16_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_transmitDataCheck32 (SPI_Regs *spi, uint32_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck8 (const SPI_Regs *spi, uint8_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck16 (const SPI_Regs *spi, uint16_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck32 (const SPI_Regs *spi, uint32_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
uint32_t DL_SPI_drainRXFIFO8 (const SPI_Regs *spi, uint8_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 8 bit access. More...
 
uint32_t DL_SPI_drainRXFIFO16 (const SPI_Regs *spi, uint16_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 16 bit access. More...
 
uint32_t DL_SPI_drainRXFIFO32 (const SPI_Regs *spi, uint32_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 32 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO8 (SPI_Regs *spi, const uint8_t *buffer, uint32_t count)
 Fill the TX FIFO using 8 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO16 (SPI_Regs *spi, const uint16_t *buffer, uint32_t count)
 Fill the TX FIFO using 16 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO32 (SPI_Regs *spi, const uint32_t *buffer, uint32_t count)
 Fill the TX FIFO using 32 bit access. More...
 
__STATIC_INLINE void DL_SPI_enableDMAReceiveEvent (SPI_Regs *spi, uint32_t interrupt)
 Enable SPI interrupt for triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_enableDMATransmitEvent (SPI_Regs *spi)
 Enable SPI interrupt for triggering the DMA transmit event. More...
 
__STATIC_INLINE void DL_SPI_disableDMAReceiveEvent (SPI_Regs *spi, uint32_t interrupt)
 Disables SPI interrupt from triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_disableDMATransmitEvent (SPI_Regs *spi)
 Disables SPI interrupt from triggering the DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEvent (const SPI_Regs *spi, uint32_t interruptMask)
 Check which SPI interrupt for DMA receive events is enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEvent (const SPI_Regs *spi)
 Check if SPI interrupt for DMA transmit event is enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEventStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of enabled SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEventStatus (const SPI_Regs *spi)
 Check interrupt flag of enabled SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawDMAReceiveEventStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of any SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawDMATransmitEventStatus (const SPI_Regs *spi)
 Check interrupt flag of any SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE DL_SPI_DMA_IIDX_RX DL_SPI_getPendingDMAReceiveEvent (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE DL_SPI_DMA_IIDX_TX DL_SPI_getPendingDMATransmitEvent (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE void DL_SPI_clearDMAReceiveEventStatus (SPI_Regs *spi, uint32_t interruptMask)
 Clear pending SPI interrupts for DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_clearDMATransmitEventStatus (SPI_Regs *spi)
 Clear pending SPI interrupt for DMA transmit event. More...
 
bool DL_SPI_saveConfiguration (const SPI_Regs *spi, DL_SPI_backupConfig *ptr)
 Save SPI configuration before entering a power loss state. More...
 
bool DL_SPI_restoreConfiguration (SPI_Regs *spi, DL_SPI_backupConfig *ptr)
 Restore SPI configuration after leaving a power loss state. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale