MSPM0C110X Driver Library  2.08.00.03
Data Structures | Macros | Enumerations | Functions
dl_dma.h File Reference

Detailed Description

Direct Memory Access (DMA) Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_dma.h:

Go to the source code of this file.

Data Structures

struct  DL_DMA_Config
 Configuration struct for DL_DMA_initChannel. More...
 

Macros

#define DL_DMA_INTERRUPT_CHANNEL0   (DMA_CPU_INT_IMASK_DMACH0_SET)
 DMA channel 0 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL1   (DMA_CPU_INT_IMASK_DMACH1_SET)
 DMA channel 1 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL2   (DMA_CPU_INT_IMASK_DMACH2_SET)
 DMA channel 2 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL3   (DMA_CPU_INT_IMASK_DMACH3_SET)
 DMA channel 3 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL4   (DMA_CPU_INT_IMASK_DMACH4_SET)
 DMA channel 4 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL5   (DMA_CPU_INT_IMASK_DMACH5_SET)
 DMA channel 5 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL6   (DMA_CPU_INT_IMASK_DMACH6_SET)
 DMA channel 6 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL7   (DMA_CPU_INT_IMASK_DMACH7_SET)
 DMA channel 7 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL8   (DMA_CPU_INT_IMASK_DMACH8_SET)
 DMA channel 8 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL9   (DMA_CPU_INT_IMASK_DMACH9_SET)
 DMA channel 9 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL10   (DMA_CPU_INT_IMASK_DMACH10_SET)
 DMA channel 10 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL12   (DMA_CPU_INT_IMASK_DMACH12_SET)
 DMA channel 12 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL13   (DMA_CPU_INT_IMASK_DMACH13_SET)
 DMA channel 13 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL14   (DMA_CPU_INT_IMASK_DMACH14_SET)
 DMA channel 14 interrupt.
 
#define DL_DMA_INTERRUPT_CHANNEL15   (DMA_CPU_INT_IMASK_DMACH15_SET)
 DMA channel 15 interrupt.
 
#define DL_DMA_INTERRUPT_ADDR_ERROR   (DMA_CPU_INT_IMASK_ADDRERR_SET)
 DMA address error, source address not reachable.
 
#define DL_DMA_INTERRUPT_DATA_ERROR   (DMA_CPU_INT_IMASK_DATAERR_SET)
 DMA data error, source data might be corrupted (PAR or ECC error)
 
#define DL_DMA_EVENT_CHANNEL0   (DMA_GEN_EVENT_IMASK_DMACH0_SET)
 DMA channel 0 interrupt.
 
#define DL_DMA_EVENT_CHANNEL1   (DMA_GEN_EVENT_IMASK_DMACH1_SET)
 DMA channel 1 interrupt.
 
#define DL_DMA_EVENT_CHANNEL2   (DMA_GEN_EVENT_IMASK_DMACH2_SET)
 DMA channel 2 interrupt.
 
#define DL_DMA_EVENT_CHANNEL3   (DMA_GEN_EVENT_IMASK_DMACH3_SET)
 DMA channel 3 interrupt.
 
#define DL_DMA_EVENT_CHANNEL4   (DMA_GEN_EVENT_IMASK_DMACH4_SET)
 DMA channel 4 interrupt.
 
#define DL_DMA_EVENT_CHANNEL5   (DMA_GEN_EVENT_IMASK_DMACH5_SET)
 DMA channel 5 interrupt.
 
#define DL_DMA_EVENT_CHANNEL6   (DMA_GEN_EVENT_IMASK_DMACH6_SET)
 DMA channel 6 interrupt.
 
#define DL_DMA_EVENT_CHANNEL7   (DMA_GEN_EVENT_IMASK_DMACH7_SET)
 DMA channel 7 interrupt.
 
#define DL_DMA_EVENT_CHANNEL8   (DMA_GEN_EVENT_IMASK_DMACH8_SET)
 DMA channel 8 interrupt.
 
#define DL_DMA_EVENT_CHANNEL9   (DMA_GEN_EVENT_IMASK_DMACH9_SET)
 DMA channel 9 interrupt.
 
#define DL_DMA_EVENT_CHANNEL10   (DMA_GEN_EVENT_IMASK_DMACH10_SET)
 DMA channel 10 interrupt.
 
#define DL_DMA_EVENT_CHANNEL12   (DMA_GEN_EVENT_IMASK_DMACH12_SET)
 DMA channel 12 interrupt.
 
#define DL_DMA_EVENT_CHANNEL13   (DMA_GEN_EVENT_IMASK_DMACH13_SET)
 DMA channel 13 interrupt.
 
#define DL_DMA_EVENT_CHANNEL14   (DMA_GEN_EVENT_IMASK_DMACH14_SET)
 DMA channel 14 interrupt.
 
#define DL_DMA_EVENT_CHANNEL15   (DMA_GEN_EVENT_IMASK_DMACH15_SET)
 DMA channel 15 interrupt.
 
#define DL_DMA_EVENT_ADDR_ERROR   (DMA_GEN_EVENT_IMASK_ADDRERR_SET)
 DMA address error, source address not reachable.
 
#define DL_DMA_EVENT_DATA_ERROR   (DMA_GEN_EVENT_IMASK_DATAERR_SET)
 DMA data error, source data might be corrupted (PAR or ECC error)
 

Enumerations

enum  DL_DMA_TRANSFER_MODE {
  DL_DMA_SINGLE_TRANSFER_MODE = DMA_DMACTL_DMATM_SINGLE,
  DL_DMA_SINGLE_BLOCK_TRANSFER_MODE = DMA_DMACTL_DMATM_BLOCK
}
 
enum  DL_DMA_EXTENDED_MODE { DL_DMA_NORMAL_MODE = DMA_DMACTL_DMAEM_NORMAL }
 
enum  DL_DMA_INCREMENT {
  DL_DMA_ADDR_UNCHANGED = DMA_DMACTL_DMASRCINCR_UNCHANGED,
  DL_DMA_ADDR_DECREMENT = DMA_DMACTL_DMASRCINCR_DECREMENT,
  DL_DMA_ADDR_INCREMENT = DMA_DMACTL_DMASRCINCR_INCREMENT,
  DL_DMA_ADDR_STRIDE_2 = DMA_DMACTL_DMASRCINCR_STRIDE_2,
  DL_DMA_ADDR_STRIDE_3 = DMA_DMACTL_DMASRCINCR_STRIDE_3,
  DL_DMA_ADDR_STRIDE_4 = DMA_DMACTL_DMASRCINCR_STRIDE_4,
  DL_DMA_ADDR_STRIDE_5 = DMA_DMACTL_DMASRCINCR_STRIDE_5,
  DL_DMA_ADDR_STRIDE_6 = DMA_DMACTL_DMASRCINCR_STRIDE_6,
  DL_DMA_ADDR_STRIDE_7 = DMA_DMACTL_DMASRCINCR_STRIDE_7,
  DL_DMA_ADDR_STRIDE_8 = DMA_DMACTL_DMASRCINCR_STRIDE_8,
  DL_DMA_ADDR_STRIDE_9 = DMA_DMACTL_DMASRCINCR_STRIDE_9
}
 
enum  DL_DMA_EARLY_INTERRUPT_THRESHOLD {
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_DISABLED = DMA_DMACTL_DMAPREIRQ_PREIRQ_DISABLE,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_1 = DMA_DMACTL_DMAPREIRQ_PREIRQ_1,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_2 = DMA_DMACTL_DMAPREIRQ_PREIRQ_2,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_4 = DMA_DMACTL_DMAPREIRQ_PREIRQ_4,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_8 = DMA_DMACTL_DMAPREIRQ_PREIRQ_8,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_32 = DMA_DMACTL_DMAPREIRQ_PREIRQ_32,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_64 = DMA_DMACTL_DMAPREIRQ_PREIRQ_64,
  DL_DMA_EARLY_INTERRUPT_THRESHOLD_HALF = DMA_DMACTL_DMAPREIRQ_PREIRQ_HALF
}
 
enum  DL_DMA_BURST_SIZE {
  DL_DMA_BURST_SIZE_INFINITY = DMA_DMAPRIO_BURSTSZ_INFINITI,
  DL_DMA_BURST_SIZE_8 = DMA_DMAPRIO_BURSTSZ_BURST_8,
  DL_DMA_BURST_SIZE_16 = DMA_DMAPRIO_BURSTSZ_BUSRT_16,
  DL_DMA_BURST_SIZE_32 = DMA_DMAPRIO_BURSTSZ_BURST_32
}
 
enum  DL_DMA_TRIGGER_TYPE {
  DL_DMA_TRIGGER_TYPE_INTERNAL = DMA_DMATCTL_DMATINT_INTERNAL,
  DL_DMA_TRIGGER_TYPE_EXTERNAL = DMA_DMATCTL_DMATINT_EXTERNAL
}
 
enum  DL_DMA_WIDTH {
  DL_DMA_WIDTH_BYTE = DMA_DMACTL_DMASRCWDTH_BYTE,
  DL_DMA_WIDTH_HALF_WORD = DMA_DMACTL_DMASRCWDTH_HALF,
  DL_DMA_WIDTH_WORD = DMA_DMACTL_DMASRCWDTH_WORD,
  DL_DMA_WIDTH_LONG = DMA_DMACTL_DMASRCWDTH_LONG
}
 
enum  DL_DMA_EVENT_IIDX {
  DL_DMA_EVENT_IIDX_NO_INTR = DMA_GEN_EVENT_IIDX_STAT_NO_INTR,
  DL_DMA_EVENT_IIDX_DMACH0 = DMA_GEN_EVENT_IIDX_STAT_DMACH0,
  DL_DMA_EVENT_IIDX_DMACH1 = DMA_GEN_EVENT_IIDX_STAT_DMACH1,
  DL_DMA_EVENT_IIDX_DMACH2 = DMA_GEN_EVENT_IIDX_STAT_DMACH2,
  DL_DMA_EVENT_IIDX_DMACH3 = DMA_GEN_EVENT_IIDX_STAT_DMACH3,
  DL_DMA_EVENT_IIDX_DMACH4 = DMA_GEN_EVENT_IIDX_STAT_DMACH4,
  DL_DMA_EVENT_IIDX_DMACH5 = DMA_GEN_EVENT_IIDX_STAT_DMACH5,
  DL_DMA_EVENT_IIDX_DMACH6 = DMA_GEN_EVENT_IIDX_STAT_DMACH6,
  DL_DMA_EVENT_IIDX_DMACH7 = DMA_GEN_EVENT_IIDX_STAT_DMACH7,
  DL_DMA_EVENT_IIDX_DMACH8 = DMA_GEN_EVENT_IIDX_STAT_DMACH8,
  DL_DMA_EVENT_IIDX_DMACH9 = DMA_GEN_EVENT_IIDX_STAT_DMACH9,
  DL_DMA_EVENT_IIDX_DMACH10 = DMA_GEN_EVENT_IIDX_STAT_DMACH10,
  DL_DMA_EVENT_IIDX_DMACH11 = DMA_GEN_EVENT_IIDX_STAT_DMACH11,
  DL_DMA_EVENT_IIDX_DMACH12 = DMA_GEN_EVENT_IIDX_STAT_DMACH12,
  DL_DMA_EVENT_IIDX_DMACH13 = DMA_GEN_EVENT_IIDX_STAT_DMACH13,
  DL_DMA_EVENT_IIDX_DMACH14 = DMA_GEN_EVENT_IIDX_STAT_DMACH14,
  DL_DMA_EVENT_IIDX_DMACH15 = DMA_GEN_EVENT_IIDX_STAT_DMACH15,
  DL_DMA_EVENT_IIDX_ADDR_ERROR = DMA_GEN_EVENT_IIDX_STAT_ADDRERR,
  DL_DMA_EVENT_IIDX_DATA_ERROR = DMA_GEN_EVENT_IIDX_STAT_DATAERR
}
 
enum  DL_DMA_PUBLISHER_INDEX { DL_DMA_PUBLISHER_INDEX_0 = 0 }
 
enum  DL_DMA_SUBSCRIBER_INDEX {
  DL_DMA_SUBSCRIBER_INDEX_0 = 0,
  DL_DMA_SUBSCRIBER_INDEX_1 = 1
}
 
enum  DL_DMA_AUTOEN { DL_DMA_AUTOEN_DISABLE = DMA_DMACTL_DMAAUTOEN_DISABLE }
 

Functions

void DL_DMA_initChannel (DMA_Regs *dma, uint8_t channelNum, const DL_DMA_Config *config)
 Initialize a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_configTransfer (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode, DL_DMA_EXTENDED_MODE extendedMode, DL_DMA_WIDTH srcWidth, DL_DMA_WIDTH destWidth, DL_DMA_INCREMENT srcIncrement, DL_DMA_INCREMENT destIncrement)
 Configure a DMA channel for a transfer. More...
 
__STATIC_INLINE void DL_DMA_enableRoundRobinPriority (DMA_Regs *dma)
 Configure the DMA for round-robin priority. More...
 
__STATIC_INLINE void DL_DMA_disableRoundRobinPriority (DMA_Regs *dma)
 Disable round-robin priority for the DMA. More...
 
__STATIC_INLINE bool DL_DMA_isRoundRobinPriorityEnabled (const DMA_Regs *dma)
 Check if round-robin priority is enabled for the DMA. More...
 
__STATIC_INLINE void DL_DMA_setBurstSize (DMA_Regs *dma, DL_DMA_BURST_SIZE burstSize)
 Set the burst size for block transfers. More...
 
__STATIC_INLINE DL_DMA_BURST_SIZE DL_DMA_getBurstSize (const DMA_Regs *dma)
 Get the burst size for block transfers. More...
 
__STATIC_INLINE void DL_DMA_enableChannel (DMA_Regs *dma, uint8_t channelNum)
 Enable a DMA channel for transfers. More...
 
__STATIC_INLINE void DL_DMA_disableChannel (DMA_Regs *dma, uint8_t channelNum)
 Disable a DMA channel for transfers. More...
 
__STATIC_INLINE bool DL_DMA_isChannelEnabled (const DMA_Regs *dma, uint8_t channelNum)
 Check if a DMA channel is enabled for transfers. More...
 
__STATIC_INLINE void DL_DMA_configMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode, DL_DMA_EXTENDED_MODE extendedMode)
 Configure the mode for a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_setTransferMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_TRANSFER_MODE transferMode)
 Set a DMA channel's transfer mode. More...
 
__STATIC_INLINE DL_DMA_TRANSFER_MODE DL_DMA_getTransferMode (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's transfer mode. More...
 
__STATIC_INLINE void DL_DMA_setExtendedMode (DMA_Regs *dma, uint8_t channelNum, DL_DMA_EXTENDED_MODE extendedMode)
 Set a DMA channel's extended mode. More...
 
__STATIC_INLINE DL_DMA_EXTENDED_MODE DL_DMA_getExtendedMode (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's extended mode. More...
 
__STATIC_INLINE void DL_DMA_startTransfer (DMA_Regs *dma, uint8_t channelNum)
 Start a DMA transfer using software. More...
 
__STATIC_INLINE void DL_DMA_setTrigger (DMA_Regs *dma, uint8_t channelNum, uint8_t trigger, DL_DMA_TRIGGER_TYPE triggerType)
 Set a channel's trigger for a DMA transfer. More...
 
__STATIC_INLINE uint32_t DL_DMA_getTrigger (const DMA_Regs *dma, uint8_t channelNum)
 Get the current trigger for a DMA channel. More...
 
__STATIC_INLINE DL_DMA_TRIGGER_TYPE DL_DMA_getTriggerType (const DMA_Regs *dma, uint8_t channelNum)
 Get the current trigger type for a DMA channel. More...
 
__STATIC_INLINE void DL_DMA_setSrcAddr (DMA_Regs *dma, uint8_t channelNum, uint32_t srcAddr)
 Set a DMA channel's source address. More...
 
__STATIC_INLINE uint32_t DL_DMA_getSrcAddr (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's source address. More...
 
__STATIC_INLINE void DL_DMA_setDestAddr (DMA_Regs *dma, uint8_t channelNum, uint32_t destAddr)
 Set a DMA channel's destination address. More...
 
__STATIC_INLINE uint32_t DL_DMA_getDestAddr (const DMA_Regs *dma, uint8_t channelNum)
 Get a DMA channel's destination address. More...
 
__STATIC_INLINE void DL_DMA_setTransferSize (DMA_Regs *dma, uint8_t channelNum, uint16_t size)
 Set the size of a block for a DMA transfer. More...
 
__STATIC_INLINE uint16_t DL_DMA_getTransferSize (const DMA_Regs *dma, uint8_t channelNum)
 Get a channel's size of block of data for a DMA transfer. More...
 
__STATIC_INLINE void DL_DMA_setSrcIncrement (DMA_Regs *dma, uint8_t channelNum, DL_DMA_INCREMENT srcIncrement)
 Set a channel's source address increment amount. More...
 
__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getSrcIncrement (const DMA_Regs *dma, uint8_t channelNum)
 Return a channel's source address increment amount. More...
 
__STATIC_INLINE void DL_DMA_setDestIncrement (DMA_Regs *dma, uint8_t channelNum, DL_DMA_INCREMENT destIncrement)
 Set a channel's destination address increment amount. More...
 
__STATIC_INLINE DL_DMA_INCREMENT DL_DMA_getDestIncrement (const DMA_Regs *dma, uint8_t channelNum)
 Return a channel's destination address increment amount. More...
 
__STATIC_INLINE void DL_DMA_setSrcWidth (DMA_Regs *dma, uint8_t channelNum, DL_DMA_WIDTH srcWidth)
 Set the width of the DMA source address for a channel. More...
 
__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getSrcWidth (const DMA_Regs *dma, uint8_t channelNum)
 Get the width of the DMA source address for a channel. More...
 
__STATIC_INLINE void DL_DMA_setDestWidth (DMA_Regs *dma, uint8_t channelNum, DL_DMA_WIDTH destWidth)
 Set the width of the DMA destination address for a channel. More...
 
__STATIC_INLINE DL_DMA_WIDTH DL_DMA_getDestWidth (const DMA_Regs *dma, uint8_t channelNum)
 Get the width of the DMA destination address for a channel. More...
 
__STATIC_INLINE void DL_DMA_enableInterrupt (DMA_Regs *dma, uint32_t interruptMask)
 Enable DMA interrupts. More...
 
__STATIC_INLINE void DL_DMA_disableInterrupt (DMA_Regs *dma, uint32_t interruptMask)
 Disable DMA interrupts. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledInterrupts (const DMA_Regs *dma, uint32_t interruptMask)
 Check which DMA interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledInterruptStatus (const DMA_Regs *dma, uint32_t interruptMask)
 Check interrupt flag of enabled DMA interrupts. More...
 
__STATIC_INLINE uint32_t DL_DMA_getRawInterruptStatus (const DMA_Regs *dma, uint32_t interruptMask)
 Check interrupt flag of any DMA interrupt. More...
 
__STATIC_INLINE DL_DMA_EVENT_IIDX DL_DMA_getPendingInterrupt (const DMA_Regs *dma)
 Get highest priority pending DMA interrupt. More...
 
__STATIC_INLINE void DL_DMA_clearInterruptStatus (DMA_Regs *dma, uint32_t interruptMask)
 Clear pending DMA interrupts. More...
 
__STATIC_INLINE void DL_DMA_setPublisherChanID (DMA_Regs *dma, DL_DMA_PUBLISHER_INDEX index, uint8_t chanID)
 Sets the event publisher channel id. More...
 
__STATIC_INLINE uint8_t DL_DMA_getPublisherChanID (DMA_Regs *dma, DL_DMA_PUBLISHER_INDEX index)
 Gets the event publisher channel id. More...
 
__STATIC_INLINE void DL_DMA_setSubscriberChanID (DMA_Regs *dma, DL_DMA_SUBSCRIBER_INDEX index, uint8_t chanID)
 Sets the event subscriber channel id. More...
 
__STATIC_INLINE uint8_t DL_DMA_getSubscriberChanID (DMA_Regs *dma, DL_DMA_SUBSCRIBER_INDEX index)
 Gets the event subscriber channel id. More...
 
__STATIC_INLINE void DL_DMA_enableEvent (DMA_Regs *dma, uint32_t eventMask)
 Enable DMA event. More...
 
__STATIC_INLINE void DL_DMA_disableEvent (DMA_Regs *dma, uint32_t eventMask)
 Disable DMA event. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledEvents (const DMA_Regs *dma, uint32_t eventMask)
 Check which dma events triggers are enabled. More...
 
__STATIC_INLINE uint32_t DL_DMA_getEnabledEventStatus (const DMA_Regs *dma, uint32_t eventMask)
 Check event flag of enabled dma event. More...
 
__STATIC_INLINE uint32_t DL_DMA_getRawEventsStatus (const DMA_Regs *dma, uint32_t eventMask)
 Check event flag of any dma event. More...
 
__STATIC_INLINE void DL_DMA_clearEventsStatus (DMA_Regs *dma, uint32_t eventMask)
 Clear pending dma events. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale