MSPM0C110X Driver Library  2.08.00.03
Enumerations | Functions
dl_crc.h File Reference

Detailed Description

Cyclic Redundancy Check (CRC) Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_crc.h:

Go to the source code of this file.

Enumerations

enum  DL_CRC_POLYNOMIAL { DL_CRC_16_POLYNOMIAL = CRC_CRCCTRL_POLYSIZE_CRC16 }
 
enum  DL_CRC_BIT {
  DL_CRC_BIT_REVERSED = CRC_CRCCTRL_BITREVERSE_REVERSED,
  DL_CRC_BIT_NOT_REVERSED = CRC_CRCCTRL_BITREVERSE_NOT_REVERSED
}
 
enum  DL_CRC_INPUT_ENDIANESS {
  DL_CRC_INPUT_ENDIANESS_LITTLE_ENDIAN,
  DL_CRC_INPUT_ENDIANESS_BIG_ENDIAN = CRC_CRCCTRL_INPUT_ENDIANNESS_BIG_ENDIAN
}
 
enum  DL_CRC_OUTPUT_BYTESWAP {
  DL_CRC_OUTPUT_BYTESWAP_ENABLED = CRC_CRCCTRL_OUTPUT_BYTESWAP_ENABLE,
  DL_CRC_OUTPUT_BYTESWAP_DISABLED = CRC_CRCCTRL_OUTPUT_BYTESWAP_DISABLE
}
 

Functions

__STATIC_INLINE void DL_CRC_enablePower (CRC_Regs *crc)
 Enables the Peripheral Write Enable (PWREN) register for the CRC. More...
 
__STATIC_INLINE void DL_CRC_disablePower (CRC_Regs *crc)
 Disables the Peripheral Write Enable (PWREN) register for the CRC. More...
 
__STATIC_INLINE bool DL_CRC_isPowerEnabled (const CRC_Regs *crc)
 Returns if the Peripheral Write Enable (PWREN) register for the CRC is enabled. More...
 
__STATIC_INLINE void DL_CRC_reset (CRC_Regs *crc)
 Resets crc peripheral. More...
 
__STATIC_INLINE bool DL_CRC_isReset (const CRC_Regs *crc)
 Returns if crc module has been reset. More...
 
__STATIC_INLINE void DL_CRC_init (CRC_Regs *crc, DL_CRC_POLYNOMIAL poly, DL_CRC_BIT bitOrd, DL_CRC_INPUT_ENDIANESS inEndianness, DL_CRC_OUTPUT_BYTESWAP outByteSwap)
 Initializes CRC. More...
 
__STATIC_INLINE void DL_CRC_setSeed16 (CRC_Regs *crc, uint16_t seed)
 Initializes the seed for a 16-bit polynomial CRC calculation. More...
 
__STATIC_INLINE void DL_CRC_setSeed32 (CRC_Regs *crc, uint32_t seed)
 Initializes the seed for a 32-bit polynomial CRC calculation. More...
 
__STATIC_INLINE void DL_CRC_feedData8 (CRC_Regs *crc, uint8_t dataIn)
 Feeds 8-bit data into the CRC calculation. More...
 
__STATIC_INLINE void DL_CRC_feedData16 (CRC_Regs *crc, uint16_t dataIn)
 Feeds 16-bit data into the CRC calculation. More...
 
__STATIC_INLINE void DL_CRC_feedData32 (CRC_Regs *crc, uint32_t dataIn)
 Feeds 32-bit data into the CRC calculation. More...
 
__STATIC_INLINE uint16_t DL_CRC_getResult16 (const CRC_Regs *crc)
 Returns the result from the 16-bit polynomial calculation. More...
 
__STATIC_INLINE uint32_t DL_CRC_getResult32 (const CRC_Regs *crc)
 Returns the result from the 32-bit polynomial calculation. More...
 
uint32_t DL_CRC_calculateBlock32 (CRC_Regs *crc, uint32_t seed, const uint32_t *ptr, uint32_t size)
 Calculates the CRC over a range of 32-bit values. More...
 
uint32_t DL_CRC_calculateMemoryRange32 (CRC_Regs *crc, uint32_t seed, uint32_t *ptrStart, const uint32_t *ptrEnd)
 Calculates the CRC over a memory range. More...
 
uint16_t DL_CRC_calculateBlock16 (CRC_Regs *crc, uint16_t seed, const uint16_t *ptr, uint16_t size)
 Calculates the CRC over a range of 16-bit values. More...
 
uint16_t DL_CRC_calculateMemoryRange16 (CRC_Regs *crc, uint16_t seed, uint16_t *ptrStart, const uint16_t *ptrEnd)
 Calculates the CRC over a memory range. More...
 
__STATIC_INLINE uintptr_t DL_CRC_getCRCINAddr (const CRC_Regs *crc)
 Returns the address of the CRC input data register. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale