MSPM0C110X Driver Library  2.08.00.03
Data Structures | Macros | Enumerations | Functions
dl_adc12.h File Reference

Detailed Description

Analog to Digital Converter (ADC)


#include <math.h>
#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
#include <ti/driverlib/m0p/dl_factoryregion.h>
Include dependency graph for dl_adc12.h:

Go to the source code of this file.

Data Structures

struct  DL_ADC12_ClockConfig
 Configuration struct for DL_ADC12_setClockConfig. More...
 

Macros

#define DL_ADC12_SEQ_END_ADDR_00   (ADC12_CTL2_ENDADD_ADDR_00)
 Sequence end address set to 00.
 
#define DL_ADC12_SEQ_END_ADDR_01   (ADC12_CTL2_ENDADD_ADDR_01)
 Sequence end address set to 01.
 
#define DL_ADC12_SEQ_END_ADDR_02   (ADC12_CTL2_ENDADD_ADDR_02)
 Sequence end address set to 02.
 
#define DL_ADC12_SEQ_END_ADDR_03   (ADC12_CTL2_ENDADD_ADDR_03)
 Sequence end address set to 03.
 
#define DL_ADC12_SEQ_END_ADDR_04   (ADC12_CTL2_ENDADD_ADDR_04)
 Sequence end address set to 04.
 
#define DL_ADC12_SEQ_END_ADDR_05   (ADC12_CTL2_ENDADD_ADDR_05)
 Sequence end address set to 05.
 
#define DL_ADC12_SEQ_END_ADDR_06   (ADC12_CTL2_ENDADD_ADDR_06)
 Sequence end address set to 06.
 
#define DL_ADC12_SEQ_END_ADDR_07   (ADC12_CTL2_ENDADD_ADDR_07)
 Sequence end address set to 07.
 
#define DL_ADC12_SEQ_END_ADDR_08   (ADC12_CTL2_ENDADD_ADDR_08)
 Sequence end address set to 08.
 
#define DL_ADC12_SEQ_END_ADDR_09   (ADC12_CTL2_ENDADD_ADDR_09)
 Sequence end address set to 09.
 
#define DL_ADC12_SEQ_END_ADDR_10   (ADC12_CTL2_ENDADD_ADDR_10)
 Sequence end address set to 10.
 
#define DL_ADC12_SEQ_END_ADDR_11   (ADC12_CTL2_ENDADD_ADDR_11)
 Sequence end address set to 11.
 
#define DL_ADC12_SEQ_START_ADDR_00   (ADC12_CTL2_STARTADD_ADDR_00)
 Sequence start address set to 00.
 
#define DL_ADC12_SEQ_START_ADDR_01   (ADC12_CTL2_STARTADD_ADDR_01)
 Sequence start address set to 01.
 
#define DL_ADC12_SEQ_START_ADDR_02   (ADC12_CTL2_STARTADD_ADDR_02)
 Sequence start address set to 02.
 
#define DL_ADC12_SEQ_START_ADDR_03   (ADC12_CTL2_STARTADD_ADDR_03)
 Sequence start address set to 03.
 
#define DL_ADC12_SEQ_START_ADDR_04   (ADC12_CTL2_STARTADD_ADDR_04)
 Sequence start address set to 04.
 
#define DL_ADC12_SEQ_START_ADDR_05   (ADC12_CTL2_STARTADD_ADDR_05)
 Sequence start address set to 05.
 
#define DL_ADC12_SEQ_START_ADDR_06   (ADC12_CTL2_STARTADD_ADDR_06)
 Sequence start address set to 06.
 
#define DL_ADC12_SEQ_START_ADDR_07   (ADC12_CTL2_STARTADD_ADDR_07)
 Sequence start address set to 07.
 
#define DL_ADC12_SEQ_START_ADDR_08   (ADC12_CTL2_STARTADD_ADDR_08)
 Sequence start address set to 08.
 
#define DL_ADC12_SEQ_START_ADDR_09   (ADC12_CTL2_STARTADD_ADDR_09)
 Sequence start address set to 09.
 
#define DL_ADC12_SEQ_START_ADDR_10   (ADC12_CTL2_STARTADD_ADDR_10)
 Sequence start address set to 10.
 
#define DL_ADC12_SEQ_START_ADDR_11   (ADC12_CTL2_STARTADD_ADDR_11)
 Sequence start address set to 11.
 
#define DL_ADC12_SAMP_MODE_SINGLE   (ADC12_CTL1_CONSEQ_SINGLE)
 Single sample mode selected.
 
#define DL_ADC12_SAMP_MODE_SINGLE_REPEAT   (ADC12_CTL1_CONSEQ_REPEATSINGLE)
 Repeat single sample mode selected.
 
#define DL_ADC12_SAMP_MODE_SEQUENCE   (ADC12_CTL1_CONSEQ_SEQUENCE)
 Sequence sample mode selected.
 
#define DL_ADC12_SAMP_MODE_SEQUENCE_REPEAT   (ADC12_CTL1_CONSEQ_REPEATSEQUENCE)
 Repeat sequence sample mode selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_DISABLED   (ADC12_CTL1_AVGN_DISABLE)
 Doesn't accumulate conversions.
 
#define DL_ADC12_HW_AVG_NUM_ACC_2   (ADC12_CTL1_AVGN_AVG_2)
 Accumulates 2 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_4   (ADC12_CTL1_AVGN_AVG_4)
 Accumulates 4 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_8   (ADC12_CTL1_AVGN_AVG_8)
 Accumulates 8 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_16   (ADC12_CTL1_AVGN_AVG_16)
 Accumulates 16 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_32   (ADC12_CTL1_AVGN_AVG_32)
 Accumulates 32 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_64   (ADC12_CTL1_AVGN_AVG_64)
 Accumulates 64 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_NUM_ACC_128   (ADC12_CTL1_AVGN_AVG_128)
 Accumulates 128 conversions and then is divided by the denominator selected.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_1   (ADC12_CTL1_AVGD_SHIFT0)
 Accumulated conversions are divided by 1.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_2   (ADC12_CTL1_AVGD_SHIFT1)
 Accumulated conversions are divided by 2.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_4   (ADC12_CTL1_AVGD_SHIFT2)
 Accumulated conversions are divided by 4.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_8   (ADC12_CTL1_AVGD_SHIFT3)
 Accumulated conversions are divided by 8.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_16   (ADC12_CTL1_AVGD_SHIFT4)
 Accumulated conversions are divided by 16.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_32   (ADC12_CTL1_AVGD_SHIFT5)
 Accumulated conversions are divided by 32.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_64   (ADC12_CTL1_AVGD_SHIFT6)
 Accumulated conversions are divided by 64.
 
#define DL_ADC12_HW_AVG_DEN_DIV_BY_128   (ADC12_CTL1_AVGD_SHIFT7)
 Accumulated conversions are divided by 128.
 
#define DL_ADC12_POWER_DOWN_MODE_AUTO   (ADC12_CTL0_PWRDN_AUTO)
 ADC12 power down mode auto.
 
#define DL_ADC12_POWER_DOWN_MODE_MANUAL   (ADC12_CTL0_PWRDN_MANUAL)
 ADC12 power down mode manual.
 
#define DL_ADC12_INPUT_CHAN_0   (ADC12_MEMCTL_CHANSEL_CHAN_0)
 ADC12 input channel 0 selected.
 
#define DL_ADC12_INPUT_CHAN_1   (ADC12_MEMCTL_CHANSEL_CHAN_1)
 ADC12 input channel 1 selected.
 
#define DL_ADC12_INPUT_CHAN_2   (ADC12_MEMCTL_CHANSEL_CHAN_2)
 ADC12 input channel 2 selected.
 
#define DL_ADC12_INPUT_CHAN_3   (ADC12_MEMCTL_CHANSEL_CHAN_3)
 ADC12 input channel 3 selected.
 
#define DL_ADC12_INPUT_CHAN_4   (ADC12_MEMCTL_CHANSEL_CHAN_4)
 ADC12 input channel 4 selected.
 
#define DL_ADC12_INPUT_CHAN_5   (ADC12_MEMCTL_CHANSEL_CHAN_5)
 ADC12 input channel 5 selected.
 
#define DL_ADC12_INPUT_CHAN_6   (ADC12_MEMCTL_CHANSEL_CHAN_6)
 ADC12 input channel 6 selected.
 
#define DL_ADC12_INPUT_CHAN_7   (ADC12_MEMCTL_CHANSEL_CHAN_7)
 ADC12 input channel 7 selected.
 
#define DL_ADC12_INPUT_CHAN_8   (ADC12_MEMCTL_CHANSEL_CHAN_8)
 ADC12 input channel 8 selected.
 
#define DL_ADC12_INPUT_CHAN_9   (ADC12_MEMCTL_CHANSEL_CHAN_9)
 ADC12 input channel 9 selected.
 
#define DL_ADC12_INPUT_CHAN_10   (ADC12_MEMCTL_CHANSEL_CHAN_10)
 ADC12 input channel 10 selected.
 
#define DL_ADC12_INPUT_CHAN_11   (ADC12_MEMCTL_CHANSEL_CHAN_11)
 ADC12 input channel 11 selected.
 
#define DL_ADC12_INPUT_CHAN_12   (ADC12_MEMCTL_CHANSEL_CHAN_12)
 ADC12 input channel 12 selected.
 
#define DL_ADC12_INPUT_CHAN_13   (ADC12_MEMCTL_CHANSEL_CHAN_13)
 ADC12 input channel 13 selected.
 
#define DL_ADC12_INPUT_CHAN_14   (ADC12_MEMCTL_CHANSEL_CHAN_14)
 ADC12 input channel 14 selected.
 
#define DL_ADC12_INPUT_CHAN_15   (ADC12_MEMCTL_CHANSEL_CHAN_15)
 ADC12 input channel 15 selected.
 
#define DL_ADC12_REFERENCE_VOLTAGE_VDDA   (ADC12_MEMCTL_VRSEL_VDDA_VSSA)
 ADC12 voltage reference VDDA.
 
#define DL_ADC12_REFERENCE_VOLTAGE_EXTREF   (ADC12_MEMCTL_VRSEL_EXTREF_VREFM)
 ADC12 voltage reference external.
 
#define DL_ADC12_REFERENCE_VOLTAGE_INTREF   (ADC12_MEMCTL_VRSEL_INTREF_VSSA)
 ADC12 voltage reference internal.
 
#define DL_ADC12_REFERENCE_VOLTAGE_VDDA_VSSA   (ADC12_MEMCTL_VRSEL_VDDA_VSSA)
 ADC12 voltage reference VDDA.
 
#define DL_ADC12_REFERENCE_VOLTAGE_EXTREF_VREFM   (ADC12_MEMCTL_VRSEL_EXTREF_VREFM)
 ADC12 voltage reference external.
 
#define DL_ADC12_REFERENCE_VOLTAGE_INTREF_VSSA   (ADC12_MEMCTL_VRSEL_INTREF_VSSA)
 ADC12 voltage reference internal.
 
#define DL_ADC12_REFERENCE_VOLTAGE_VDDA_VREFM   (ADC12_MEMCTL_VRSEL_VDDA_VREFM)
 ADC12 voltage reference VDDA and VREFM connected to VREF+.
 
#define DL_ADC12_REFERENCE_VOLTAGE_INTREF_VREFM   (ADC12_MEMCTL_VRSEL_INTREF_VREFM)
 ADC12 voltage reference INTREF and VREFM connected to VREF+ and VREF-.
 
#define DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0   (ADC12_MEMCTL_STIME_SEL_SCOMP0)
 ADC12 sample adc12 source 0.
 
#define DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP1   (ADC12_MEMCTL_STIME_SEL_SCOMP1)
 ADC12 sample adc12 source 1.
 
#define DL_ADC12_AVERAGING_MODE_ENABLED   (ADC12_MEMCTL_AVGEN_ENABLE)
 ADC12 averaging mode enabled.
 
#define DL_ADC12_AVERAGING_MODE_DISABLED   (ADC12_MEMCTL_AVGEN_DISABLE)
 ADC12 averaging mode disabled.
 
#define DL_ADC12_BURN_OUT_SOURCE_ENABLED   (ADC12_MEMCTL_BCSEN_ENABLE)
 ADC12 burn out current source enabled.
 
#define DL_ADC12_BURN_OUT_SOURCE_DISABLED   (ADC12_MEMCTL_BCSEN_DISABLE)
 ADC12 burn out current source disabled.
 
#define DL_ADC12_TRIGGER_MODE_AUTO_NEXT   (ADC12_MEMCTL_TRIG_AUTO_NEXT)
 ADC12 trigger automatically step to next memory conversion register.
 
#define DL_ADC12_TRIGGER_MODE_TRIGGER_NEXT   (ADC12_MEMCTL_TRIG_TRIGGER_NEXT)
 ADC12 valid trigger will step to next memory conversion register.
 
#define DL_ADC12_WINDOWS_COMP_MODE_ENABLED   (ADC12_MEMCTL_WINCOMP_ENABLE)
 ADC12 window comparator enabled.
 
#define DL_ADC12_WINDOWS_COMP_MODE_DISABLED   (ADC12_MEMCTL_WINCOMP_DISABLE)
 ADC12 window comparator disabled.
 
#define DL_ADC12_STATUS_CONVERSION_ACTIVE   (ADC12_STATUS_BUSY_ACTIVE)
 Indicates sample or conversion is in progress.
 
#define DL_ADC12_STATUS_CONVERSION_IDLE   (ADC12_STATUS_BUSY_IDLE)
 Indicates sample or conversion is not in progress.
 
#define DL_ADC12_STATUS_REFERENCE_READY   (ADC12_STATUS_REFBUFRDY_READY)
 Indicates reference buffer is powered up and ready.
 
#define DL_ADC12_STATUS_REFERENCE_NOTREADY   (ADC12_STATUS_REFBUFRDY_NOTREADY)
 Indicates reference buffer is not ready.
 
#define DL_ADC12_INTERRUPT_OVERFLOW   (ADC12_CPU_INT_IMASK_OVIFG_SET)
 ADC12 MEMRESX overflow.
 
#define DL_ADC12_INTERRUPT_TRIG_OVF   (ADC12_CPU_INT_IMASK_TOVIFG_SET)
 ADC12 sequence conversion trigger overflow.
 
#define DL_ADC12_INTERRUPT_WINDOW_COMP_HIGH   (ADC12_CPU_INT_IMASK_HIGHIFG_SET)
 ADC12 MEMRESx result higher than window comparator high threshold.
 
#define DL_ADC12_INTERRUPT_WINDOW_COMP_LOW   (ADC12_CPU_INT_IMASK_LOWIFG_SET)
 ADC12 MEMRESx result lower than window comparator low threshold.
 
#define DL_ADC12_INTERRUPT_INIFG   (ADC12_CPU_INT_IMASK_INIFG_SET)
 ADC12 MEMRESx result is between low and high window comparator threshold.
 
#define DL_ADC12_INTERRUPT_DMA_DONE   (ADC12_CPU_INT_IMASK_DMADONE_SET)
 ADC12 DMA done.
 
#define DL_ADC12_INTERRUPT_UNDERFLOW   (ADC12_CPU_INT_IMASK_UVIFG_SET)
 ADC12 MEMRESX underflow.
 
#define DL_ADC12_INTERRUPT_MEM0_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG0_SET)
 ADC12 MEM0 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM1_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG1_SET)
 ADC12 MEM1 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM2_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG2_SET)
 ADC12 MEM2 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM3_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG3_SET)
 ADC12 MEM3 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM4_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG4_SET)
 ADC12 MEM4 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM5_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG5_SET)
 ADC12 MEM5 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM6_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG6_SET)
 ADC12 MEM6 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM7_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG7_SET)
 ADC12 MEM7 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM8_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG8_SET)
 ADC12 MEM8 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM9_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG9_SET)
 ADC12 MEM9 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM10_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG10_SET)
 ADC12 MEM10 result loaded interrupt.
 
#define DL_ADC12_INTERRUPT_MEM11_RESULT_LOADED   (ADC12_CPU_INT_IMASK_MEMRESIFG11_SET)
 ADC12 MEM12 result loaded interrupt.
 
#define DL_ADC12_EVENT_WINDOW_COMP_HIGH   (ADC12_GEN_EVENT_IMASK_HIGHIFG_SET)
 ADC12 MEMRESx result higher than window comparator high threshold.
 
#define DL_ADC12_EVENT_WINDOW_COMP_LOW   (ADC12_GEN_EVENT_IMASK_LOWIFG_SET)
 ADC12 MEMRESx result lower than window comparator low threshold.
 
#define DL_ADC12_EVENT_INIFG   (ADC12_GEN_EVENT_IMASK_INIFG_SET)
 ADC12 MEMRESx result between high and low window comparator threshold.
 
#define DL_ADC12_EVENT_MEM0_RESULT_LOADED   (ADC12_GEN_EVENT_IMASK_MEMRESIFG0_SET)
 ADC12 MEM0 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM0_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG0_SET)
 ADC12 MEM0 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM1_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG1_SET)
 ADC12 MEM1 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM2_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG2_SET)
 ADC12 MEM2 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM3_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG3_SET)
 ADC12 MEM3 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM4_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG4_SET)
 ADC12 MEM4 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM5_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG5_SET)
 ADC12 MEM5 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM6_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG6_SET)
 ADC12 MEM6 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM7_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG7_SET)
 ADC12 MEM7 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM8_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG8_SET)
 ADC12 MEM8 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM9_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG9_SET)
 ADC12 MEM9 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM10_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG10_SET)
 ADC12 MEM10 result loaded interrupt.
 
#define DL_ADC12_DMA_MEM11_RESULT_LOADED   (ADC12_DMA_TRIG_IMASK_MEMRESIFG11_SET)
 ADC12 MEM11 result loaded interrupt.
 
#define DL_ADC12_SVT_OFFSET   ((uint32_t)0x555000 >> (uint32_t)2)
 This is an internal macro is used to resolve the offset to ADC12 SVT. More...
 

Enumerations

enum  DL_ADC12_MEM_IDX {
  DL_ADC12_MEM_IDX_0 = 0,
  DL_ADC12_MEM_IDX_1 = 1,
  DL_ADC12_MEM_IDX_2 = 2,
  DL_ADC12_MEM_IDX_3 = 3,
  DL_ADC12_MEM_IDX_4 = 4,
  DL_ADC12_MEM_IDX_5 = 5,
  DL_ADC12_MEM_IDX_6 = 6,
  DL_ADC12_MEM_IDX_7 = 7,
  DL_ADC12_MEM_IDX_8 = 8,
  DL_ADC12_MEM_IDX_9 = 9,
  DL_ADC12_MEM_IDX_10 = 10,
  DL_ADC12_MEM_IDX_11 = 11
}
 
enum  DL_ADC12_REPEAT_MODE {
  DL_ADC12_REPEAT_MODE_ENABLED = ADC12_CTL1_CONSEQ_REPEATSINGLE,
  DL_ADC12_REPEAT_MODE_DISABLED = ADC12_CTL1_CONSEQ_SINGLE
}
 
enum  DL_ADC12_SAMPLING_SOURCE {
  DL_ADC12_SAMPLING_SOURCE_AUTO = ADC12_CTL1_SAMPMODE_AUTO,
  DL_ADC12_SAMPLING_SOURCE_MANUAL = ADC12_CTL1_SAMPMODE_MANUAL
}
 
enum  DL_ADC12_TRIG_SRC {
  DL_ADC12_TRIG_SRC_SOFTWARE = ADC12_CTL1_TRIGSRC_SOFTWARE,
  DL_ADC12_TRIG_SRC_EVENT = ADC12_CTL1_TRIGSRC_EVENT
}
 
enum  DL_ADC12_SAMP_CONV_RES {
  DL_ADC12_SAMP_CONV_RES_12_BIT = ADC12_CTL2_RES_BIT_12,
  DL_ADC12_SAMP_CONV_RES_10_BIT = ADC12_CTL2_RES_BIT_10,
  DL_ADC12_SAMP_CONV_RES_8_BIT = ADC12_CTL2_RES_BIT_8
}
 
enum  DL_ADC12_SAMP_CONV_DATA_FORMAT {
  DL_ADC12_SAMP_CONV_DATA_FORMAT_UNSIGNED = ADC12_CTL2_DF_UNSIGNED,
  DL_ADC12_SAMP_CONV_DATA_FORMAT_SIGNED = ADC12_CTL2_DF_SIGNED
}
 
enum  DL_ADC12_IIDX {
  DL_ADC12_IIDX_OVERFLOW = ADC12_CPU_INT_IIDX_STAT_OVIFG,
  DL_ADC12_IIDX_TRIG_OVERFLOW = ADC12_CPU_INT_IIDX_STAT_TOVIFG,
  DL_ADC12_IIDX_WINDOW_COMP_HIGH = ADC12_CPU_INT_IIDX_STAT_HIGHIFG,
  DL_ADC12_IIDX_WINDOW_COMP_LOW = ADC12_CPU_INT_IIDX_STAT_LOWIFG,
  DL_ADC12_IIDX_INIFG = ADC12_CPU_INT_IIDX_STAT_INIFG,
  DL_ADC12_IIDX_DMA_DONE = ADC12_CPU_INT_IIDX_STAT_DMADONE,
  DL_ADC12_IIDX_UNDERFLOW = ADC12_CPU_INT_IIDX_STAT_UVIFG,
  DL_ADC12_IIDX_MEM0_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG0,
  DL_ADC12_IIDX_MEM1_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG1,
  DL_ADC12_IIDX_MEM2_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG2,
  DL_ADC12_IIDX_MEM3_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG3,
  DL_ADC12_IIDX_MEM4_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG4,
  DL_ADC12_IIDX_MEM5_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG5,
  DL_ADC12_IIDX_MEM6_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG6,
  DL_ADC12_IIDX_MEM7_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG7,
  DL_ADC12_IIDX_MEM8_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG8,
  DL_ADC12_IIDX_MEM9_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG9,
  DL_ADC12_IIDX_MEM10_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG10,
  DL_ADC12_IIDX_MEM11_RESULT_LOADED = ADC12_CPU_INT_IIDX_STAT_MEMRESIFG11
}
 
enum  DL_ADC12_CLOCK {
  DL_ADC12_CLOCK_SYSOSC = ADC12_CLKCFG_SAMPCLK_SYSOSC,
  DL_ADC12_CLOCK_ULPCLK = ADC12_CLKCFG_SAMPCLK_ULPCLK,
  DL_ADC12_CLOCK_HFCLK = ADC12_CLKCFG_SAMPCLK_HFCLK
}
 
enum  DL_ADC12_CLOCK_DIVIDE {
  DL_ADC12_CLOCK_DIVIDE_1 = ADC12_CTL0_SCLKDIV_DIV_BY_1,
  DL_ADC12_CLOCK_DIVIDE_2 = ADC12_CTL0_SCLKDIV_DIV_BY_2,
  DL_ADC12_CLOCK_DIVIDE_4 = ADC12_CTL0_SCLKDIV_DIV_BY_4,
  DL_ADC12_CLOCK_DIVIDE_8 = ADC12_CTL0_SCLKDIV_DIV_BY_8,
  DL_ADC12_CLOCK_DIVIDE_16 = ADC12_CTL0_SCLKDIV_DIV_BY_16,
  DL_ADC12_CLOCK_DIVIDE_24 = ADC12_CTL0_SCLKDIV_DIV_BY_24,
  DL_ADC12_CLOCK_DIVIDE_32 = ADC12_CTL0_SCLKDIV_DIV_BY_32,
  DL_ADC12_CLOCK_DIVIDE_48 = ADC12_CTL0_SCLKDIV_DIV_BY_48
}
 
enum  DL_ADC12_CLOCK_FREQ_RANGE {
  DL_ADC12_CLOCK_FREQ_RANGE_1_TO_4 = ADC12_CLKFREQ_FRANGE_RANGE1TO4,
  DL_ADC12_CLOCK_FREQ_RANGE_4_TO_8 = ADC12_CLKFREQ_FRANGE_RANGE4TO8,
  DL_ADC12_CLOCK_FREQ_RANGE_8_TO_16 = ADC12_CLKFREQ_FRANGE_RANGE8TO16,
  DL_ADC12_CLOCK_FREQ_RANGE_16_TO_20 = ADC12_CLKFREQ_FRANGE_RANGE16TO20,
  DL_ADC12_CLOCK_FREQ_RANGE_20_TO_24 = ADC12_CLKFREQ_FRANGE_RANGE20TO24,
  DL_ADC12_CLOCK_FREQ_RANGE_24_TO_32 = ADC12_CLKFREQ_FRANGE_RANGE24TO32,
  DL_ADC12_CLOCK_FREQ_RANGE_32_TO_40 = ADC12_CLKFREQ_FRANGE_RANGE32TO40,
  DL_ADC12_CLOCK_FREQ_RANGE_40_TO_48 = ADC12_CLKFREQ_FRANGE_RANGE40TO48
}
 

Functions

__STATIC_INLINE void DL_ADC12_enablePower (ADC12_Regs *adc12)
 Enables the Peripheral Write Enable (PWREN) register for the ADC12. More...
 
__STATIC_INLINE void DL_ADC12_disablePower (ADC12_Regs *adc12)
 Disables the Peripheral Write Enable (PWREN) register for the ADC12. More...
 
__STATIC_INLINE bool DL_ADC12_isPowerEnabled (const ADC12_Regs *adc12)
 Returns if the Peripheral Write Enable (PWREN) register for the ADC12 is enabled. More...
 
__STATIC_INLINE void DL_ADC12_reset (ADC12_Regs *adc12)
 Resets adc12 peripheral. More...
 
__STATIC_INLINE bool DL_ADC12_isReset (const ADC12_Regs *adc12)
 Returns if adc12 peripheral was reset. More...
 
__STATIC_INLINE void DL_ADC12_initSingleSample (ADC12_Regs *adc12, uint32_t repeatMode, uint32_t sampleMode, uint32_t trigSrc, uint32_t resolution, uint32_t dataFormat)
 Initializes ADC12 for single sampling mode operation. This initialization configures MEMCTL0 as the default memory control register for the conversion. If the conversion needs use a different memory control register the user can call DL_ADC12_setStartAddress to specify a different control register. More...
 
__STATIC_INLINE void DL_ADC12_setStartAddress (ADC12_Regs *adc12, uint32_t startAdd)
 Sets the start address for ADC conversion. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getStartAddress (const ADC12_Regs *adc12)
 Gets start address for ADC conversion. More...
 
__STATIC_INLINE void DL_ADC12_setEndAddress (ADC12_Regs *adc12, uint32_t endAdd)
 Sets the end address for ADC conversion. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEndAddress (const ADC12_Regs *adc12)
 Gets end address for ADC conversion. More...
 
__STATIC_INLINE void DL_ADC12_initSeqSample (ADC12_Regs *adc12, uint32_t repeatMode, uint32_t sampleMode, uint32_t trigSrc, uint32_t startAdd, uint32_t endAdd, uint32_t resolution, uint32_t dataFormat)
 Initializes ADC12 for sequence sampling mode operation. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getResolution (const ADC12_Regs *adc12)
 Returns ADC12 resolution. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getDataFormat (const ADC12_Regs *adc12)
 Returns ADC12 data format. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getSamplingSource (const ADC12_Regs *adc12)
 Returns ADC12 sampling source. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getSampleMode (const ADC12_Regs *adc12)
 Returns ADC12 sampling mode. More...
 
__STATIC_INLINE DL_ADC12_TRIG_SRC DL_ADC12_getTriggerSource (const ADC12_Regs *adc12)
 Returns ADC12 trigger mode. More...
 
__STATIC_INLINE void DL_ADC12_startConversion (ADC12_Regs *adc12)
 Start ADC12 conversion. More...
 
__STATIC_INLINE void DL_ADC12_stopConversion (ADC12_Regs *adc12)
 Stop ADC12 conversion. More...
 
__STATIC_INLINE bool DL_ADC12_isConversionStarted (const ADC12_Regs *adc12)
 Check if ADC12 conversion is started. More...
 
__STATIC_INLINE void DL_ADC12_enableDMA (ADC12_Regs *adc12)
 Enables DMA for data transfer. More...
 
__STATIC_INLINE void DL_ADC12_disableDMA (ADC12_Regs *adc12)
 Disables DMA for data transfer. More...
 
__STATIC_INLINE bool DL_ADC12_isDMAEnabled (const ADC12_Regs *adc12)
 Check if DMA is enabled. More...
 
__STATIC_INLINE void DL_ADC12_setDMASamplesCnt (ADC12_Regs *adc12, uint8_t sampCnt)
 Set number of ADC results to be transfer on a DMA trigger. More...
 
__STATIC_INLINE uint8_t DL_ADC12_getDMASampleCnt (const ADC12_Regs *adc12)
 Get number of ADC results to be transfer on a DMA trigger. More...
 
__STATIC_INLINE void DL_ADC12_enableFIFO (ADC12_Regs *adc12)
 Enables FIFO mode. More...
 
__STATIC_INLINE void DL_ADC12_disableFIFO (ADC12_Regs *adc12)
 Disables FIFO mode. More...
 
__STATIC_INLINE bool DL_ADC12_isFIFOEnabled (const ADC12_Regs *adc12)
 Checks if FIFO mode is enabled. More...
 
void DL_ADC12_setClockConfig (ADC12_Regs *adc12, const DL_ADC12_ClockConfig *config)
 Configures ADC12 sample clock divider and sample clock frequency range. More...
 
void DL_ADC12_getClockConfig (const ADC12_Regs *adc12, DL_ADC12_ClockConfig *config)
 Returns ADC12 sample clock configuration. More...
 
__STATIC_INLINE void DL_ADC12_setPowerDownMode (ADC12_Regs *adc12, uint32_t powerDownMode)
 Configures ADC12 power down mode. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getPowerDownMode (const ADC12_Regs *adc12)
 Returns ADC power down mode. More...
 
__STATIC_INLINE void DL_ADC12_enableConversions (ADC12_Regs *adc12)
 Enable ADC12 conversion. More...
 
__STATIC_INLINE void DL_ADC12_disableConversions (ADC12_Regs *adc12)
 Disable ADC12 conversion. More...
 
__STATIC_INLINE bool DL_ADC12_isConversionsEnabled (const ADC12_Regs *adc12)
 Check if ADC12 conversion is enabled. More...
 
__STATIC_INLINE void DL_ADC12_configHwAverage (ADC12_Regs *adc12, uint32_t numerator, uint32_t denominator)
 Configure ADC12 hardware average. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getHwAverageConfig (const ADC12_Regs *adc12)
 Return the hardware average configuration. More...
 
__STATIC_INLINE void DL_ADC12_setSampleTime0 (ADC12_Regs *adc12, uint16_t adcclks)
 Set sample time 0. More...
 
__STATIC_INLINE uint16_t DL_ADC12_getSampleTime0 (const ADC12_Regs *adc12)
 Get sample time 0. More...
 
__STATIC_INLINE void DL_ADC12_setSampleTime1 (ADC12_Regs *adc12, uint16_t adcclks)
 Set sample time 1. More...
 
__STATIC_INLINE uint16_t DL_ADC12_getSampleTime1 (const ADC12_Regs *adc12)
 Get sample time 1. More...
 
__STATIC_INLINE void DL_ADC12_configWinCompLowThld (ADC12_Regs *adc12, uint16_t threshold)
 Configures window comparator low threshold. More...
 
__STATIC_INLINE void DL_ADC12_configWinCompHighThld (ADC12_Regs *adc12, uint16_t threshold)
 Configures window comparator high threshold. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getFIFOData (const ADC12_Regs *adc12)
 Returns the data from the top of FIFO. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getFIFOAddress (const ADC12_Regs *adc12)
 Returns the address of FIFO data register. More...
 
__STATIC_INLINE void DL_ADC12_configConversionMem (ADC12_Regs *adc12, DL_ADC12_MEM_IDX idx, uint32_t chansel, uint32_t vref, uint32_t stime, uint32_t avgen, uint32_t bcsen, uint32_t trig, uint32_t wincomp)
 Configures conversion memory. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getConversionMemConfig (const ADC12_Regs *adc12, DL_ADC12_MEM_IDX idx)
 Returns conversion memory configuration. More...
 
__STATIC_INLINE uint16_t DL_ADC12_getMemResult (const ADC12_Regs *adc12, DL_ADC12_MEM_IDX idx)
 Returns the conversion result for the selected memory index. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getMemResultAddress (const ADC12_Regs *adc12, DL_ADC12_MEM_IDX idx)
 Returns the conversion result memory address. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getStatus (const ADC12_Regs *adc12)
 Returns ADC12 status. More...
 
__STATIC_INLINE void DL_ADC12_disableForcingSYSOSCOnInRunMode (ADC12_Regs *adc12)
 Allows SYSOSC to not run at base frequency when device is in RUN mode. More...
 
__STATIC_INLINE void DL_ADC12_forceSYSOSCOnInRunMode (ADC12_Regs *adc12)
 Forces SYSOSC to run at base frequency when device is in RUN mode. More...
 
__STATIC_INLINE void DL_ADC12_disableForcingSYSOSCOnInStopMode (ADC12_Regs *adc12)
 Allows SYSOSC to not run at base frequency when device is in STOP mode. More...
 
__STATIC_INLINE void DL_ADC12_forceSYSOSCOnInStopMode (ADC12_Regs *adc12)
 Forces SYSOSC to run at base frequency when device is in STOP mode. More...
 
__STATIC_INLINE void DL_ADC12_enableInterrupt (ADC12_Regs *adc12, uint32_t interruptMask)
 Enable ADC12 interrupt. More...
 
__STATIC_INLINE void DL_ADC12_disableInterrupt (ADC12_Regs *adc12, uint32_t interruptMask)
 Disable ADC12 interrupt. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledInterrupts (const ADC12_Regs *adc12, uint32_t interruptMask)
 Check which ADC12 interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledInterruptStatus (const ADC12_Regs *adc12, uint32_t interruptMask)
 Check interrupt flag of enabled ADC12 interrupt. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getRawInterruptStatus (const ADC12_Regs *adc12, uint32_t interruptMask)
 Check interrupt flag of any ADC12 interrupt. More...
 
__STATIC_INLINE DL_ADC12_IIDX DL_ADC12_getPendingInterrupt (const ADC12_Regs *adc12)
 Get highest priority pending ADC12 interrupt. More...
 
__STATIC_INLINE void DL_ADC12_clearInterruptStatus (ADC12_Regs *adc12, uint32_t interruptMask)
 Clear pending ADC12 interrupt. More...
 
__STATIC_INLINE void DL_ADC12_setPublisherChanID (ADC12_Regs *adc12, uint8_t chanID)
 Sets the event publisher channel id. More...
 
__STATIC_INLINE uint8_t DL_ADC12_getPublisherChanID (const ADC12_Regs *adc12)
 Gets the event publisher channel id. More...
 
__STATIC_INLINE void DL_ADC12_setSubscriberChanID (ADC12_Regs *adc12, uint8_t chanID)
 Sets the event subscriber channel id. More...
 
__STATIC_INLINE uint8_t DL_ADC12_getSubscriberChanID (const ADC12_Regs *adc12)
 Gets the event subscriber channel id. More...
 
__STATIC_INLINE void DL_ADC12_enableEvent (ADC12_Regs *adc12, uint32_t eventMask)
 Enable ADC12 event. More...
 
__STATIC_INLINE void DL_ADC12_disableEvent (ADC12_Regs *adc12, uint32_t eventMask)
 Disable ADC12 event. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledEvents (const ADC12_Regs *adc12, uint32_t eventMask)
 Check which ADC12 events are enabled. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledEventStatus (const ADC12_Regs *adc12, uint32_t eventMask)
 Check event flag of enabled adc12 event. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getRawEventsStatus (const ADC12_Regs *adc12, uint32_t eventMask)
 Check event flag of any adc12 event. More...
 
__STATIC_INLINE void DL_ADC12_clearEventsStatus (ADC12_Regs *adc12, uint32_t eventMask)
 Clear pending adc12 events. More...
 
__STATIC_INLINE void DL_ADC12_enableDMATrigger (ADC12_Regs *adc12, uint32_t dmaMask)
 Enable ADC12 DMA triggers. More...
 
__STATIC_INLINE void DL_ADC12_disableDMATrigger (ADC12_Regs *adc12, uint32_t dmaMask)
 Disable ADC12 DMA triggers. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledDMATrigger (const ADC12_Regs *adc12, uint32_t dmaMask)
 Check which adc12 DMA triggers are enabled. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getEnabledDMATriggerStatus (const ADC12_Regs *adc12, uint32_t dmaMask)
 Check event flag of enabled adc12 DMA triggers. More...
 
__STATIC_INLINE uint32_t DL_ADC12_getRawDMATriggerStatus (const ADC12_Regs *adc12, uint32_t dmaMask)
 Check DMA triggers flag of any adc12 dma trigger. More...
 
__STATIC_INLINE void DL_ADC12_clearDMATriggerStatus (ADC12_Regs *adc12, uint32_t dmaMask)
 Clear pending adc12 DMA triggers. More...
 
__STATIC_INLINE int16_t DL_ADC12_getADCOffsetCalibration (float userRef)
 Get calibration ADC offset value. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale