MSPM0G1X0X_G3X0X Driver Library  2.10.00.04
Macros | Enumerations | Functions
dl_gpio.h File Reference

Detailed Description

General Purpose Input/Output Driver Library.


#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
Include dependency graph for dl_gpio.h:

Go to the source code of this file.

Macros

#define DL_GPIO_PIN_0   (0x00000001)
 GPIO Pin 0.
 
#define DL_GPIO_PIN_1   (0x00000002)
 GPIO Pin 1.
 
#define DL_GPIO_PIN_2   (0x00000004)
 GPIO Pin 2.
 
#define DL_GPIO_PIN_3   (0x00000008)
 GPIO Pin 3.
 
#define DL_GPIO_PIN_4   (0x00000010)
 GPIO Pin 4.
 
#define DL_GPIO_PIN_5   (0x00000020)
 GPIO Pin 5.
 
#define DL_GPIO_PIN_6   (0x00000040)
 GPIO Pin 6.
 
#define DL_GPIO_PIN_7   (0x00000080)
 GPIO Pin 7.
 
#define DL_GPIO_PIN_8   (0x00000100)
 GPIO Pin 8.
 
#define DL_GPIO_PIN_9   (0x00000200)
 GPIO Pin 9.
 
#define DL_GPIO_PIN_10   (0x00000400)
 GPIO Pin 10.
 
#define DL_GPIO_PIN_11   (0x00000800)
 GPIO Pin 11.
 
#define DL_GPIO_PIN_12   (0x00001000)
 GPIO Pin 12.
 
#define DL_GPIO_PIN_13   (0x00002000)
 GPIO Pin 13.
 
#define DL_GPIO_PIN_14   (0x00004000)
 GPIO Pin 14.
 
#define DL_GPIO_PIN_15   (0x00008000)
 GPIO Pin 15.
 
#define DL_GPIO_PIN_16   (0x00010000)
 GPIO Pin 16.
 
#define DL_GPIO_PIN_17   (0x00020000)
 GPIO Pin 17.
 
#define DL_GPIO_PIN_18   (0x00040000)
 GPIO Pin 18.
 
#define DL_GPIO_PIN_19   (0x00080000)
 GPIO Pin 19.
 
#define DL_GPIO_PIN_20   (0x00100000)
 GPIO Pin 20.
 
#define DL_GPIO_PIN_21   (0x00200000)
 GPIO Pin 21.
 
#define DL_GPIO_PIN_22   (0x00400000)
 GPIO Pin 22.
 
#define DL_GPIO_PIN_23   (0x00800000)
 GPIO Pin 23.
 
#define DL_GPIO_PIN_24   (0x01000000)
 GPIO Pin 24.
 
#define DL_GPIO_PIN_25   (0x02000000)
 GPIO Pin 25.
 
#define DL_GPIO_PIN_26   (0x04000000)
 GPIO Pin 26.
 
#define DL_GPIO_PIN_27   (0x08000000)
 GPIO Pin 27.
 
#define DL_GPIO_PIN_28   (0x10000000)
 GPIO Pin 28.
 
#define DL_GPIO_PIN_29   (0x20000000)
 GPIO Pin 29.
 
#define DL_GPIO_PIN_30   (0x40000000)
 GPIO Pin 30.
 
#define DL_GPIO_PIN_31   (0x80000000)
 GPIO Pin 31.
 
#define DL_GPIO_PIN_0_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO0_DISABLE)
 GPIO Pin 0, disable edge detection.
 
#define DL_GPIO_PIN_0_EDGE_RISE   (GPIO_POLARITY15_0_DIO0_RISE)
 GPIO Pin 0, enable detection on rising edge.
 
#define DL_GPIO_PIN_0_EDGE_FALL   (GPIO_POLARITY15_0_DIO0_FALL)
 GPIO Pin 0, enable detection on falling edge.
 
#define DL_GPIO_PIN_0_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO0_RISE_FALL)
 GPIO Pin 0, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_1_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO1_DISABLE)
 GPIO Pin 1, disable edge detection.
 
#define DL_GPIO_PIN_1_EDGE_RISE   (GPIO_POLARITY15_0_DIO1_RISE)
 GPIO Pin 1, enable detection on rising edge.
 
#define DL_GPIO_PIN_1_EDGE_FALL   (GPIO_POLARITY15_0_DIO1_FALL)
 GPIO Pin 1, enable detection on falling edge.
 
#define DL_GPIO_PIN_1_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO1_RISE_FALL)
 GPIO Pin 1, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_2_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO2_DISABLE)
 GPIO Pin 2, disable edge detection.
 
#define DL_GPIO_PIN_2_EDGE_RISE   (GPIO_POLARITY15_0_DIO2_RISE)
 GPIO Pin 2, enable detection on rising edge.
 
#define DL_GPIO_PIN_2_EDGE_FALL   (GPIO_POLARITY15_0_DIO2_FALL)
 GPIO Pin 2, enable detection on falling edge.
 
#define DL_GPIO_PIN_2_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO2_RISE_FALL)
 GPIO Pin 2, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_3_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO3_DISABLE)
 GPIO Pin 3, disable edge detection.
 
#define DL_GPIO_PIN_3_EDGE_RISE   (GPIO_POLARITY15_0_DIO3_RISE)
 GPIO Pin 3, enable detection on rising edge.
 
#define DL_GPIO_PIN_3_EDGE_FALL   (GPIO_POLARITY15_0_DIO3_FALL)
 GPIO Pin 3, enable detection on falling edge.
 
#define DL_GPIO_PIN_3_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO3_RISE_FALL)
 GPIO Pin 3, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_4_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO4_DISABLE)
 GPIO Pin 4, disable edge detection.
 
#define DL_GPIO_PIN_4_EDGE_RISE   (GPIO_POLARITY15_0_DIO4_RISE)
 GPIO Pin 4, enable detection on rising edge.
 
#define DL_GPIO_PIN_4_EDGE_FALL   (GPIO_POLARITY15_0_DIO4_FALL)
 GPIO Pin 4, enable detection on falling edge.
 
#define DL_GPIO_PIN_4_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO4_RISE_FALL)
 GPIO Pin 4, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_5_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO5_DISABLE)
 GPIO Pin 5, disable edge detection.
 
#define DL_GPIO_PIN_5_EDGE_RISE   (GPIO_POLARITY15_0_DIO5_RISE)
 GPIO Pin 5, enable detection on rising edge.
 
#define DL_GPIO_PIN_5_EDGE_FALL   (GPIO_POLARITY15_0_DIO5_FALL)
 GPIO Pin 5, enable detection on falling edge.
 
#define DL_GPIO_PIN_5_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO5_RISE_FALL)
 GPIO Pin 5, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_6_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO6_DISABLE)
 GPIO Pin 6, disable edge detection.
 
#define DL_GPIO_PIN_6_EDGE_RISE   (GPIO_POLARITY15_0_DIO6_RISE)
 GPIO Pin 6, enable detection on rising edge.
 
#define DL_GPIO_PIN_6_EDGE_FALL   (GPIO_POLARITY15_0_DIO6_FALL)
 GPIO Pin 6, enable detection on falling edge.
 
#define DL_GPIO_PIN_6_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO6_RISE_FALL)
 GPIO Pin 6, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_7_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO7_DISABLE)
 GPIO Pin 7, disable edge detection.
 
#define DL_GPIO_PIN_7_EDGE_RISE   (GPIO_POLARITY15_0_DIO7_RISE)
 GPIO Pin 7, enable detection on rising edge.
 
#define DL_GPIO_PIN_7_EDGE_FALL   (GPIO_POLARITY15_0_DIO7_FALL)
 GPIO Pin 7, enable detection on falling edge.
 
#define DL_GPIO_PIN_7_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO7_RISE_FALL)
 GPIO Pin 7, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_8_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO8_DISABLE)
 GPIO Pin 8, disable edge detection.
 
#define DL_GPIO_PIN_8_EDGE_RISE   (GPIO_POLARITY15_0_DIO8_RISE)
 GPIO Pin 8, enable detection on rising edge.
 
#define DL_GPIO_PIN_8_EDGE_FALL   (GPIO_POLARITY15_0_DIO8_FALL)
 GPIO Pin 8, enable detection on falling edge.
 
#define DL_GPIO_PIN_8_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO8_RISE_FALL)
 GPIO Pin 8, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_9_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO9_DISABLE)
 GPIO Pin 9, disable edge detection.
 
#define DL_GPIO_PIN_9_EDGE_RISE   (GPIO_POLARITY15_0_DIO9_RISE)
 GPIO Pin 9, enable detection on rising edge.
 
#define DL_GPIO_PIN_9_EDGE_FALL   (GPIO_POLARITY15_0_DIO9_FALL)
 GPIO Pin 9, enable detection on falling edge.
 
#define DL_GPIO_PIN_9_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO9_RISE_FALL)
 GPIO Pin 9, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_10_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO10_DISABLE)
 GPIO Pin 10, disable edge detection.
 
#define DL_GPIO_PIN_10_EDGE_RISE   (GPIO_POLARITY15_0_DIO10_RISE)
 GPIO Pin 10, enable detection on rising edge.
 
#define DL_GPIO_PIN_10_EDGE_FALL   (GPIO_POLARITY15_0_DIO10_FALL)
 GPIO Pin 10, enable detection on falling edge.
 
#define DL_GPIO_PIN_10_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO10_RISE_FALL)
 GPIO Pin 10, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_11_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO11_DISABLE)
 GPIO Pin 11, disable edge detection.
 
#define DL_GPIO_PIN_11_EDGE_RISE   (GPIO_POLARITY15_0_DIO11_RISE)
 GPIO Pin 11, enable detection on rising edge.
 
#define DL_GPIO_PIN_11_EDGE_FALL   (GPIO_POLARITY15_0_DIO11_FALL)
 GPIO Pin 11, enable detection on falling edge.
 
#define DL_GPIO_PIN_11_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO11_RISE_FALL)
 GPIO Pin 11, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_12_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO12_DISABLE)
 GPIO Pin 12, disable edge detection.
 
#define DL_GPIO_PIN_12_EDGE_RISE   (GPIO_POLARITY15_0_DIO12_RISE)
 GPIO Pin 12, enable detection on rising edge.
 
#define DL_GPIO_PIN_12_EDGE_FALL   (GPIO_POLARITY15_0_DIO12_FALL)
 GPIO Pin 12, enable detection on falling edge.
 
#define DL_GPIO_PIN_12_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO12_RISE_FALL)
 GPIO Pin 12, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_13_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO13_DISABLE)
 GPIO Pin 13, disable edge detection.
 
#define DL_GPIO_PIN_13_EDGE_RISE   (GPIO_POLARITY15_0_DIO13_RISE)
 GPIO Pin 13, enable detection on rising edge.
 
#define DL_GPIO_PIN_13_EDGE_FALL   (GPIO_POLARITY15_0_DIO13_FALL)
 GPIO Pin 13, enable detection on falling edge.
 
#define DL_GPIO_PIN_13_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO13_RISE_FALL)
 GPIO Pin 13, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_14_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO14_DISABLE)
 GPIO Pin 14, disable edge detection.
 
#define DL_GPIO_PIN_14_EDGE_RISE   (GPIO_POLARITY15_0_DIO14_RISE)
 GPIO Pin 14, enable detection on rising edge.
 
#define DL_GPIO_PIN_14_EDGE_FALL   (GPIO_POLARITY15_0_DIO14_FALL)
 GPIO Pin 14, enable detection on falling edge.
 
#define DL_GPIO_PIN_14_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO14_RISE_FALL)
 GPIO Pin 14, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_15_EDGE_DISABLE   (GPIO_POLARITY15_0_DIO15_DISABLE)
 GPIO Pin 15, disable edge detection.
 
#define DL_GPIO_PIN_15_EDGE_RISE   (GPIO_POLARITY15_0_DIO15_RISE)
 GPIO Pin 15, enable detection on rising edge.
 
#define DL_GPIO_PIN_15_EDGE_FALL   (GPIO_POLARITY15_0_DIO15_FALL)
 GPIO Pin 15, enable detection on falling edge.
 
#define DL_GPIO_PIN_15_EDGE_RISE_FALL   (GPIO_POLARITY15_0_DIO15_RISE_FALL)
 GPIO Pin 15, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_16_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO16_DISABLE)
 GPIO Pin 16, disable edge detection.
 
#define DL_GPIO_PIN_16_EDGE_RISE   (GPIO_POLARITY31_16_DIO16_RISE)
 GPIO Pin 16, enable detection on rising edge.
 
#define DL_GPIO_PIN_16_EDGE_FALL   (GPIO_POLARITY31_16_DIO16_FALL)
 GPIO Pin 16, enable detection on falling edge.
 
#define DL_GPIO_PIN_16_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO16_RISE_FALL)
 GPIO Pin 16, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_17_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO17_DISABLE)
 GPIO Pin 17, disable edge detection.
 
#define DL_GPIO_PIN_17_EDGE_RISE   (GPIO_POLARITY31_16_DIO17_RISE)
 GPIO Pin 17, enable detection on rising edge.
 
#define DL_GPIO_PIN_17_EDGE_FALL   (GPIO_POLARITY31_16_DIO17_FALL)
 GPIO Pin 17, enable detection on falling edge.
 
#define DL_GPIO_PIN_17_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO17_RISE_FALL)
 GPIO Pin 17, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_18_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO18_DISABLE)
 GPIO Pin 18, disable edge detection.
 
#define DL_GPIO_PIN_18_EDGE_RISE   (GPIO_POLARITY31_16_DIO18_RISE)
 GPIO Pin 18, enable detection on rising edge.
 
#define DL_GPIO_PIN_18_EDGE_FALL   (GPIO_POLARITY31_16_DIO18_FALL)
 GPIO Pin 18, enable detection on falling edge.
 
#define DL_GPIO_PIN_18_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO18_RISE_FALL)
 GPIO Pin 18, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_19_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO19_DISABLE)
 GPIO Pin 19, disable edge detection.
 
#define DL_GPIO_PIN_19_EDGE_RISE   (GPIO_POLARITY31_16_DIO19_RISE)
 GPIO Pin 19, enable detection on rising edge.
 
#define DL_GPIO_PIN_19_EDGE_FALL   (GPIO_POLARITY31_16_DIO19_FALL)
 GPIO Pin 19, enable detection on falling edge.
 
#define DL_GPIO_PIN_19_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO19_RISE_FALL)
 GPIO Pin 19, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_20_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO20_DISABLE)
 GPIO Pin 20, disable edge detection.
 
#define DL_GPIO_PIN_20_EDGE_RISE   (GPIO_POLARITY31_16_DIO20_RISE)
 GPIO Pin 20, enable detection on rising edge.
 
#define DL_GPIO_PIN_20_EDGE_FALL   (GPIO_POLARITY31_16_DIO20_FALL)
 GPIO Pin 20, enable detection on falling edge.
 
#define DL_GPIO_PIN_20_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO20_RISE_FALL)
 GPIO Pin 20, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_21_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO21_DISABLE)
 GPIO Pin 21, disable edge detection.
 
#define DL_GPIO_PIN_21_EDGE_RISE   (GPIO_POLARITY31_16_DIO21_RISE)
 GPIO Pin 21, enable detection on rising edge.
 
#define DL_GPIO_PIN_21_EDGE_FALL   (GPIO_POLARITY31_16_DIO21_FALL)
 GPIO Pin 21, enable detection on falling edge.
 
#define DL_GPIO_PIN_21_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO21_RISE_FALL)
 GPIO Pin 21, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_22_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO22_DISABLE)
 GPIO Pin 22, disable edge detection.
 
#define DL_GPIO_PIN_22_EDGE_RISE   (GPIO_POLARITY31_16_DIO22_RISE)
 GPIO Pin 22, enable detection on rising edge.
 
#define DL_GPIO_PIN_22_EDGE_FALL   (GPIO_POLARITY31_16_DIO22_FALL)
 GPIO Pin 22, enable detection on falling edge.
 
#define DL_GPIO_PIN_22_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO22_RISE_FALL)
 GPIO Pin 22, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_23_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO23_DISABLE)
 GPIO Pin 23, disable edge detection.
 
#define DL_GPIO_PIN_23_EDGE_RISE   (GPIO_POLARITY31_16_DIO23_RISE)
 GPIO Pin 23, enable detection on rising edge.
 
#define DL_GPIO_PIN_23_EDGE_FALL   (GPIO_POLARITY31_16_DIO23_FALL)
 GPIO Pin 23, enable detection on falling edge.
 
#define DL_GPIO_PIN_23_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO23_RISE_FALL)
 GPIO Pin 23, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_24_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO24_DISABLE)
 GPIO Pin 24, disable edge detection.
 
#define DL_GPIO_PIN_24_EDGE_RISE   (GPIO_POLARITY31_16_DIO24_RISE)
 GPIO Pin 24, enable detection on rising edge.
 
#define DL_GPIO_PIN_24_EDGE_FALL   (GPIO_POLARITY31_16_DIO24_FALL)
 GPIO Pin 24, enable detection on falling edge.
 
#define DL_GPIO_PIN_24_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO24_RISE_FALL)
 GPIO Pin 24, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_25_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO25_DISABLE)
 GPIO Pin 25, disable edge detection.
 
#define DL_GPIO_PIN_25_EDGE_RISE   (GPIO_POLARITY31_16_DIO25_RISE)
 GPIO Pin 25, enable detection on rising edge.
 
#define DL_GPIO_PIN_25_EDGE_FALL   (GPIO_POLARITY31_16_DIO25_FALL)
 GPIO Pin 25, enable detection on falling edge.
 
#define DL_GPIO_PIN_25_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO25_RISE_FALL)
 GPIO Pin 25, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_26_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO26_DISABLE)
 GPIO Pin 26, disable edge detection.
 
#define DL_GPIO_PIN_26_EDGE_RISE   (GPIO_POLARITY31_16_DIO26_RISE)
 GPIO Pin 26, enable detection on rising edge.
 
#define DL_GPIO_PIN_26_EDGE_FALL   (GPIO_POLARITY31_16_DIO26_FALL)
 GPIO Pin 26, enable detection on falling edge.
 
#define DL_GPIO_PIN_26_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO26_RISE_FALL)
 GPIO Pin 26, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_27_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO27_DISABLE)
 GPIO Pin 27, disable edge detection.
 
#define DL_GPIO_PIN_27_EDGE_RISE   (GPIO_POLARITY31_16_DIO27_RISE)
 GPIO Pin 27, enable detection on rising edge.
 
#define DL_GPIO_PIN_27_EDGE_FALL   (GPIO_POLARITY31_16_DIO27_FALL)
 GPIO Pin 27, enable detection on falling edge.
 
#define DL_GPIO_PIN_27_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO27_RISE_FALL)
 GPIO Pin 27, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_28_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO28_DISABLE)
 GPIO Pin 28, disable edge detection.
 
#define DL_GPIO_PIN_28_EDGE_RISE   (GPIO_POLARITY31_16_DIO28_RISE)
 GPIO Pin 28, enable detection on rising edge.
 
#define DL_GPIO_PIN_28_EDGE_FALL   (GPIO_POLARITY31_16_DIO28_FALL)
 GPIO Pin 28, enable detection on falling edge.
 
#define DL_GPIO_PIN_28_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO28_RISE_FALL)
 GPIO Pin 28, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_29_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO29_DISABLE)
 GPIO Pin 29, disable edge detection.
 
#define DL_GPIO_PIN_29_EDGE_RISE   (GPIO_POLARITY31_16_DIO29_RISE)
 GPIO Pin 29, enable detection on rising edge.
 
#define DL_GPIO_PIN_29_EDGE_FALL   (GPIO_POLARITY31_16_DIO29_FALL)
 GPIO Pin 29, enable detection on falling edge.
 
#define DL_GPIO_PIN_29_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO29_RISE_FALL)
 GPIO Pin 29, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_30_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO30_DISABLE)
 GPIO Pin 30, disable edge detection.
 
#define DL_GPIO_PIN_30_EDGE_RISE   (GPIO_POLARITY31_16_DIO30_RISE)
 GPIO Pin 30, enable detection on rising edge.
 
#define DL_GPIO_PIN_30_EDGE_FALL   (GPIO_POLARITY31_16_DIO30_FALL)
 GPIO Pin 30, enable detection on falling edge.
 
#define DL_GPIO_PIN_30_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO30_RISE_FALL)
 GPIO Pin 30, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_31_EDGE_DISABLE   (GPIO_POLARITY31_16_DIO31_DISABLE)
 GPIO Pin 31, disable edge detection.
 
#define DL_GPIO_PIN_31_EDGE_RISE   (GPIO_POLARITY31_16_DIO31_RISE)
 GPIO Pin 31, enable detection on rising edge.
 
#define DL_GPIO_PIN_31_EDGE_FALL   (GPIO_POLARITY31_16_DIO31_FALL)
 GPIO Pin 31, enable detection on falling edge.
 
#define DL_GPIO_PIN_31_EDGE_RISE_FALL   (GPIO_POLARITY31_16_DIO31_RISE_FALL)
 GPIO Pin 31, enable detection on both rising and falling edge.
 
#define DL_GPIO_PIN_0_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN0_DISABLE)
 GPIO Pin 0, disable input filter.
 
#define DL_GPIO_PIN_0_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN0_ONE_CYCLE)
 GPIO Pin 0, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_0_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN0_THREE_CYCLE)
 GPIO Pin 0, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_0_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN0_EIGHT_CYCLE)
 GPIO Pin 0, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_1_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN1_DISABLE)
 GPIO Pin 1, disable input filter.
 
#define DL_GPIO_PIN_1_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN1_ONE_CYCLE)
 GPIO Pin 1, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_1_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN1_THREE_CYCLE)
 GPIO Pin 1, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_1_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN1_EIGHT_CYCLE)
 GPIO Pin 1, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_2_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN2_DISABLE)
 GPIO Pin 2, disable input filter.
 
#define DL_GPIO_PIN_2_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN2_ONE_CYCLE)
 GPIO Pin 2, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_2_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN2_THREE_CYCLE)
 GPIO Pin 2, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_2_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN2_EIGHT_CYCLE)
 GPIO Pin 2, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_3_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN3_DISABLE)
 GPIO Pin 3, disable input filter.
 
#define DL_GPIO_PIN_3_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN3_ONE_CYCLE)
 GPIO Pin 3, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_3_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN3_THREE_CYCLE)
 GPIO Pin 3, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_3_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN3_EIGHT_CYCLE)
 GPIO Pin 3, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_4_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN4_DISABLE)
 GPIO Pin 4, disable input filter.
 
#define DL_GPIO_PIN_4_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN4_ONE_CYCLE)
 GPIO Pin 4, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_4_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN4_THREE_CYCLE)
 GPIO Pin 4, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_4_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN4_EIGHT_CYCLE)
 GPIO Pin 4, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_5_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN5_DISABLE)
 GPIO Pin 5, disable input filter.
 
#define DL_GPIO_PIN_5_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN5_ONE_CYCLE)
 GPIO Pin 5, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_5_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN5_THREE_CYCLE)
 GPIO Pin 5, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_5_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN5_EIGHT_CYCLE)
 GPIO Pin 5, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_6_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN6_DISABLE)
 GPIO Pin 6, disable input filter.
 
#define DL_GPIO_PIN_6_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN6_ONE_CYCLE)
 GPIO Pin 6, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_6_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN6_THREE_CYCLE)
 GPIO Pin 6, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_6_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN6_EIGHT_CYCLE)
 GPIO Pin 6, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_7_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN7_DISABLE)
 GPIO Pin 7, disable input filter.
 
#define DL_GPIO_PIN_7_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN7_ONE_CYCLE)
 GPIO Pin 7, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_7_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN7_THREE_CYCLE)
 GPIO Pin 7, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_7_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN7_EIGHT_CYCLE)
 GPIO Pin 7, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_8_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN8_DISABLE)
 GPIO Pin 8, disable input filter.
 
#define DL_GPIO_PIN_8_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN8_ONE_CYCLE)
 GPIO Pin 8, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_8_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN8_THREE_CYCLE)
 GPIO Pin 8, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_8_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN8_EIGHT_CYCLE)
 GPIO Pin 8, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_9_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN9_DISABLE)
 GPIO Pin 9, disable input filter.
 
#define DL_GPIO_PIN_9_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN9_ONE_CYCLE)
 GPIO Pin 9, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_9_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN9_THREE_CYCLE)
 GPIO Pin 9, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_9_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN9_EIGHT_CYCLE)
 GPIO Pin 9, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_10_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN10_DISABLE)
 GPIO Pin 10, disable input filter.
 
#define DL_GPIO_PIN_10_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN10_ONE_CYCLE)
 GPIO Pin 10, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_10_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN10_THREE_CYCLE)
 GPIO Pin 10, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_10_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN10_EIGHT_CYCLE)
 GPIO Pin 10, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_11_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN11_DISABLE)
 GPIO Pin 11, disable input filter.
 
#define DL_GPIO_PIN_11_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN11_ONE_CYCLE)
 GPIO Pin 11, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_11_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN11_THREE_CYCLE)
 GPIO Pin 11, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_11_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN11_EIGHT_CYCLE)
 GPIO Pin 11, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_12_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN12_DISABLE)
 GPIO Pin 12, disable input filter.
 
#define DL_GPIO_PIN_12_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN12_ONE_CYCLE)
 GPIO Pin 12, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_12_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN12_THREE_CYCLE)
 GPIO Pin 12, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_12_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN12_EIGHT_CYCLE)
 GPIO Pin 12, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_13_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN13_DISABLE)
 GPIO Pin 13, disable input filter.
 
#define DL_GPIO_PIN_13_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN13_ONE_CYCLE)
 GPIO Pin 13, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_13_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN13_THREE_CYCLE)
 GPIO Pin 13, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_13_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN13_EIGHT_CYCLE)
 GPIO Pin 13, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_14_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN14_DISABLE)
 GPIO Pin 14, disable input filter.
 
#define DL_GPIO_PIN_14_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN14_ONE_CYCLE)
 GPIO Pin 14, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_14_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN14_THREE_CYCLE)
 GPIO Pin 14, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_14_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN14_EIGHT_CYCLE)
 GPIO Pin 14, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_15_INPUT_FILTER_DISABLE   (GPIO_FILTEREN15_0_DIN15_DISABLE)
 GPIO Pin 15, disable input filter.
 
#define DL_GPIO_PIN_15_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN15_0_DIN15_ONE_CYCLE)
 GPIO Pin 15, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_15_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN15_0_DIN15_THREE_CYCLE)
 GPIO Pin 15, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_15_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN15_0_DIN15_EIGHT_CYCLE)
 GPIO Pin 15, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_16_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN16_DISABLE)
 GPIO Pin 16, disable input filter.
 
#define DL_GPIO_PIN_16_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN16_ONE_CYCLE)
 GPIO Pin 16, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_16_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN16_THREE_CYCLE)
 GPIO Pin 16, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_16_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN16_EIGHT_CYCLE)
 GPIO Pin 16, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_17_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN17_DISABLE)
 GPIO Pin 17, disable input filter.
 
#define DL_GPIO_PIN_17_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN17_ONE_CYCLE)
 GPIO Pin 17, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_17_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN17_THREE_CYCLE)
 GPIO Pin 17, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_17_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN17_EIGHT_CYCLE)
 GPIO Pin 17, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_18_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN18_DISABLE)
 GPIO Pin 18, disable input filter.
 
#define DL_GPIO_PIN_18_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN18_ONE_CYCLE)
 GPIO Pin 18, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_18_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN18_THREE_CYCLE)
 GPIO Pin 18, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_18_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN18_EIGHT_CYCLE)
 GPIO Pin 18, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_19_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN19_DISABLE)
 GPIO Pin 19, disable input filter.
 
#define DL_GPIO_PIN_19_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN19_ONE_CYCLE)
 GPIO Pin 19, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_19_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN19_THREE_CYCLE)
 GPIO Pin 19, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_19_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN19_EIGHT_CYCLE)
 GPIO Pin 19, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_20_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN20_DISABLE)
 GPIO Pin 20, disable input filter.
 
#define DL_GPIO_PIN_20_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN20_ONE_CYCLE)
 GPIO Pin 20, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_20_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN20_THREE_CYCLE)
 GPIO Pin 20, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_20_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN20_EIGHT_CYCLE)
 GPIO Pin 20, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_21_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN21_DISABLE)
 GPIO Pin 21, disable input filter.
 
#define DL_GPIO_PIN_21_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN21_ONE_CYCLE)
 GPIO Pin 21, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_21_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN21_THREE_CYCLE)
 GPIO Pin 21, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_21_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN21_EIGHT_CYCLE)
 GPIO Pin 21, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_22_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN22_DISABLE)
 GPIO Pin 22, disable input filter.
 
#define DL_GPIO_PIN_22_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN22_ONE_CYCLE)
 GPIO Pin 22, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_22_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN22_THREE_CYCLE)
 GPIO Pin 22, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_22_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN22_EIGHT_CYCLE)
 GPIO Pin 22, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_23_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN23_DISABLE)
 GPIO Pin 23, disable input filter.
 
#define DL_GPIO_PIN_23_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN23_ONE_CYCLE)
 GPIO Pin 23, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_23_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN23_THREE_CYCLE)
 GPIO Pin 23, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_23_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN23_EIGHT_CYCLE)
 GPIO Pin 23, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_24_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN24_DISABLE)
 GPIO Pin 24, disable input filter.
 
#define DL_GPIO_PIN_24_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN24_ONE_CYCLE)
 GPIO Pin 24, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_24_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN24_THREE_CYCLE)
 GPIO Pin 24, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_24_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN24_EIGHT_CYCLE)
 GPIO Pin 24, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_25_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN25_DISABLE)
 GPIO Pin 25, disable input filter.
 
#define DL_GPIO_PIN_25_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN25_ONE_CYCLE)
 GPIO Pin 25, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_25_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN25_THREE_CYCLE)
 GPIO Pin 25, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_25_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN25_EIGHT_CYCLE)
 GPIO Pin 25, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_26_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN26_DISABLE)
 GPIO Pin 26, disable input filter.
 
#define DL_GPIO_PIN_26_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN26_ONE_CYCLE)
 GPIO Pin 26, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_26_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN26_THREE_CYCLE)
 GPIO Pin 26, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_26_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN26_EIGHT_CYCLE)
 GPIO Pin 26, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_27_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN27_DISABLE)
 GPIO Pin 27, disable input filter.
 
#define DL_GPIO_PIN_27_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN27_ONE_CYCLE)
 GPIO Pin 27, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_27_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN27_THREE_CYCLE)
 GPIO Pin 27, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_27_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN27_EIGHT_CYCLE)
 GPIO Pin 27, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_28_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN28_DISABLE)
 GPIO Pin 28, disable input filter.
 
#define DL_GPIO_PIN_28_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN28_ONE_CYCLE)
 GPIO Pin 28, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_28_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN28_THREE_CYCLE)
 GPIO Pin 28, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_28_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN28_EIGHT_CYCLE)
 GPIO Pin 28, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_29_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN29_DISABLE)
 GPIO Pin 29, disable input filter.
 
#define DL_GPIO_PIN_29_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN29_ONE_CYCLE)
 GPIO Pin 29, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_29_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN29_THREE_CYCLE)
 GPIO Pin 29, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_29_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN29_EIGHT_CYCLE)
 GPIO Pin 29, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_30_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN30_DISABLE)
 GPIO Pin 30, disable input filter.
 
#define DL_GPIO_PIN_30_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN30_ONE_CYCLE)
 GPIO Pin 30, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_30_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN30_THREE_CYCLE)
 GPIO Pin 30, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_30_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN30_EIGHT_CYCLE)
 GPIO Pin 30, enable input filter to 8 ulpclk periods.
 
#define DL_GPIO_PIN_31_INPUT_FILTER_DISABLE   (GPIO_FILTEREN31_16_DIN31_DISABLE)
 GPIO Pin 31, disable input filter.
 
#define DL_GPIO_PIN_31_INPUT_FILTER_1_CYCLE   (GPIO_FILTEREN31_16_DIN31_ONE_CYCLE)
 GPIO Pin 31, enable input filter to 1 ulpclk period.
 
#define DL_GPIO_PIN_31_INPUT_FILTER_3_CYCLES   (GPIO_FILTEREN31_16_DIN31_THREE_CYCLE)
 GPIO Pin 31, enable input filter to 3 ulpclk periods.
 
#define DL_GPIO_PIN_31_INPUT_FILTER_8_CYCLES   (GPIO_FILTEREN31_16_DIN31_EIGHT_CYCLE)
 GPIO Pin 31, enable input filter to 8 ulpclk periods.
 

Enumerations

enum  DL_GPIO_INVERSION {
  DL_GPIO_INVERSION_ENABLE = IOMUX_PINCM_INV_ENABLE,
  DL_GPIO_INVERSION_DISABLE = IOMUX_PINCM_INV_DISABLE
}
 
enum  DL_GPIO_DRIVE_STRENGTH {
  DL_GPIO_DRIVE_STRENGTH_LOW = IOMUX_PINCM_DRV_DRVVAL0,
  DL_GPIO_DRIVE_STRENGTH_HIGH = IOMUX_PINCM_DRV_DRVVAL1
}
 
enum  DL_GPIO_RESISTOR {
  DL_GPIO_RESISTOR_NONE,
  DL_GPIO_RESISTOR_PULL_UP,
  DL_GPIO_RESISTOR_PULL_DOWN
}
 
enum  DL_GPIO_HYSTERESIS {
  DL_GPIO_HYSTERESIS_ENABLE = IOMUX_PINCM_HYSTEN_ENABLE,
  DL_GPIO_HYSTERESIS_DISABLE = IOMUX_PINCM_HYSTEN_DISABLE
}
 
enum  DL_GPIO_WAKEUP {
  DL_GPIO_WAKEUP_ENABLE = IOMUX_PINCM_WUEN_ENABLE,
  DL_GPIO_WAKEUP_DISABLE = IOMUX_PINCM_WUEN_DISABLE,
  DL_GPIO_WAKEUP_ON_0 = (IOMUX_PINCM_WUEN_ENABLE | IOMUX_PINCM_WCOMP_MATCH0),
  DL_GPIO_WAKEUP_ON_1 = (IOMUX_PINCM_WUEN_ENABLE | IOMUX_PINCM_WCOMP_MATCH1)
}
 
enum  DL_GPIO_WAKEUP_COMPARE_VALUE {
  DL_GPIO_WAKEUP_COMPARE_VALUE_0 = IOMUX_PINCM_WCOMP_MATCH0,
  DL_GPIO_WAKEUP_COMPARE_VALUE_1 = IOMUX_PINCM_WCOMP_MATCH1
}
 
enum  DL_GPIO_HIZ {
  DL_GPIO_HIZ_ENABLE = IOMUX_PINCM_HIZ1_ENABLE,
  DL_GPIO_HIZ_DISABLE = IOMUX_PINCM_HIZ1_DISABLE
}
 
enum  DL_GPIO_EVENT_ROUTE {
  DL_GPIO_EVENT_ROUTE_1 = 0,
  DL_GPIO_EVENT_ROUTE_2 = 12
}
 
enum  DL_GPIO_PUBLISHER_INDEX {
  DL_GPIO_PUBLISHER_INDEX_0 = 0,
  DL_GPIO_PUBLISHER_INDEX_1 = 1
}
 
enum  DL_GPIO_SUBSCRIBER_INDEX {
  DL_GPIO_SUBSCRIBER_INDEX_0 = 0,
  DL_GPIO_SUBSCRIBER_INDEX_1 = 1
}
 
enum  DL_GPIO_SUBSCRIBER_OUT_POLICY {
  DL_GPIO_SUBSCRIBER_OUT_POLICY_SET = GPIO_SUB0CFG_OUTPOLICY_SET,
  DL_GPIO_SUBSCRIBER_OUT_POLICY_CLEAR = GPIO_SUB0CFG_OUTPOLICY_CLR,
  DL_GPIO_SUBSCRIBER_OUT_POLICY_TOGGLE = GPIO_SUB0CFG_OUTPOLICY_TOGGLE
}
 
enum  DL_GPIO_SUBSCRIBERx_PIN {
  DL_GPIO_SUBSCRIBER0_PIN_0 = 0x00000000,
  DL_GPIO_SUBSCRIBER0_PIN_1 = 0x00010000,
  DL_GPIO_SUBSCRIBER0_PIN_2 = 0x00020000,
  DL_GPIO_SUBSCRIBER0_PIN_3 = 0x00030000,
  DL_GPIO_SUBSCRIBER0_PIN_4 = 0x00040000,
  DL_GPIO_SUBSCRIBER0_PIN_5 = 0x00050000,
  DL_GPIO_SUBSCRIBER0_PIN_6 = 0x00060000,
  DL_GPIO_SUBSCRIBER0_PIN_7 = 0x00070000,
  DL_GPIO_SUBSCRIBER0_PIN_8 = 0x00080000,
  DL_GPIO_SUBSCRIBER0_PIN_9 = 0x00090000,
  DL_GPIO_SUBSCRIBER0_PIN_10 = 0x000A0000,
  DL_GPIO_SUBSCRIBER0_PIN_11 = 0x000B0000,
  DL_GPIO_SUBSCRIBER0_PIN_12 = 0x000C0000,
  DL_GPIO_SUBSCRIBER0_PIN_13 = 0x000D0000,
  DL_GPIO_SUBSCRIBER0_PIN_14 = 0x000E0000,
  DL_GPIO_SUBSCRIBER0_PIN_15 = 0x000F0000,
  DL_GPIO_SUBSCRIBER1_PIN_16 = 0x00000000,
  DL_GPIO_SUBSCRIBER1_PIN_17 = 0x00010000,
  DL_GPIO_SUBSCRIBER1_PIN_18 = 0x00020000,
  DL_GPIO_SUBSCRIBER1_PIN_19 = 0x00030000,
  DL_GPIO_SUBSCRIBER1_PIN_20 = 0x00040000,
  DL_GPIO_SUBSCRIBER1_PIN_21 = 0x00050000,
  DL_GPIO_SUBSCRIBER1_PIN_22 = 0x00060000,
  DL_GPIO_SUBSCRIBER1_PIN_23 = 0x00070000,
  DL_GPIO_SUBSCRIBER1_PIN_24 = 0x00080000,
  DL_GPIO_SUBSCRIBER1_PIN_25 = 0x00090000,
  DL_GPIO_SUBSCRIBER1_PIN_26 = 0x000A0000,
  DL_GPIO_SUBSCRIBER1_PIN_27 = 0x000B0000,
  DL_GPIO_SUBSCRIBER1_PIN_28 = 0x000C0000,
  DL_GPIO_SUBSCRIBER1_PIN_29 = 0x000D0000,
  DL_GPIO_SUBSCRIBER1_PIN_30 = 0x000E0000,
  DL_GPIO_SUBSCRIBER1_PIN_31 = 0x000F0000
}
 
enum  DL_GPIO_IIDX {
  DL_GPIO_IIDX_NO_INTR = GPIO_CPU_INT_IIDX_STAT_NO_INTR,
  DL_GPIO_IIDX_DIO0 = GPIO_CPU_INT_IIDX_STAT_DIO0,
  DL_GPIO_IIDX_DIO1 = GPIO_CPU_INT_IIDX_STAT_DIO1,
  DL_GPIO_IIDX_DIO2 = GPIO_CPU_INT_IIDX_STAT_DIO2,
  DL_GPIO_IIDX_DIO3 = GPIO_CPU_INT_IIDX_STAT_DIO3,
  DL_GPIO_IIDX_DIO4 = GPIO_CPU_INT_IIDX_STAT_DIO4,
  DL_GPIO_IIDX_DIO5 = GPIO_CPU_INT_IIDX_STAT_DIO5,
  DL_GPIO_IIDX_DIO6 = GPIO_CPU_INT_IIDX_STAT_DIO6,
  DL_GPIO_IIDX_DIO7 = GPIO_CPU_INT_IIDX_STAT_DIO7,
  DL_GPIO_IIDX_DIO8 = GPIO_CPU_INT_IIDX_STAT_DIO8,
  DL_GPIO_IIDX_DIO9 = GPIO_CPU_INT_IIDX_STAT_DIO9,
  DL_GPIO_IIDX_DIO10 = GPIO_CPU_INT_IIDX_STAT_DIO10,
  DL_GPIO_IIDX_DIO11 = GPIO_CPU_INT_IIDX_STAT_DIO11,
  DL_GPIO_IIDX_DIO12 = GPIO_CPU_INT_IIDX_STAT_DIO12,
  DL_GPIO_IIDX_DIO13 = GPIO_CPU_INT_IIDX_STAT_DIO13,
  DL_GPIO_IIDX_DIO14 = GPIO_CPU_INT_IIDX_STAT_DIO14,
  DL_GPIO_IIDX_DIO15 = GPIO_CPU_INT_IIDX_STAT_DIO15,
  DL_GPIO_IIDX_DIO16 = GPIO_CPU_INT_IIDX_STAT_DIO16,
  DL_GPIO_IIDX_DIO17 = GPIO_CPU_INT_IIDX_STAT_DIO17,
  DL_GPIO_IIDX_DIO18 = GPIO_CPU_INT_IIDX_STAT_DIO18,
  DL_GPIO_IIDX_DIO19 = GPIO_CPU_INT_IIDX_STAT_DIO19,
  DL_GPIO_IIDX_DIO20 = GPIO_CPU_INT_IIDX_STAT_DIO20,
  DL_GPIO_IIDX_DIO21 = GPIO_CPU_INT_IIDX_STAT_DIO21,
  DL_GPIO_IIDX_DIO22 = GPIO_CPU_INT_IIDX_STAT_DIO22,
  DL_GPIO_IIDX_DIO23 = GPIO_CPU_INT_IIDX_STAT_DIO23,
  DL_GPIO_IIDX_DIO24 = GPIO_CPU_INT_IIDX_STAT_DIO24,
  DL_GPIO_IIDX_DIO25 = GPIO_CPU_INT_IIDX_STAT_DIO25,
  DL_GPIO_IIDX_DIO26 = GPIO_CPU_INT_IIDX_STAT_DIO26,
  DL_GPIO_IIDX_DIO27 = GPIO_CPU_INT_IIDX_STAT_DIO27,
  DL_GPIO_IIDX_DIO28 = GPIO_CPU_INT_IIDX_STAT_DIO28,
  DL_GPIO_IIDX_DIO29 = GPIO_CPU_INT_IIDX_STAT_DIO29,
  DL_GPIO_IIDX_DIO30 = GPIO_CPU_INT_IIDX_STAT_DIO30,
  DL_GPIO_IIDX_DIO31 = GPIO_CPU_INT_IIDX_STAT_DIO31
}
 

Functions

__STATIC_INLINE void DL_GPIO_enablePower (GPIO_Regs *gpio)
 Enables the Peripheral Write Enable (PWREN) register for the GPIO. More...
 
__STATIC_INLINE void DL_GPIO_disablePower (GPIO_Regs *gpio)
 Disables the Peripheral Write Enable (PWREN) register for the GPIO. More...
 
__STATIC_INLINE bool DL_GPIO_isPowerEnabled (GPIO_Regs *gpio)
 Returns if the Peripheral Write Enable (PWREN) register for the GPIO is enabled. More...
 
__STATIC_INLINE void DL_GPIO_reset (GPIO_Regs *gpio)
 Resets gpio peripheral. More...
 
__STATIC_INLINE bool DL_GPIO_isReset (GPIO_Regs *gpio)
 Returns if gpio peripheral was reset. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalOutput (uint32_t pincmIndex)
 Configures a pin as a basic GPIO output. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalOutputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ)
 Configures a pin as a GPIO output. More...
 
__STATIC_INLINE void DL_GPIO_setDigitalInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor)
 Configures internal resistor for digital pin. More...
 
__STATIC_INLINE void DL_GPIO_setAnalogInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor)
 Configures internal resistor for analog pin. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalInput (uint32_t pincmIndex)
 Configures a pin as a basic GPIO input. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalInputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup)
 Configures a pin as a GPIO input. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral output functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ)
 Configure a pin to operate with peripheral output functionality with optional features. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralInputFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral input functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralInputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup)
 Configure a pin to operate with peripheral input functionality with optional features. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralAnalogFunction (uint32_t pincmIndex)
 Configure a pin to operate with analog functionality. More...
 
__STATIC_INLINE void DL_GPIO_enableWakeUp (uint32_t pincmIndex)
 Set GPIO pin's wakeup enable bit. More...
 
__STATIC_INLINE void DL_GPIO_disableWakeUp (uint32_t pincmIndex)
 Clear GPIO pin's wakeup enable bit. More...
 
__STATIC_INLINE bool DL_GPIO_isWakeUpEnabled (uint32_t pincmIndex)
 Returns if GPIO pin's wake up bit is enabled. More...
 
__STATIC_INLINE void DL_GPIO_setWakeupCompareValue (uint32_t pincmIndex, DL_GPIO_WAKEUP_COMPARE_VALUE value)
 Set the compare value to use for wake for the specified pin. More...
 
__STATIC_INLINE DL_GPIO_WAKEUP_COMPARE_VALUE DL_GPIO_getWakeupCompareValue (uint32_t pincmIndex)
 Get the compare value to use for wake for the specified pin. More...
 
__STATIC_INLINE bool DL_GPIO_isWakeStateGenerated (uint32_t pincmIndex)
 Checks if the GPIO pin's Wake State bit is active. More...
 
__STATIC_INLINE uint32_t DL_GPIO_readPins (GPIO_Regs *gpio, uint32_t pins)
 Read a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_writePins (GPIO_Regs *gpio, uint32_t pins)
 Write a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_writePinsVal (GPIO_Regs *gpio, uint32_t pinsMask, uint32_t pinsVal)
 Update the value of one or more GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_setPins (GPIO_Regs *gpio, uint32_t pins)
 Set a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_clearPins (GPIO_Regs *gpio, uint32_t pins)
 Clear a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_togglePins (GPIO_Regs *gpio, uint32_t pins)
 Toggle a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_enableOutput (GPIO_Regs *gpio, uint32_t pins)
 Enable output on a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_disableOutput (GPIO_Regs *gpio, uint32_t pins)
 Disable output on a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_enableDMAAccess (GPIO_Regs *gpio, uint32_t pins)
 Enable DMA access on a group of pins. More...
 
__STATIC_INLINE void DL_GPIO_disableDMAAccess (GPIO_Regs *gpio, uint32_t pins)
 Disable DMA access on a group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_isDMAccessEnabled (GPIO_Regs *gpio, uint32_t pins)
 Check if DMA access is enabled on a group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setLowerPinsPolarity (GPIO_Regs *gpio, uint32_t polarity)
 Set the polarity of all bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setUpperPinsPolarity (GPIO_Regs *gpio, uint32_t polarity)
 Set the polarity of all bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsPolarity (GPIO_Regs *gpio)
 Get the polarity of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsPolarity (GPIO_Regs *gpio)
 Get the polarity of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setLowerPinsInputFilter (GPIO_Regs *gpio, uint32_t filter)
 Set the input filter of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setUpperPinsInputFilter (GPIO_Regs *gpio, uint32_t filter)
 Set the input filter of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsInputFilter (GPIO_Regs *gpio)
 Get the input filter of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsInputFilter (GPIO_Regs *gpio)
 Get the input filter of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_enableGlobalFastWake (GPIO_Regs *gpio)
 Enable Global Fast Wake. More...
 
__STATIC_INLINE void DL_GPIO_disableGlobalFastWake (GPIO_Regs *gpio)
 Disable Global Fast Wake. More...
 
__STATIC_INLINE void DL_GPIO_enableFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Enable fast wake for pins. More...
 
__STATIC_INLINE void DL_GPIO_disableFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Disable fast wake for pins. More...
 
__STATIC_INLINE void DL_GPIO_enableHiZ (uint32_t pincmIndex)
 Enable Hi-Z for the pin. More...
 
__STATIC_INLINE void DL_GPIO_disableHiZ (uint32_t pincmIndex)
 Disable Hi-Z for the pin. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Check which pins have fast wake feature enabled. More...
 
__STATIC_INLINE void DL_GPIO_enableInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Enable GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_disableInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Disable GPIO interrupts. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterrupts (GPIO_Regs *gpio, uint32_t pins)
 Check which GPIO interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Check interrupt flag of enabled GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_setInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Set interrupt flag of any GPIO. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getRawInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Check interrupt flag of any GPIO interrupt. More...
 
__STATIC_INLINE DL_GPIO_IIDX DL_GPIO_getPendingInterrupt (GPIO_Regs *gpio)
 Get highest priority pending GPIO interrupt. More...
 
__STATIC_INLINE void DL_GPIO_clearInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Clear pending GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_configSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, DL_GPIO_SUBSCRIBER_OUT_POLICY policy, DL_GPIO_SUBSCRIBERx_PIN pinIndex)
 Configures GPIO subscriber. This API preserves enable/disbale status of subscriber. More...
 
__STATIC_INLINE void DL_GPIO_enableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Enables GPIO subscriber. More...
 
__STATIC_INLINE void DL_GPIO_disableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Disables GPIO subscriber. More...
 
__STATIC_INLINE bool DL_GPIO_isSubscriberEnabled (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Returns if GPIO subscriber is enabled. More...
 
__STATIC_INLINE void DL_GPIO_setPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index, uint8_t chanID)
 Sets the event publisher channel id. More...
 
__STATIC_INLINE uint8_t DL_GPIO_getPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index)
 Gets the event publisher channel id. More...
 
__STATIC_INLINE void DL_GPIO_setSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, uint8_t chanID)
 Sets the event subscriber channel id. More...
 
__STATIC_INLINE uint8_t DL_GPIO_getSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Gets the event subscriber channel id. More...
 
__STATIC_INLINE void DL_GPIO_enableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Enables GPIO events. More...
 
__STATIC_INLINE void DL_GPIO_disableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Disable GPIO events. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Check which GPIO events are enabled. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Checks if any of the GPIO events which were previously enabled are pending. More...
 
__STATIC_INLINE void DL_GPIO_clearEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Clear pending GPIO event. More...
 
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale