88 #ifndef ALGOLIB_FOC_INCLUDE_ABNORMALSPEEDSTALLDETECT_H_ 89 #define ALGOLIB_FOC_INCLUDE_ABNORMALSPEEDSTALLDETECT_H_ 155 *pAbnormalSpeedStall)
Abnormal Speed Detect flags Structure.
Definition: abnormalSpeedStallDetect.h:94
Abnormal Speed Detect Working Structure.
Definition: abnormalSpeedStallDetect.h:117
void abnormalSpeedStallDetectRun(ABNORMAL_SPEED_STALL_DETECT_T *pAbnormalSpeed)
Abnormal Speed Detect Run.
Definition: abnormalSpeedStallDetect.c:84
ABNORMAL_SPEED_STALL_DETECT_FLAGS_T flags
Definition: abnormalSpeedStallDetect.h:135
int32_t maximumSpeed
Definition: abnormalSpeedStallDetect.h:125
_Bool getAbnormalSpeedStallDetectStatus(ABNORMAL_SPEED_STALL_DETECT_T *pAbnormalSpeedStall)
Abnormal Speed Detect Status check.
Definition: abnormalSpeedStallDetect.h:154
uint16_t countMax
Definition: abnormalSpeedStallDetect.h:129
uint16_t w
Definition: abnormalSpeedStallDetect.h:112
_Bool status
Definition: abnormalSpeedStallDetect.h:101
Abnormal Speed Detect flags.
Definition: abnormalSpeedStallDetect.h:97
void abnormalSpeedStallDetectInit(ABNORMAL_SPEED_STALL_DETECT_T *pAbnormalSpeed)
Abnormal Speed Detect Init.
Definition: abnormalSpeedStallDetect.c:78
struct ABNORMAL_SPEED_STALL_DETECT_FLAGS_T::abnormalSpeedStallDetectFlags b
const int32_t * pSpeed
Definition: abnormalSpeedStallDetect.h:121