MSPM0L111X TI-Driver Library  2.05.01.00
Data Structures | Macros | Enumerations
ADCMSPM0.h File Reference

Detailed Description

ADC driver implementation for the ADC peripheral on MSPM0 devices.


#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ADC.h>
#include <ti/driverlib/dl_adc12.h>
#include <ti/devices/DeviceFamily.h>
Include dependency graph for ADCMSPM0.h:

Go to the source code of this file.

Data Structures

struct  ADCMSPM0_HWAttrs
 ADCMSPM0 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. Currently the Single channel single conversion and the Repeat single channel conversion are supported. For the other conversion modes, user has to modify or add the needed parameters to below structure. More...
 
struct  ADCMSPM0_Object
 ADCMSPM0 Object. More...
 

Macros

#define ADC_ALL_INTERRUPTS_MASK   0xFFFFFFFFUL
 

Enumerations

enum  ADCMSPM0_Resolution_Bits {
  ADCMSPM0_RESOLUTION_12_BIT = DL_ADC12_SAMP_CONV_RES_12_BIT,
  ADCMSPM0_RESOLUTION_10_BIT = DL_ADC12_SAMP_CONV_RES_10_BIT,
  ADCMSPM0_RESOLUTION_8_BIT = DL_ADC12_SAMP_CONV_RES_8_BIT
}
 Resolution of ADC-conversion. More...
 
enum  ADCMSPM0_Reference_Source {
  ADCMSPM0_VDDA_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_VDDA,
  ADCMSPM0_INTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_INTREF,
  ADCMSPM0_EXTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_EXTREF
}
 Specifies the source of the ADC reference voltage. More...
 
enum  ADCMSPM0_Clock_Divider {
  ADCMSPM0_CLKDIV_1 = DL_ADC12_CLOCK_DIVIDE_1,
  ADCMSPM0_CLKDIV_2 = DL_ADC12_CLOCK_DIVIDE_2,
  ADCMSPM0_CLKDIV_4 = DL_ADC12_CLOCK_DIVIDE_4,
  ADCMSPM0_CLKDIV_8 = DL_ADC12_CLOCK_DIVIDE_8,
  ADCMSPM0_CLKDIV_16 = DL_ADC12_CLOCK_DIVIDE_16,
  ADCMSPM0_CLKDIV_24 = DL_ADC12_CLOCK_DIVIDE_24,
  ADCMSPM0_CLKDIV_32 = DL_ADC12_CLOCK_DIVIDE_32,
  ADCMSPM0_CLKDIV_48 = DL_ADC12_CLOCK_DIVIDE_48
}
 ADC clock-divider. More...
 
enum  ADCMSPM0_Clock_Select {
  ADCMSPM0_CLK_SYSOSC = DL_ADC12_CLOCK_SYSOSC,
  ADCMSPM0_CLK_ULPCLK = DL_ADC12_CLOCK_ULPCLK,
  ADCMSPM0_CLK_HFCLK = DL_ADC12_CLOCK_HFCLK
}
 ADC clock source select. More...
 
enum  ADCMSPM0_Freq_Range {
  ADCMSPM0_CLK_FREQ_RANGE_1TO4 = DL_ADC12_CLOCK_FREQ_RANGE_1_TO_4,
  ADCMSPM0_CLK_FREQ_RANGE_4TO8 = DL_ADC12_CLOCK_FREQ_RANGE_4_TO_8,
  ADCMSPM0_CLK_FREQ_RANGE_8TO16 = DL_ADC12_CLOCK_FREQ_RANGE_8_TO_16,
  ADCMSPM0_CLK_FREQ_RANGE_16TO20 = DL_ADC12_CLOCK_FREQ_RANGE_16_TO_20,
  ADCMSPM0_CLK_FREQ_RANGE_20TO24 = DL_ADC12_CLOCK_FREQ_RANGE_20_TO_24,
  ADCMSPM0_CLK_FREQ_RANGE_24TO32 = DL_ADC12_CLOCK_FREQ_RANGE_24_TO_32,
  ADCMSPM0_CLK_FREQ_RANGE_32TO40 = DL_ADC12_CLOCK_FREQ_RANGE_32_TO_40,
  ADCMSPM0_CLK_FREQ_RANGE_40TO48 = DL_ADC12_CLOCK_FREQ_RANGE_40_TO_48
}
 ADC clock freq range. More...
 
enum  ADCMSPM0_Conversion_Mode {
  ADCMSPM0_SINGLE_CH_SINGLE_CONV = DL_ADC12_SAMP_MODE_SINGLE,
  ADCMSPM0_MULTI_CH_SEQUENCE_CONV = DL_ADC12_SAMP_MODE_SEQUENCE
}
 ADC conversion mode. More...
 
enum  ADCMSPM0_Repeat_Conversion_Mode {
  ADCMSPM0_REPEAT_MODE_ENABLED = DL_ADC12_REPEAT_MODE_ENABLED,
  ADCMSPM0_REPEAT_MODE_DISABLED = DL_ADC12_REPEAT_MODE_DISABLED
}
 ADC Repeat conversion mode. More...
 
enum  ADCMSPM0_Sampling_Mode {
  ADCMSPM0_SAMPLING_MODE_AUTO = DL_ADC12_SAMPLING_SOURCE_AUTO,
  ADCMSPM0_SAMPLING_MODE_MANUAL = DL_ADC12_SAMPLING_SOURCE_MANUAL
}
 ADC sampling mode. More...
 
enum  ADCMSPM0_Sampling_Trg {
  ADCMSPM0_SAMPLING_TRIG_SW = DL_ADC12_TRIG_SRC_SOFTWARE,
  ADCMSPM0_SAMPLING_TRIG_EVENT = DL_ADC12_TRIG_SRC_EVENT
}
 ADC sampling trigger source. More...
 
enum  ADCMSPM0_Conv_Data_Format {
  ADCMSPM0_CONV_DATA_FORMAT_UNSIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_UNSIGNED,
  ADCMSPM0_CONV_DATA_FORMAT_SIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_SIGNED
}
 ADC conversion data format. More...
 
enum  ADCMSPM0_Sample_Timer_Source {
  ADCMSPM0_SAMP_TMR_SOURCE_SCOMP0 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0,
  ADCMSPM0_SAMP_TMR_SOURCE_SCOMP1 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP1
}
 ADC sample timer source. More...
 
enum  ADCMSPM0_Conv_Trig_Src {
  ADCMSPM0_NEXT_CONV_AUTO = DL_ADC12_TRIGGER_MODE_AUTO_NEXT,
  ADCMSPM0_NEXT_CONV_WITH_TRIG = DL_ADC12_TRIGGER_MODE_TRIGGER_NEXT
}
 ADC conversion trigger. More...
 
enum  ADCMSPM0_HW_Avg {
  ADCMSPM0_HW_AVG_ENABLED = DL_ADC12_AVERAGING_MODE_ENABLED,
  ADCMSPM0_HW_AVG_DISABLED = DL_ADC12_AVERAGING_MODE_DISABLED
}
 ADC HW averaging. More...
 
enum  ADCMSPM0_AVGN {
  ADCMSPM0_HW_AVG_NUM_ACC_DISABLED = DL_ADC12_HW_AVG_NUM_ACC_DISABLED,
  ADCMSPM0_HW_AVG_NUM_ACC_2 = DL_ADC12_HW_AVG_NUM_ACC_2,
  ADCMSPM0_HW_AVG_NUM_ACC_4 = DL_ADC12_HW_AVG_NUM_ACC_4,
  ADCMSPM0_HW_AVG_NUM_ACC_8 = DL_ADC12_HW_AVG_NUM_ACC_8,
  ADCMSPM0_HW_AVG_NUM_ACC_16 = DL_ADC12_HW_AVG_NUM_ACC_16,
  ADCMSPM0_HW_AVG_NUM_ACC_32 = DL_ADC12_HW_AVG_NUM_ACC_32,
  ADCMSPM0_HW_AVG_NUM_ACC_64 = DL_ADC12_HW_AVG_NUM_ACC_64,
  ADCMSPM0_HW_AVG_NUM_ACC_128 = DL_ADC12_HW_AVG_NUM_ACC_128
}
 Hardware averager numerator. More...
 
enum  ADCMSPM0_AVGD {
  ADCMSPM0_HW_AVG_DEN_DIV_BY_1 = DL_ADC12_HW_AVG_DEN_DIV_BY_1,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_2 = DL_ADC12_HW_AVG_DEN_DIV_BY_2,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_4 = DL_ADC12_HW_AVG_DEN_DIV_BY_4,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_8 = DL_ADC12_HW_AVG_DEN_DIV_BY_8,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_16 = DL_ADC12_HW_AVG_DEN_DIV_BY_16,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_32 = DL_ADC12_HW_AVG_DEN_DIV_BY_32,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_64 = DL_ADC12_HW_AVG_DEN_DIV_BY_64,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_128 = DL_ADC12_HW_AVG_DEN_DIV_BY_128
}
 Hardware averager denominator. More...
 
enum  ADCMSPM0_Pwr_Dn_Mode {
  ADCMSPM0_Pwr_Dn_MODE_AUTO = DL_ADC12_POWER_DOWN_MODE_AUTO,
  ADCMSPM0_Pwr_Dn_MODE_MANUAL = DL_ADC12_POWER_DOWN_MODE_MANUAL
}
 ADC power down mode. More...
 
enum  ADCMSPM0_CONV_START_ADDRESS {
  ADCMSPM0_SEQ_START_ADDR_00 = DL_ADC12_SEQ_START_ADDR_00,
  ADCMSPM0_SEQ_START_ADDR_01 = DL_ADC12_SEQ_START_ADDR_01,
  ADCMSPM0_SEQ_START_ADDR_02 = DL_ADC12_SEQ_START_ADDR_02,
  ADCMSPM0_SEQ_START_ADDR_03 = DL_ADC12_SEQ_START_ADDR_03,
  ADCMSPM0_SEQ_START_ADDR_04 = DL_ADC12_SEQ_START_ADDR_04,
  ADCMSPM0_SEQ_START_ADDR_05 = DL_ADC12_SEQ_START_ADDR_05,
  ADCMSPM0_SEQ_START_ADDR_06 = DL_ADC12_SEQ_START_ADDR_06,
  ADCMSPM0_SEQ_START_ADDR_07 = DL_ADC12_SEQ_START_ADDR_07,
  ADCMSPM0_SEQ_START_ADDR_08 = DL_ADC12_SEQ_START_ADDR_08,
  ADCMSPM0_SEQ_START_ADDR_09 = DL_ADC12_SEQ_START_ADDR_09,
  ADCMSPM0_SEQ_START_ADDR_10 = DL_ADC12_SEQ_START_ADDR_10,
  ADCMSPM0_SEQ_START_ADDR_11 = DL_ADC12_SEQ_START_ADDR_11
}
 Sequence start address. More...
 
enum  ADCMSPM0_CONV_END_ADDRESS {
  ADCMSPM0_SEQ_END_ADDR_00 = DL_ADC12_SEQ_END_ADDR_00,
  ADCMSPM0_SEQ_END_ADDR_01 = DL_ADC12_SEQ_END_ADDR_01,
  ADCMSPM0_SEQ_END_ADDR_02 = DL_ADC12_SEQ_END_ADDR_02,
  ADCMSPM0_SEQ_END_ADDR_03 = DL_ADC12_SEQ_END_ADDR_03,
  ADCMSPM0_SEQ_END_ADDR_04 = DL_ADC12_SEQ_END_ADDR_04,
  ADCMSPM0_SEQ_END_ADDR_05 = DL_ADC12_SEQ_END_ADDR_05,
  ADCMSPM0_SEQ_END_ADDR_06 = DL_ADC12_SEQ_END_ADDR_06,
  ADCMSPM0_SEQ_END_ADDR_07 = DL_ADC12_SEQ_END_ADDR_07,
  ADCMSPM0_SEQ_END_ADDR_08 = DL_ADC12_SEQ_END_ADDR_08,
  ADCMSPM0_SEQ_END_ADDR_09 = DL_ADC12_SEQ_END_ADDR_09,
  ADCMSPM0_SEQ_END_ADDR_10 = DL_ADC12_SEQ_END_ADDR_10,
  ADCMSPM0_SEQ_END_ADDR_11 = DL_ADC12_SEQ_END_ADDR_11
}
 Sequence end address. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale