![]() |
![]() |
|
MSPM0GX51X TI-Driver Library
2.05.01.00
|
DMA driver implementation for MSPM0.
#include <stdbool.h>#include <stdint.h>#include <ti/driverlib/dl_dma.h>#include <ti/drivers/dpl/HwiP.h>

Go to the source code of this file.
Data Structures | |
| struct | DMAMSPM0_HWAttrs |
| DMAMSPM0 Hardware attributes. More... | |
| struct | DMAMSPM0_Transfer |
| DMAMSPM0 channel based Transfer configuration. More... | |
| struct | DMAMSPM0_Object |
| DMAMSPM0 object. More... | |
| struct | DMAMSPM0_Cfg |
| DMAMSPM0 Global configuration. More... | |
Macros | |
| #define | NUM_DMA_CHANNELS (DMA_SYS_N_DMA_CHANNEL) |
| Number of DMA channels supported by Device. The same can be used to define the number of interrupts. More... | |
Typedefs | |
| typedef void(* | DMAMSPM0_IsrFxn) (uintptr_t arg) |
| DMA error function pointers. | |
| typedef DMAMSPM0_Cfg * | DMAMSPM0_Handle |
| A handle that is returned from a DMAMSPM0_open() call. | |
Functions | |
| void | DMAMSPM0_close (DMA_Regs *handle, uint8_t channelNum) |
| Function to close the DMA channel. More... | |
| bool | DMAMSPM0_init (void) |
| Function to initialize the MSPM0 DMA driver. More... | |
| DMAMSPM0_Handle | DMAMSPM0_open (uint_least8_t index, uint8_t channelNum) |
| Function to initialize the MSPM0 DMA peripheral and corresponding interrupt. More... | |
| bool | DMAMSPM0_setupTransfer (DMAMSPM0_Transfer *transfer, DL_DMA_Config *DMACfg) |
| Function to set up a DMA channel for data transfer. More... | |
| DMAMSPM0_Handle | DMA_Init (DMAMSPM0_Transfer *dmaParams, DL_DMA_Config *DMACfg, uint8_t noOfChs) |
| One Function that initialize DMA by calling all needed functions in sequence. User may call this function to initialize DMA without calling other needed functions separately. More... | |
| void | DMAMSPM0_disableChannel (DMAMSPM0_Handle handle, uint8_t dmaChannel) |
| This function will disable the channel and related flags. More... | |
| uint16_t | DMAMSPM0_getCurrTransferSize (uint8_t dmaChannel) |
| This function will return the DMA transfer size in bytes for given channel. More... | |
| void | DMA_Params_init (DMAMSPM0_Transfer *params) |
| This function will initialize the default params. More... | |
| void | DMAMSPM0_copyDMAParams (DMAMSPM0_Transfer *dmaParams, DL_DMA_Config *dmaConfig) |
| This function will extract parameters from DMA Config struct to DMA Transfer struct. More... | |
Variables | |
| const DMAMSPM0_Cfg | DMAMSPM0_Config [] |
| Instance of a DMA Config structure. | |
| const uint_least8_t | DMA_Count |
| Number of DMA channels. | |