47 #ifndef ti_dl_dl_common__include 48 #define ti_dl_dl_common__include 50 #include <ti/devices/msp/msp.h> 64 volatile uint32_t *reg, uint32_t val, uint32_t mask)
70 *reg = tmp | (val & mask);
__STATIC_INLINE void DL_Common_updateReg(volatile uint32_t *reg, uint32_t val, uint32_t mask)
Writes value to specified register - retaining bits unaffected by mask.
Definition: dl_common.h:63
void DL_Common_delayCycles(uint32_t cycles)
Consumes the number of CPU cycles specified.