MSPM0L111X Driver Library  2.05.01.00
Macros | Functions
dl_systick.h File Reference

Detailed Description

System Tick Timer (SysTick) Driver Library.


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
Include dependency graph for dl_systick.h:

Go to the source code of this file.

Macros

#define DL_SYSTICK_config(x)   SysTick_Config(x)
 Redirects DL_SYSTICK_config to CMSIS standard SysTick_Config.
 

Functions

__STATIC_INLINE void DL_SYSTICK_init (uint32_t period)
 Initializes the System Tick Timer (SysTick) More...
 
__STATIC_INLINE void DL_SYSTICK_setPeriod (uint32_t period)
 Set the period for the SysTick. More...
 
__STATIC_INLINE void DL_SYSTICK_resetValue (void)
 Reset the current value of the SysTick. More...
 
__STATIC_INLINE uint32_t DL_SYSTICK_getPeriod (void)
 Get the period for the SysTick. More...
 
__STATIC_INLINE uint32_t DL_SYSTICK_getValue (void)
 Get the current value of SysTick counter. More...
 
__STATIC_INLINE void DL_SYSTICK_enableInterrupt (void)
 Enable the SysTick interrupt.
 
__STATIC_INLINE void DL_SYSTICK_disableInterrupt (void)
 Disable the SysTick interrupt.
 
__STATIC_INLINE void DL_SYSTICK_enable (void)
 Enable the SysTick, starts counting once enabled. More...
 
__STATIC_INLINE void DL_SYSTICK_disable (void)
 Disable the SysTick, stops counting once disabled.
 
__STATIC_INLINE bool DL_SYSTICK_isEnabled (void)
 Checks if the SysTick is enabled. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale