51 #ifndef ti_dl_dl_mcan__include 52 #define ti_dl_dl_mcan__include 57 #include <ti/devices/msp/msp.h> 60 #ifdef __MSPM0_HAS_MCAN__ 71 #define DL_MCAN_INTR_MASK_ALL (MCAN_IR_RF0N_MASK | \ 104 #define DL_MCAN_MAX_PAYLOAD_BYTES (64U) 113 #define DL_MCAN_INTERRUPT_ARA (MCAN_IR_ARA_MASK) 118 #define DL_MCAN_INTERRUPT_PED (MCAN_IR_PED_MASK) 123 #define DL_MCAN_INTERRUPT_PEA (MCAN_IR_PEA_MASK) 128 #define DL_MCAN_INTERRUPT_WDI (MCAN_IR_WDI_MASK) 133 #define DL_MCAN_INTERRUPT_BO (MCAN_IR_BO_MASK) 138 #define DL_MCAN_INTERRUPT_EW (MCAN_IR_EW_MASK) 143 #define DL_MCAN_INTERRUPT_EP (MCAN_IR_EP_MASK) 148 #define DL_MCAN_INTERRUPT_ELO (MCAN_IR_ELO_MASK) 153 #define DL_MCAN_INTERRUPT_BEU (MCAN_IR_BEU_MASK) 158 #define DL_MCAN_INTERRUPT_DRX (MCAN_IR_DRX_MASK) 163 #define DL_MCAN_INTERRUPT_TOO (MCAN_IR_TOO_MASK) 168 #define DL_MCAN_INTERRUPT_MRAF (MCAN_IR_MRAF_MASK) 173 #define DL_MCAN_INTERRUPT_TSW (MCAN_IR_TSW_MASK) 178 #define DL_MCAN_INTERRUPT_TEFL (MCAN_IR_TEFL_MASK) 183 #define DL_MCAN_INTERRUPT_TEFF (MCAN_IR_TEFF_MASK) 188 #define DL_MCAN_INTERRUPT_TEFW (MCAN_IR_TEFW_MASK) 193 #define DL_MCAN_INTERRUPT_TEFN (MCAN_IR_TEFN_MASK) 198 #define DL_MCAN_INTERRUPT_TFE (MCAN_IR_TFE_MASK) 203 #define DL_MCAN_INTERRUPT_TCF (MCAN_IR_TCF_MASK) 208 #define DL_MCAN_INTERRUPT_TC (MCAN_IR_TC_MASK) 213 #define DL_MCAN_INTERRUPT_HPM (MCAN_IR_HPM_MASK) 218 #define DL_MCAN_INTERRUPT_RF1L (MCAN_IR_RF1L_MASK) 223 #define DL_MCAN_INTERRUPT_RF1F (MCAN_IR_RF1F_MASK) 228 #define DL_MCAN_INTERRUPT_RF1W (MCAN_IR_RF1W_MASK) 233 #define DL_MCAN_INTERRUPT_RF1N (MCAN_IR_RF1N_MASK) 238 #define DL_MCAN_INTERRUPT_RF0L (MCAN_IR_RF0L_MASK) 243 #define DL_MCAN_INTERRUPT_RF0F (MCAN_IR_RF0F_MASK) 248 #define DL_MCAN_INTERRUPT_RF0W (MCAN_IR_RF0W_MASK) 253 #define DL_MCAN_INTERRUPT_RF0N (MCAN_IR_RF0N_MASK) 263 #define DL_MCAN_MSP_INTERRUPT_WAKEUP (MCAN_IMASK_WAKEUP_SET) 268 #define DL_MCAN_MSP_INTERRUPT_TIMESTAMP_OVERFLOW (MCAN_IMASK_EXT_TS_CNTR_OVFL_SET) 273 #define DL_MCAN_MSP_INTERRUPT_DOUBLE_ERROR_DETECTION (MCAN_IMASK_DED_SET) 278 #define DL_MCAN_MSP_INTERRUPT_SINGLE_ERROR_CORRECTION (MCAN_IMASK_SEC_SET) 283 #define DL_MCAN_MSP_INTERRUPT_LINE1 (MCAN_IMASK_INTL1_SET) 288 #define DL_MCAN_MSP_INTERRUPT_LINE0 (MCAN_IMASK_INTL0_SET) 298 #define DL_MCAN_INTR_SRC_RX_FIFO0_NEW_MSG (MCAN_IR_RF0N_MASK) 303 #define DL_MCAN_INTR_SRC_RX_FIFO0_WATERMARK (MCAN_IR_RF0W_MASK) 308 #define DL_MCAN_INTR_SRC_RX_FIFO0_FULL (MCAN_IR_RF0F_MASK) 313 #define DL_MCAN_INTR_SRC_RX_FIFO0_MSG_LOST (MCAN_IR_RF0L_MASK) 318 #define DL_MCAN_INTR_SRC_RX_FIFO1_NEW_MSG (MCAN_IR_RF1N_MASK) 323 #define DL_MCAN_INTR_SRC_RX_FIFO1_WATERMARK (MCAN_IR_RF1W_MASK) 328 #define DL_MCAN_INTR_SRC_RX_FIFO1_FULL (MCAN_IR_RF1F_MASK) 333 #define DL_MCAN_INTR_SRC_RX_FIFO1_MSG_LOST (MCAN_IR_RF1L_MASK) 338 #define DL_MCAN_INTR_SRC_HIGH_PRIO_MSG (MCAN_IR_HPM_MASK) 343 #define DL_MCAN_INTR_SRC_TRANS_COMPLETE (MCAN_IR_TC_MASK) 348 #define DL_MCAN_INTR_SRC_TRANS_CANCEL_FINISH (MCAN_IR_TCF_MASK) 353 #define DL_MCAN_INTR_SRC_TX_FIFO_EMPTY (MCAN_IR_TFE_MASK) 358 #define DL_MCAN_INTR_SRC_TX_EVT_FIFO_NEW_ENTRY (MCAN_IR_TEFN_MASK) 363 #define DL_MCAN_INTR_SRC_TX_EVT_FIFO_WATERMARK (MCAN_IR_TEFW_MASK) 368 #define DL_MCAN_INTR_SRC_TX_EVT_FIFO_FULL (MCAN_IR_TEFF_MASK) 373 #define DL_MCAN_INTR_SRC_TX_EVT_FIFO_ELEM_LOST (MCAN_IR_TEFL_MASK) 378 #define DL_MCAN_INTR_SRC_TIMESTAMP_WRAPAROUND (MCAN_IR_TSW_MASK) 383 #define DL_MCAN_INTR_SRC_MSG_RAM_ACCESS_FAILURE (MCAN_IR_MRAF_MASK) 388 #define DL_MCAN_INTR_SRC_TIMEOUT (MCAN_IR_TOO_MASK) 393 #define DL_MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG (MCAN_IR_DRX_MASK) 398 #define DL_MCAN_INTR_SRC_BIT_ERR_UNCORRECTED (MCAN_IR_BEU_MASK) 403 #define DL_MCAN_INTR_SRC_ERR_LOG_OVRFLW (MCAN_IR_ELO_MASK) 408 #define DL_MCAN_INTR_SRC_ERR_PASSIVE (MCAN_IR_EP_MASK) 413 #define DL_MCAN_INTR_SRC_WARNING_STATUS (MCAN_IR_EW_MASK) 418 #define DL_MCAN_INTR_SRC_BUS_OFF_STATUS (MCAN_IR_BO_MASK) 423 #define DL_MCAN_INTR_SRC_WATCHDOG (MCAN_IR_WDI_MASK) 428 #define DL_MCAN_INTR_SRC_PROTOCOL_ERR_ARB (MCAN_IR_PEA_MASK) 433 #define DL_MCAN_INTR_SRC_PROTOCOL_ERR_DATA (MCAN_IR_PED_MASK) 438 #define DL_MCAN_INTR_SRC_RES_ADDR_ACCESS (MCAN_IR_ARA_MASK) 446 #define DL_MCAN_DBTP_DSJW_MAX (0xFU) 450 #define DL_MCAN_DBTP_DTSEG2_MAX (0xFU) 454 #define DL_MCAN_DBTP_DTSEG1_MAX (0x1FU) 458 #define DL_MCAN_DBTP_DBRP_MAX (0x1FU) 462 #define DL_MCAN_NBTP_NSJW_MAX (0x7FU) 466 #define DL_MCAN_NBTP_NTSEG2_MAX (0x7FU) 470 #define DL_MCAN_NBTP_NTSEG1_MAX (0xFFU) 474 #define DL_MCAN_NBTP_NBRP_MAX (0x1FFU) 478 #define DL_MCAN_RWD_WDC_MAX (0xFFU) 482 #define DL_MCAN_TDCR_TDCF_MAX (0x7FU) 486 #define DL_MCAN_TDCR_TDCO_MAX (0x7FU) 490 #define DL_MCAN_XIDAM_EIDM_MAX (0x1FFFFFFFU) 494 #define DL_MCAN_TSCC_TCP_MAX (0xFU) 498 #define DL_MCAN_TOCC_TOP_MAX (0xFFFFU) 2050 MCAN_Regs *mcan, uint32_t intrMask, uint32_t lineNum);
2128 MCAN_Regs *mcan, uint32_t fifoNum, uint32_t idx);
2189 MCAN_Regs *mcan, uint32_t bufNum,
bool enable);
2203 const MCAN_Regs *mcan, uint32_t bufNum,
bool enable);
2579 mcan->MCANSS.PWREN = (MCAN_PWREN_KEY_UNLOCK_W | MCAN_PWREN_ENABLE_ENABLE);
2594 mcan->MCANSS.PWREN = (MCAN_PWREN_KEY_UNLOCK_W | MCAN_PWREN_ENABLE_DISABLE);
2615 return ((mcan->MCANSS.PWREN & MCAN_PWREN_ENABLE_MASK) ==
2616 MCAN_PWREN_ENABLE_ENABLE);
2626 mcan->MCANSS.RSTCTL =
2627 (MCAN_RSTCTL_KEY_UNLOCK_W | MCAN_RSTCTL_RESETSTKYCLR_CLR |
2628 MCAN_RSTCTL_RESETASSERT_ASSERT);
2642 return ((mcan->MCANSS.STAT & MCAN_STAT_RESETSTKY_MASK) ==
2643 MCAN_STAT_RESETSTKY_RESET);
2655 MCAN_Regs *mcan, uint32_t interruptMask)
2657 mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.IMASK |= interruptMask;
2669 MCAN_Regs *mcan, uint32_t interruptMask)
2671 mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.IMASK &= ~(interruptMask);
2687 const MCAN_Regs *mcan, uint32_t interruptMask)
2689 return (mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.IMASK & interruptMask);
2708 const MCAN_Regs *mcan, uint32_t interruptMask)
2710 return (mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.MIS & interruptMask);
2729 const MCAN_Regs *mcan, uint32_t interruptMask)
2731 return (mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.RIS & interruptMask);
2749 return ((DL_MCAN_IIDX) mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.IIDX);
2761 MCAN_Regs *mcan, uint32_t interruptMask)
2763 mcan->MCANSS.TI_WRAPPER.MSP.CPU_INT.ICLR = interruptMask;
2776 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKEN &
2777 MCAN_CLKEN_CLK_REQEN_MASK) == MCAN_CLKEN_CLK_REQEN_SET);
2788 mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKEN = MCAN_CLKEN_CLK_REQEN_SET;
2799 mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKEN = MCAN_CLKEN_CLK_REQEN_CLR;
2813 mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKDIV & MCAN_CLKDIV_RATIO_MASK);
2826 MCAN_Regs *mcan, uint32_t clkdiv)
2829 MCAN_CLKDIV_RATIO_MASK);
2841 const MCAN_Regs *mcan)
2843 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKCTL &
2844 MCAN_CLKCTL_STOPREQ_MASK) == MCAN_CLKCTL_STOPREQ_ENABLE);
2856 MCAN_CLKCTL_STOPREQ_ENABLE, MCAN_CLKCTL_STOPREQ_MASK);
2868 MCAN_CLKCTL_STOPREQ_DISABLE, MCAN_CLKCTL_STOPREQ_MASK);
2881 const MCAN_Regs *mcan)
2883 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKCTL &
2884 MCAN_CLKCTL_WAKEUP_INT_EN_MASK) ==
2885 MCAN_CLKCTL_WAKEUP_INT_EN_ENABLE);
2897 MCAN_CLKCTL_WAKEUP_INT_EN_ENABLE, MCAN_CLKCTL_WAKEUP_INT_EN_MASK);
2909 MCAN_CLKCTL_WAKEUP_INT_EN_DISABLE, MCAN_CLKCTL_WAKEUP_INT_EN_MASK);
2925 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKCTL &
2926 MCAN_CLKCTL_WKUP_GLTFLT_EN_MASK) ==
2927 MCAN_CLKCTL_WKUP_GLTFLT_EN_ENABLE);
2942 MCAN_CLKCTL_WKUP_GLTFLT_EN_ENABLE, MCAN_CLKCTL_WKUP_GLTFLT_EN_MASK);
2957 MCAN_CLKCTL_WKUP_GLTFLT_EN_DISABLE, MCAN_CLKCTL_WKUP_GLTFLT_EN_MASK);
2969 const MCAN_Regs *mcan)
2971 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKSTS &
2972 MCAN_CLKSTS_CLKSTOP_ACKSTS_MASK) ==
2973 MCAN_CLKSTS_CLKSTOP_ACKSTS_SET);
2988 const MCAN_Regs *mcan)
2990 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKSTS &
2991 MCAN_CLKSTS_STOPREQ_HW_OVR_MASK) ==
2992 MCAN_CLKSTS_STOPREQ_HW_OVR_SET);
3004 const MCAN_Regs *mcan)
3006 return ((mcan->MCANSS.TI_WRAPPER.MSP.MCANSS_CLKSTS &
3007 MCAN_CLKSTS_CCLKDONE_MASK) == MCAN_CLKSTS_CCLKDONE_SET);
Definition: dl_mcan.h:571
uint32_t eleLost
Definition: dl_mcan.h:1229
__STATIC_INLINE bool DL_MCAN_getClockStopAcknowledgeStatus(const MCAN_Regs *mcan)
Gets the clock stop acknowledge status.
Definition: dl_mcan.h:2968
uint32_t esi
Definition: dl_mcan.h:1477
int32_t DL_MCAN_config(MCAN_Regs *mcan, const DL_MCAN_ConfigParams *configParams)
This API will configure MCAN module.
__STATIC_INLINE void DL_Common_updateReg(volatile uint32_t *reg, uint32_t val, uint32_t mask)
Writes value to specified register - retaining bits unaffected by mask.
Definition: dl_common.h:63
uint32_t bit2
Definition: dl_mcan.h:1247
Definition: dl_mcan.h:674
DL_MCAN_FCLK
Enum to select source clock for CANCLK.
Definition: dl_mcan.h:513
Definition: dl_mcan.h:529
Definition: dl_mcan.h:689
__STATIC_INLINE void DL_MCAN_enableClockStopWakeupInterrupt(MCAN_Regs *mcan)
Enables the MCAN clock stop wakeup interrupt.
Definition: dl_mcan.h:2894
int32_t DL_MCAN_init(MCAN_Regs *mcan, const DL_MCAN_InitParams *initParams)
This API will initialize MCAN module.
uint32_t errPassive
Definition: dl_mcan.h:982
Definition: dl_mcan.h:1719
DL_MCAN_ECC_ERR_TYPE
Enum to represent the ECC Error Types.
Definition: dl_mcan.h:649
uint32_t dedErr
Definition: dl_mcan.h:1269
uint32_t flesa
Definition: dl_mcan.h:1042
void DL_MCAN_readTxEventFIFO(const MCAN_Regs *mcan, DL_MCAN_TxEventFIFOElement *txEventElem)
This API is used to read message form Tx Event FIFO.
uint32_t sfid1
Definition: dl_mcan.h:1515
void DL_MCAN_getHighPriorityMsgStatus(const MCAN_Regs *mcan, DL_MCAN_HighPriorityMsgInfo *hpm)
This API will return High Priority Message Status.
uint32_t scheme
Definition: dl_mcan.h:1311
DL_MCAN_INTR_SRC_MCAN
Enum to select the MCAN instance.
Definition: dl_mcan.h:637
Definition: dl_mcan.h:643
uint32_t getIdx
Definition: dl_mcan.h:1199
Definition: dl_mcan.h:730
Definition: dl_mcan.h:725
DL_MCAN_ID_TYPE
Enum to represent the MCAN Identifier Type.
Definition: dl_mcan.h:546
uint32_t txEventFIFOSize
Definition: dl_mcan.h:1077
Definition: dl_mcan.h:683
uint32_t canErrLogCnt
Definition: dl_mcan.h:963
uint32_t fillLvl
Definition: dl_mcan.h:1214
uint32_t major
Definition: dl_mcan.h:1315
uint32_t major
Definition: dl_mcan.h:1350
uint32_t stdFiltIDConf
Definition: dl_mcan.h:1623
Definition: dl_mcan.h:705
Definition: dl_mcan.h:604
DL_MCAN_ERR_CODE
Enum to represent MCAN's Error Code.
Definition: dl_mcan.h:695
__STATIC_INLINE bool DL_MCAN_getClockStopHardwareOverrideStatus(const MCAN_Regs *mcan)
Gets the clock stop hardware override status.
Definition: dl_mcan.h:2987
uint32_t anfs
Definition: dl_mcan.h:829
uint32_t mon
Definition: dl_mcan.h:1295
uint32_t rbrs
Definition: dl_mcan.h:1007
__STATIC_INLINE uint32_t DL_MCAN_getModuleClockDivider(const MCAN_Regs *mcan)
Gets the MCAN functional module clock divide ratio.
Definition: dl_mcan.h:2810
uint32_t tsPrescalar
Definition: dl_mcan.h:920
uint32_t errForce
Definition: dl_mcan.h:1253
uint32_t txDelCompConf
Definition: dl_mcan.h:1608
uint32_t DL_MCAN_getTOCounterVal(const MCAN_Regs *mcan)
This API will return current time-out counter value.
void DL_MCAN_getBitTime(const MCAN_Regs *mcan, DL_MCAN_BitTimingParams *configParams)
This API will get the configured bit timings for MCAN module.
int32_t DL_MCAN_getTxBufCancellationIntrEnable(const MCAN_Regs *mcan, uint32_t bufNum, bool enable)
This API is used to enable/disable Tx Buffer Cancellation Finished Interrupt.
int32_t DL_MCAN_writeTxEventFIFOAck(MCAN_Regs *mcan, uint32_t idx)
This API will write Event FIFO Acknowledge Index.
uint32_t DL_MCAN_getIntrStatus(const MCAN_Regs *mcan)
This API will return interrupt status.
uint32_t brs
Definition: dl_mcan.h:1386
void DL_MCAN_eccWriteEOI(MCAN_Regs *mcan, uint32_t errType)
This API is used to write End of Interrupt for ECC interrupt.
uint32_t rxDataSize
Definition: dl_mcan.h:1641
uint32_t freeLvl
Definition: dl_mcan.h:1195
uint32_t txFIFOSize
Definition: dl_mcan.h:1062
#define DL_MCAN_MAX_PAYLOAD_BYTES
Maximum payload supported by CAn-FD protocol in bytes.
Definition: dl_mcan.h:104
uint32_t efid2
Definition: dl_mcan.h:1560
Structure for MCAN High Priority Message.
Definition: dl_mcan.h:1135
void DL_MCAN_extTSClearRawStatus(MCAN_Regs *mcan)
This API will clear External TimeStamp Counter Overflow Interrupt raw status for MCAN module...
uint32_t enableRdModWr
Definition: dl_mcan.h:1338
uint32_t fillLvl
Definition: dl_mcan.h:1176
bool DL_MCAN_isFDOpEnable(const MCAN_Regs *mcan)
This API will return flexible data rate operation status MCAN module.
Definition: dl_mcan.h:699
DL_MCAN_COM_STATE
Enum to represent MCAN's communication state.
Definition: dl_mcan.h:681
Definition: dl_mcan.h:507
void DL_MCAN_addClockStopRequest(MCAN_Regs *mcan, bool enable)
This API add clock stop request for MCAN module to put it in power down mode.
Definition: dl_mcan.h:594
__STATIC_INLINE void DL_MCAN_enableInterrupt(MCAN_Regs *mcan, uint32_t interruptMask)
Enable MCAN interrupts.
Definition: dl_mcan.h:2654
__STATIC_INLINE bool DL_MCAN_isPowerEnabled(const MCAN_Regs *mcan)
Returns if the Peripheral Write Enable (PWREN) register for the MCAN is enabled.
Definition: dl_mcan.h:2613
DL_MCAN_FCLK clockSel
Definition: dl_mcan.h:745
Structure for accessing Revision ID of ECC AGGR.
Definition: dl_mcan.h:1309
uint32_t DL_MCAN_getExtIDANDMask(const MCAN_Regs *mcan)
This API will get the configured Extended ID AND Mask.
uint32_t fdf
Definition: dl_mcan.h:1443
uint32_t ctrlConf
Definition: dl_mcan.h:1587
void DL_MCAN_getRevisionId(const MCAN_Regs *mcan, DL_MCAN_RevisionId *revId)
This API is used get the MCAN revision ID.
uint32_t dlec
Definition: dl_mcan.h:997
uint32_t edcConf0
Definition: dl_mcan.h:1677
uint32_t msi
Definition: dl_mcan.h:1147
uint32_t recErrCnt
Definition: dl_mcan.h:956
void DL_MCAN_addExtMsgIDFilter(MCAN_Regs *mcan, uint32_t filtNum, const DL_MCAN_ExtMsgIDFilterElement *elem)
This API is used to add Extended Message ID Filter Element.
DL_MCAN_MEM_TYPE
Enum to represent the MCAN Message RAM type.
Definition: dl_mcan.h:569
uint32_t dataRatePrescalar
Definition: dl_mcan.h:775
uint32_t rxFIFO0ElemSize
Definition: dl_mcan.h:1127
uint32_t statusLow
Definition: dl_mcan.h:1162
Definition: dl_mcan.h:606
uint32_t asmEnable
Definition: dl_mcan.h:916
void DL_MCAN_getTxEventFIFOStatus(const MCAN_Regs *mcan, DL_MCAN_TxEventFIFOStatus *fifoStatus)
This API will Tx Event FIFO status.
void DL_MCAN_eccClearErrorStatus(MCAN_Regs *mcan, uint32_t errType)
This API is used to clear the ECC Error status.
uint32_t tdcf
Definition: dl_mcan.h:797
uint32_t wkupReqEnable
Definition: dl_mcan.h:876
uint32_t enable
Definition: dl_mcan.h:1328
uint32_t sfid2
Definition: dl_mcan.h:1513
uint32_t bit1
Definition: dl_mcan.h:1245
void DL_MCAN_enableIntrLine(MCAN_Regs *mcan, uint32_t lineNum, bool enable)
This API is used to enable/disable selected interrupt line.
uint32_t dataBitTimeConf
Definition: dl_mcan.h:1593
Definition: dl_mcan.h:608
bool DL_MCAN_isMemInitDone(const MCAN_Regs *mcan)
This function checks if the memory initialization is done for MCAN module.
Structure for ECC Error Status.
Definition: dl_mcan.h:1259
Structure for MCAN error logging counters status.
Definition: dl_mcan.h:952
void DL_MCAN_enableIntr(MCAN_Regs *mcan, uint32_t intrMask, bool enable)
This API is used to enable/disable interrupts.
__STATIC_INLINE void DL_MCAN_enablePower(MCAN_Regs *mcan)
Enables the Peripheral Write Enable (PWREN) register for the MCAN.
Definition: dl_mcan.h:2577
uint32_t warningStatus
Definition: dl_mcan.h:988
Definition: dl_mcan.h:614
int32_t DL_MCAN_setBitTime(MCAN_Regs *mcan, const DL_MCAN_BitTimingParams *configParams)
This API will configure a bit timings for MCAN module.
uint32_t pxe
Definition: dl_mcan.h:1018
Structure for MCAN protocol status.
Definition: dl_mcan.h:969
uint32_t modId
Definition: dl_mcan.h:1348
DL_MCAN_TIMEOUT_SELECT
Enum to represent the MCAN time-out counter configuration.
Definition: dl_mcan.h:622
uint32_t rxFIFO0Conf
Definition: dl_mcan.h:1632
uint32_t DL_MCAN_extTSGetUnservicedIntrCount(const MCAN_Regs *mcan)
This API returns Number of unserviced rollover/overflow interrupts for external TimeStamp counter...
uint32_t intLnSelConf
Definition: dl_mcan.h:1614
uint32_t year
Definition: dl_mcan.h:1297
DL_MCAN_RX_FIFO_NUM
Enum to represent the MCAN Rx FIFO number.
Definition: dl_mcan.h:580
uint32_t step
Definition: dl_mcan.h:1301
uint32_t dlc
Definition: dl_mcan.h:1485
uint32_t rxFIFO1ElemSize
Definition: dl_mcan.h:1129
uint32_t rxFIFO1Conf
Definition: dl_mcan.h:1638
DL_MCAN_LPBK_MODE
Enum to select the MCAN Loopback mode.
Definition: dl_mcan.h:660
uint32_t timeOutConf
Definition: dl_mcan.h:1602
uint32_t rxFIFO1startAddr
Definition: dl_mcan.h:1104
bool DL_MCAN_restoreConfiguration(MCAN_Regs *mcan, DL_MCAN_backupConfig *ptr)
Restore MCAN configuration after leaving STOP or STANDBY mode.
DL_MCAN_FCLK_DIV
Enum to select CANCLK divider.
Definition: dl_mcan.h:523
uint32_t errOnce
Definition: dl_mcan.h:1251
void DL_MCAN_resetTSCounter(MCAN_Regs *mcan)
This API will reset timestamp counter value.
void DL_MCAN_addStdMsgIDFilter(MCAN_Regs *mcan, uint32_t filtNum, const DL_MCAN_StdMsgIDFilterElement *elem)
This API is used to add Standard Message ID Filter Element.
uint32_t clkEnConf
Definition: dl_mcan.h:1584
uint32_t id
Definition: dl_mcan.h:1360
uint32_t txEvntFIFOConf
Definition: dl_mcan.h:1656
uint32_t scheme
Definition: dl_mcan.h:1285
uint32_t fifoFull
Definition: dl_mcan.h:1206
uint32_t fidx
Definition: dl_mcan.h:1445
uint32_t et
Definition: dl_mcan.h:1503
uint32_t id
Definition: dl_mcan.h:1462
uint32_t timeOutCntVal
Definition: dl_mcan.h:1605
uint32_t txEventFIFOWaterMark
Definition: dl_mcan.h:1083
Structure for accessing Revision ID of ECC wrapper.
Definition: dl_mcan.h:1344
uint32_t timeoutSelect
Definition: dl_mcan.h:931
uint32_t subStep
Definition: dl_mcan.h:1299
Definition: dl_mcan.h:626
uint32_t txBuffTxIntConf
Definition: dl_mcan.h:1650
Definition: dl_mcan.h:1698
uint32_t esi
Definition: dl_mcan.h:1375
void DL_MCAN_eccConfig(MCAN_Regs *mcan, const DL_MCAN_ECCConfigParams *configParams)
This API will enable/disable ECC on the Message RAM.
void DL_MCAN_getErrCounters(const MCAN_Regs *mcan, DL_MCAN_ErrCntStatus *errCounter)
This API will return error counter status for MCAN module.
Structure for bit timing calculation. Bit timing related to data phase will be valid only in case whe...
Definition: dl_mcan.h:755
uint32_t tdcv
Definition: dl_mcan.h:1020
uint32_t fdMode
Definition: dl_mcan.h:840
Definition: dl_mcan.h:551
uint32_t dlc
Definition: dl_mcan.h:1433
uint32_t rxts
Definition: dl_mcan.h:1427
Definition: dl_mcan.h:1715
void DL_MCAN_getTxFIFOQueStatus(const MCAN_Regs *mcan, DL_MCAN_TxFIFOStatus *fifoStatus)
This API will Tx FIFO status.
__STATIC_INLINE void DL_MCAN_disableClockStopGateRequest(MCAN_Regs *mcan)
Disables the MCAN clock gating request.
Definition: dl_mcan.h:2865
Definition: dl_mcan.h:537
DL_MCAN_CLOCK_DIVIDE
Definition: dl_mcan.h:1694
uint32_t efid1
Definition: dl_mcan.h:1544
bool DL_MCAN_isInReset(const MCAN_Regs *mcan)
This function checks if the MCAN module is in Reset.
uint32_t rpStatus
Definition: dl_mcan.h:961
uint32_t txStartAddr
Definition: dl_mcan.h:1050
bool DL_MCAN_saveConfiguration(const MCAN_Regs *mcan, DL_MCAN_backupConfig *ptr)
Saves MCAN configuration before entering STOP or STANDBY mode.
uint32_t tsSelect
Definition: dl_mcan.h:927
void DL_MCAN_getNewDataStatus(const MCAN_Regs *mcan, DL_MCAN_RxNewDataStatus *newDataStatus)
This API will return New Data Message Status.
bool DL_MCAN_extTSIsIntrEnable(const MCAN_Regs *mcan)
This API returns External TimeStamp Counter Overflow Interrupt enable status for MCAN module...
__STATIC_INLINE uint32_t DL_MCAN_getEnabledInterrupts(const MCAN_Regs *mcan, uint32_t interruptMask)
Check which MCAN interrupts are enabled.
Definition: dl_mcan.h:2686
uint32_t DL_MCAN_getRxPinState(const MCAN_Regs *mcan)
This API will return Rx pin state of MCAN module.
uint32_t esi
Definition: dl_mcan.h:1425
Definition: dl_mcan.h:573
uint32_t nomTimeSeg2
Definition: dl_mcan.h:767
uint32_t tdco
Definition: dl_mcan.h:801
DL_MCAN_IIDX
Definition: dl_mcan.h:1704
uint32_t testConf
Definition: dl_mcan.h:1686
uint32_t edcConf2
Definition: dl_mcan.h:1671
uint32_t minor
Definition: dl_mcan.h:1352
uint32_t putIdx
Definition: dl_mcan.h:1201
uint32_t txBuffConf
Definition: dl_mcan.h:1644
__STATIC_INLINE bool DL_MCAN_isGlitchFilterWakeupEnabled(const MCAN_Regs *mcan)
Checks if the glitch filter on MCAN RXD input is enabled.
Definition: dl_mcan.h:2923
uint32_t enableChk
Definition: dl_mcan.h:1333
DL_MCAN_FCLK_DIV divider
Definition: dl_mcan.h:747
uint32_t mm
Definition: dl_mcan.h:1505
int32_t DL_MCAN_msgRAMConfig(MCAN_Regs *mcan, const DL_MCAN_MsgRAMConfigParams *msgRAMConfigParams)
This API will configure Different sections of Message RAM.
Definition: dl_mcan.h:685
__STATIC_INLINE void DL_MCAN_disableClockStopWakeupInterrupt(MCAN_Regs *mcan)
Disables the MCAN clock stop wakeup interrupt.
Definition: dl_mcan.h:2906
uint32_t sft
Definition: dl_mcan.h:1536
void DL_MCAN_getRxFIFOStatus(const MCAN_Regs *mcan, DL_MCAN_RxFIFOStatus *fifoStatus)
This API will Rx FIFO status.
__STATIC_INLINE DL_MCAN_IIDX DL_MCAN_getPendingInterrupt(const MCAN_Regs *mcan)
Get highest priority pending MCAN interrupt.
Definition: dl_mcan.h:2746
void DL_MCAN_setTxPinState(MCAN_Regs *mcan, uint32_t state)
This API will set Tx pin state of MCAN module.
uint32_t wdcPreload
Definition: dl_mcan.h:890
Structure for MCAN Global Filter Configuration parameters.
Definition: dl_mcan.h:807
uint32_t DL_MCAN_eccGetIntrStatus(const MCAN_Regs *mcan, uint32_t errType)
This API is used to get ECC interrupt status.
uint32_t efbi
Definition: dl_mcan.h:858
Definition: dl_mcan.h:517
uint32_t secErr
Definition: dl_mcan.h:1264
uint32_t rxFIFO1OpMode
Definition: dl_mcan.h:1121
uint32_t DL_MCAN_getClockStopAck(const MCAN_Regs *mcan)
This API get clock stop acknowledgement for MCAN module. It return whether MCAN is power down mode or...
Definition: dl_mcan.h:1712
__STATIC_INLINE void DL_MCAN_enableGlitchFilterWakeup(MCAN_Regs *mcan)
Enables the glitch filter on MCAN RXD input.
Definition: dl_mcan.h:2939
__STATIC_INLINE void DL_MCAN_disablePower(MCAN_Regs *mcan)
Disables the Peripheral Write Enable (PWREN) register for the MCAN.
Definition: dl_mcan.h:2592
DL_MCAN_PIN_TYPE
Enum to represent the MCAN pin type.
Definition: dl_mcan.h:590
uint32_t lss
Definition: dl_mcan.h:1040
uint32_t pxhddisable
Definition: dl_mcan.h:865
uint32_t DL_MCAN_getTSCounterVal(const MCAN_Regs *mcan)
This API will return current timestamp counter value.
uint32_t intEnConf
Definition: dl_mcan.h:1611
uint32_t clkConf
Definition: dl_mcan.h:1581
Definition: dl_mcan.h:703
Structure for MCAN Extended Message ID Filter Element.
Definition: dl_mcan.h:1542
Structure for ECC Error forcing.
Definition: dl_mcan.h:1235
Definition: dl_mcan.h:560
uint32_t rxFIFO0OpMode
Definition: dl_mcan.h:1102
__STATIC_INLINE bool DL_MCAN_getControllerClockRequestStatus(const MCAN_Regs *mcan)
Gets the status of MCAN controller clock request from GPRCM.
Definition: dl_mcan.h:3003
DL_MCAN_TDCConfig tdcConfig
Definition: dl_mcan.h:894
uint32_t darEnable
Definition: dl_mcan.h:871
Definition: dl_mcan.h:527
void DL_MCAN_extTSWriteEOI(MCAN_Regs *mcan)
This API is used to write End of Interrupt for External TimeStamp Counter Overflow Interrupt...
uint32_t rfdf
Definition: dl_mcan.h:1013
uint32_t rtr
Definition: dl_mcan.h:1467
bool DL_MCAN_isReady(DL_MCAN_INSTANCE instance)
if MCAN instance is ready to be configured
uint32_t xtd
Definition: dl_mcan.h:1420
void DL_MCAN_extTSEnableIntr(MCAN_Regs *mcan, bool enable)
This API will enable/disable External TimeStamp Counter Overflow Interrupt for MCAN module...
Definition: dl_mcan.h:612
uint32_t timeCntVal
Definition: dl_mcan.h:1599
Definition: dl_mcan.h:628
uint32_t scheme
Definition: dl_mcan.h:1346
void DL_MCAN_eccEnableIntr(MCAN_Regs *mcan, uint32_t errType, bool enable)
This API is used to enable ECC interrupt.
__STATIC_INLINE void DL_MCAN_enableModuleClock(MCAN_Regs *mcan)
Enables the MCAN functional module clock.
Definition: dl_mcan.h:2786
Structure for MCAN Tx Event FIFO Status.
Definition: dl_mcan.h:1212
Definition: dl_mcan.h:1706
uint32_t rxBuffConf
Definition: dl_mcan.h:1635
Definition: dl_mcan.h:641
Structure for MCAN Transmitter Delay Compensation parameters.
Definition: dl_mcan.h:793
DL_MCAN_INTR_LINE_NUM
Enum to select the MCAN interrupt lines.
Definition: dl_mcan.h:535
void DL_MCAN_extTSCounterEnable(MCAN_Regs *mcan, bool enable)
This API will enable/disable fast external time stamp counter for MCAN module.
uint32_t getIdx
Definition: dl_mcan.h:1216
__STATIC_INLINE void DL_MCAN_setModuleClockDivider(MCAN_Regs *mcan, uint32_t clkdiv)
Configures clock divide settings for the MCAN functional module clock.
Definition: dl_mcan.h:2825
uint32_t DL_MCAN_getTxBufReqPend(const MCAN_Regs *mcan)
This API will return Tx Buffer Request Pending status.
uint32_t timeCntConf
Definition: dl_mcan.h:1596
uint32_t rxFIFO0waterMark
Definition: dl_mcan.h:1097
Definition: dl_mcan.h:687
uint32_t rxFIFO0size
Definition: dl_mcan.h:1091
uint32_t fifoFull
Definition: dl_mcan.h:1185
Definition: dl_mcan.h:1700
uint32_t fdf
Definition: dl_mcan.h:1391
DL_MCAN_GlobalFiltConfig filterConfig
Definition: dl_mcan.h:946
Definition: dl_mcan.h:525
__STATIC_INLINE void DL_MCAN_disableGlitchFilterWakeup(MCAN_Regs *mcan)
Disables the glitch filter on MCAN RXD input.
Definition: dl_mcan.h:2954
uint32_t rrfs
Definition: dl_mcan.h:817
uint32_t fdf
Definition: dl_mcan.h:1495
void DL_MCAN_extTSSetRawStatus(MCAN_Regs *mcan)
This API will set External TimeStamp Counter Overflow Interrupt Raw status for MCAN module...
uint32_t bufIdx
Definition: dl_mcan.h:1139
uint32_t brsEnable
Definition: dl_mcan.h:846
uint32_t getIdx
Definition: dl_mcan.h:1178
void DL_MCAN_eccForceError(MCAN_Regs *mcan, const DL_MCAN_ECCErrForceParams *eccErr)
This API will Force Error on ECC.
Definition: dl_mcan.h:602
uint32_t num
Definition: dl_mcan.h:1174
uint32_t txpEnable
Definition: dl_mcan.h:852
uint32_t monEnable
Definition: dl_mcan.h:910
uint32_t modId
Definition: dl_mcan.h:1287
uint32_t globFiltIDConf
Definition: dl_mcan.h:1620
uint32_t sfec
Definition: dl_mcan.h:1529
uint32_t lse
Definition: dl_mcan.h:1048
uint32_t transErrLogCnt
Definition: dl_mcan.h:954
uint32_t DL_MCAN_getOpMode(const MCAN_Regs *mcan)
This API will return MCAN module mode of operation.
Structure for MCAN Tx Buffer element.
Definition: dl_mcan.h:1358
int32_t DL_MCAN_txBufCancellationReq(MCAN_Regs *mcan, uint32_t buffNum)
This API will set Tx Buffer Cancellation Request.
Definition: dl_mcan.h:639
__STATIC_INLINE bool DL_MCAN_isReset(const MCAN_Regs *mcan)
Returns if mcan peripheral was reset.
Definition: dl_mcan.h:2640
void DL_MCAN_clearNewDataStatus(MCAN_Regs *mcan, const DL_MCAN_RxNewDataStatus *newDataStatus)
This API clear New Data Message Status.
Definition: dl_mcan.h:651
void DL_MCAN_readMsgRam(const MCAN_Regs *mcan, uint32_t memType, uint32_t bufNum, uint32_t fifoNum, DL_MCAN_RxBufElement *elem)
This API is used to read received message form message RAM.
uint32_t txts
Definition: dl_mcan.h:1479
uint32_t rtr
Definition: dl_mcan.h:1415
void DL_MCAN_getProtocolStatus(const MCAN_Regs *mcan, DL_MCAN_ProtocolStatus *protStatus)
This API will return protocol status for MCAN module.
uint32_t DL_MCAN_getTxBufTransmissionStatus(const MCAN_Regs *mcan)
This API will return Tx Buffer Transmission Occurred status.
void DL_MCAN_setOpMode(MCAN_Regs *mcan, uint32_t mode)
This API will set MCAN module mode of operation.
uint32_t rxFIFO1size
Definition: dl_mcan.h:1110
uint32_t statusHigh
Definition: dl_mcan.h:1164
Definition: dl_mcan.h:610
Definition: dl_mcan.h:1709
Definition: dl_mcan.h:735
uint32_t rxBufElemSize
Definition: dl_mcan.h:1125
uint32_t resi
Definition: dl_mcan.h:1002
void DL_MCAN_eccClearIntrStatus(MCAN_Regs *mcan, uint32_t errType)
This API is used to clear ECC interrupt status.
uint32_t DL_MCAN_getEndianVal(const MCAN_Regs *mcan)
This function return endianness value of MCAN module.
uint32_t nomTimeSeg1
Definition: dl_mcan.h:763
uint32_t errType
Definition: dl_mcan.h:1239
uint32_t efec
Definition: dl_mcan.h:1558
Structure for MCAN Rx FIFO Status.
Definition: dl_mcan.h:1170
uint32_t txBuffCancIntConf
Definition: dl_mcan.h:1653
uint32_t rxBufStartAddr
Definition: dl_mcan.h:1123
uint32_t rxFIFO1waterMark
Definition: dl_mcan.h:1116
uint32_t autoWkupEnable
Definition: dl_mcan.h:881
uint32_t DL_MCAN_getClkStopAck(const MCAN_Regs *mcan)
This API will return clock stop acknowledgement for MCAN module.
__STATIC_INLINE void DL_MCAN_disableModuleClock(MCAN_Regs *mcan)
Disables the MCAN functional module clock.
Definition: dl_mcan.h:2797
int32_t DL_MCAN_setExtIDAndMask(MCAN_Regs *mcan, uint32_t idMask)
This API will configure Extended ID AND Mask.
uint32_t minor
Definition: dl_mcan.h:1291
uint32_t busOffStatus
Definition: dl_mcan.h:993
void DL_MCAN_selectIntrLine(MCAN_Regs *mcan, uint32_t intrMask, uint32_t lineNum)
This API is used to select interrupt line.
uint32_t bit1
Definition: dl_mcan.h:1275
uint32_t clkDivConf
Definition: dl_mcan.h:1578
Definition: dl_mcan.h:539
__STATIC_INLINE void DL_MCAN_enableClockStopGateRequest(MCAN_Regs *mcan)
Enables the MCAN clock gating request.
Definition: dl_mcan.h:2853
uint32_t dataSynchJumpWidth
Definition: dl_mcan.h:787
uint32_t ssIntEnConf
Definition: dl_mcan.h:1662
void DL_MCAN_eccGetErrorStatus(MCAN_Regs *mcan, DL_MCAN_ECCErrStatus *eccErr)
This API will return ECC Error status.
uint32_t msgLost
Definition: dl_mcan.h:1187
__STATIC_INLINE bool DL_MCAN_isClockStopWakeupInterruptEnabled(const MCAN_Regs *mcan)
Checks if the MCAN clock stop wakeup interrupt is enabled.
Definition: dl_mcan.h:2880
uint32_t dataTimeSeg2
Definition: dl_mcan.h:783
uint32_t efc
Definition: dl_mcan.h:1396
uint32_t edcConf1
Definition: dl_mcan.h:1674
uint32_t brs
Definition: dl_mcan.h:1490
Structure for MCAN Rx Buffer element.
Definition: dl_mcan.h:1408
uint32_t eft
Definition: dl_mcan.h:1568
__STATIC_INLINE void DL_MCAN_reset(MCAN_Regs *mcan)
Resets mcan peripheral.
Definition: dl_mcan.h:2624
uint32_t row
Definition: dl_mcan.h:1273
uint32_t dlc
Definition: dl_mcan.h:1381
Definition: dl_mcan.h:624
Definition: dl_mcan.h:715
uint32_t mm
Definition: dl_mcan.h:1398
uint32_t filterIdx
Definition: dl_mcan.h:1149
Structure for CANCLK configuration.
Definition: dl_mcan.h:742
uint32_t rel
Definition: dl_mcan.h:1303
Definition: dl_mcan.h:616
Structure for accessing Revision ID and Core Release Info. of MCAN module.
Definition: dl_mcan.h:1283
int32_t DL_MCAN_TXBufTransIntrEnable(MCAN_Regs *mcan, uint32_t bufNum, bool enable)
This API is used to enable/disable Tx Buffer Transmission Interrupt.
uint32_t fifoFull
Definition: dl_mcan.h:1223
bool backupRdy
Definition: dl_mcan.h:1690
__STATIC_INLINE uint32_t DL_MCAN_getRawInterruptStatus(const MCAN_Regs *mcan, uint32_t interruptMask)
Check interrupt flag of any MCAN interrupt.
Definition: dl_mcan.h:2728
uint32_t nomBitTimeConf
Definition: dl_mcan.h:1590
Definition: dl_mcan.h:653
DL_MCAN_OPERATION_MODE
Enum to represent the MCAN mode of operation.
Definition: dl_mcan.h:558
void DL_MCAN_getClockConfig(MCAN_Regs *mcan, DL_MCAN_ClockConfig *config)
Get CANCLK clock configuration.
__STATIC_INLINE bool DL_MCAN_isClockStopGateRequestEnabled(const MCAN_Regs *mcan)
Checks if the MCAN clock gating request is enabled.
Definition: dl_mcan.h:2840
uint32_t DL_MCAN_getTxPinState(const MCAN_Regs *mcan)
This API will return Tx pin state of MCAN module.
__STATIC_INLINE uint32_t DL_MCAN_getEnabledInterruptStatus(const MCAN_Regs *mcan, uint32_t interruptMask)
Check interrupt flag of enabled MCAN interrupts.
Definition: dl_mcan.h:2707
uint32_t day
Definition: dl_mcan.h:1293
uint32_t flssa
Definition: dl_mcan.h:1034
uint32_t rowNum
Definition: dl_mcan.h:1241
uint32_t DL_MCAN_getIntrLineSelectStatus(const MCAN_Regs *mcan)
This API is used to get interrupt line selected for each interrupt.
uint32_t txBufMode
Definition: dl_mcan.h:1067
Structure for MCAN Message RAM Configuration Parameters. Message RAM can contain following sections: ...
Definition: dl_mcan.h:1032
Definition: dl_mcan.h:1717
Structure for MCAN Tx Event FIFO element.
Definition: dl_mcan.h:1460
int32_t DL_MCAN_TXBufAddReq(MCAN_Regs *mcan, uint32_t bufNum)
This API will set Tx Buffer Add Request.
__STATIC_INLINE void DL_MCAN_clearInterruptStatus(MCAN_Regs *mcan, uint32_t interruptMask)
Clear pending MCAN interrupts.
Definition: dl_mcan.h:2760
uint32_t anfe
Definition: dl_mcan.h:823
uint32_t xtd
Definition: dl_mcan.h:1472
uint32_t act
Definition: dl_mcan.h:977
uint32_t exFiltIDConf
Definition: dl_mcan.h:1626
Structure for MCAN Standard Message ID Filter Element.
Definition: dl_mcan.h:1511
uint32_t exFiltIDMsk
Definition: dl_mcan.h:1629
uint32_t putIdx
Definition: dl_mcan.h:1218
Configuration structure to backup MCAN peripheral state before entering STOP or STANDBY mode...
Definition: dl_mcan.h:1576
uint32_t nomRatePrescalar
Definition: dl_mcan.h:759
uint32_t txBufNum
Definition: dl_mcan.h:1056
uint32_t putIdx
Definition: dl_mcan.h:1180
void DL_MCAN_writeMsgRam(MCAN_Regs *mcan, uint32_t memType, uint32_t bufNum, const DL_MCAN_TxBufElement *elem)
This API is used to write Tx message to message RAM.
Definition: dl_mcan.h:582
uint32_t txDataSize
Definition: dl_mcan.h:1647
Definition: dl_mcan.h:515
uint32_t filterList
Definition: dl_mcan.h:1154
void DL_MCAN_lpbkModeEnable(MCAN_Regs *mcan, uint32_t lpbkMode, bool enable)
This API will enable/disable Loop Back Test Mode for MCAN module.
Structure for MCAN ECC configuration parameters.
Definition: dl_mcan.h:1323
uint32_t timeoutPreload
Definition: dl_mcan.h:937
uint32_t lastErrCode
Definition: dl_mcan.h:973
uint32_t xtd
Definition: dl_mcan.h:1370
uint32_t preSclConf
Definition: dl_mcan.h:1665
Structure for MCAN initialization parameters.
Definition: dl_mcan.h:835
Definition: dl_mcan.h:630
Structure for MCAN configuration parameters.
Definition: dl_mcan.h:905
Definition: dl_mcan.h:592
uint32_t modId
Definition: dl_mcan.h:1313
void DL_MCAN_setClockConfig(MCAN_Regs *mcan, const DL_MCAN_ClockConfig *config)
Configure CANCLK source clock.
uint32_t brs
Definition: dl_mcan.h:1438
uint32_t rrfe
Definition: dl_mcan.h:812
Definition: dl_mcan.h:1696
uint32_t ramWDConf
Definition: dl_mcan.h:1683
uint32_t id
Definition: dl_mcan.h:1410
Structure for MCAN Tx FIFO Status.
Definition: dl_mcan.h:1193
DL_MCAN_INSTANCE
Enum to select the MCAN instance.
Definition: dl_mcan.h:505
int32_t DL_MCAN_writeRxFIFOAck(MCAN_Regs *mcan, uint32_t fifoNum, uint32_t idx)
This API will write Rx FIFO Acknowledgement.
uint32_t dataTimeSeg1
Definition: dl_mcan.h:779
uint32_t tdcEnable
Definition: dl_mcan.h:899
Definition: dl_mcan.h:562
void DL_MCAN_eccWrapGetRevisionId(MCAN_Regs *mcan, DL_MCAN_ECCWrapRevisionId *revId)
This API is used get the ECC Wrapper revision ID.
uint32_t ssCtrlConf
Definition: dl_mcan.h:1659
Definition: dl_mcan.h:549
uint32_t timeoutCntEnable
Definition: dl_mcan.h:942
__STATIC_INLINE bool DL_MCAN_isModuleClockEnabled(const MCAN_Regs *mcan)
Checks if the MCAN module clock request is enabled.
Definition: dl_mcan.h:2774
uint32_t txEventFIFOStartAddr
Definition: dl_mcan.h:1071
Definition: dl_mcan.h:665
void DL_MCAN_eccAggrGetRevisionId(const MCAN_Regs *mcan, DL_MCAN_ECCAggrRevisionId *revId)
This API is used get the ECC AGGR revision ID.
Structure for MCAN new data flag for Rx buffer.
Definition: dl_mcan.h:1160
uint32_t rxFIFO0startAddr
Definition: dl_mcan.h:1085
void DL_MCAN_extTSCounterConfig(MCAN_Regs *mcan, uint32_t prescalar)
This API will configure external timestamp counter for MCAN module.
uint32_t anmf
Definition: dl_mcan.h:1450
__STATIC_INLINE void DL_MCAN_disableInterrupt(MCAN_Regs *mcan, uint32_t interruptMask)
Disable MCAN interrupts.
Definition: dl_mcan.h:2668
uint32_t DL_MCAN_txBufCancellationStatus(const MCAN_Regs *mcan)
This API will return Transmit Buffer Cancellation Finished status.
uint32_t intLnEnableConf
Definition: dl_mcan.h:1617
uint32_t intEvnt0Conf
Definition: dl_mcan.h:1680
void DL_MCAN_clearIntrStatus(MCAN_Regs *mcan, uint32_t intrMask, DL_MCAN_INTR_SRC_MCAN eoi)
This API is used to clear the interrupt status.
uint32_t txBufElemSize
Definition: dl_mcan.h:1069
uint32_t rtr
Definition: dl_mcan.h:1365
uint32_t nomSynchJumpWidth
Definition: dl_mcan.h:771
Definition: dl_mcan.h:584
uint32_t major
Definition: dl_mcan.h:1289
uint32_t edcVecConf
Definition: dl_mcan.h:1668
Definition: dl_mcan.h:709
uint32_t minor
Definition: dl_mcan.h:1317
uint32_t emulationEnable
Definition: dl_mcan.h:886
DL_MCAN_ELEM_SIZE
Enum to represent FIFO/Buffer element Size.
Definition: dl_mcan.h:600