88 #ifndef ALGOLIB_LOAD_INCLUDE_TRISTATE_H_ 89 #define ALGOLIB_LOAD_INCLUDE_TRISTATE_H_ _Bool getTriStateStatus(TRISTATE_T *pTriState)
TriState Status check.
Definition: triState.h:142
void triStateRun(TRISTATE_T *pTriState)
TriState Run.
Definition: triState.c:84
uint32_t w
Definition: triState.h:108
_Bool status
Definition: triState.h:101
void triStateInit(TRISTATE_T *pTriState)
TriState Init.
Definition: triState.c:79
TriState Flags Structure.
Definition: triState.h:97
TriState Working Structure.
Definition: triState.h:113
TRI_STATE_FLAGS_T flags
Definition: triState.h:124
uint16_t countMax
Definition: triState.h:118
TriState Flags Working Structure.
Definition: triState.h:94
struct TRI_STATE_FLAGS_T::triStateFlags b