88 #ifndef APPUSEROUTPUTS_H 89 #define APPUSEROUTPUTS_H APP_VERSION_T appVersion
Definition: appUserOutputs.h:235
appVersion register
Definition: appUserOutputs.h:196
int32_t torqueLimit
Definition: appUserOutputs.h:229
Definition: appUserOutputs.h:108
int32_t d
Definition: appUserOutputs.h:175
Definition: appUserOutputs.h:112
User output structure.
Definition: appUserOutputs.h:205
Definition: appUserOutputs.h:102
Definition: appUserOutputs.h:139
Definition: appUserOutputs.h:124
Definition: appUserOutputs.h:118
Definition: appUserOutputs.h:106
uint32_t w
Definition: appUserOutputs.h:201
float kp
Definition: appUserOutputs.h:156
DQ structure.
Definition: appUserOutputs.h:172
OUTPUTS_PI_T piId
Definition: appUserOutputs.h:221
Definition: appUserOutputs.h:141
Definition: appUserOutputs.h:143
USER_STATUS_INTERFACE_T * pUserStatusRegs
pointer to userOutputs
OUTPUT_DQ_T VdqFilt
Definition: appUserOutputs.h:213
Definition: appUserOutputs.h:126
Definition: appUserOutputs.h:130
OUTPUTS_PI_T piSpeed
Definition: appUserOutputs.h:217
int32_t reference
Definition: appUserOutputs.h:166
PI output structure.
Definition: appUserOutputs.h:163
uint32_t controllerFaultStatus
controller fault status register for external reporting
Definition: appUserOutputs.h:233
Motor Control Library Module.
Definition: appUserOutputs.h:128
MOTOR_STATE_TYPES_T
Motor states.
Definition: appUserOutputs.h:99
Definition: appUserOutputs.h:110
Definition: appUserOutputs.h:104
OUTPUTS_CURRENT_PI_T currentPI
Definition: appUserOutputs.h:215
USER_FAULT_TYPES
Fault types.
Definition: appUserOutputs.h:134
Definition: appUserOutputs.h:122
PI Current output structure.
Definition: appUserOutputs.h:153
Definition: appUserOutputs.h:114
float ki
Definition: appUserOutputs.h:158
USER_FAULT_TYPES systemFaultStatus
Definition: appUserOutputs.h:209
Definition: appUserOutputs.h:137
int32_t estimatedSpeed
Definition: appUserOutputs.h:225
Definition: appUserOutputs.h:145
int32_t feedback
Definition: appUserOutputs.h:168
int32_t dcBusVoltage
Definition: appUserOutputs.h:227
int32_t q
Definition: appUserOutputs.h:177
Definition: appUserOutputs.h:147
uint32_t gateDriverFaultStatus
Gate driver faults status register for external reporting.
Definition: appUserOutputs.h:231
Definition: appUserOutputs.h:116
MOTOR_STATE_TYPES_T motorState
Definition: appUserOutputs.h:211
Definition: appUserOutputs.h:149
Definition: appUserOutputs.h:120
appVersion b
Definition: appUserOutputs.h:199
appVersion structure
Definition: appUserOutputs.h:182
OUTPUTS_PI_T piIq
Definition: appUserOutputs.h:223
OUTPUTS_PI_T piPower
Definition: appUserOutputs.h:219