![]() |
![]() |
|
MSPM0C1106BrushedMotorControlLibrary
1.0
|
Brushed Motor Driver Library HAL Module.
#include "ti_msp_dl_config.h"#include <ti/iqmath/include/IQmathLib.h>

Go to the source code of this file.
Macros | |
| #define | HIGH (PIN_MODE_OUTPUT_HIGH) |
| Set GPIO output to high. | |
| #define | LOW (PIN_MODE_OUTPUT_LOW) |
| Set GPIO output to low. | |
Enumerations | |
| enum | PIN_MODE { PIN_MODE_OUTPUT_LOW = 0, PIN_MODE_OUTPUT_HIGH, PIN_MODE_INPUT_PU, PIN_MODE_INPUT_PD, PIN_MODE_INPUT_HZ, PIN_MODE_PERIPHERAL, PIN_MODE_MAX } |
| enum | PWM_CHANNELS { PWM_CHANNEL_0 = 0, PWM_CHANNEL_1, PWM_CHANNELS_MAX } |
| Channels described here simply references individual PWM output pins. This means a micro-controller can have a single peripheral such as a timer that can be used to generate 1 or more different PWM signals. Each of those PWM signals are considered seperate PWM channels. More... | |
| enum | SPI_CHANNELS { SPI_CHANNEL_0 = 0, SPI_CHANNELS_MAX } |
| Channels described usually references individual SPI peripheral instances ie ( SCLK, PICO and POCI). More... | |
| enum | SPI_CS { SPI_CS_0 = 0, SPI_CS_1, SPI_CS_2, SPI_CS_3, SPI_CS_MAX } |
| The chip select number here has no relationship with the physical chip select that the SPI peripheral instance has. For example, SPI_CS_0 can be mapped to the peripheral's CS2 or even a GPIO pin that is being used as a chip select. More... | |
| enum | GPIO_OUTPUT_PINS { GPIO_OUTPUT_PIN_0 = 0, GPIO_OUTPUT_PIN_1, GPIO_OUTPUT_PIN_2, GPIO_OUTPUT_PIN_3, GPIO_OUTPUT_PIN_4, GPIO_OUTPUT_PINS_MAX } |
| enum | GPIO_INPUT_PINS { GPIO_INPUT_PIN_0 = 0, GPIO_INPUT_PINS_MAX } |
| enum | ADC_CHANS { ADC_CHAN_0 = 0, ADC_CHAN_1, ADC_CHANS_MAX } |
Functions | |
| void | HAL_setDutyCycle (PWM_CHANNELS pwmChan, uint8_t targetDutyCycle) |
| Sets the PWM duty cycle for a specific channel. More... | |
| void | HAL_setPWMFreq (PWM_CHANNELS pwmChan, uint32_t targetFreq) |
| Sets the PWM frequency for a specific channel. More... | |
| void | HAL_configurePWMPin (PWM_CHANNELS pwmChan, PIN_MODE mode) |
| Sets the PWM pin to specified pin mode. More... | |
| void | HAL_writeSPI8withTimeout (SPI_CHANNELS spi_chan, SPI_CS cs_chan, uint8_t data, uint32_t timeout) |
| Performs a 8-bit SPI write with timeout. More... | |
| uint8_t | HAL_readSPI8withTimeout (SPI_CHANNELS spi_chan, SPI_CS cs_chan, uint32_t timeout) |
| Performs a 8-bit SPI read with timeout. More... | |
| void | HAL_writeSPI16withTimeout (SPI_CHANNELS spi_chan, SPI_CS cs_chan, uint16_t data, int32_t timeout) |
| Performs a 16-bit SPI write with timeout. More... | |
| uint16_t | HAL_readSPI16withTimeout (SPI_CHANNELS spi_chan, SPI_CS cs_chan, int32_t timeout) |
| Performs a 16-bit SPI write with timeout. More... | |
| void | HAL_delayMicroSeconds (uint32_t num_us) |
| Delay function in microseconds. More... | |
| void | HAL_delayMilliSeconds (uint32_t num_us) |
| Delay function in milliseconds. More... | |
| bool | HAL_readGPIOInput (GPIO_INPUT_PINS pin) |
| Read GPIO input pin value. More... | |
| void | HAL_setGPIOOutput (GPIO_OUTPUT_PINS pin, PIN_MODE mode) |
| Set output pin's value. More... | |
| void | HAL_Init () |
| Function called to run initialization code needed by the HAL. | |
| void | HAL_setADCRefVoltage (ADC_CHANS adcChan, uint16_t voltage_mV) |
| Set the reference voltage that specified ADC channel is using. The software doesn't know what reference voltage is associated with the ADC channel so this needs to be manually configured. More... | |
| uint16_t | HAL_getRawADCValue (ADC_CHANS adcChan) |
| Return the latest raw ADC value from the specified ADC channel. More... | |
| uint32_t | HAL_getmVfromADC (ADC_CHANS adcChan) |
| Returns the voltage in mV read from the specified ADC channel. Important This function depends on the correct ADC reference voltage being set HAL_setADCRefVoltage. More... | |
| _iq20 | HAL_getIQ20VoltageFromADC (ADC_CHANS adcChan) |
| Returns the voltage in mV in IQ20 format read from the specified ADC channel Important This function depends on the correct ADC reference voltage being set HAL_setADCRefVoltage. More... | |
| DL_ADC12_IIDX | HAL_processADCIRQ (ADC12_Regs *adcInst) |
| Function to process ADC interrupts and read converted ADC values. Should only be used in ADC irqs. More... | |