Hall Sensored Trap Motor Control Library HAL Module.
|
| enum | HAL_GPIO_STATE {
HAL_GPIO_PIN_LOW = 0,
HAL_GPIO_PIN_HIGH
} |
| |
| enum | HAL_ADC_CHAN {
HAL_ADC_CHAN_0 = 0,
HAL_ADC_CHAN_1,
HAL_ADC_CHAN_2,
HAL_ADC_CHAN_3,
HAL_ADC_CHAN_4,
HAL_ADC_CHAN_5,
HAL_ADC_CHAN_6,
HAL_ADC_CHAN_MAX
} |
| |
| enum | HAL_GPIO_IN {
HAL_GPIO_IN_01 = 0,
HAL_GPIO_IN_02,
HAL_GPIO_IN_03,
HAL_GPIO_IN_04,
HAL_GPIO_IN_MAX
} |
| |
| enum | HAL_GPIO_OUT {
HAL_GPIO_OUT_01 = 0,
HAL_GPIO_OUT_02,
HAL_GPIO_OUT_03,
HAL_GPIO_OUT_MAX
} |
| |
| enum | HAL_PWM {
HAL_PWM_01 = 0,
HAL_PWM_02,
HAL_PWM_03,
HAL_PWM_MAX
} |
| |
| enum | HAL_CAPTURE_TIMER {
HAL_CAPTURE_TIMER_01 = 0,
HAL_CAPTURE_TIMER_MAX
} |
| |
| enum | HAL_FAULT_INPUT {
HAL_FAULT_INPUT_1,
HAL_FAULT_INPUT_MAX
} |
| |
| enum | HAL_SPI_CHAN {
HAL_SPI_CHAN_0 = 0,
HAL_SPI_CHAN_MAX
} |
| |
| enum | HAL_SPI_CS {
HAL_SPI_CS_0 = 0,
HAL_SPI_CS_1,
HAL_SPI_CS_2,
HAL_SPI_CS_3,
HAL_SPI_CS_MAX
} |
| |
| enum | HAL_ADC_VREF {
HAL_ADC_VREF_VDDA = 0,
HAL_ADC_VREF_INTERNAL,
HAL_ADC_VREF_EXTERNAL
} |
| |
| enum | HAL_ADC_INT_VREF {
HAL_ADC_INT_VREF_2P5V = DL_VREF_BUFCONFIG_OUTPUT_2_5V,
HAL_ADC_INT_VREF_1P4V = DL_VREF_BUFCONFIG_OUTPUT_1_4V
} |
| |
| enum | HAL_ADC_IIDX {
HAL_ADC_IIDX_OVERFLOW = DL_ADC12_IIDX_OVERFLOW,
HAL_ADC_IIDX_TRIG_OVERFLOW = DL_ADC12_IIDX_TRIG_OVERFLOW,
HAL_ADC_IIDX_WINDOW_COMP_HIGH = DL_ADC12_IIDX_WINDOW_COMP_HIGH,
HAL_ADC_IIDX_WINDOW_COMP_LOW = DL_ADC12_IIDX_WINDOW_COMP_LOW,
HAL_ADC_IIDX_INIFG = DL_ADC12_IIDX_INIFG,
HAL_ADC_IIDX_DMA_DONE = DL_ADC12_IIDX_DMA_DONE,
HAL_ADC_IIDX_UNDERFLOW = DL_ADC12_IIDX_UNDERFLOW,
HAL_ADC_IIDX_MEM0_RESULT_LOADED = DL_ADC12_IIDX_MEM0_RESULT_LOADED,
HAL_ADC_IIDX_MEM1_RESULT_LOADED = DL_ADC12_IIDX_MEM1_RESULT_LOADED,
HAL_ADC_IIDX_MEM2_RESULT_LOADED = DL_ADC12_IIDX_MEM2_RESULT_LOADED,
HAL_ADC_IIDX_MEM3_RESULT_LOADED = DL_ADC12_IIDX_MEM3_RESULT_LOADED,
HAL_ADC_IIDX_MEM4_RESULT_LOADED = DL_ADC12_IIDX_MEM4_RESULT_LOADED,
HAL_ADC_IIDX_MEM5_RESULT_LOADED = DL_ADC12_IIDX_MEM5_RESULT_LOADED,
HAL_ADC_IIDX_MEM6_RESULT_LOADED = DL_ADC12_IIDX_MEM6_RESULT_LOADED,
HAL_ADC_IIDX_MEM7_RESULT_LOADED = DL_ADC12_IIDX_MEM7_RESULT_LOADED,
HAL_ADC_IIDX_MEM8_RESULT_LOADED = DL_ADC12_IIDX_MEM8_RESULT_LOADED,
HAL_ADC_IIDX_MEM9_RESULT_LOADED = DL_ADC12_IIDX_MEM9_RESULT_LOADED,
HAL_ADC_IIDX_MEM10_RESULT_LOADED = DL_ADC12_IIDX_MEM10_RESULT_LOADED,
HAL_ADC_IIDX_MEM11_RESULT_LOADED = DL_ADC12_IIDX_MEM11_RESULT_LOADED
} |
| |
|
| void | HAL_init () |
| | Initializes the hal object. More...
|
| |
| bool | HAL_readGPIOPin (HAL_GPIO_IN pin) |
| | Reads a GPIOpin. More...
|
| |
| void | HAL_writeGPIOPin (HAL_GPIO_OUT pin, HAL_GPIO_STATE value) |
| | Write to GPIOpin. More...
|
| |
| void | HAL_setDeadband (HAL_PWM pwm, uint16_t deadband) |
| | Sets deadband for timer. More...
|
| |
| void | HAL_setPWMFreq (HAL_PWM pwm, uint32_t PWMFreq) |
| | Sets PWMfreq for all timers. More...
|
| |
| void | HAL_writeSPI16 (HAL_SPI_CHAN chan, HAL_SPI_CS cs, uint16_t data) |
| | Write data to spi. More...
|
| |
| uint16_t | HAL_readSPI16 (HAL_SPI_CHAN chan, HAL_SPI_CS cs) |
| | Read data from spi. More...
|
| |
| void | HAL_setADCRefVoltage (HAL_ADC_CHAN chan, uint16_t voltage_mV) |
| | Set ADC reference voltage. More...
|
| |
| uint32_t | HAL_getmvFromADC (HAL_ADC_CHAN chan) |
| | Get milli volts from ADC. More...
|
| |
| _iq20 | HAL_getIQ20VoltageFromADC (HAL_ADC_CHAN chan) |
| | Get volts from ADC in _IQ20. More...
|
| |
| HAL_ADC_IIDX | HAL_processADCIRQ (ADC12_Regs *adcInst) |
| | Read ADC values from results. More...
|
| |
| void | HAL_enableADCInterrupt (HAL_ADC_CHAN chan) |
| | Enables ADC interrupts. More...
|
| |
| void | HAL_enableGPIOInterrupt (HAL_GPIO_IN pin) |
| | Enables GPIO interrupts. More...
|
| |
| void | HAL_enablePWMInterrupt (HAL_PWM PWM) |
| | Enables PWM interrupts. More...
|
| |
| void | HAL_enableCaptureInterrupt (HAL_CAPTURE_TIMER capture) |
| | Enables capture interrupts. More...
|
| |
| void | HAL_setADCVRefVDDA (HAL_ADC_CHAN chan) |
| | Set ADC voltage reference to VDDA. More...
|
| |
| void | HAL_setADCVRefInternal (HAL_ADC_CHAN chan, HAL_ADC_INT_VREF internalVRef) |
| | Set ADC voltage reference to internal reference. More...
|
| |
| void | HAL_setADCVRefExternal (HAL_ADC_CHAN chan, uint16_t externalVRef) |
| | Set ADC voltage reference to external reference. More...
|
| |
| void | HAL_clearTimerFault (HAL_FAULT_INPUT fault) |
| | Clear the PWM timer fault bit. More...
|
| |
| bool | HAL_getTimerFaultStatus (HAL_FAULT_INPUT fault) |
| | Read the PWM timer fault bit. More...
|
| |
| uint32_t | HAL_getCaptureFrequency (HAL_CAPTURE_TIMER capture) |
| | Calculates the capture frequency. More...
|
| |
| void | HAL_ADCVRefSel (HAL_ADC_VREF adcRef, HAL_ADC_CHAN chan, HAL_ADC_INT_VREF internalVRef, uint16_t externalVRef) |
| | updates the adc voltage reference More...
|
| |
| __STATIC_INLINE void | HAL_delayMicroSeconds (uint32_t microSeconds) |
| | Delays for specific time in microseconds. More...
|
| |
| __STATIC_INLINE void | HAL_updatePWM (const HAL_PWM posPhase, const HAL_PWM gndPhase, const HAL_PWM opnPhase, const uint16_t PWMDuty) |
| | Writes the pwm to the pinouts. More...
|
| |
| __STATIC_INLINE void | HAL_PWMOutputLow (const HAL_PWM gndPhase_1, const HAL_PWM gndPhase_2, const HAL_PWM gndPhase_3) |
| | Set all PWM outputs low. More...
|
| |
| __STATIC_INLINE void | HAL_PWMOutputHigh (const HAL_PWM gndPhase_1, const HAL_PWM gndPhase_2, const HAL_PWM gndPhase_3) |
| | Set complementary PWM outputs high. More...
|
| |