MSPM0G1X0X_G3X0X TI-Driver Library  2.05.01.00
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
I2CTarget.h File Reference

Detailed Description

I2CTarget driver interface.


This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  I2CTarget_Params
 I2CTarget Parameters. More...
 
struct  I2CTarget_Config_
 I2CTarget Global configuration. More...
 

Macros

#define I2CTarget_STATUS_SUCCESS   (0)
 Successful status code returned by application event callback function. More...
 
#define I2CTarget_STATUS_ERROR   (-1)
 Generic error status code returned by application event callback function. More...
 
#define I2C_TARGET_OWN_ADDRESS   (0x48)
 Default own address of the I2C Target.
 

Typedefs

typedef struct I2CTarget_Config_I2CTarget_Handle
 A handle that is returned from a I2CTarget_open() call.
 
typedef int_fast16_t(* I2CTarget_EventCallbackFxn) (I2CTarget_Handle handle, I2CTarget_Event event, uint8_t *val)
 I2CTarget event callback function. More...
 
typedef struct I2CTarget_Config_ I2CTarget_Config
 I2CTarget Global configuration. More...
 

Enumerations

enum  I2CTarget_Event {
  I2CTarget_Event_WRITE_REQUESTED,
  I2CTarget_Event_READ_REQUESTED,
  I2CTarget_Event_WRITE_RECEIVED,
  I2CTarget_Event_READ_PROCESSED,
  I2CTarget_Event_STOP
}
 I2CTarget events that the application's I2CTarget_EventCallbackFxn must support. More...
 

Functions

void I2CTarget_init (void)
 Function to initializes the I2CTarget module. More...
 
void I2CTarget_Params_init (I2CTarget_Params *params)
 Function to initialize the I2CTarget_Params struct to its defaults. More...
 
I2CTarget_Handle I2CTarget_open (uint_least8_t index, I2CTarget_Params *params)
 Function to initialize a given I2C target peripheral specified by the particular index value. The parameter specifies which mode the I2CTarget will operate. More...
 
void I2CTarget_start (I2CTarget_Handle handle)
 Start I2CTarget driver listening on I2C bus. More...
 
void I2CTarget_stop (I2CTarget_Handle handle)
 Stop I2CTarget driver from listening on I2C bus. More...
 
void I2CTarget_close (I2CTarget_Handle handle)
 

Variables

const I2CTarget_Config I2CTarget_config []
 
const uint_least8_t I2CTarget_count
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale