![]() |
![]() |
|
MSPM0L111X TI-Driver Library
2.05.00.05
|
General Purpose I/O driver interface.


Go to the source code of this file.
Data Structures | |
| struct | GPIO_Config |
| GPIO driver configuration structure. More... | |
Macros | |
| #define | GPIO_PIN_TO_MASK(pin) (1 << (pin)) |
| Convert the pin index to mask. | |
| #define | GPIO_STATUS_SUCCESS (0) |
| Successful status code returned by GPI_setConfig(). More... | |
| #define | GPIO_STATUS_ERROR (-1) |
| Generic error status code returned by GPI_setConfig(). More... | |
| #define | GPIO_INVALID_INDEX 0xFF |
| Dummy value for "this pin is not assigned to a GPIO". More... | |
GPIO_PinConfig output pin configuration macros. | |
| #define | GPIO_CFG_OUTPUT |
| #define | GPIO_CFG_OUT_STD |
| #define | GPIO_CFG_OUT_OD_NOPULL |
| #define | GPIO_CFG_OUT_OD_PU |
| #define | GPIO_CFG_OUT_OD_PD |
| #define | GPIO_CFG_OUT_STR_LOW |
| #define | GPIO_CFG_OUT_STR_MED |
| #define | GPIO_CFG_OUT_STR_HIGH |
| #define | GPIO_CFG_OUT_HIGH |
| #define | GPIO_CFG_OUT_LOW |
GPIO_PinConfig input pin configuration macros | |
| #define | GPIO_CFG_INPUT |
| #define | GPIO_CFG_IN_NOPULL |
| #define | GPIO_CFG_IN_PU |
| #define | GPIO_CFG_IN_PD |
GPIO_PinConfig pin inversion configuration macros. | |
| #define | GPIO_CFG_INVERT_OFF |
| #define | GPIO_CFG_INVERT_ON |
GPIO_PinConfig pin hysteresis configuration macros. | |
| #define | GPIO_CFG_HYSTERESIS_OFF |
| #define | GPIO_CFG_HYSTERESIS_ON |
GPIO_PinConfig pin Hi-Z configuration macros. | |
| #define | GPIO_CFG_HIZ_OFF |
| #define | GPIO_CFG_HIZ_ON |
GPIO_PinConfig interrupt configuration macros. | |
| #define | GPIO_CFG_IN_INT_NONE |
| #define | GPIO_CFG_IN_INT_RISING |
| #define | GPIO_CFG_IN_INT_FALLING |
| #define | GPIO_CFG_IN_INT_BOTH_EDGES |
| #define | GPIO_CFG_IN_INT_LOW |
| #define | GPIO_CFG_IN_INT_HIGH |
GPIO_PinConfig wakeup configuration macros. | |
| #define | GPIO_CFG_WAKEUP_DISABLE |
| #define | GPIO_CFG_WAKEUP_ON_0 |
| #define | GPIO_CFG_WAKEUP_ON_1 |
Special GPIO_PinConfig configuration macros. | |
| #define | GPIO_DO_NOT_CONFIG |
| Use this GPIO_PinConfig definition to inform GPIO_init() NOT to configure the corresponding pin. More... | |
GPIO_Mux configuration macros | |
For additional muxing options, see the directions in the device-specific GPIO driver. | |
| #define | GPIO_MUX_GPIO |
Typedefs | |
| typedef uint32_t | GPIO_PinConfig |
| GPIO pin configuration settings. More... | |
| typedef void(* | GPIO_CallbackFxn) (uint_least8_t index) |
| GPIO callback function type. More... | |
Functions | |
| void | GPIO_clearInt (uint_least8_t index) |
| Clear a GPIO pin interrupt flag. More... | |
| void | GPIO_disableInt (uint_least8_t index) |
| Disable a GPIO pin interrupt. More... | |
| void | GPIO_enableInt (uint_least8_t index) |
| Enable a GPIO pin interrupt. More... | |
| void | GPIO_init () |
| Initializes the GPIO module. More... | |
| uint_fast8_t | GPIO_read (uint_least8_t index) |
| Reads the value of a GPIO pin. More... | |
| void | GPIO_toggle (uint_least8_t index) |
| Toggles the current state of a GPIO. More... | |
| void | GPIO_write (uint_least8_t index, unsigned int value) |
| Writes the value to a GPIO pin. More... | |
| void | GPIO_setCallback (uint_least8_t index, GPIO_CallbackFxn callback) |
| Bind a callback function to a GPIO pin interrupt. More... | |
| GPIO_CallbackFxn | GPIO_getCallback (uint_least8_t index) |
| Gets the callback associated with a GPIO pin. More... | |
| int_fast16_t | GPIO_setConfig (uint_least8_t index, GPIO_PinConfig pinConfig) |
| Configure the gpio pin. More... | |
| void | GPIO_setInterruptConfig (uint_least8_t index, GPIO_PinConfig config) |
| Configure the gpio pin. More... | |
| void | GPIO_getConfig (uint_least8_t index, GPIO_PinConfig *pinConfig) |
| Get the current configuration for a gpio pin. More... | |
| void | GPIO_resetConfig (uint_least8_t index) |
| Resets the configuration for a gpio pin to the default value. More... | |
| uint32_t | GPIO_getMux (uint_least8_t index) |
| Get the current mux for a gpio pin. More... | |
| int_fast16_t | GPIO_setConfigAndMux (uint_least8_t index, GPIO_PinConfig pinConfig, uint32_t mux) |
| Configure the gpio pin's config and mux in a single write. More... | |
| void | GPIO_setUserArg (uint_least8_t index, void *arg) |
| Set the user argument for a gpio pin. More... | |
| void * | GPIO_getUserArg (uint_least8_t index) |
| Get the user argument for a gpio pin. More... | |