MSPM0GX51X TI-Driver Library  2.05.00.05
Functions
I2CSupport.h File Reference

Detailed Description

Holder of common helper functions for the I2C driver.


#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/driverlib/dl_i2c.h>
#include <ti/drivers/I2C.h>
Include dependency graph for I2CSupport.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

void I2CSupport_controllerFinish (I2C_HWAttrs const *hwAttrs)
 Function to send a finish command to the controller module. More...
 
void I2CSupport_powerSetConstraint (void)
 Function to set power constraint.
 
void I2CSupport_powerRelConstraint (void)
 Function to release power constraint.
 
int_fast16_t I2CSupport_primeTransfer (I2C_Handle handle, I2C_Transaction *transaction)
 Function to initialize transfers. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale