52 #ifndef ti_dl_dl_rtc_common__include 53 #define ti_dl_dl_rtc_common__include 58 #include <ti/devices/msp/msp.h> 61 #if defined __MSPM0_HAS_RTC_A__ || defined __MSPM0_HAS_RTC_B__ || \ 62 defined __MSPM0_HAS_RTC__ || defined(DOXYGEN__INCLUDE) 77 #define DL_RTC_COMMON_INTERRUPT_CALENDAR_ALARM1 (RTC_CPU_INT_IMASK_RTCA1_SET) 82 #define DL_RTC_COMMON_INTERRUPT_CALENDAR_ALARM2 (RTC_CPU_INT_IMASK_RTCA2_SET) 87 #define DL_RTC_COMMON_INTERRUPT_PRESCALER0 (RTC_CPU_INT_IMASK_RT0PS_SET) 92 #define DL_RTC_COMMON_INTERRUPT_PRESCALER1 (RTC_CPU_INT_IMASK_RT1PS_SET) 94 #ifdef __MSPM0_HAS_RTC_A__ 98 #define DL_RTC_COMMON_INTERRUPT_PRESCALER2 (RTC_CPU_INT_IMASK_RT2PS_SET) 104 #define DL_RTC_COMMON_INTERRUPT_INTERVAL_ALARM (RTC_CPU_INT_IMASK_RTCTEV_SET) 109 #define DL_RTC_COMMON_INTERRUPT_READY (RTC_CPU_INT_IMASK_RTCRDY_SET) 111 #ifdef __MSPM0_HAS_RTC_A__ 115 #define DL_RTC_COMMON_INTERRUPT_TSEVT (RTC_CPU_INT_IMASK_TSEVT_SET) 127 #define DL_RTC_COMMON_EVENT_CALENDAR_ALARM1 (RTC_GEN_EVENT_IMASK_RTCA1_SET) 132 #define DL_RTC_COMMON_EVENT_CALENDAR_ALARM2 (RTC_GEN_EVENT_IMASK_RTCA2_SET) 137 #define DL_RTC_COMMON_EVENT_PRESCALER0 (RTC_GEN_EVENT_IMASK_RT0PS_SET) 142 #define DL_RTC_COMMON_EVENT_PRESCALER1 (RTC_GEN_EVENT_IMASK_RT1PS_SET) 144 #ifdef __MSPM0_HAS_RTC_A__ 148 #define DL_RTC_COMMON_EVENT_PRESCALER2 (RTC_GEN_EVENT_IMASK_RT2PS_SET) 154 #define DL_RTC_COMMON_EVENT_INTERVAL_ALARM (RTC_GEN_EVENT_IMASK_RTCTEV_SET) 159 #define DL_RTC_COMMON_EVENT_READY (RTC_GEN_EVENT_IMASK_RTCRDY_SET) 161 #ifdef __MSPM0_HAS_RTC_A__ 165 #define DL_RTC_COMMON_EVENT_TSEVT (RTC_GEN_EVENT_IMASK_TSEVT_SET) 170 #ifdef __MSPM0_HAS_RTC_A__ 178 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_0 (RTC_TSSTAT_TSTIOEVT0_SET) 183 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_1 (RTC_TSSTAT_TSTIOEVT1_SET) 188 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_2 (RTC_TSSTAT_TSTIOEVT2_SET) 193 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_3 (RTC_TSSTAT_TSTIOEVT3_SET) 198 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_4 (RTC_TSSTAT_TSTIOEV4_SET) 203 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_5 (RTC_TSSTAT_TSTIOEVT5_SET) 208 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_6 (RTC_TSSTAT_TSTIOEVT6_SET) 213 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_7 (RTC_TSSTAT_TSTIOEVT7_SET) 218 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_8 (RTC_TSSTAT_TSTIOEV8_SET) 223 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_9 (RTC_TSSTAT_TSTIOEVT9_SET) 228 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_10 (RTC_TSSTAT_TSTIOEVT10_SET) 233 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_11 (RTC_TSSTAT_TSTIOEVT11_SET) 238 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_12 (RTC_TSSTAT_TSTIOEVT12_SET) 243 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_13 (RTC_TSSTAT_TSTIOEVT13_SET) 248 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_14 (RTC_TSSTAT_TSTIOEVT14_SET) 253 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_TIO_15 (RTC_TSSTAT_TSTIOEVT15_SET) 258 #define DL_RTC_COMMON_TIME_STAMP_EVENT_CAUSE_VDD_LOSS (RTC_TSSTAT_TSVDDEVT_SET) 269 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_0 (RTC_TSCTL_TSTIOEN0_ENABLE) 274 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_1 (RTC_TSCTL_TSTIOEN1_ENABLE) 279 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_2 (RTC_TSCTL_TSTIOEN2_ENABLE) 284 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_3 (RTC_TSCTL_TSTIOEN3_ENABLE) 289 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_4 (RTC_TSCTL_TSTIOEN4_ENABLE) 294 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_5 (RTC_TSCTL_TSTIOEN5_ENABLE) 299 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_6 (RTC_TSCTL_TSTIOEN6_ENABLE) 304 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_7 (RTC_TSCTL_TSTIOEN8_ENABLE) 309 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_8 (RTC_TSCTL_TSTIOEN8_ENABLE) 314 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_9 (RTC_TSCTL_TSTIOEN9_ENABLE) 319 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_10 (RTC_TSCTL_TSTIOEN10_ENABLE) 324 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_11 (RTC_TSCTL_TSTIOEN11_ENABLE) 329 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_12 (RTC_TSCTL_TSTIOEN12_ENABLE) 334 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_13 (RTC_TSCTL_TSTIOEN13_ENABLE) 339 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_14 (RTC_TSCTL_TSTIOEN14_ENABLE) 344 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_TIO_15 (RTC_TSCTL_TSTIOEN15_ENABLE) 349 #define DL_RTC_COMMON_TIME_STAMP_EVENT_SOURCE_VDD_LOSS (RTC_TSCTL_TSVDDEN_ENABLE) 388 #ifdef __MSPM0_HAS_RTC__ 392 #ifdef __MSPM0_HAS_RTC_A__ 394 DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY_32_KHZ = LFSS_CAL_RTCCALFX_F32KHZ,
495 #ifdef __MSPM0_HAS_RTC_A__ 496 DL_RTC_COMMON_IIDX_TSEVT = RTC_CPU_INT_IIDX_STAT_TSEVT,
498 DL_RTC_COMMON_IIDX_TAMPER_IO_0 = RTC_CPU_INT_IIDX_STAT_TIO0,
500 DL_RTC_COMMON_IIDX_TAMPER_IO_1 = RTC_CPU_INT_IIDX_STAT_TIO1,
502 DL_RTC_COMMON_IIDX_TAMPER_IO_2 = RTC_CPU_INT_IIDX_STAT_TIO2,
504 DL_RTC_COMMON_IIDX_TAMPER_IO_3 = RTC_CPU_INT_IIDX_STAT_TIO3,
506 DL_RTC_COMMON_IIDX_TAMPER_IO_4 = RTC_CPU_INT_IIDX_STAT_TIO4,
508 DL_RTC_COMMON_IIDX_TAMPER_IO_5 = RTC_CPU_INT_IIDX_STAT_TIO5,
510 DL_RTC_COMMON_IIDX_TAMPER_IO_6 = RTC_CPU_INT_IIDX_STAT_TIO6,
512 DL_RTC_COMMON_IIDX_TAMPER_IO_7 = RTC_CPU_INT_IIDX_STAT_TIO7,
514 DL_RTC_COMMON_IIDX_TAMPER_IO_8 = RTC_CPU_INT_IIDX_STAT_TIO8,
516 DL_RTC_COMMON_IIDX_TAMPER_IO_9 = RTC_CPU_INT_IIDX_STAT_TIO9,
518 DL_RTC_COMMON_IIDX_TAMPER_IO_10 = RTC_CPU_INT_IIDX_STAT_TIO10,
520 DL_RTC_COMMON_IIDX_TAMPER_IO_11 = RTC_CPU_INT_IIDX_STAT_TIO11,
522 DL_RTC_COMMON_IIDX_TAMPER_IO_12 = RTC_CPU_INT_IIDX_STAT_TIO12,
524 DL_RTC_COMMON_IIDX_TAMPER_IO_13 = RTC_CPU_INT_IIDX_STAT_TIO13,
526 DL_RTC_COMMON_IIDX_TAMPER_IO_14 = RTC_CPU_INT_IIDX_STAT_TIO14,
528 DL_RTC_COMMON_IIDX_TAMPER_IO_15 = RTC_CPU_INT_IIDX_STAT_TIO15,
532 #ifdef __MSPM0_HAS_RTC_A__ 536 DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE_FIRST = RTC_TSCTL_TSCAPTURE_FIRST,
538 DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE_LAST = RTC_TSCTL_TSCAPTURE_LAST,
539 } DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE;
606 const RTC_Regs *rtc_common)
608 return ((rtc_common->CLKSEL & RTC_CLKSEL_LFCLK_SEL_MASK) ==
609 RTC_CLKSEL_LFCLK_SEL_MASK);
621 rtc_common->CLKCTL = RTC_CLKCTL_MODCLKEN_ENABLE;
631 rtc_common->CLKCTL = RTC_CLKCTL_MODCLKEN_DISABLE;
645 rtc_common->GPRCM.PWREN =
646 (RTC_PWREN_KEY_UNLOCK_W | RTC_PWREN_ENABLE_ENABLE);
661 rtc_common->GPRCM.PWREN =
662 (RTC_PWREN_KEY_UNLOCK_W | RTC_PWREN_ENABLE_DISABLE);
683 return ((rtc_common->GPRCM.PWREN & RTC_PWREN_ENABLE_MASK) ==
684 RTC_PWREN_ENABLE_ENABLE);
695 rtc_common->GPRCM.RSTCTL =
696 (RTC_RSTCTL_KEY_UNLOCK_W | RTC_RSTCTL_RESETSTKYCLR_CLR |
697 RTC_RSTCTL_RESETASSERT_ASSERT);
711 return ((rtc_common->GPRCM.STAT & RTC_STAT_RESETSTKY_MASK) ==
712 RTC_STAT_RESETSTKY_RESET);
724 rtc_common->DBGCTL |= RTC_DBGCTL_DBGINT_ON;
737 rtc_common->DBGCTL &= ~(RTC_DBGCTL_DBGINT_MASK);
748 rtc_common->DBGCTL |= RTC_DBGCTL_DBGRUN_RUN;
759 rtc_common->DBGCTL &= ~(RTC_DBGCTL_DBGRUN_MASK);
772 RTC_Regs *rtc_common, DL_RTC_COMMON_FORMAT formatSelect)
774 rtc_common->CTL |= (uint32_t) formatSelect;
788 const RTC_Regs *rtc_common)
790 uint32_t format = (rtc_common->CTL & RTC_CTL_RTCBCD_MASK);
792 return (DL_RTC_COMMON_FORMAT)(format);
812 RTC_Regs *rtc_common, DL_RTC_COMMON_INTERVAL_ALARM alarmEvent)
815 &rtc_common->CTL, (uint32_t) alarmEvent, RTC_CTL_RTCTEVTX_MASK);
833 const RTC_Regs *rtc_common)
835 uint32_t alarm = (rtc_common->CTL & RTC_CTL_RTCTEVTX_MASK);
837 return (DL_RTC_COMMON_INTERVAL_ALARM)(alarm);
859 return ((rtc_common->STA & RTC_STA_RTCRDY_MASK) == RTC_STA_RTCRDY_READY);
872 const RTC_Regs *rtc_common)
875 (rtc_common->STA & RTC_STA_RTCTCRDY_MASK) == RTC_STA_RTCTCRDY_READY);
888 const RTC_Regs *rtc_common)
890 return ((rtc_common->STA & RTC_STA_RTCTCOK_MASK) == RTC_STA_RTCTCOK_OK);
906 RTC_Regs *rtc_common,
907 DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY offsetFrequency)
910 &rtc_common->CAL, (uint32_t) offsetFrequency, RTC_CAL_RTCCALFX_MASK);
929 RTC_Regs *rtc_common, DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN offsetSign,
933 ((uint32_t) offsetSign | (uint32_t) offsetValue),
934 (RTC_CAL_RTCOCALX_MASK | RTC_CAL_RTCOCALS_MASK));
960 DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY offsetFrequency,
961 DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN offsetSign, uint8_t offsetValue)
963 rtc_common->CAL = (offsetValue & RTC_CAL_RTCOCALX_MASK) |
964 (uint32_t) offsetFrequency | (uint32_t) offsetSign;
976 __STATIC_INLINE DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY
979 uint32_t freq = (rtc_common->CAL & RTC_CAL_RTCCALFX_MASK);
981 return (DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY)(freq);
993 __STATIC_INLINE DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN
996 uint32_t sign = (rtc_common->CAL & RTC_CAL_RTCOCALS_MASK);
998 return (DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN)(sign);
1018 RTC_Regs *rtc_common, DL_RTC_COMMON_TEMP_CALIBRATION offsetDirection,
1019 uint32_t offsetValue)
1022 (offsetValue & RTC_TCMP_RTCTCMPX_MASK) | (uint32_t) offsetDirection;
1037 const RTC_Regs *rtc_common)
1039 return (rtc_common->TCMP);
1050 RTC_Regs *rtc_common, uint8_t seconds)
1052 rtc_common->SEC = ((uint32_t) seconds << RTC_SEC_SECLOWBCD_OFS) &
1053 (RTC_SEC_SECLOWBCD_MASK | RTC_SEC_SECHIGHBCD_MASK);
1071 const RTC_Regs *rtc_common)
1073 return (uint8_t)((rtc_common->SEC &
1074 (RTC_SEC_SECLOWBCD_MASK | RTC_SEC_SECHIGHBCD_MASK)) >>
1075 RTC_SEC_SECLOWBCD_OFS);
1086 RTC_Regs *rtc_common, uint8_t minutes)
1088 rtc_common->MIN = ((uint32_t) minutes << RTC_MIN_MINLOWBCD_OFS) &
1089 (RTC_MIN_MINLOWBCD_MASK | RTC_MIN_MINHIGHBCD_MASK);
1107 const RTC_Regs *rtc_common)
1109 return (uint8_t)((rtc_common->MIN &
1110 (RTC_MIN_MINLOWBCD_MASK | RTC_MIN_MINHIGHBCD_MASK)) >>
1111 RTC_MIN_MINLOWBCD_OFS);
1122 RTC_Regs *rtc_common, uint8_t hours)
1124 rtc_common->HOUR = ((uint32_t) hours << RTC_HOUR_HOURLOWBCD_OFS) &
1125 (RTC_HOUR_HOURLOWBCD_MASK | RTC_HOUR_HOURHIGHBCD_MASK);
1143 const RTC_Regs *rtc_common)
1145 return (uint8_t)((rtc_common->HOUR & (RTC_HOUR_HOURLOWBCD_MASK |
1146 RTC_HOUR_HOURHIGHBCD_MASK)) >>
1147 RTC_HOUR_HOURLOWBCD_OFS);
1158 RTC_Regs *rtc_common, uint8_t day)
1178 const RTC_Regs *rtc_common)
1180 return (uint8_t)(rtc_common->DAY & RTC_DAY_DOW_MASK);
1191 RTC_Regs *rtc_common, uint8_t day)
1194 (uint32_t) day << RTC_DAY_DOMLOWBCD_OFS,
1195 (RTC_DAY_DOMLOWBCD_MASK | RTC_DAY_DOMHIGHBCD_MASK));
1213 const RTC_Regs *rtc_common)
1215 return (uint8_t)((rtc_common->DAY &
1216 (RTC_DAY_DOMLOWBCD_MASK | RTC_DAY_DOMHIGHBCD_MASK)) >>
1217 RTC_DAY_DOMLOWBCD_OFS);
1228 RTC_Regs *rtc_common, uint8_t month)
1230 rtc_common->MON = ((uint32_t) month << RTC_MON_MONLOWBCD_OFS) &
1231 (RTC_MON_MONLOWBCD_MASK | RTC_MON_MONHIGHBCD_MASK);
1249 const RTC_Regs *rtc_common)
1251 return (uint8_t)((rtc_common->MON &
1252 (RTC_MON_MONLOWBCD_MASK | RTC_MON_MONHIGHBCD_MASK)) >>
1253 RTC_MON_MONLOWBCD_OFS);
1264 RTC_Regs *rtc_common, uint16_t year)
1267 ((uint32_t) year << RTC_YEAR_YEARLOWESTBCD_OFS) &
1268 (RTC_YEAR_YEARLOWESTBCD_MASK | RTC_YEAR_DECADEBCD_MASK |
1269 RTC_YEAR_CENTLOWBCD_MASK | RTC_YEAR_CENTHIGHBCD_MASK);
1287 const RTC_Regs *rtc_common)
1291 (RTC_YEAR_YEARLOWESTBCD_MASK | RTC_YEAR_DECADEBCD_MASK |
1292 RTC_YEAR_CENTLOWBCD_MASK | RTC_YEAR_CENTHIGHBCD_MASK)) >>
1293 RTC_YEAR_YEARLOWESTBCD_OFS);
1304 rtc_common->A1MIN |= RTC_A1MIN_AMINAEBCD_ENABLE;
1314 RTC_Regs *rtc_common)
1316 rtc_common->A1MIN &= ~(RTC_A1MIN_AMINAEBCD_MASK);
1328 RTC_Regs *rtc_common, uint8_t minutes)
1331 ((uint32_t) minutes << RTC_A1MIN_AMINLOWBCD_OFS) &
1332 (RTC_A1MIN_AMINLOWBCD_MASK | RTC_A1MIN_AMINHIGHBCD_MASK);
1346 const RTC_Regs *rtc_common)
1348 return (uint8_t)((rtc_common->A1MIN & (RTC_A1MIN_AMINLOWBCD_MASK |
1349 RTC_A1MIN_AMINHIGHBCD_MASK)) >>
1350 RTC_A1MIN_AMINLOWBCD_OFS);
1361 rtc_common->A1HOUR |= RTC_A1HOUR_AHOURAEBIN_ENABLE;
1372 rtc_common->A1HOUR &= ~(RTC_A1HOUR_AHOURAEBIN_MASK);
1383 RTC_Regs *rtc_common, uint8_t hours)
1385 rtc_common->A1HOUR =
1386 ((uint32_t) hours << RTC_A1HOUR_AHOURLOWBCD_OFS) &
1387 (RTC_A1HOUR_AHOURLOWBCD_MASK | RTC_A1HOUR_AHOURHIGHBCD_MASK);
1401 const RTC_Regs *rtc_common)
1404 (rtc_common->A1HOUR &
1405 (RTC_A1HOUR_AHOURLOWBCD_MASK | RTC_A1HOUR_AHOURHIGHBCD_MASK)) >>
1406 RTC_A1HOUR_AHOURLOWBCD_OFS);
1416 RTC_Regs *rtc_common)
1418 rtc_common->A1DAY |= RTC_A1DAY_ADOWAE_ENABLE;
1428 RTC_Regs *rtc_common)
1430 rtc_common->A1DAY &= ~(RTC_A1DAY_ADOWAE_MASK);
1441 RTC_Regs *rtc_common, uint8_t day)
1457 const RTC_Regs *rtc_common)
1459 return (uint8_t)(rtc_common->DAY & RTC_A1DAY_ADOW_MASK);
1469 RTC_Regs *rtc_common)
1471 rtc_common->A1DAY |= RTC_A1DAY_ADOMAEBCD_ENABLE;
1481 RTC_Regs *rtc_common)
1483 rtc_common->A1DAY &= ~(RTC_A1DAY_ADOMAEBCD_MASK);
1494 RTC_Regs *rtc_common, uint8_t day)
1497 (uint32_t) day << RTC_A1DAY_ADOMLOWBCD_OFS,
1498 (RTC_A1DAY_ADOMLOWBCD_MASK | RTC_A1DAY_ADOMHIGHBCD_MASK));
1512 const RTC_Regs *rtc_common)
1514 return (uint8_t)((rtc_common->A1DAY & (RTC_A1DAY_ADOMLOWBCD_MASK |
1515 RTC_A1DAY_ADOMHIGHBCD_MASK)) >>
1516 RTC_A1DAY_ADOMLOWBCD_OFS);
1527 rtc_common->A2MIN |= RTC_A2MIN_AMINAEBCD_ENABLE;
1537 RTC_Regs *rtc_common)
1539 rtc_common->A2MIN &= ~(RTC_A2MIN_AMINAEBCD_MASK);
1551 RTC_Regs *rtc_common, uint8_t minutes)
1554 ((uint32_t) minutes << RTC_A2MIN_AMINLOWBCD_OFS) &
1555 (RTC_A2MIN_AMINLOWBCD_MASK | RTC_A2MIN_AMINHIGHBCD_MASK);
1569 const RTC_Regs *rtc_common)
1571 return (uint8_t)((rtc_common->A2MIN & (RTC_A2MIN_AMINLOWBCD_MASK |
1572 RTC_A2MIN_AMINHIGHBCD_MASK)) >>
1573 RTC_A2MIN_AMINLOWBCD_OFS);
1584 rtc_common->A2HOUR |= RTC_A2HOUR_AHOURAEBIN_ENABLE;
1595 rtc_common->A2HOUR &= ~(RTC_A2HOUR_AHOURAEBIN_MASK);
1606 RTC_Regs *rtc_common, uint8_t hours)
1608 rtc_common->A2HOUR =
1609 ((uint32_t) hours << RTC_A2HOUR_AHOURLOWBCD_OFS) &
1610 (RTC_A2HOUR_AHOURLOWBCD_MASK | RTC_A2HOUR_AHOURHIGHBCD_MASK);
1624 const RTC_Regs *rtc_common)
1627 (rtc_common->A2HOUR &
1628 (RTC_A2HOUR_AHOURLOWBCD_MASK | RTC_A2HOUR_AHOURHIGHBCD_MASK)) >>
1629 RTC_A2HOUR_AHOURLOWBCD_OFS);
1639 RTC_Regs *rtc_common)
1641 rtc_common->A2DAY |= RTC_A2DAY_ADOWAE_ENABLE;
1651 RTC_Regs *rtc_common)
1653 rtc_common->A2DAY &= ~(RTC_A2DAY_ADOWAE_MASK);
1664 RTC_Regs *rtc_common, uint8_t day)
1680 const RTC_Regs *rtc_common)
1682 return (uint8_t)(rtc_common->DAY & RTC_A2DAY_ADOW_MASK);
1692 RTC_Regs *rtc_common)
1694 rtc_common->A2DAY |= RTC_A2DAY_ADOMAEBCD_ENABLE;
1704 RTC_Regs *rtc_common)
1706 rtc_common->A2DAY &= ~(RTC_A2DAY_ADOMAEBCD_MASK);
1717 RTC_Regs *rtc_common, uint8_t day)
1720 (uint32_t) day << RTC_A2DAY_ADOMLOWBCD_OFS,
1721 (RTC_A2DAY_ADOMLOWBCD_MASK | RTC_A2DAY_ADOMHIGHBCD_MASK));
1735 const RTC_Regs *rtc_common)
1737 return (uint8_t)((rtc_common->A2DAY & (RTC_A2DAY_ADOMLOWBCD_MASK |
1738 RTC_A2DAY_ADOMHIGHBCD_MASK)) >>
1739 RTC_A2DAY_ADOMLOWBCD_OFS);
1750 RTC_Regs *rtc_common, uint8_t seconds)
1752 rtc_common->SEC = (seconds & RTC_SEC_SECBIN_MASK);
1770 const RTC_Regs *rtc_common)
1772 return (uint8_t)(rtc_common->SEC & RTC_SEC_SECBIN_MASK);
1783 RTC_Regs *rtc_common, uint8_t minutes)
1785 rtc_common->MIN = (minutes & RTC_MIN_MINBIN_MASK);
1803 const RTC_Regs *rtc_common)
1805 return (uint8_t)(rtc_common->MIN & RTC_MIN_MINBIN_MASK);
1816 RTC_Regs *rtc_common, uint8_t hours)
1818 rtc_common->HOUR = (hours & RTC_HOUR_HOURBIN_MASK);
1836 const RTC_Regs *rtc_common)
1838 return (uint8_t)(rtc_common->HOUR & RTC_HOUR_HOURBIN_MASK);
1849 RTC_Regs *rtc_common, uint8_t day)
1869 const RTC_Regs *rtc_common)
1871 return (uint8_t)(rtc_common->DAY & RTC_DAY_DOW_MASK);
1882 RTC_Regs *rtc_common, uint8_t day)
1885 RTC_DAY_DOMBIN_MASK);
1903 const RTC_Regs *rtc_common)
1906 (rtc_common->DAY & RTC_DAY_DOMBIN_MASK) >> RTC_DAY_DOMBIN_OFS);
1917 RTC_Regs *rtc_common, uint8_t month)
1919 rtc_common->MON = (month & RTC_MON_MONBIN_MASK);
1937 const RTC_Regs *rtc_common)
1939 return (uint8_t)(rtc_common->MON & RTC_MON_MONBIN_MASK);
1950 RTC_Regs *rtc_common, uint16_t year)
1952 rtc_common->YEAR = ((uint32_t) year & (RTC_YEAR_YEARLOWBIN_MASK |
1953 RTC_YEAR_YEARHIGHBIN_MASK));
1971 const RTC_Regs *rtc_common)
1973 return (uint16_t)(rtc_common->YEAR &
1974 (RTC_YEAR_YEARLOWBIN_MASK | RTC_YEAR_YEARHIGHBIN_MASK));
1984 RTC_Regs *rtc_common)
1986 rtc_common->A1MIN |= RTC_A1MIN_AMINAEBIN_ENABLE;
1996 RTC_Regs *rtc_common)
1998 rtc_common->A1MIN &= ~(RTC_A1MIN_AMINAEBIN_MASK);
2010 RTC_Regs *rtc_common, uint8_t minutes)
2012 rtc_common->A1MIN = (minutes & RTC_A1MIN_AMINBIN_MASK);
2026 const RTC_Regs *rtc_common)
2028 return (uint8_t)(rtc_common->A1MIN & RTC_A1MIN_AMINBIN_MASK);
2038 RTC_Regs *rtc_common)
2040 rtc_common->A1HOUR |= RTC_A1HOUR_AHOURAEBIN_ENABLE;
2050 RTC_Regs *rtc_common)
2052 rtc_common->A1HOUR &= ~(RTC_A1HOUR_AHOURAEBIN_MASK);
2063 RTC_Regs *rtc_common, uint8_t hours)
2065 rtc_common->A1HOUR = (hours & RTC_A1HOUR_AHOURBIN_MASK);
2079 const RTC_Regs *rtc_common)
2081 return (uint8_t)(rtc_common->A1HOUR & RTC_A1HOUR_AHOURBIN_MASK);
2091 RTC_Regs *rtc_common)
2093 rtc_common->A1DAY |= RTC_A1DAY_ADOWAE_ENABLE;
2103 RTC_Regs *rtc_common)
2105 rtc_common->A1DAY &= ~(RTC_A1DAY_ADOWAE_MASK);
2116 RTC_Regs *rtc_common, uint8_t day)
2132 const RTC_Regs *rtc_common)
2134 return (uint8_t)(rtc_common->A1DAY & RTC_A1DAY_ADOW_MASK);
2144 RTC_Regs *rtc_common)
2146 rtc_common->A1DAY |= RTC_A1DAY_ADOMAEBIN_ENABLE;
2156 RTC_Regs *rtc_common)
2158 rtc_common->A1DAY &= ~(RTC_A1DAY_ADOMAEBIN_MASK);
2169 RTC_Regs *rtc_common, uint8_t day)
2172 (uint32_t) day << RTC_A1DAY_ADOMBIN_OFS, RTC_A1DAY_ADOMBIN_MASK);
2186 const RTC_Regs *rtc_common)
2189 (rtc_common->A1DAY & RTC_A1DAY_ADOMBIN_MASK) >> RTC_A1DAY_ADOMBIN_OFS);
2199 RTC_Regs *rtc_common)
2201 rtc_common->A2MIN |= RTC_A2MIN_AMINAEBIN_ENABLE;
2211 RTC_Regs *rtc_common)
2213 rtc_common->A2MIN &= ~(RTC_A2MIN_AMINAEBIN_MASK);
2225 RTC_Regs *rtc_common, uint8_t minutes)
2227 rtc_common->A2MIN = (minutes & RTC_A2MIN_AMINBIN_MASK);
2241 const RTC_Regs *rtc_common)
2243 return (uint8_t)(rtc_common->A2MIN & RTC_A2MIN_AMINBIN_MASK);
2253 RTC_Regs *rtc_common)
2255 rtc_common->A2HOUR |= RTC_A2HOUR_AHOURAEBIN_ENABLE;
2265 RTC_Regs *rtc_common)
2267 rtc_common->A2HOUR &= ~(RTC_A2HOUR_AHOURAEBIN_MASK);
2278 RTC_Regs *rtc_common, uint8_t hours)
2280 rtc_common->A2HOUR = (hours & RTC_A2HOUR_AHOURBIN_MASK);
2294 const RTC_Regs *rtc_common)
2296 return (uint8_t)(rtc_common->A2HOUR & RTC_A2HOUR_AHOURBIN_MASK);
2306 RTC_Regs *rtc_common)
2308 rtc_common->A2DAY |= RTC_A2DAY_ADOWAE_ENABLE;
2318 RTC_Regs *rtc_common)
2320 rtc_common->A2DAY &= ~(RTC_A2DAY_ADOWAE_MASK);
2331 RTC_Regs *rtc_common, uint8_t day)
2347 const RTC_Regs *rtc_common)
2349 return (uint8_t)(rtc_common->A2DAY & RTC_A2DAY_ADOW_MASK);
2359 RTC_Regs *rtc_common)
2361 rtc_common->A2DAY |= RTC_A2DAY_ADOMAEBIN_ENABLE;
2371 RTC_Regs *rtc_common)
2373 rtc_common->A2DAY &= ~(RTC_A2DAY_ADOMAEBIN_MASK);
2384 RTC_Regs *rtc_common, uint8_t day)
2387 (uint32_t) day << RTC_A2DAY_ADOMBIN_OFS, RTC_A2DAY_ADOMBIN_MASK);
2401 const RTC_Regs *rtc_common)
2404 (rtc_common->A2DAY & RTC_A2DAY_ADOMBIN_MASK) >> RTC_A2DAY_ADOMBIN_OFS);
2427 DL_RTC_COMMON_PRESCALER0_DIVIDE prescaler0Divider,
2428 DL_RTC_COMMON_PRESCALER1_DIVIDE prescaler1Divider,
2429 DL_RTC_COMMON_PRESCALER2_DIVIDE prescaler2Divider)
2432 (((uint32_t) prescaler0Divider & RTC_PSCTL_RT0IP_MASK) |
2433 ((uint32_t) prescaler1Divider & RTC_PSCTL_RT1IP_MASK));
2434 rtc_common->EXTPSCTL =
2435 ((uint32_t) prescaler2Divider & RTC_EXTPSCTL_RT2PS_MASK);
2448 RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER0_DIVIDE prescaler0Divider)
2451 RTC_PSCTL_RT0IP_MASK);
2464 RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER1_DIVIDE prescaler1Divider)
2467 RTC_PSCTL_RT1IP_MASK);
2479 RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER2_DIVIDE prescaler2Divider)
2482 RTC_EXTPSCTL_RT2PS_MASK);
2496 const RTC_Regs *rtc_common)
2498 uint32_t prescaler = (rtc_common->PSCTL & RTC_PSCTL_RT0IP_MASK);
2500 return (DL_RTC_COMMON_PRESCALER0_DIVIDE)(prescaler);
2513 const RTC_Regs *rtc_common)
2515 uint32_t prescaler = (rtc_common->PSCTL & RTC_PSCTL_RT1IP_MASK);
2517 return (DL_RTC_COMMON_PRESCALER1_DIVIDE)(prescaler);
2530 const RTC_Regs *rtc_common)
2532 uint32_t prescaler = (rtc_common->EXTPSCTL & RTC_EXTPSCTL_RT2PS_MASK);
2534 return (DL_RTC_COMMON_PRESCALER2_DIVIDE)(prescaler);
2552 const RTC_Regs *rtc_common)
2554 return (uint8_t)((rtc_common->TSSEC & (RTC_TSSEC_SECLOWBCD_MASK |
2555 RTC_TSSEC_SECHIGHBCD_MASK)) >>
2556 RTC_TSSEC_SECLOWBCD_OFS);
2574 const RTC_Regs *rtc_common)
2576 return (uint8_t)((rtc_common->TSMIN & (RTC_TSMIN_MINLOWBCD_MASK |
2577 RTC_TSMIN_MINHIGHBCD_MASK)) >>
2578 RTC_TSMIN_MINLOWBCD_OFS);
2596 const RTC_Regs *rtc_common)
2598 return (uint8_t)((rtc_common->TSHOUR & (RTC_TSHOUR_HOURLOWBCD_MASK |
2599 RTC_TSHOUR_HOURHIGHBCD_MASK)) >>
2600 RTC_TSHOUR_HOURLOWBCD_OFS);
2618 const RTC_Regs *rtc_common)
2620 return (uint8_t)(rtc_common->TSDAY & RTC_TSDAY_DOW_MASK);
2638 const RTC_Regs *rtc_common)
2640 return (uint8_t)((rtc_common->TSDAY & (RTC_TSDAY_DOMLOWBCD_MASK |
2641 RTC_TSDAY_DOMHIGHBCD_MASK)) >>
2642 RTC_TSDAY_DOMLOWBCD_OFS);
2660 const RTC_Regs *rtc_common)
2662 return (uint8_t)((rtc_common->TSMON & (RTC_TSMON_MONLOWBCD_MASK |
2663 RTC_TSMON_MONHIGHBCD_MASK)) >>
2664 RTC_TSMON_MONLOWBCD_OFS);
2682 const RTC_Regs *rtc_common)
2685 (rtc_common->TSYEAR &
2686 (RTC_TSYEAR_YERARLOWESTBCD_MASK | RTC_TSYEAR_DECADEBCD_MASK |
2687 RTC_TSYEAR_CENTLOWBCD_MASK | RTC_TSYEAR_CENTHIGHBCD_MASK)) >>
2688 RTC_TSYEAR_YERARLOWESTBCD_OFS);
2705 const RTC_Regs *rtc_common)
2707 return (uint8_t)(rtc_common->TSSEC & RTC_TSSEC_SECBIN_MASK);
2725 const RTC_Regs *rtc_common)
2727 return (uint8_t)(rtc_common->TSMIN & RTC_TSMIN_MINBIN_MASK);
2745 const RTC_Regs *rtc_common)
2747 return (uint8_t)(rtc_common->TSHOUR & RTC_TSHOUR_HOURBIN_MASK);
2765 const RTC_Regs *rtc_common)
2767 return (uint8_t)(rtc_common->TSDAY & RTC_TSDAY_DOW_MASK);
2785 const RTC_Regs *rtc_common)
2788 (rtc_common->TSDAY & RTC_TSDAY_DOMBIN_MASK) >> RTC_TSDAY_DOMBIN_OFS);
2806 const RTC_Regs *rtc_common)
2808 return (uint8_t)(rtc_common->TSMON & RTC_TSMON_MONBIN_MASK);
2826 const RTC_Regs *rtc_common)
2828 return (uint16_t)(rtc_common->TSYEAR & (RTC_TSYEAR_YEARLOWBIN_MASK |
2829 RTC_TSYEAR_YEARHIGHBIN_MASK));
2841 RTC_Regs *rtc_common, uint32_t interruptMask)
2843 rtc_common->CPU_INT.IMASK |= interruptMask;
2855 RTC_Regs *rtc_common, uint32_t interruptMask)
2857 rtc_common->CPU_INT.IMASK &= ~(interruptMask);
2873 const RTC_Regs *rtc_common, uint32_t interruptMask)
2875 return (rtc_common->CPU_INT.IMASK & interruptMask);
2896 const RTC_Regs *rtc_common, uint32_t interruptMask)
2898 return (rtc_common->CPU_INT.MIS & interruptMask);
2917 const RTC_Regs *rtc_common, uint32_t interruptMask)
2919 return (rtc_common->CPU_INT.RIS & interruptMask);
2935 const RTC_Regs *rtc_common)
2937 return (DL_RTC_COMMON_IIDX)(rtc_common->CPU_INT.IIDX);
2949 RTC_Regs *rtc_common, uint32_t interruptMask)
2951 rtc_common->CPU_INT.ICLR = interruptMask;
2962 RTC_Regs *rtc_common, uint32_t eventMask)
2964 rtc_common->GEN_EVENT.IMASK |= (eventMask);
2975 RTC_Regs *rtc_common, uint32_t eventMask)
2977 rtc_common->GEN_EVENT.IMASK &= ~(eventMask);
2992 const RTC_Regs *rtc_common, uint32_t eventMask)
2994 return ((rtc_common->GEN_EVENT.IMASK) & (eventMask));
3014 const RTC_Regs *rtc_common, uint32_t eventMask)
3016 return ((rtc_common->GEN_EVENT.MIS) & eventMask);
3034 const RTC_Regs *rtc_common, uint32_t eventMask)
3036 return ((rtc_common->GEN_EVENT.RIS) & eventMask);
3047 RTC_Regs *rtc_common, uint32_t eventMask)
3049 rtc_common->GEN_EVENT.ICLR |= (eventMask);
3061 RTC_Regs *rtc_common, uint8_t chanID)
3063 rtc_common->FPUB_0 = (chanID & RTC_FPUB_0_CHANID_MAXIMUM);
3076 const RTC_Regs *rtc_common)
3078 return (uint8_t)(rtc_common->FPUB_0 & RTC_FPUB_0_CHANID_MAXIMUM);
3081 #ifdef __MSPM0_HAS_RTC_A__ 3093 __STATIC_INLINE uint32_t DL_RTC_Common_getTimeStampEventCause(
3094 const RTC_Regs *rtc_common, uint32_t tsEventMask)
3096 return (rtc_common->TSSTAT & tsEventMask);
3129 const RTC_Regs *rtc_common);
3153 const RTC_Regs *rtc_common);
3193 const RTC_Regs *rtc_common);
3211 #ifdef __MSPM0_HAS_RTC_A__ 3224 __STATIC_INLINE
void DL_RTC_Common_setTimeStampEventSource(
3225 RTC_Regs *rtc_common, uint32_t sourceMask)
3227 rtc_common->TSCTL |= (RTC_TSCTL_KEY_UNLOCK_W | sourceMask);
3242 __STATIC_INLINE uint32_t DL_RTC_Common_getTimeStampEventSource(
3243 const RTC_Regs *rtc_common, uint32_t sourceMask)
3245 return (rtc_common->TSCTL & sourceMask);
3259 __STATIC_INLINE
void DL_RTC_Common_setTimeStampEventCapture(
3260 RTC_Regs *rtc_common, DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE capture)
3263 (RTC_TSCTL_KEY_UNLOCK_W | (uint32_t) capture),
3264 (RTC_TSCTL_TSCAPTURE_MASK | RTC_TSCTL_KEY_MASK));
3280 __STATIC_INLINE DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE
3281 DL_RTC_Common_getTimeStampEventCapture(
const RTC_Regs *rtc_common)
3283 uint32_t capture = (rtc_common->TSCTL & RTC_TSCTL_TSCAPTURE_MASK);
3285 return (DL_RTC_COMMON_TIME_STAMP_EVENT_CAPTURE)(capture);
3296 __STATIC_INLINE
void DL_RTC_Common_clearTimeStamp(RTC_Regs *rtc_common)
3298 rtc_common->TSCLR = (RTC_TSCLR_KEY_UNLOCK_W | RTC_TSCLR_CLR_CLR);
3310 __STATIC_INLINE
void DL_RTC_Common_enableWriteProtect(RTC_Regs *rtc_common)
3312 rtc_common->RTCLOCK = (RTC_RTCLOCK_PROTECT_SET | RTC_RTCLOCK_KEY_UNLOCK_W);
3326 __STATIC_INLINE
bool DL_RTC_Common_isWriteProtectEnabled(
3327 const RTC_Regs *rtc_common)
3329 return ((rtc_common->RTCLOCK & RTC_RTCLOCK_PROTECT_MASK) ==
3330 RTC_RTCLOCK_PROTECT_SET);
3339 __STATIC_INLINE
void DL_RTC_Common_disableWriteProtect(RTC_Regs *rtc_common)
3341 rtc_common->RTCLOCK = (RTC_RTCLOCK_PROTECT_CLR | RTC_RTCLOCK_KEY_UNLOCK_W);
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampDayOfWeekBCD(const RTC_Regs *rtc_common)
Get the day of the week in BCD in the time stamp.
Definition: dl_rtc_common.h:2617
Definition: dl_rtc_common.h:439
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampDayOfMonthBCD(const RTC_Regs *rtc_common)
Get the day of the month in BCD in the time stamp.
Definition: dl_rtc_common.h:2637
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1DayOfWeekBinary(const RTC_Regs *rtc_common)
Get the day of the week in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2131
__STATIC_INLINE void DL_RTC_Common_setAlarm1DayOfMonthBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1493
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarHoursBCD(const RTC_Regs *rtc_common)
Get the hours in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1142
__STATIC_INLINE void DL_RTC_Common_setCalendarDayOfMonthBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1881
__STATIC_INLINE uint32_t DL_RTC_Common_getEnabledInterrupts(const RTC_Regs *rtc_common, uint32_t interruptMask)
Check which RTC Common interrupts are enabled.
Definition: dl_rtc_common.h:2872
__STATIC_INLINE void DL_Common_updateReg(volatile uint32_t *reg, uint32_t val, uint32_t mask)
Writes value to specified register - retaining bits unaffected by mask.
Definition: dl_common.h:63
DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY
Definition: dl_rtc_common.h:387
__STATIC_INLINE void DL_RTC_Common_enableDebugMode(RTC_Regs *rtc_common)
Enables the RTC Common modules debug mode.
Definition: dl_rtc_common.h:746
__STATIC_INLINE uint32_t DL_RTC_Common_getRawEventsStatus(const RTC_Regs *rtc_common, uint32_t eventMask)
Check interrupt flag of any RTC Common event.
Definition: dl_rtc_common.h:3033
Definition: dl_rtc_common.h:417
__STATIC_INLINE uint8_t DL_RTC_Common_getPublisherChanID(const RTC_Regs *rtc_common)
Gets the event publisher channel ID.
Definition: dl_rtc_common.h:3075
__STATIC_INLINE void DL_RTC_Common_setPeriodicAlarm0(RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER0_DIVIDE prescaler0Divider)
Set periodic alarm 0.
Definition: dl_rtc_common.h:2447
Definition: dl_rtc_common.h:373
__STATIC_INLINE void DL_RTC_Common_setOffsetCalibrationFrequency(RTC_Regs *rtc_common, DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY offsetFrequency)
Sets output frequency for offset calibration.
Definition: dl_rtc_common.h:905
__STATIC_INLINE uint32_t DL_RTC_Common_getEnabledInterruptStatus(const RTC_Regs *rtc_common, uint32_t interruptMask)
Check interrupt flag of enabled RTC Common interrupts.
Definition: dl_rtc_common.h:2895
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampSecondsBCD(const RTC_Regs *rtc_common)
Get the seconds in BCD in the time stamp.
Definition: dl_rtc_common.h:2551
uint8_t minutes
Definition: dl_rtc_common.h:577
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampMonthBCD(const RTC_Regs *rtc_common)
Get the month of the year in BCD in the time stamp.
Definition: dl_rtc_common.h:2659
__STATIC_INLINE void DL_RTC_Common_setCalendarYearBinary(RTC_Regs *rtc_common, uint16_t year)
Set the year in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1949
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1MinutesBCD(const RTC_Regs *rtc_common)
Get the minutes in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1345
Definition: dl_rtc_common.h:375
uint8_t hours
Definition: dl_rtc_common.h:580
__STATIC_INLINE void DL_RTC_Common_setAlarm1DayOfWeekBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1440
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2DayOfMonthBCD(const RTC_Regs *rtc_common)
Get the day of the month in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1734
__STATIC_INLINE void DL_RTC_Common_setAlarm2DayOfMonthBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2383
Definition: dl_rtc_common.h:383
Definition: dl_rtc_common.h:359
__STATIC_INLINE bool DL_RTC_Common_isCalibrationWriteResultOK(const RTC_Regs *rtc_common)
Checks if RTC Common new calibration values were written OK.
Definition: dl_rtc_common.h:887
__STATIC_INLINE void DL_RTC_Common_disableAlarm2MinutesBinary(RTC_Regs *rtc_common)
Disable minutes in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2210
__STATIC_INLINE bool DL_RTC_Common_isSafeToRead(const RTC_Regs *rtc_common)
Checks if RTC Common is safe for reading.
Definition: dl_rtc_common.h:857
__STATIC_INLINE bool DL_RTC_Common_isPowerEnabled(const RTC_Regs *rtc_common)
Returns if the Peripheral Write Enable (PWREN) register for the RTC is enabled.
Definition: dl_rtc_common.h:681
uint8_t dayOfMonth
Definition: dl_rtc_common.h:586
__STATIC_INLINE void DL_RTC_Common_setAlarm1DayOfWeekBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2115
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2DayOfWeekBCD(const RTC_Regs *rtc_common)
Get the day of the week in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1679
DL_RTC_COMMON_FORMAT
Definition: dl_rtc_common.h:413
DL_RTC_Common_CalendarAlarm DL_RTC_Common_getCalendarAlarm2(const RTC_Regs *rtc_common)
Get calendar alarm 2.
void DL_RTC_Common_initCalendar(RTC_Regs *rtc_common, DL_RTC_Common_Calendar calendarTime, DL_RTC_COMMON_FORMAT formatSelect)
Initializes the settings to operate the RTC Common in Calendar mode.
__STATIC_INLINE DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY DL_RTC_Common_getOffsetCalibrationFrequency(const RTC_Regs *rtc_common)
Gets the offset calibration frequency.
Definition: dl_rtc_common.h:977
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarHoursBinary(const RTC_Regs *rtc_common)
Get the hours in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1835
void DL_RTC_Common_enableCalendarAlarm1(RTC_Regs *rtc_common)
Enable calendar alarm 1.
void DL_RTC_Common_setCalendarAlarm2(RTC_Regs *rtc_common, DL_RTC_Common_CalendarAlarm alarmTime)
Set calendar alarm 2.
__STATIC_INLINE uint16_t DL_RTC_Common_getCalendarYearBinary(const RTC_Regs *rtc_common)
Get the year in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1970
Definition: dl_rtc_common.h:409
__STATIC_INLINE void DL_RTC_Common_enableAlarm1DayOfMonthBinary(RTC_Regs *rtc_common)
Enable day of the month in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2143
__STATIC_INLINE uint16_t DL_RTC_Common_getTimeStampYearBinary(const RTC_Regs *rtc_common)
Get the year in binary in the time stamp.
Definition: dl_rtc_common.h:2825
__STATIC_INLINE void DL_RTC_Common_enableAlarm2DayOfMonthBinary(RTC_Regs *rtc_common)
Enable day of the month in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2358
__STATIC_INLINE void DL_RTC_Common_reset(RTC_Regs *rtc_common)
Resets all registers in the RTC Common module.
Definition: dl_rtc_common.h:693
__STATIC_INLINE uint32_t DL_RTC_Common_getRawInterruptStatus(const RTC_Regs *rtc_common, uint32_t interruptMask)
Check interrupt flag of any RTC Common interrupt.
Definition: dl_rtc_common.h:2916
Definition: dl_rtc_common.h:481
__STATIC_INLINE void DL_RTC_Common_enableClockControl(RTC_Regs *rtc_common)
Enables the supply of the 32kHz clock to the RTC Common. It will not power up the 32kHz crystal oscil...
Definition: dl_rtc_common.h:619
__STATIC_INLINE void DL_RTC_Common_setCalendarSecondsBCD(RTC_Regs *rtc_common, uint8_t seconds)
Set the seconds in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1049
__STATIC_INLINE void DL_RTC_Common_disableAlarm2HoursBCD(RTC_Regs *rtc_common)
Disable hours in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1593
uint8_t dayOfWeek
Definition: dl_rtc_common.h:583
DL_RTC_COMMON_PRESCALER2_DIVIDE
Definition: dl_rtc_common.h:469
Definition: dl_rtc_common.h:463
__STATIC_INLINE void DL_RTC_Common_enableAlarm2HoursBCD(RTC_Regs *rtc_common)
Enable hours in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1582
__STATIC_INLINE void DL_RTC_Common_disableAlarm2HoursBinary(RTC_Regs *rtc_common)
Disable hours in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2264
Definition: dl_rtc_common.h:399
uint8_t dayOfMonth
Definition: dl_rtc_common.h:562
__STATIC_INLINE void DL_RTC_Common_disableDebugMode(RTC_Regs *rtc_common)
Disables the RTC Common modules debug mode.
Definition: dl_rtc_common.h:757
__STATIC_INLINE uint32_t DL_RTC_Common_getEnabledEvents(const RTC_Regs *rtc_common, uint32_t eventMask)
Check which RTC Common events are enabled.
Definition: dl_rtc_common.h:2991
__STATIC_INLINE void DL_RTC_Common_enableInterrupt(RTC_Regs *rtc_common, uint32_t interruptMask)
Enable RTC Common interrupts.
Definition: dl_rtc_common.h:2840
__STATIC_INLINE void DL_RTC_Common_enableAlarm1DayOfWeekBinary(RTC_Regs *rtc_common)
Enable day of the week in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2090
uint8_t minutes
Definition: dl_rtc_common.h:553
__STATIC_INLINE void DL_RTC_Common_enableAlarm1MinutesBCD(RTC_Regs *rtc_common)
Enable minutes in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1302
__STATIC_INLINE void DL_RTC_Common_disableAlarm1DayOfMonthBinary(RTC_Regs *rtc_common)
Disable day of the month in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2155
__STATIC_INLINE void DL_RTC_Common_enableAlarm1DayOfMonthBCD(RTC_Regs *rtc_common)
Enable day of the month in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1468
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1DayOfMonthBCD(const RTC_Regs *rtc_common)
Get the day of the month in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1511
__STATIC_INLINE void DL_RTC_Common_disableEvent(RTC_Regs *rtc_common, uint32_t eventMask)
Disable RTC Common event.
Definition: dl_rtc_common.h:2974
DL_RTC_COMMON_INTERVAL_ALARM
Definition: dl_rtc_common.h:421
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarSecondsBinary(const RTC_Regs *rtc_common)
Get the seconds in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1769
__STATIC_INLINE void DL_RTC_Common_setCalendarMonthBinary(RTC_Regs *rtc_common, uint8_t month)
Set the month in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1916
Definition: dl_rtc_common.h:401
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampHoursBinary(const RTC_Regs *rtc_common)
Get the hours in binary in the time stamp.
Definition: dl_rtc_common.h:2744
__STATIC_INLINE void DL_RTC_Common_enableDebugInterrupts(RTC_Regs *rtc_common)
Enables interrupts when the CPU is in debug mode. Interrupt requests are signaled to the interrupt co...
Definition: dl_rtc_common.h:722
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1HoursBinary(const RTC_Regs *rtc_common)
Get the hours in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2078
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampHoursBCD(const RTC_Regs *rtc_common)
Get the hours in BCD in the time stamp.
Definition: dl_rtc_common.h:2595
__STATIC_INLINE void DL_RTC_Common_enableAlarm2HoursBinary(RTC_Regs *rtc_common)
Enable hours in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2252
Definition: dl_rtc_common.h:473
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1MinutesBinary(const RTC_Regs *rtc_common)
Get the minutes in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2025
Definition: dl_rtc_common.h:461
Definition: dl_rtc_common.h:491
DL_RTC_COMMON_IIDX
Definition: dl_rtc_common.h:479
__STATIC_INLINE DL_RTC_COMMON_PRESCALER0_DIVIDE DL_RTC_Common_getPrescaler0(const RTC_Regs *rtc_common)
Get prescaler 0 interrupt interval.
Definition: dl_rtc_common.h:2495
__STATIC_INLINE void DL_RTC_Common_setClockFormat(RTC_Regs *rtc_common, DL_RTC_COMMON_FORMAT formatSelect)
Set the format of the real-time clock.
Definition: dl_rtc_common.h:771
__STATIC_INLINE void DL_RTC_Common_setOffsetCalibration(RTC_Regs *rtc_common, DL_RTC_COMMON_OFFSET_CALIBRATION_FREQUENCY offsetFrequency, DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN offsetSign, uint8_t offsetValue)
Sets the offset error calibration.
Definition: dl_rtc_common.h:959
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarDayOfWeekBinary(const RTC_Regs *rtc_common)
Get the day of the week in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1868
Definition: dl_rtc_common.h:471
DL_RTC_Common_CalendarAlarm DL_RTC_Common_getCalendarAlarm1(const RTC_Regs *rtc_common)
Get calendar alarm 1.
__STATIC_INLINE void DL_RTC_Common_clearInterruptStatus(RTC_Regs *rtc_common, uint32_t interruptMask)
Clear pending RTC Common interrupts.
Definition: dl_rtc_common.h:2948
__STATIC_INLINE bool DL_RTC_Common_isReadyToCalibrate(const RTC_Regs *rtc_common)
Checks if RTC Common is ready to get new calibration values.
Definition: dl_rtc_common.h:871
Definition: dl_rtc_common.h:425
__STATIC_INLINE void DL_RTC_Common_enableAlarm2DayOfMonthBCD(RTC_Regs *rtc_common)
Enable day of the month in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1691
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2MinutesBinary(const RTC_Regs *rtc_common)
Get the minutes in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2240
__STATIC_INLINE void DL_RTC_Common_disableAlarm1DayOfMonthBCD(RTC_Regs *rtc_common)
Disable day of the month in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1480
Definition: dl_rtc_common.h:451
Definition: dl_rtc_common.h:367
Definition: dl_rtc_common.h:435
__STATIC_INLINE void DL_RTC_Common_setOffsetCalibrationAdjValue(RTC_Regs *rtc_common, DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN offsetSign, uint8_t offsetValue)
Sets the offset error calibration adjustment value.
Definition: dl_rtc_common.h:928
Calendar struct to use in DL_RTC_Common_initCalendar()
Definition: dl_rtc_common.h:571
Definition: dl_rtc_common.h:415
__STATIC_INLINE void DL_RTC_Common_setCalendarYearBCD(RTC_Regs *rtc_common, uint16_t year)
Set the year in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1263
__STATIC_INLINE void DL_RTC_Common_setCalendarDayOfMonthBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1190
Definition: dl_rtc_common.h:457
__STATIC_INLINE void DL_RTC_Common_setAlarm2MinutesBCD(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1550
__STATIC_INLINE void DL_RTC_Common_setAlarm1HoursBinary(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2062
Definition: dl_rtc_common.h:465
__STATIC_INLINE uint32_t DL_RTC_Common_getEnabledEventStatus(const RTC_Regs *rtc_common, uint32_t eventMask)
Check event flag of enabled RTC Common event.
Definition: dl_rtc_common.h:3013
__STATIC_INLINE void DL_RTC_Common_setAlarm2HoursBinary(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2277
uint8_t month
Definition: dl_rtc_common.h:589
__STATIC_INLINE void DL_RTC_Common_setAlarm1HoursBCD(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1382
Alarm struct to use in DL_RTC_Common_setCalendarAlarm.
Definition: dl_rtc_common.h:550
__STATIC_INLINE void DL_RTC_Common_setCalendarHoursBCD(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1121
__STATIC_INLINE void DL_RTC_Common_enableAlarm2MinutesBCD(RTC_Regs *rtc_common)
Enable minutes in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1525
__STATIC_INLINE void DL_RTC_Common_enableAlarm2DayOfWeekBinary(RTC_Regs *rtc_common)
Enable day of the week in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2305
__STATIC_INLINE void DL_RTC_Common_disableAlarm1DayOfWeekBCD(RTC_Regs *rtc_common)
Disable day of the week in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1427
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2DayOfMonthBinary(const RTC_Regs *rtc_common)
Get the day of the month in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2400
__STATIC_INLINE uint16_t DL_RTC_Common_getTimeStampYearBCD(const RTC_Regs *rtc_common)
Get the year in BCD in the time stamp.
Definition: dl_rtc_common.h:2681
uint8_t hours
Definition: dl_rtc_common.h:556
__STATIC_INLINE void DL_RTC_Common_setAlarm1MinutesBinary(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2009
Definition: dl_rtc_common.h:357
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampDayOfMonthBinary(const RTC_Regs *rtc_common)
Get the day of the month in binary in the time stamp.
Definition: dl_rtc_common.h:2784
__STATIC_INLINE void DL_RTC_Common_enableAlarm1HoursBinary(RTC_Regs *rtc_common)
Enable hours in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2037
DL_RTC_COMMON_PRESCALER0_DIVIDE
Definition: dl_rtc_common.h:433
DL_RTC_COMMON_STATUS
Definition: dl_rtc_common.h:355
__STATIC_INLINE void DL_RTC_Common_setAlarm2MinutesBinary(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2224
__STATIC_INLINE uint32_t DL_RTC_Common_getTemperatureCompensation(const RTC_Regs *rtc_common)
Get the RTC Common temperature compensation.
Definition: dl_rtc_common.h:1036
__STATIC_INLINE void DL_RTC_Common_setAlarm2DayOfMonthBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1716
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarDayOfMonthBinary(const RTC_Regs *rtc_common)
Get the day of the month in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1902
__STATIC_INLINE void DL_RTC_Common_disableAlarm2DayOfWeekBCD(RTC_Regs *rtc_common)
Disable day of the week in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1650
Definition: dl_rtc_common.h:483
void DL_RTC_Common_disableCalendarAlarm1(RTC_Regs *rtc_common)
Disable calendar alarm 1.
Definition: dl_rtc_common.h:487
Definition: dl_rtc_common.h:475
__STATIC_INLINE void DL_RTC_Common_enableAlarm1MinutesBinary(RTC_Regs *rtc_common)
Enable minutes in binary in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1983
Definition: dl_rtc_common.h:397
__STATIC_INLINE void DL_RTC_Common_disableAlarm2DayOfMonthBCD(RTC_Regs *rtc_common)
Disable day of the month in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1703
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1DayOfMonthBinary(const RTC_Regs *rtc_common)
Get the day of the month in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2185
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampSecondsBinary(const RTC_Regs *rtc_common)
Get the seconds in binary in the time stamp.
Definition: dl_rtc_common.h:2704
Definition: dl_rtc_common.h:485
__STATIC_INLINE void DL_RTC_Common_disableAlarm2DayOfMonthBinary(RTC_Regs *rtc_common)
Disable day of the month in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2370
__STATIC_INLINE void DL_RTC_Common_enableEvent(RTC_Regs *rtc_common, uint32_t eventMask)
Enable RTC Common event.
Definition: dl_rtc_common.h:2961
DL_RTC_COMMON_PRESCALER1_DIVIDE
Definition: dl_rtc_common.h:449
__STATIC_INLINE void DL_RTC_Common_disablePower(RTC_Regs *rtc_common)
Disables the Peripheral Write Enable (PWREN) register for the RTC.
Definition: dl_rtc_common.h:659
__STATIC_INLINE DL_RTC_COMMON_INTERVAL_ALARM DL_RTC_Common_getIntervalAlarm(const RTC_Regs *rtc_common)
Gets the interval alarm event condition.
Definition: dl_rtc_common.h:832
__STATIC_INLINE void DL_RTC_Common_setCalendarHoursBinary(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1815
Definition: dl_rtc_common.h:429
Definition: dl_rtc_common.h:443
__STATIC_INLINE DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN DL_RTC_Common_getOffsetCalibrationSign(const RTC_Regs *rtc_common)
Gets the offset calibration sign.
Definition: dl_rtc_common.h:994
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarMinutesBinary(const RTC_Regs *rtc_common)
Get the minutes in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1802
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarMinutesBCD(const RTC_Regs *rtc_common)
Get the minutes in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1106
__STATIC_INLINE void DL_RTC_Common_enableAlarm2DayOfWeekBCD(RTC_Regs *rtc_common)
Enable day of the week in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1638
DL_RTC_COMMON_COMPENSATION_WRITE_RESULT
Definition: dl_rtc_common.h:371
__STATIC_INLINE void DL_RTC_Common_setCalendarMonthBCD(RTC_Regs *rtc_common, uint8_t month)
Set the month in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1227
__STATIC_INLINE void DL_RTC_Common_disableClockControl(RTC_Regs *rtc_common)
Disables the supply of the 32kHz clock to the RTC Common.
Definition: dl_rtc_common.h:629
Definition: dl_rtc_common.h:365
Definition: dl_rtc_common.h:459
Definition: dl_rtc_common.h:455
__STATIC_INLINE void DL_RTC_Common_enableAlarm2MinutesBinary(RTC_Regs *rtc_common)
Enable minutes in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2198
__STATIC_INLINE void DL_RTC_Common_setAlarm2HoursBCD(RTC_Regs *rtc_common, uint8_t hours)
Set the hours in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1605
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarDayOfMonthBCD(const RTC_Regs *rtc_common)
Get the day of the month in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1212
__STATIC_INLINE void DL_RTC_Common_enablePower(RTC_Regs *rtc_common)
Enables the Peripheral Write Enable (PWREN) register for the RTC.
Definition: dl_rtc_common.h:643
__STATIC_INLINE void DL_RTC_Common_setTemperatureCompensation(RTC_Regs *rtc_common, DL_RTC_COMMON_TEMP_CALIBRATION offsetDirection, uint32_t offsetValue)
Set the specified RTC Common temperature compensation.
Definition: dl_rtc_common.h:1017
Definition: dl_rtc_common.h:390
__STATIC_INLINE void DL_RTC_Common_setCalendarMinutesBinary(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1782
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampMinutesBCD(const RTC_Regs *rtc_common)
Get the minutes in BCD in the time stamp.
Definition: dl_rtc_common.h:2573
DL_RTC_COMMON_TEMP_CALIBRATION
Definition: dl_rtc_common.h:405
__STATIC_INLINE void DL_RTC_Common_setPeriodicAlarm1(RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER1_DIVIDE prescaler1Divider)
Set periodic alarm 1.
Definition: dl_rtc_common.h:2463
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2DayOfWeekBinary(const RTC_Regs *rtc_common)
Get the day of the week in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2346
__STATIC_INLINE void DL_RTC_Common_setCalendarDayOfWeekBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1848
uint8_t dayOfWeek
Definition: dl_rtc_common.h:559
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1DayOfWeekBCD(const RTC_Regs *rtc_common)
Get the day of the week in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1456
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarMonthBinary(const RTC_Regs *rtc_common)
Get the month of the year in binary in the RTC Common calendar.
Definition: dl_rtc_common.h:1936
Definition: dl_rtc_common.h:437
__STATIC_INLINE void DL_RTC_Common_disableInterrupt(RTC_Regs *rtc_common, uint32_t interruptMask)
Disable RTC Common interrupts.
Definition: dl_rtc_common.h:2854
__STATIC_INLINE void DL_RTC_Common_disableAlarm2MinutesBCD(RTC_Regs *rtc_common)
Disable minutes in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1536
uint16_t year
Definition: dl_rtc_common.h:592
Definition: dl_rtc_common.h:423
__STATIC_INLINE void DL_RTC_Common_disableAlarm1HoursBinary(RTC_Regs *rtc_common)
Disable hours in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2049
Definition: dl_rtc_common.h:381
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2HoursBCD(const RTC_Regs *rtc_common)
Get the hours in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1623
__STATIC_INLINE DL_RTC_COMMON_PRESCALER2_DIVIDE DL_RTC_Common_getPrescaler2(const RTC_Regs *rtc_common)
Get prescaler 2 interrupt interval.
Definition: dl_rtc_common.h:2529
__STATIC_INLINE void DL_RTC_Common_setIntervalAlarm(RTC_Regs *rtc_common, DL_RTC_COMMON_INTERVAL_ALARM alarmEvent)
Sets the interval alarm event condition.
Definition: dl_rtc_common.h:811
__STATIC_INLINE DL_RTC_COMMON_PRESCALER1_DIVIDE DL_RTC_Common_getPrescaler1(const RTC_Regs *rtc_common)
Get prescaler 1 interrupt interval.
Definition: dl_rtc_common.h:2512
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampMinutesBinary(const RTC_Regs *rtc_common)
Get the minutes in binary in the time stamp.
Definition: dl_rtc_common.h:2724
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2HoursBinary(const RTC_Regs *rtc_common)
Get the hours in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2293
DL_RTC_Common_Calendar DL_RTC_Common_getCalendarTime(const RTC_Regs *rtc_common)
Returns the Calendar Time.
__STATIC_INLINE void DL_RTC_Common_setPrescalerEvents(RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER0_DIVIDE prescaler0Divider, DL_RTC_COMMON_PRESCALER1_DIVIDE prescaler1Divider, DL_RTC_COMMON_PRESCALER2_DIVIDE prescaler2Divider)
Set prescale interrupt interval for timer 0 and 1.
Definition: dl_rtc_common.h:2426
Definition: dl_rtc_common.h:441
Definition: dl_rtc_common.h:427
__STATIC_INLINE void DL_RTC_Common_setCalendarSecondsBinary(RTC_Regs *rtc_common, uint8_t seconds)
Set the seconds in binary the RTC Common calendar.
Definition: dl_rtc_common.h:1749
__STATIC_INLINE void DL_RTC_Common_enableAlarm1HoursBCD(RTC_Regs *rtc_common)
Enable hours in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1359
__STATIC_INLINE void DL_RTC_Common_setAlarm2DayOfWeekBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1663
__STATIC_INLINE bool DL_RTC_Common_isReset(const RTC_Regs *rtc_common)
Returns if the RTC Common module was reset.
Definition: dl_rtc_common.h:709
__STATIC_INLINE void DL_RTC_Common_enableAlarm1DayOfWeekBCD(RTC_Regs *rtc_common)
Enable day of the week in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1415
__STATIC_INLINE void DL_RTC_Common_disableAlarm1MinutesBCD(RTC_Regs *rtc_common)
Disable minutes in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1313
__STATIC_INLINE void DL_RTC_Common_setPublisherChanID(RTC_Regs *rtc_common, uint8_t chanID)
Sets the event publisher channel ID.
Definition: dl_rtc_common.h:3060
__STATIC_INLINE void DL_RTC_Common_setAlarm1DayOfMonthBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the month in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2168
__STATIC_INLINE void DL_RTC_Common_disableDebugInterrupts(RTC_Regs *rtc_common)
Disables interrupts when the CPU is in debug mode. Interrupts of the RTC Common module will not be ca...
Definition: dl_rtc_common.h:735
__STATIC_INLINE void DL_RTC_Common_disableAlarm1MinutesBinary(RTC_Regs *rtc_common)
Disable minutes in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1995
__STATIC_INLINE void DL_RTC_Common_setCalendarDayOfWeekBCD(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1157
__STATIC_INLINE bool DL_RTC_Common_isClockSourceLFCLK(const RTC_Regs *rtc_common)
Returns if LFCLK is selected as clock source.
Definition: dl_rtc_common.h:605
void DL_RTC_Common_setCalendarAlarm1(RTC_Regs *rtc_common, DL_RTC_Common_CalendarAlarm alarmTime)
Set calendar alarm 1.
void DL_RTC_Common_disableCalendarAlarm2(RTC_Regs *rtc_common)
Disable calendar alarm 2.
DL_RTC_COMMON_COMPENSATION_STATUS
Definition: dl_rtc_common.h:363
__STATIC_INLINE void DL_RTC_Common_setCalendarMinutesBCD(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1085
uint8_t seconds
Definition: dl_rtc_common.h:574
Definition: dl_rtc_common.h:445
__STATIC_INLINE void DL_RTC_Common_setAlarm2DayOfWeekBinary(RTC_Regs *rtc_common, uint8_t day)
Set the day of the week in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2330
Definition: dl_rtc_common.h:453
Definition: dl_rtc_common.h:407
__STATIC_INLINE void DL_RTC_Common_setAlarm1MinutesBCD(RTC_Regs *rtc_common, uint8_t minutes)
Set the minutes in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1327
__STATIC_INLINE void DL_RTC_Common_disableAlarm1HoursBCD(RTC_Regs *rtc_common)
Disable hours in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1370
__STATIC_INLINE void DL_RTC_Common_disableAlarm2DayOfWeekBinary(RTC_Regs *rtc_common)
Disable day of the week in binary for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:2317
__STATIC_INLINE DL_RTC_COMMON_IIDX DL_RTC_Common_getPendingInterrupt(const RTC_Regs *rtc_common)
Get highest priority pending RTC Common interrupt.
Definition: dl_rtc_common.h:2934
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm2MinutesBCD(const RTC_Regs *rtc_common)
Get the minutes in BCD for RTC Common Calendar Alarm 2.
Definition: dl_rtc_common.h:1568
__STATIC_INLINE DL_RTC_COMMON_FORMAT DL_RTC_Common_getClockFormat(const RTC_Regs *rtc_common)
Get the format currently being used for counting the real-time clock.
Definition: dl_rtc_common.h:787
__STATIC_INLINE void DL_RTC_Common_setPeriodicAlarm2(RTC_Regs *rtc_common, DL_RTC_COMMON_PRESCALER2_DIVIDE prescaler2Divider)
Set periodic alarm 2.
Definition: dl_rtc_common.h:2478
__STATIC_INLINE uint16_t DL_RTC_Common_getCalendarYearBCD(const RTC_Regs *rtc_common)
Get the year in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1286
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampDayOfWeekBinary(const RTC_Regs *rtc_common)
Get the day of the week in binary in the time stamp.
Definition: dl_rtc_common.h:2764
Definition: dl_rtc_common.h:489
Definition: dl_rtc_common.h:493
__STATIC_INLINE void DL_RTC_Common_clearEventsStatus(RTC_Regs *rtc_common, uint32_t eventMask)
Clear pending RTC Common events.
Definition: dl_rtc_common.h:3046
DL_RTC_COMMON_OFFSET_CALIBRATION_SIGN
Definition: dl_rtc_common.h:379
__STATIC_INLINE uint8_t DL_RTC_Common_getAlarm1HoursBCD(const RTC_Regs *rtc_common)
Get the hours in BCD for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:1400
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarDayOfWeekBCD(const RTC_Regs *rtc_common)
Get the day of the week in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1177
void DL_RTC_Common_enableCalendarAlarm2(RTC_Regs *rtc_common)
Enable calendar alarm 2.
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarSecondsBCD(const RTC_Regs *rtc_common)
Get the seconds in in BCD the RTC Common calendar.
Definition: dl_rtc_common.h:1070
__STATIC_INLINE void DL_RTC_Common_disableAlarm1DayOfWeekBinary(RTC_Regs *rtc_common)
Disable day of the week in binary for RTC Common Calendar Alarm 1.
Definition: dl_rtc_common.h:2102
__STATIC_INLINE uint8_t DL_RTC_Common_getTimeStampMonthBinary(const RTC_Regs *rtc_common)
Get the month of the year in binary in the time stamp.
Definition: dl_rtc_common.h:2805
__STATIC_INLINE uint8_t DL_RTC_Common_getCalendarMonthBCD(const RTC_Regs *rtc_common)
Get the month of the year in BCD in the RTC Common calendar.
Definition: dl_rtc_common.h:1248