MSPM0C110X Driver Library  2.05.00.05
Macros | Enumerations | Functions
dl_sysctl_mspm0c110x.h File Reference

Detailed Description

System Control (SysCtl)


#include <stdbool.h>
#include <stdint.h>
#include <ti/devices/msp/msp.h>
#include <ti/driverlib/dl_common.h>
#include <ti/driverlib/m0p/dl_factoryregion.h>
Include dependency graph for dl_sysctl_mspm0c110x.h:

Go to the source code of this file.

Macros

#define DL_SYSCTL_RESET_SYSRST   (SYSCTL_RESETLEVEL_LEVEL_CPU)
 Perform a SYSRST. More...
 
#define DL_SYSCTL_RESET_CPU   (DL_SYSCTL_RESET_SYSRST)
 
#define DL_SYSCTL_RESET_BOOT   (SYSCTL_RESETLEVEL_LEVEL_BOOT)
 Perform a Boot reset. More...
 
#define DL_SYSCTL_RESET_POR   (SYSCTL_RESETLEVEL_LEVEL_POR)
 Perform a POR reset. More...
 
#define DL_SYSCTL_RESET_BOOTLOADER_EXIT   (SYSCTL_RESETLEVEL_LEVEL_BOOTLOADEREXIT)
 Perform system reset and exit bootloader to the application.
 
#define DL_SYSCTL_RESET_BOOTLOADER_ENTRY   (SYSCTL_RESETLEVEL_LEVEL_BOOTLOADERENTRY)
 Perform system reset and run bootloader.
 
#define DL_SYSCTL_INTERRUPT_LFOSC_GOOD   (SYSCTL_IMASK_LFOSCGOOD_ENABLE)
 Low Frequency Oscillator is stabilized and ready to use.
 
#define DL_SYSCTL_INTERRUPT_ANALOG_CLOCK_ERROR   (SYSCTL_IMASK_ANACLKERR_ENABLE)
 Analog clocking consistency error.
 
#define DL_SYSCTL_NMI_WWDT0_FAULT   (SYSCTL_NMIISET_WWDT0_SET)
 Non-maskable interrupt for Watchdog 0 Fault.
 
#define DL_SYSCTL_NMI_BORLVL   (SYSCTL_NMIISET_BORLVL_SET)
 Non-maskable interrupt for early BOR.
 
#define DL_SYSCTL_CLK_STATUS_FCL_ON   (SYSCTL_CLKSTATUS_FCLMODE_ENABLED)
 SYSOSC Frequency Correcting Loop Mode ON.
 
#define DL_SYSCTL_CLK_STATUS_LFOSC_GOOD   (SYSCTL_CLKSTATUS_LFOSCGOOD_TRUE)
 LFOSC is Valid.
 
#define DL_SYSCTL_CLK_STATUS_MCLK_SOURCE_LFCLK   (SYSCTL_CLKSTATUS_CURMCLKSEL_LFCLK)
 MCLK now sourced from LFCLK.
 
#define DL_SYSCTL_CLK_STATUS_MCLK_SOURCE_HSCLK   (SYSCTL_CLKSTATUS_HSCLKMUX_HSCLK)
 MCLK now sourced from HSCLK, otherwise SYSOSC.
 
#define DL_SYSCTL_CLK_STATUS_ANALOG_CLOCK_ERROR   (SYSCTL_CLKSTATUS_ANACLKERR_TRUE)
 Analog clocking error.
 
#define DL_SYSCTL_CLK_STATUS_FCC_DONE   (SYSCTL_CLKSTATUS_FCCDONE_DONE)
 Frequency Clock Counter (FCC) done.
 
#define DL_SYSCTL_CLK_STATUS_LFCLK_SOURCE_EXLF   (SYSCTL_CLKSTATUS_LFCLKMUX_EXLF)
 = LFCLK sourced from LFCLK_IN (external digital clock input)
 
#define DL_SYSCTL_CLK_STATUS_SYSOSC_4MHZ   (SYSCTL_CLKSTATUS_SYSOSCFREQ_SYSOSC4M)
 = SYSOSC is at low frequency (4MHz)
 
#define DL_SYSCTL_CLK_STATUS_SYSOSC_USERTRIM_FREQ   (SYSCTL_CLKSTATUS_SYSOSCFREQ_SYSOSCUSER)
 = SYSOSC is at the user-trimmed frequency (16 or 24MHz)
 
#define DL_SYSCTL_STATUS_SHUTDOWN_IO_LOCK_TRUE   (SYSCTL_SYSSTATUS_SHDNIOLOCK_TRUE)
 IO is locked due to SHUTDOWN.
 
#define DL_SYSCTL_STATUS_EXT_RESET_PIN_DISABLED   (SYSCTL_SYSSTATUS_EXTRSTPINDIS_TRUE)
 User has disabled external reset pin.
 
#define DL_SYSCTL_STATUS_SWD_DISABLED   (SYSCTL_SYSSTATUS_SWDCFGDIS_TRUE)
 User has disabled SWD port.
 
#define DL_SYSCTL_STATUS_PMU_IFREF_GOOD   (SYSCTL_SYSSTATUS_PMUIREFGOOD_TRUE)
 PMU IFREF good.
 
#define DL_SYSCTL_STATUS_VBOOST_GOOD   (SYSCTL_SYSSTATUS_ANACPUMPGOOD_TRUE)
 VBOOST (Analog Charge Pump) started up properly.
 
#define DL_SYSCTL_STATUS_BOR_EVENT   (SYSCTL_SYSSTATUS_BORLVL_TRUE)
 Brown Out Reset event status indicator.
 
#define DL_SYSCTL_STATUS_BOR_LEVEL0   (SYSCTL_SYSSTATUS_BORCURTHRESHOLD_BORMIN)
 Current Brown Out Reset minimum level.
 
#define DL_SYSCTL_STATUS_BOR_LEVEL1   (SYSCTL_SYSSTATUS_BORCURTHRESHOLD_BORLEVEL1)
 Current Brown Out Reset level 1.
 
#define DL_SYSCTL_STATUS_BOR_LEVEL2   (SYSCTL_SYSSTATUS_BORCURTHRESHOLD_BORLEVEL2)
 Current Brown Out Reset level 2.
 
#define DL_SYSCTL_STATUS_BOR_LEVEL3   (SYSCTL_SYSSTATUS_BORCURTHRESHOLD_BORLEVEL3)
 Current Brown Out Reset level 3.
 
#define DL_SYSCTL_setMCLKSource(current, next, ...)   DL_SYSCTL_switchMCLKfrom##current##to##next(__VA_ARGS__);
 Change MCLK source. More...
 

Enumerations

enum  DL_SYSCTL_IIDX {
  DL_SYSCTL_IIDX_LFOSC_GOOD = SYSCTL_IIDX_STAT_LFOSCGOOD,
  DL_SYSCTL_IIDX_ANALOG_CLOCK_ERROR = SYSCTL_IIDX_STAT_ANACLKERR
}
 
enum  DL_SYSCTL_NMI_IIDX {
  DL_SYSCTL_NMI_IIDX_WWDT0_FAULT = SYSCTL_NMIIIDX_STAT_WWDT0,
  DL_SYSCTL_NMI_IIDX_BORLVL = SYSCTL_NMIIIDX_STAT_BORLVL,
  DL_SYSCTL_NMI_IIDX_NO_INT = SYSCTL_NMIIIDX_STAT_NO_INTR
}
 
enum  DL_SYSCTL_ERROR_BEHAVIOR {
  DL_SYSCTL_ERROR_BEHAVIOR_RESET = 0x0,
  DL_SYSCTL_ERROR_BEHAVIOR_NMI = 0x1
}
 
enum  DL_SYSCTL_SYSOSC_FREQ {
  DL_SYSCTL_SYSOSC_FREQ_4M = (SYSCTL_SYSOSCCFG_FREQ_SYSOSC4M),
  DL_SYSCTL_SYSOSC_FREQ_BASE = (SYSCTL_SYSOSCCFG_FREQ_SYSOSCBASE),
  DL_SYSCTL_SYSOSC_FREQ_USERTRIM = (SYSCTL_SYSOSCCFG_FREQ_SYSOSCUSER)
}
 
enum  DL_SYSCTL_MCLK_SOURCE {
  DL_SYSCTL_MCLK_SOURCE_SYSOSC = SYSCTL_MCLKCFG_USEHSCLK_DISABLE,
  DL_SYSCTL_MCLK_SOURCE_HSCLK = SYSCTL_MCLKCFG_USEHSCLK_ENABLE,
  DL_SYSCTL_MCLK_SOURCE_LFCLK = SYSCTL_MCLKCFG_USELFCLK_ENABLE
}
 
enum  DL_SYSCTL_MCLK_DIVIDER {
  DL_SYSCTL_MCLK_DIVIDER_DISABLE = 0x0,
  DL_SYSCTL_MCLK_DIVIDER_2 = 0x1,
  DL_SYSCTL_MCLK_DIVIDER_3 = 0x2,
  DL_SYSCTL_MCLK_DIVIDER_4 = 0x3,
  DL_SYSCTL_MCLK_DIVIDER_5 = 0x4,
  DL_SYSCTL_MCLK_DIVIDER_6 = 0x5,
  DL_SYSCTL_MCLK_DIVIDER_7 = 0x6,
  DL_SYSCTL_MCLK_DIVIDER_8 = 0x7,
  DL_SYSCTL_MCLK_DIVIDER_9 = 0x8,
  DL_SYSCTL_MCLK_DIVIDER_10 = 0x9,
  DL_SYSCTL_MCLK_DIVIDER_11 = 0xA,
  DL_SYSCTL_MCLK_DIVIDER_12 = 0xB,
  DL_SYSCTL_MCLK_DIVIDER_13 = 0xC,
  DL_SYSCTL_MCLK_DIVIDER_14 = 0xD,
  DL_SYSCTL_MCLK_DIVIDER_15 = 0xE,
  DL_SYSCTL_MCLK_DIVIDER_16 = 0xF
}
 
enum  DL_SYSCTL_CLK_OUT_SOURCE {
  DL_SYSCTL_CLK_OUT_SOURCE_SYSOSC = SYSCTL_GENCLKCFG_EXCLKSRC_SYSOSC,
  DL_SYSCTL_CLK_OUT_SOURCE_ULPCLK = SYSCTL_GENCLKCFG_EXCLKSRC_ULPCLK,
  DL_SYSCTL_CLK_OUT_SOURCE_LFCLK = SYSCTL_GENCLKCFG_EXCLKSRC_LFCLK,
  DL_SYSCTL_CLK_OUT_SOURCE_MFPCLK = SYSCTL_GENCLKCFG_EXCLKSRC_MFPCLK,
  DL_SYSCTL_CLK_OUT_SOURCE_HFCLK = SYSCTL_GENCLKCFG_EXCLKSRC_HFCLK
}
 
enum  DL_SYSCTL_CLK_OUT_DIVIDE {
  DL_SYSCTL_CLK_OUT_DIVIDE_DISABLE = SYSCTL_GENCLKCFG_EXCLKDIVEN_PASSTHRU,
  DL_SYSCTL_CLK_OUT_DIVIDE_2,
  DL_SYSCTL_CLK_OUT_DIVIDE_4,
  DL_SYSCTL_CLK_OUT_DIVIDE_6,
  DL_SYSCTL_CLK_OUT_DIVIDE_8,
  DL_SYSCTL_CLK_OUT_DIVIDE_10,
  DL_SYSCTL_CLK_OUT_DIVIDE_12,
  DL_SYSCTL_CLK_OUT_DIVIDE_14,
  DL_SYSCTL_CLK_OUT_DIVIDE_16
}
 
enum  DL_SYSCTL_VBOOST {
  DL_SYSCTL_VBOOST_ONDEMAND = SYSCTL_GENCLKCFG_ANACPUMPCFG_ONDEMAND,
  DL_SYSCTL_VBOOST_ONACTIVE = SYSCTL_GENCLKCFG_ANACPUMPCFG_ONACTIVE,
  DL_SYSCTL_VBOOST_ONALWAYS = SYSCTL_GENCLKCFG_ANACPUMPCFG_ONALWAYS
}
 
enum  DL_SYSCTL_FCC_TRIG_TYPE {
  DL_SYSCTL_FCC_TRIG_TYPE_RISE_RISE = SYSCTL_GENCLKCFG_FCCLVLTRIG_RISE2RISE,
  DL_SYSCTL_FCC_TRIG_TYPE_LEVEL = SYSCTL_GENCLKCFG_FCCLVLTRIG_LEVEL
}
 
enum  DL_SYSCTL_FCC_TRIG_SOURCE {
  DL_SYSCTL_FCC_TRIG_SOURCE_FCC_IN = SYSCTL_GENCLKCFG_FCCTRIGSRC_EXTPIN,
  DL_SYSCTL_FCC_TRIG_SOURCE_LFCLK = SYSCTL_GENCLKCFG_FCCTRIGSRC_LFCLK
}
 
enum  DL_SYSCTL_FCC_CLOCK_SOURCE {
  DL_SYSCTL_FCC_CLOCK_SOURCE_MCLK = SYSCTL_GENCLKCFG_FCCSELCLK_MCLK,
  DL_SYSCTL_FCC_CLOCK_SOURCE_SYSOSC = SYSCTL_GENCLKCFG_FCCSELCLK_SYSOSC,
  DL_SYSCTL_FCC_CLOCK_SOURCE_HFCLK = SYSCTL_GENCLKCFG_FCCSELCLK_HFCLK,
  DL_SYSCTL_FCC_CLOCK_SOURCE_CLK_OUT = SYSCTL_GENCLKCFG_FCCSELCLK_EXTCLK,
  DL_SYSCTL_FCC_CLOCK_SOURCE_FCC_IN = SYSCTL_GENCLKCFG_FCCSELCLK_FCCIN
}
 
enum  DL_SYSCTL_FCC_TRIG_CNT {
  DL_SYSCTL_FCC_TRIG_CNT_01,
  DL_SYSCTL_FCC_TRIG_CNT_02,
  DL_SYSCTL_FCC_TRIG_CNT_03,
  DL_SYSCTL_FCC_TRIG_CNT_04,
  DL_SYSCTL_FCC_TRIG_CNT_05,
  DL_SYSCTL_FCC_TRIG_CNT_06,
  DL_SYSCTL_FCC_TRIG_CNT_07,
  DL_SYSCTL_FCC_TRIG_CNT_08,
  DL_SYSCTL_FCC_TRIG_CNT_09,
  DL_SYSCTL_FCC_TRIG_CNT_10,
  DL_SYSCTL_FCC_TRIG_CNT_11,
  DL_SYSCTL_FCC_TRIG_CNT_12,
  DL_SYSCTL_FCC_TRIG_CNT_13,
  DL_SYSCTL_FCC_TRIG_CNT_14,
  DL_SYSCTL_FCC_TRIG_CNT_15,
  DL_SYSCTL_FCC_TRIG_CNT_16,
  DL_SYSCTL_FCC_TRIG_CNT_17,
  DL_SYSCTL_FCC_TRIG_CNT_18,
  DL_SYSCTL_FCC_TRIG_CNT_19,
  DL_SYSCTL_FCC_TRIG_CNT_20,
  DL_SYSCTL_FCC_TRIG_CNT_21,
  DL_SYSCTL_FCC_TRIG_CNT_22,
  DL_SYSCTL_FCC_TRIG_CNT_23,
  DL_SYSCTL_FCC_TRIG_CNT_24,
  DL_SYSCTL_FCC_TRIG_CNT_25,
  DL_SYSCTL_FCC_TRIG_CNT_26,
  DL_SYSCTL_FCC_TRIG_CNT_27,
  DL_SYSCTL_FCC_TRIG_CNT_28,
  DL_SYSCTL_FCC_TRIG_CNT_29,
  DL_SYSCTL_FCC_TRIG_CNT_30,
  DL_SYSCTL_FCC_TRIG_CNT_31,
  DL_SYSCTL_FCC_TRIG_CNT_32
}
 
enum  DL_SYSCTL_POWER_POLICY_RUN_SLEEP {
  DL_SYSCTL_POWER_POLICY_RUN_SLEEP_NOT_ENABLED = 0x0,
  DL_SYSCTL_POWER_POLICY_RUN_SLEEP0 = 0x1,
  DL_SYSCTL_POWER_POLICY_RUN_SLEEP1 = 0x2,
  DL_SYSCTL_POWER_POLICY_RUN_SLEEP2 = 0x3
}
 
enum  DL_SYSCTL_POWER_POLICY_STOP {
  DL_SYSCTL_POWER_POLICY_STOP_NOT_ENABLED = 0x0,
  DL_SYSCTL_POWER_POLICY_STOP0 = 0x1,
  DL_SYSCTL_POWER_POLICY_STOP2 = 0x3
}
 
enum  DL_SYSCTL_POWER_POLICY_STANDBY {
  DL_SYSCTL_POWER_POLICY_STANDBY_NOT_ENABLED = 0x0,
  DL_SYSCTL_POWER_POLICY_STANDBY0 = 0x1,
  DL_SYSCTL_POWER_POLICY_STANDBY1 = 0x2
}
 
enum  DL_SYSCTL_BOR_THRESHOLD_LEVEL { DL_SYSCTL_BOR_THRESHOLD_LEVEL_0 = SYSCTL_BORTHRESHOLD_LEVEL_BORMIN }
 
enum  DL_SYSCTL_SHUTDOWN_STORAGE_BYTE {
  DL_SYSCTL_SHUTDOWN_STORAGE_BYTE_0 = 0x0,
  DL_SYSCTL_SHUTDOWN_STORAGE_BYTE_1 = 0x1,
  DL_SYSCTL_SHUTDOWN_STORAGE_BYTE_2 = 0x2,
  DL_SYSCTL_SHUTDOWN_STORAGE_BYTE_3 = 0x3
}
 
enum  DL_SYSCTL_RESET_CAUSE {
  DL_SYSCTL_RESET_CAUSE_NO_RESET = SYSCTL_RSTCAUSE_ID_NORST,
  DL_SYSCTL_RESET_CAUSE_POR_HW_FAILURE = SYSCTL_RSTCAUSE_ID_PORHWFAIL,
  DL_SYSCTL_RESET_CAUSE_POR_EXTERNAL_NRST = SYSCTL_RSTCAUSE_ID_POREXNRST,
  DL_SYSCTL_RESET_CAUSE_POR_SW_TRIGGERED = SYSCTL_RSTCAUSE_ID_PORSW,
  DL_SYSCTL_RESET_CAUSE_BOR_SUPPLY_FAILURE = SYSCTL_RSTCAUSE_ID_BORSUPPLY,
  DL_SYSCTL_RESET_CAUSE_BOR_WAKE_FROM_SHUTDOWN,
  DL_SYSCTL_RESET_CAUSE_BOOTRST_NON_PMU_PARITY_FAULT,
  DL_SYSCTL_RESET_CAUSE_BOOTRST_CLOCK_FAULT = SYSCTL_RSTCAUSE_ID_BOOTCLKFAIL,
  DL_SYSCTL_RESET_CAUSE_BOOTRST_SW_TRIGGERED = SYSCTL_RSTCAUSE_ID_BOOTSW,
  DL_SYSCTL_RESET_CAUSE_BOOTRST_EXTERNAL_NRST,
  DL_SYSCTL_RESET_CAUSE_SYSRST_BSL_EXIT = SYSCTL_RSTCAUSE_ID_SYSBSLEXIT,
  DL_SYSCTL_RESET_CAUSE_SYSRST_BSL_ENTRY = SYSCTL_RSTCAUSE_ID_SYSBSLENTRY,
  DL_SYSCTL_RESET_CAUSE_SYSRST_WWDT0_VIOLATION = SYSCTL_RSTCAUSE_ID_SYSWWDT0,
  DL_SYSCTL_RESET_CAUSE_SYSRST_WWDT1_VIOLATION = SYSCTL_RSTCAUSE_ID_SYSWWDT1,
  DL_SYSCTL_RESET_CAUSE_SYSRST_FLASH_ECC_ERROR,
  DL_SYSCTL_RESET_CAUSE_SYSRST_CPU_LOCKUP_VIOLATION,
  DL_SYSCTL_RESET_CAUSE_SYSRST_DEBUG_TRIGGERED = SYSCTL_RSTCAUSE_ID_SYSDBG,
  DL_SYSCTL_RESET_CAUSE_SYSRST_SW_TRIGGERED = SYSCTL_RSTCAUSE_ID_SYSSW,
  DL_SYSCTL_RESET_CAUSE_CPURST_DEBUG_TRIGGERED = SYSCTL_RSTCAUSE_ID_CPUDBG,
  DL_SYSCTL_RESET_CAUSE_CPURST_SW_TRIGGERED = SYSCTL_RSTCAUSE_ID_CPUSW
}
 
enum  DL_SYSCTL_BEEPER_FREQ {
  DL_SYSCTL_BEEPER_FREQ_1KHZ = SYSCTL_BEEPCFG_FREQ_1KHZ,
  DL_SYSCTL_BEEPER_FREQ_2KHZ = SYSCTL_BEEPCFG_FREQ_2KHZ,
  DL_SYSCTL_BEEPER_FREQ_4KHZ = SYSCTL_BEEPCFG_FREQ_4KHZ,
  DL_SYSCTL_BEEPER_FREQ_8KHZ = SYSCTL_BEEPCFG_FREQ_8KHZ
}
 

Functions

__STATIC_INLINE void DL_SYSCTL_enableSleepOnExit (void)
 Enable sleep on exit. More...
 
__STATIC_INLINE void DL_SYSCTL_disableSleepOnExit (void)
 Disable sleep on exit. More...
 
__STATIC_INLINE bool DL_SYSCTL_isSleepOnExitEnabled (void)
 Check if sleep on exit is enabled.
 
__STATIC_INLINE void DL_SYSCTL_enableEventOnPend (void)
 Enable send event on pending bit. More...
 
__STATIC_INLINE void DL_SYSCTL_disableEventOnPend (void)
 Disable send event on pending bit. More...
 
__STATIC_INLINE bool DL_SYSCTL_isEventOnPendEnabled (void)
 Check if send event on pending bit is enabled. More...
 
void DL_SYSCTL_switchMCLKfromSYSOSCtoLFCLK (bool disableSYSOSC)
 Change MCLK source from SYSOSC to LFCLK. More...
 
void DL_SYSCTL_switchMCLKfromLFCLKtoSYSOSC (void)
 Change MCLK source from LFCLK to SYSOSC. More...
 
void DL_SYSCTL_switchMCLKfromSYSOSCtoHSCLK (void)
 Change MCLK source from SYSOSC to HSCLK. More...
 
void DL_SYSCTL_switchMCLKfromHSCLKtoSYSOSC (void)
 Change MCLK source from HSCLK to SYSOSC. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicyRUN0SLEEP0 (void)
 Set the RUN/SLEEP mode power policy to RUN0/SLEEP0. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicyRUN1SLEEP1 (void)
 Set the RUN/SLEEP mode power policy to RUN1/SLEEP1. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicyRUN2SLEEP2 (void)
 Set the RUN/SLEEP mode power policy to RUN2/SLEEP2. More...
 
DL_SYSCTL_POWER_POLICY_RUN_SLEEP DL_SYSCTL_getPowerPolicyRUNSLEEP (void)
 Get the RUN/SLEEP mode power policy. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicySTOP0 (void)
 Set the STOP mode power policy to STOP0. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicySTOP2 (void)
 Set the STOP mode power policy to STOP2. More...
 
DL_SYSCTL_POWER_POLICY_STOP DL_SYSCTL_getPowerPolicySTOP (void)
 Get the STOP mode power policy. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicySTANDBY0 (void)
 Set the STANDBY mode power policy to STANDBY0. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicySTANDBY1 (void)
 Set the STANDBY mode power policy to STANDBY1. More...
 
DL_SYSCTL_POWER_POLICY_STANDBY DL_SYSCTL_getPowerPolicySTANDBY (void)
 Get the STANDBY mode power policy. More...
 
__STATIC_INLINE void DL_SYSCTL_setPowerPolicySHUTDOWN (void)
 Set power policy to SHUTDOWN mode. More...
 
__STATIC_INLINE void DL_SYSCTL_setBORThreshold (DL_SYSCTL_BOR_THRESHOLD_LEVEL thresholdLevel)
 Set the brown-out reset (BOR) threshold level. More...
 
__STATIC_INLINE DL_SYSCTL_BOR_THRESHOLD_LEVEL DL_SYSCTL_getBORThreshold (void)
 Get the brown-out reset (BOR) threshold level. More...
 
__STATIC_INLINE void DL_SYSCTL_activateBORThreshold (void)
 Activate the BOR threshold level. More...
 
__STATIC_INLINE void DL_SYSCTL_resetDevice (uint32_t resetType)
 Resets the device. More...
 
__STATIC_INLINE void DL_SYSCTL_enableInterrupt (uint32_t interruptMask)
 Enable SYSCTL interrupts. More...
 
__STATIC_INLINE void DL_SYSCTL_disableInterrupt (uint32_t interruptMask)
 Disable SYSCTL interrupts. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getEnabledInterrupts (uint32_t interruptMask)
 Check which SYSCTL interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getEnabledInterruptStatus (uint32_t interruptMask)
 Check interrupt flag of enabled SYSCTL interrupts. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getRawInterruptStatus (uint32_t interruptMask)
 Check interrupt flag of any SYSCTL interrupt. More...
 
__STATIC_INLINE DL_SYSCTL_IIDX DL_SYSCTL_getPendingInterrupt (void)
 Get highest priority pending SYSCTL interrupt. More...
 
__STATIC_INLINE void DL_SYSCTL_clearInterruptStatus (uint32_t interruptMask)
 Clear pending SYSCTL interrupts. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getRawNonMaskableInterruptStatus (uint32_t interruptMask)
 Check interrupt flag of any SYSCTL non-maskable interrupt. More...
 
__STATIC_INLINE DL_SYSCTL_NMI_IIDX DL_SYSCTL_getPendingNonMaskableInterrupt (void)
 Get highest priority pending SYSCTL non-maskable interrupt. More...
 
__STATIC_INLINE void DL_SYSCTL_clearNonMaskableInterruptStatus (uint32_t interruptMask)
 Clear pending SYSCTL non-maskable interrupts. More...
 
__STATIC_INLINE void DL_SYSCTL_setWWDT0ErrorBehavior (DL_SYSCTL_ERROR_BEHAVIOR behavior)
 Set the behavior when a WWDT0 error occurs. More...
 
__STATIC_INLINE DL_SYSCTL_ERROR_BEHAVIOR DL_SYSCTL_getWWDT0ErrorBehavior (void)
 Get the behavior when a WWDT0 error occurs. More...
 
__STATIC_INLINE void DL_SYSCTL_setMCLKDivider (DL_SYSCTL_MCLK_DIVIDER divider)
 Set the Main Clock (MCLK) divider (MDIV) More...
 
__STATIC_INLINE DL_SYSCTL_MCLK_DIVIDER DL_SYSCTL_getMCLKDivider (void)
 Get the Main Clock (MCLK) divider (MDIV) More...
 
__STATIC_INLINE DL_SYSCTL_MCLK_SOURCE DL_SYSCTL_getMCLKSource (void)
 Get the source for the Main Clock (MCLK) More...
 
__STATIC_INLINE void DL_SYSCTL_setSYSOSCFreq (DL_SYSCTL_SYSOSC_FREQ freq)
 Set the target frequency of the System Oscillator (SYSOSC) More...
 
__STATIC_INLINE DL_SYSCTL_SYSOSC_FREQ DL_SYSCTL_getTargetSYSOSCFreq (void)
 Get the target frequency of the System Oscillator (SYSOSC) Target/desired SYSOSC frequency may be different than current/actual SYSOSC frequency during gear shift and other operations. This function matches what is input by DL_SYSCTL_setSYSOSCFreq. More...
 
__STATIC_INLINE DL_SYSCTL_SYSOSC_FREQ DL_SYSCTL_getCurrentSYSOSCFreq (void)
 Get the current frequency of the System Oscillator (SYSOSC) Current/actual SYSOSC frequency may be different than target/desired SYSOSC frequency during gear shift and other operations. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getClockStatus (void)
 Returns status of the different clocks in CKM. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getStatus (void)
 Returns general status of SYSCTL. More...
 
__STATIC_INLINE void DL_SYSCTL_clearECCErrorStatus (void)
 Clear the ECC error bits in SYSSTATUS. More...
 
__STATIC_INLINE void DL_SYSCTL_setLFCLKSourceEXLF (void)
 Change LFCLK source to external digital LFCLK_IN. More...
 
__STATIC_INLINE void DL_SYSCTL_setHFCLKSourceHFCLKIN (void)
 Change HFCLK source to external digital HFCLK_IN. More...
 
__STATIC_INLINE void DL_SYSCTL_enableMFCLK (void)
 Enable the Medium Frequency Clock (MFCLK) More...
 
__STATIC_INLINE void DL_SYSCTL_disableMFCLK (void)
 Disable the Medium Frequency Clock (MFCLK)
 
__STATIC_INLINE void DL_SYSCTL_enableExternalClock (DL_SYSCTL_CLK_OUT_SOURCE source, DL_SYSCTL_CLK_OUT_DIVIDE divider)
 Enable the External Clock (CLK_OUT) More...
 
__STATIC_INLINE void DL_SYSCTL_disableExternalClock (void)
 Disable the External Clock (CLK_OUT) More...
 
__STATIC_INLINE void DL_SYSCTL_disableExternalClockDivider (void)
 Disable the External Clock (CLK_OUT) Divider. More...
 
__STATIC_INLINE void DL_SYSCTL_enableMFPCLK (void)
 Enable the Middle Frequency Precision Clock (MFPCLK) More...
 
__STATIC_INLINE void DL_SYSCTL_disableMFPCLK (void)
 Disable the Middle Frequency Precision Clock (MFPCLK) More...
 
__STATIC_INLINE void DL_SYSCTL_blockAllAsyncFastClockRequests (void)
 Blocks all asynchronous fast clock requests. More...
 
__STATIC_INLINE void DL_SYSCTL_allowAllAsyncFastClockRequests (void)
 Allows all asynchronous fast clock requests. More...
 
__STATIC_INLINE void DL_SYSCTL_enableFastCPUEventHandling (void)
 Generates an asynchronous fast clock request upon any IRQ request to CPU. More...
 
__STATIC_INLINE void DL_SYSCTL_disableFastCPUEventHandling (void)
 Maintains current system clock speed for IRQ request to CPU. More...
 
__STATIC_INLINE void DL_SYSCTL_setSRAMBoundaryAddress (uint32_t address)
 Set the SRAM boundary address to act as partition for read-execute permission. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getSRAMBoundaryAddress (void)
 Get the SRAM boundary address. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_readFCC (void)
 Read Frequency Clock Counter (FCC) More...
 
__STATIC_INLINE void DL_SYSCTL_startFCC (void)
 Start Frequency Clock Counter (FCC) More...
 
__STATIC_INLINE bool DL_SYSCTL_isFCCDone (void)
 Returns whether FCC is done capturing. More...
 
void DL_SYSCTL_configFCC (DL_SYSCTL_FCC_TRIG_TYPE trigLvl, DL_SYSCTL_FCC_TRIG_SOURCE trigSrc, DL_SYSCTL_FCC_CLOCK_SOURCE clkSrc)
 Configure the Frequency Clock Counter (FCC) More...
 
__STATIC_INLINE void DL_SYSCTL_setFCCPeriods (DL_SYSCTL_FCC_TRIG_CNT periods)
 Sets number of rising-edge to rising-edge period for Frequency Clock Counter (FCC) More...
 
__STATIC_INLINE DL_SYSCTL_FCC_TRIG_CNT DL_SYSCTL_getFCCPeriods (void)
 Gets number of rising-edge to rising-edge period for Frequency Clock Counter (FCC) More...
 
__STATIC_INLINE void DL_SYSCTL_enableSYSOSCFCL (void)
 Enable Frequency Correction Loop (FCL) in Internal Resistor mode. More...
 
__STATIC_INLINE void DL_SYSCTL_enableWriteLock (void)
 Enable write protection of selected SYSCTL registers. More...
 
__STATIC_INLINE void DL_SYSCTL_disableWriteLock (void)
 Disable write protection of selected SYSCTL registers. More...
 
__STATIC_INLINE void DL_SYSCTL_setVBOOSTConfig (DL_SYSCTL_VBOOST setting)
 Sets operating mode of VBOOST (analog charge pump) More...
 
__STATIC_INLINE DL_SYSCTL_VBOOST DL_SYSCTL_getVBOOSTConfig (void)
 Gets operating mode of VBOOST (analog charge pump) More...
 
__STATIC_INLINE uint8_t DL_SYSCTL_getShutdownStorageByte (DL_SYSCTL_SHUTDOWN_STORAGE_BYTE index)
 Return byte that was saved through SHUTDOWN. More...
 
__STATIC_INLINE void DL_SYSCTL_setShutdownStorageByte (DL_SYSCTL_SHUTDOWN_STORAGE_BYTE index, uint8_t data)
 Save a byte to SHUTDOWN memory. More...
 
__STATIC_INLINE void DL_SYSCTL_releaseShutdownIO (void)
 Enable SHUTDOWN IO Release. More...
 
__STATIC_INLINE void DL_SYSCTL_disableNRSTPin (void)
 Disable the reset functionality of the NRST pin. More...
 
__STATIC_INLINE void DL_SYSCTL_disableSWD (void)
 Disable Serial Wire Debug (SWD) functionality. More...
 
__STATIC_INLINE DL_SYSCTL_RESET_CAUSE DL_SYSCTL_getResetCause (void)
 Return byte that is stored in RSTCAUSE. More...
 
__STATIC_INLINE uint32_t DL_SYSCTL_getTempCalibrationConstant (void)
 Retrieves the calibration constant of the temperature sensor to be used in temperature calculation. More...
 
__STATIC_INLINE void DL_SYSCTL_enableBeeperOutput (void)
 Enable Beeper output. More...
 
__STATIC_INLINE void DL_SYSCTL_disableBeeperOutput (void)
 Disable Beeper output.
 
__STATIC_INLINE void DL_SYSCTL_setBeeperFreq (DL_SYSCTL_BEEPER_FREQ freq)
 Set the target frequency of the Beeper output. More...
 
__STATIC_INLINE DL_SYSCTL_BEEPER_FREQ DL_SYSCTL_getBeeperFreq (void)
 Get the target frequency of the the Beeper output. More...
 
__STATIC_INLINE bool DL_SYSCTL_isBeeperEnabled (void)
 Check if Beeper is enabled. More...
 
__STATIC_INLINE bool DL_SYSCTL_isFlashBankSwapEnabled (void)
 Checks if Flash Bank swapping is enabled. More...
 
__STATIC_INLINE bool DL_SYSCTL_isExecuteFromUpperFlashBank (void)
 Checks if executing from upper flash bank. More...
 
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale