88 #ifndef FOC_INCLUDE_IDREFERENCING_H_ 89 #define FOC_INCLUDE_IDREFERENCING_H_ 106 fluxWeakeningEnable: 1,
Flux Weakening Working Structure.
Definition: fluxWeak.h:97
Id reference Flags Structure.
Definition: idReferencing.h:96
FLUX_WEAK_T fluxWeak
Definition: idReferencing.h:123
uint16_t w
Definition: idReferencing.h:114
MTPA Working Structure.
Definition: mtpa.h:96
Id reference Working Structure.
Definition: idReferencing.h:119
ID_REFERENCING_FLAGS_T flags
Definition: idReferencing.h:137
MTPA_T mtpa
Definition: idReferencing.h:127
int32_t idRefFluxModeSet
Definition: idReferencing.h:131
void idRefLowPriorityRun(ID_REF_T *pIdRef)
Id Reference Low Priority Run.
Definition: idReferencing.c:86
void idRefInit(ID_REF_T *pIdRef)
Id Reference Init Init.
Definition: idReferencing.c:78
Id Ref Flags Structure.
Definition: idReferencing.h:100