Sensored FOC Motor Control Library Overview

Software Overview

Hall Effect Sensored Field-Oriented Control (FOC) Library is made of three main layers: Application layer, HAL Layer, and MSPM0 DriverLib.

Sensored FOC Architecture

Fig. 1 Sensored FOC Architecture

1. Application Layer

Application Layer is a software layer that does specific functions like Motor control. If any application perform any hardware specific actions, it is done through the HAL Layer APIs.

FOC Library

FOC library is a library that contains generic motor control algorithms algorithms for 3-phase Sensored FOC motor control.

This Library has the following modules integrated :

  • HALL Sensor Calibration

  • Deadtime compensation

  • PI controllers

  • Openloop

  • Closeloop

  • Hall Estimator

  • MTPA

  • Field Weakening

  • Brake

  • Reverse Drive

FOC library also contains the Motor control state machines.

Motor Control Application

Motor control Application takes care of register value conversions from users inputs and feeds to the FOC library.

Application Module

appInterface : This folder contains the header files for the Input, Control and Status variables.

User can add their custom Input / Ctrl configurations to “appUserInputRegsConfig” API which is periodically called by the application every 200mS when the motor is in not spinning.

ConfigTables All the register map tuning configurations for a given index is defined in the Config tables.

User can add custom values to these tables based on the application use case

Main Application

Main application contains the user code which initializes the application modules and periodically calls the configuration updates in While(1) loop.

main.h Configurations

User Can define the Default System Configurations from the main.h

Base Address : The default RAM address space for the Input,Ctrl & Status register map structures are defined in main.h. It is recommended to not alter the address space as these will be used by the GUI application for variable referencing.

Hardware Configurations

Gate Driver Selection - Select the connected HW using #ifdef Macro with the available Gate Driver Configurations. Ex: DRV8316/TIDA010251/CUSTOM_BOARD in the gatedriver.h file at project_root/modules/hal/gateDriverInterface/include/gateDriver.h

If user selects a Custom gate driver , It is recommended to choose any of the Gate driver configurations as a starting point and update the SYSCONFIG and HAL based on the pin configurations. The DRV8316/DRV8323 has SPI based Gate Driver Communication with Three Shunt Configuration & DRV8329 Example is based on Single Shunt configuration without SPI communication.

Current Shunt Configuration - User can choose the Current shunt configurations based on the actual number of Shunt Resistors used for Current Sensing.

“#define CURRENT_SHUNT_CONFIG” Macro will be used for the definition of given shunt configuration

Below #ifdef Macro’s can be used to select various current shunt configurations available in the FW.

  • __CURRENT_THREE_SHUNT_DYNAMIC - For three shunt configuration with dynamic selection of any two shunts based on the Sector

  • __CURRENT_THREE_SHUNT_XY_Z - For three shunt configuration with Fixed current sensing where XY phases are used for simultaneous sampling and Z phase used for lateral sample.

  • __CURRENT_TWO_SHUNT_X_Y - For Dual Shunt configurations with X & Y as the respective phases of the three phases used for current sensing

  • __CURRENT_SINGLE_SHUNT - For Single Shunt current sense Configuration.

For Single shunt configuration user can select _NONINVERT_ISEN or _INVERT_ISEN based on the amplifier input configuration.

For Inverted Isense Configuration - The Voltage across the amplifier decreases as the Current increases.

FULL_SCALE_CURRENT_BASE - Set the Maximum measurable current based on the Current Shunt Amplifier Gain and the Current Sense Resistor.

DC_VOLTAGE_BASE - Set the Maximum measurable phase Voltage based on the Scaled down voltage fed to ADC from the Voltage Divider Circuit.

2. HAL Layer

The Hardware Abstraction Layer (HAL) creates an abstraction layer that provides APIs to configure different pins and peripherals. The goal of using HAL is to abstract all device specific configurations which simplifies porting of the library to various hardware by minimizing the updates needed to other components. The HAL is meant to abstract only the required pins or peripherals required for the application while still having flexibility and scalability for porting to other MSPM0 MCUs or motor drivers.

HAL uses the defines generated from TI SysConfig, so it is very easy to change the pin in the TI SysConfig GUI. The HAL automatically follows this without the user having to change any code in the HAL layer.

For Example below is the define for direction pin PORT it is referred by HAL Layer through FOC_GPIO_IN_PORT, this define is mapped to the port number by the TI SysConfig. Thus by changing the PORT in TI SysConfig GUI the direction pin PORT number can be controlled.

/*! @brief GPIO port for direction pin */
#define FOC_GPIO_DIR_PORT           (FOC_GPIO_IN_PORT)

Gate Driver Interface Library

Gate Driver Interface Library provides the APIs for reading the currents and voltage channels. Also if the DRV is used it configured the CSA gain and other gate driver register configurations.

Gate Driver Interface

Fig. 2 Gate Driver Interface

The gate driver Interface has 3 parts:

  • Gate driver Library

Has the APIs to configure the gate driver registers through SPI if the gate driver is a SPI based.

  • Gate driver peripheral peripheral defines

The Gate driver peripheral defines are in gateDriver.h. Here the ADC memory indexes used for reading the current and voltages are defined.

Gate Driver peripheral defines

Fig. 3 Gate Driver peripheral defines

In the above image we can see that phase U voltage is mapped to ADC channel 6 and the U phase voltage memory index is ADC1_ADCMEM_0, ie A1.6/PB19 is the pin used for U phase voltage, this pin has to be connected to the gate drivers U phase voltage pin. Please refer to the Hardware Guide to know how to connect the Gate driver to the launchpad to make the pin connections.

  • Gate driver HAL Interface

Gate driver HAL Interface handles the configurations of ADC channels to convert phase voltage inputs and phase current inputs from gate driver.

Single Shunt PWM Configurations:

In single shunt based current sensing method, the three phase currents are estimated based on sampled DC bus current from multiple instances. Unlike in three phase current sensing, where the currents are sampled at center of PWM’s, the currents in 1-shunt method are sampled at various phase switching points within one PWM cycle. To realize this, the PWM’s are dynamically shifted to enable sampling at different voltage vectors in a given sector. This way enough margin is created for current sampling in the non overlapping regions. For this reason, the PWM’s are not center aligned and we assign Compare B indexes of Timer A to achieve this shifting. It is important for user to configure the Compare B index for the PWM’s based on the Pin configuration.

Compare B Index Configuration

Fig. 4 Compare B Index Configuration

In the above example for TIDA010251 ,The primary compare events are selected based on HS PWM pins and the corresponding Timer A0 Compare ports as C2-C3-C1 respectively for U-V-W phases from available primary ports from C0 to C3. The secondary Compare events are selected from the remaining Compare indexes from 0-5 as CC0-CC4-CC5.

Enabling simultaneous current sampling :

Simultaneous current sampling helps to sample the current signals at the same time. This feature helps to improve the performance of FOC by improving the rotor position estimations.

In MSPM0 to enable simultaneous current sampling we need to use both ADCs 0 and 1 and trigger both at the same time. For implementing Simultaneous sampling we need to have any one phase current input connected to both ADC 0 and ADC 1, this additional connection is the minimum requirement needed so that we can sample all the dual current sensing configurations.

The simultaneous current sampling is implemented in DRV8316 gate driver library, refer to drv8316_focHalInterface.c for the implementation code. In DRV8316 gate driver library phase B current is routed for both the ADC 0 & 1 channels to achieve simultaneous sampling in all the dual current sensing configurations : AB, BC, CA (ie, in AB, A is sampled by ADC 0 and B by ADC 1. In BC ,B is sampled by ADC 0 and C by ADC 1).

Controller Interface Library

Controller Interface Library provides HAL APIs for controlling the peripherals like timer, gpio etc. The Controller Interface Library uses the gate driver Interface library to set the correct phase and voltage channel configurations to the ADC.

Peripheral defines in focPeripheralInit.h

Fig. 5 Peripheral defines in focPeripheralInit.h

Important Peripherals and configurations used in FOC

1. GPIOs

Following are the GPIO’s used by the Application code:

  1. Brake input:

Pin input for applying brake

  1. Direction pin

Pin input for selecting direction

  1. Nfault

Output pin, set low if any fault is detected

  1. nSleep

Output pin, sets the gate driver sleep input

  1. HALL Sensor Input

Three Hall Sensor Input Pins, Timer Capture events are Triggered based on the Hall Pin Edges. All the three GPIO pins for Hall Sesnsing are to be selected from the same GPIO Port.

User can change the GPIO pin selection in the TI SysConfig to select any desired pin as shown below.

GPIO sysconfig

Fig. 6 GPIO sysconfig

2. SPI

SPI is configured in Sysconfig for gate drivers having SPI interface. The SPI configurations used are given below

SPI

Description

Bit rate

5Mhz

Word size

16 bits

Bit Order

MSB First

Chip select

Active low

Frame Format

4 wire

mode

Controller

Clock polarity

Low

Clock Phase

Data on Second clock edge

User can use the same SPI connection to interface any other device, but need to see if the gate driver spi transmission is busy. Also user need to take care of using a different chip select line.

3. PWM

Three PWM channels with complementary outputs are used to drive the motor and one channel is used to trigger the ADC to convert the voltages and currents. TIMER A0 is reserved for generating the PWMs for FOC motor control and user should not use this timer.

TIMER A0 triggers the ADC using event channels, the event channels used are specified in focPeripheralInit.h, user should not use the same event channel used by the Library.

4. ADC

The ADC configurations used are given below:

ADC

Description

Conversion Mode

Sequence sampling

Trigger Source

Event triggered

Sample timer

Sample timer 0

Chip select

Active low

Hardware averaging

4 conversions

ADC hardware averaging is used to remove any noise in the signal

ADC is used in converting DC bus voltage, three phase currents and three phase voltages. The gate driver library defines the ADC channel used for conversion and the memory index of the ADC used. Memory indexes used for current and voltages are listed in gateDriver.h. ADC Interrupt occurs after all currents or voltages are sampled.

If user wishes to use ADC to convert any new channels the user should add new memory index by incrementing the Sequence End address in the TI SysConfig and modify the Trigger mode of the new index to “Valid trigger ..” as shown in the below images. Also note to change the Trigger mode of the default Sequence End address to “Trigger will automatically ..” while adding a new sequence end address. The user should not change the ADC interrupt used by FOC, user can enable a new ADC interrupt for their use case.

ADC sysconfig

Fig. 7 ADC sysconfig

ADC Trigger

Fig. 8 ADC Trigger

For phase voltage and phase current configuration the Library sets the channel using the channel listed in gateDriver.h. For DC bus voltage conversion the pin is specified by TI SysConfig and user needs to take care to update the defines in gateDriver.h, if the pin is changed in TI SysConfig.

The first Two memory indexes of the ADC 0 & 1 are used for the Current Sampling / Voltage sampling and shound’t be modified. The DC bus Voltage is sampled from the 2nd Memory Index and user can choose to use any other Memory Index apart from 0 & 1 of ADC 0 & ADC 1 for any custom ADC addition.

In the existing FOC architecture, The ADC-0 is configured to generate the core FOC Interrupt. User needs to configure this interrupt based on the phase current memory indices as below.

In case all three phase currents are chosen from the same ADC, then memory Index 2 or higher is to be selected for the Interrupt generation.

In case two phase currents are chosen from 1 ADC instance & third phase current is from different ADC instance , memory index 1 or higher to be choosen from the Interrupts.

Note : If none of the phase currents/ Voltages / any sensing pins are connected to ADC-0 , Dummy memory indices are to be created to generate the ADC-0 interrupt matching with above criteria.

Single Shunt FOC Current Sensing ADC Configurations

In Single shunt current sensing , First two ADC indices of a selected ADC are to be allocated for sampling the Current sensing pin. Also for the 0th memory index , trigger option to be selected as Valid Trigger will step to next conversion register. The last memory index of this ADC is to be selected again with Valid Trigger will step to next conversion register .The in between memory indices if used are to be selected with Trigger will automatically step to next conversion register

In the below configuration, Memory Index 0 & 1 are the only two ADC indices used thus both are set with “Valid trigger…”

ADC sysconfig

Fig. 9 ADC sysconfig

Single Shunt FOC Trigger configurations

In single shunt operation, Timer A1’s compare down events are allocated for triggering the ADC. Timer A1 is cross triggered from Timer A0 thus Timer A0/Timer A1 are never to be stopped by the application code.

Two triggers are generated for FOC algorithm with a minimum seperation of “Sampling time + Settling time” requirements to read the Single shunt current sample.

Either of ADC -0 or ADC - 1 used for sampling the DC Bus current is triggered from Timer A1 - compare down Events 0 & 1. First sample is associated with Channel ‘1’ compare down Event and Second ADC sample is linked with Channel ‘0’ compare down event.

Timer A1 sysconfig

Fig. 10 Timer A1 sysconfig

Note : If ADC-1 is chosen for sampling the DC Bus current, ADC 0 is also to be triggered with Timer -A1 compare down channel 0 event as the core FOC interrupt is associated with ADC-0 interrupt. This ensures timely interrupt at the end of ADC-1 current sample. #### 5. Timers

Capture Timer for Speed Measurement :

A 32 Bit Timer TIMG12 is used by the Sensored FOC application in Capture mode to count the time difference between the two hall edges and compute the motor electrical speed. It is important to use high resolution 32bit timer to accurately measure the time difference between Hall events at very low speeds. The timer is configured to subscribe the Events from Hall GPIO rising and Falling edge detection in down counting mode.

Periodic Timer for State Machine:

A 16bit Timer TIMG0 is used to count a period of 1mS and trigger an interrupt to execute the Low Priority State Machine and other House keeping Tasks.

6. DAC

The DAC configurations used are given below:

DAC

Description

Sample Time Generator Rate

100kSPS

Output Resolution

12 bit

Positive Voltage Reference

VDDA

Negative Voltage Reference

VSSA

DAC is used for real time output of the algorithm variables.

NOTE: While enabling the DAC in TI SysConfig user needs to make sure the DAC output pin is not used

Communication Interface Library

Communication Interface Library helps to access the memory of the device using communication peripherals like UART, I2C etc. User can Read or write to the FOC Application registers through the communication peripheral to control the motor externally.

In the current library the UART communication is implementation. Please refer to UART Communication User Guide for more details on communication protocol.

For enabling UART communication with an external device use the below pinouts:

For DRV8316

UART comm pin

LP-MSPM0G3507

LP-MSPM0G3519

UART TX

PA26

PA8

UART RX

PA13

PA9

3. MSPM0 DriverLib Overview

MSPM0 DriverLib is a set of fully functional APIs used to configure, control, and manipulate the hardware peripherals of the MSPM0 platform. Please refer to the DriverLib documentation for more information.