![]() |
![]() |
|
MSPM0L111X TI-Driver Library
2.03.00.07
|
UART driver interface.
#include <stdbool.h>#include <stdint.h>#include <stdlib.h>#include <ti/driverlib/dl_gpio.h>#include <ti/driverlib/dl_uart_main.h>

Go to the source code of this file.
Data Structures | |
| struct | UART_Params |
| UART Parameters. More... | |
Macros | |
| #define | UART_STATUS_SUCCESS (0) |
| Successful status code returned by UART APIs. | |
| #define | UART_STATUS_SREADTIMEOUT (1) |
| A read timeout occurred (not an error). | |
| #define | UART_STATUS_EFRAMING (-1) |
| A framing error occurred. | |
| #define | UART_STATUS_EPARITY (-2) |
| A parity error occurred. | |
| #define | UART_STATUS_EBREAK (-4) |
| A break error occurred. | |
| #define | UART_STATUS_EOVERRUN (-8) |
| A FIFO overrun occurred. | |
| #define | UART_STATUS_EINUSE (-9) |
| The UART is currently in use. | |
| #define | UART_STATUS_EINVALID (-10) |
| An invalid argument or UART_Params field was passed to UART API. | |
| #define | UART_STATUS_EFAIL (-11) |
| General failure status returned by UART API. | |
| #define | UART_STATUS_EMEMORY (-12) |
| A memory allocation failure occurred. | |
| #define | UART_STATUS_ETIMEOUT (-13) |
| A timeout occurred for a blocking UART_read or UART_write call. | |
| #define | UART_STATUS_ECANCELLED (-14) |
| A UART_write() or UART_read() operation was cancelled. | |
| #define | UART_STATUS_ENOTOPEN (-15) |
| A UART_write() or UART_read() called on a device not opened. | |
| #define | UART_STATUS_EAGAIN (-16) |
| A UART_write() or UART_read() in UART_Mode_NONBLOCKING would have blocked. | |
Typedefs | |
| typedef struct UART_Config_ * | UART_Handle |
| A handle that is returned from a UART_open() call. | |
| typedef void(* | UART_Callback) (UART_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status) |
| The definition of a callback function used by the UART driver when used in UART_Mode_CALLBACK. The callback can occur in task or interrupt context. More... | |
| typedef void(* | UART_EventCallback) (UART_Handle handle, uint32_t event, uint32_t data, void *userArg) |
| The definition of a callback function used by the UART driver. The callback can occur in task or interrupt context. More... | |
Enumerations | |
| enum | UART_Mode { UART_Mode_BLOCKING = 0, UART_Mode_CALLBACK, UART_Mode_NONBLOCKING } |
| UART mode settings. More... | |
| enum | UART_ReadReturnMode { UART_ReadReturnMode_FULL = 0, UART_ReadReturnMode_PARTIAL } |
| UART return mode settings. More... | |
| enum | UART_DataLen { UART_DataLen_5 = DL_UART_WORD_LENGTH_5_BITS, UART_DataLen_6 = DL_UART_WORD_LENGTH_6_BITS, UART_DataLen_7 = DL_UART_WORD_LENGTH_7_BITS, UART_DataLen_8 = DL_UART_WORD_LENGTH_8_BITS } |
| UART data length settings. More... | |
| enum | UART_StopBits { UART_StopBits_1 = DL_UART_STOP_BITS_ONE, UART_StopBits_2 = DL_UART_STOP_BITS_TWO } |
| UART stop bit settings. More... | |
| enum | UART_Parity { UART_Parity_NONE = DL_UART_PARITY_NONE, UART_Parity_EVEN = DL_UART_PARITY_EVEN, UART_Parity_ODD = DL_UART_PARITY_ODD, UART_Parity_ZERO = DL_UART_PARITY_STICK_ZERO, UART_Parity_ONE = DL_UART_PARITY_STICK_ONE } |
| UART parity type settings. More... | |
Functions | |
| void | UART_Params_init (UART_Params *params) |
| Function to initialize the UART_Params struct to its defaults. More... | |
| UART_Handle | UART_open (uint_least8_t index, UART_Params *params) |
| Function to initialize a given UART peripheral. More... | |
| void | UART_close (UART_Handle handle) |
| Function to close a UART peripheral specified by the UART handle. More... | |
| int_fast16_t | UART_read (UART_Handle handle, void *buf, size_t size, size_t *bytesRead) |
| Function that reads data from a UART. More... | |
| int_fast16_t | UART_write (UART_Handle handle, const void *buf, size_t size, size_t *bytesWritten) |
| Function that writes data to a UART. More... | |
| int_fast16_t | UART_readTimeout (UART_Handle handle, void *buf, size_t size, size_t *bytesRead, uint32_t timeout) |
| UART read with timeout. Note that the timeout parameter is different from the hardware read timeout. More... | |
| int_fast16_t | UART_writeTimeout (UART_Handle handle, const void *buf, size_t size, size_t *bytesWritten, uint32_t timeout) |
| UART write with timeout. Note that the timeout parameter is different from the hardware read timeout. More... | |
| void | UART_readCancel (UART_Handle handle) |
| Function that cancels a UART_read() function call. More... | |
| void | UART_writeCancel (UART_Handle handle) |
| Function that cancels a UART_write() function call. More... | |
| void | UART_rxDisable (UART_Handle handle) |
| Function that disables collecting of RX data into the circular buffer. More... | |
| void | UART_rxEnable (UART_Handle handle) |
| Function that enables collecting of RX data into the circular buffer. More... | |
| void | UART_flushRx (UART_Handle handle) |
| Function to flush data in the UART RX FIFO. More... | |
| void | UART_getRxCount (UART_Handle handle) |
| Get the number of bytes available in the circular buffer. More... | |