|
| void | DL_I2C_setClockConfig (I2C_Regs *i2c, DL_I2C_ClockConfig *config) |
| | Configure I2C source clock. More...
|
| |
| void | DL_I2C_getClockConfig (I2C_Regs *i2c, DL_I2C_ClockConfig *config) |
| | Get I2C source clock configuration. More...
|
| |
| uint16_t | DL_I2C_fillControllerTXFIFO (I2C_Regs *i2c, uint8_t *buffer, uint16_t count) |
| | Fills the controller TX FIFO with data. More...
|
| |
| void | DL_I2C_flushControllerTXFIFO (I2C_Regs *i2c) |
| | Flushes/removes all elements in the controller TX FIFO. More...
|
| |
| void | DL_I2C_flushControllerRXFIFO (I2C_Regs *i2c) |
| | Flushes/removes all elements in the controller RX FIFO. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerTXFIFOFull (I2C_Regs *i2c) |
| | Checks if controller TX FIFO is full. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerTXFIFOEmpty (I2C_Regs *i2c) |
| | Checks if controller TX FIFO is empty. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerRXFIFOEmpty (I2C_Regs *i2c) |
| | Checks if controller RX FIFO is empty. More...
|
| |
| __STATIC_INLINE void | DL_I2C_resetControllerTransfer (I2C_Regs *i2c) |
| | Reset transfers from from I2C controller. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startControllerTransfer (I2C_Regs *i2c, uint32_t targetAddr, DL_I2C_CONTROLLER_DIRECTION direction, uint16_t length) |
| | Sets up a transfer from I2C controller. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startControllerTransferAdvanced (I2C_Regs *i2c, uint32_t targetAddr, DL_I2C_CONTROLLER_DIRECTION direction, uint16_t length, DL_I2C_CONTROLLER_START start, DL_I2C_CONTROLLER_STOP stop, DL_I2C_CONTROLLER_ACK ack) |
| | Sets up a transfer from I2C controller with control of START, STOP and ACK. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXFIFOFull (I2C_Regs *i2c) |
| | Checks if target TX FIFO is full. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXFIFOEmpty (I2C_Regs *i2c) |
| | Checks if target TX FIFO is empty. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetRXFIFOEmpty (I2C_Regs *i2c) |
| | Checks if target RX FIFO is empty. More...
|
| |
| uint8_t | DL_I2C_fillTargetTXFIFO (I2C_Regs *i2c, uint8_t *buffer, uint8_t count) |
| | Fills the target TX FIFO with data. More...
|
| |
| void | DL_I2C_flushTargetTXFIFO (I2C_Regs *i2c) |
| | Flushes/removes all elements in the target TX FIFO. More...
|
| |
| void | DL_I2C_flushTargetRXFIFO (I2C_Regs *i2c) |
| | Flushes/removes all elements in the target RX FIFO. More...
|
| |
| void | DL_I2C_transmitTargetDataBlocking (I2C_Regs *i2c, uint8_t data) |
| | Transmit target data, waiting until transmit request. More...
|
| |
| bool | DL_I2C_transmitTargetDataCheck (I2C_Regs *i2c, uint8_t data) |
| | Transmit target data. More...
|
| |
| uint8_t | DL_I2C_receiveTargetDataBlocking (I2C_Regs *i2c) |
| | Receive target data, waiting until receive request. More...
|
| |
| bool | DL_I2C_receiveTargetDataCheck (I2C_Regs *i2c, uint8_t *buffer) |
| | Receive target data. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enablePower (I2C_Regs *i2c) |
| | Enables power on I2C module. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disablePower (I2C_Regs *i2c) |
| | Disables power on i2c module. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isPowerEnabled (I2C_Regs *i2c) |
| | Returns if power on i2c module. More...
|
| |
| __STATIC_INLINE void | DL_I2C_reset (I2C_Regs *i2c) |
| | Resets i2c peripheral. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isReset (I2C_Regs *i2c) |
| | Returns if i2c peripheral was reset. More...
|
| |
| __STATIC_INLINE void | DL_I2C_selectClockSource (I2C_Regs *i2c, DL_I2C_CLOCK clockSource) |
| | Set Clock Source. More...
|
| |
| __STATIC_INLINE void | DL_I2C_selectClockDivider (I2C_Regs *i2c, DL_I2C_CLOCK_DIVIDE clockDivider) |
| | Set Clock Divider. More...
|
| |
| __STATIC_INLINE DL_I2C_ANALOG_GLITCH_FILTER_WIDTH | DL_I2C_getAnalogGlitchFilterPulseWidth (I2C_Regs *i2c) |
| | Get Analog Glitch Suppression Pulse Width. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setAnalogGlitchFilterPulseWidth (I2C_Regs *i2c, DL_I2C_ANALOG_GLITCH_FILTER_WIDTH filterWidth) |
| | Set Analog Glitch Suppression Pulse Width. More...
|
| |
| __STATIC_INLINE DL_I2C_DIGITAL_GLITCH_FILTER_WIDTH | DL_I2C_getDigitalGlitchFilterPulseWidth (I2C_Regs *i2c) |
| | Get Digital Glitch Suppression Pulse Width. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setDigitalGlitchFilterPulseWidth (I2C_Regs *i2c, DL_I2C_DIGITAL_GLITCH_FILTER_WIDTH filterWidth) |
| | Set Digital Glitch Suppression Pulse Width. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableAnalogGlitchFilter (I2C_Regs *i2c) |
| | Disable Analog Glitch Suppression. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isAnalogGlitchFilterEnabled (I2C_Regs *i2c) |
| | Checks if analog glitch suppression is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableAnalogGlitchFilter (I2C_Regs *i2c) |
| | Enable Analog Glitch Suppression. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_DIRECTION | DL_I2C_getControllerDirection (I2C_Regs *i2c) |
| | Get direction of next controller operation. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setControllerDirection (I2C_Regs *i2c, DL_I2C_CONTROLLER_DIRECTION direction) |
| | Set direction of next controller operation. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetAddress (I2C_Regs *i2c) |
| | Get the address of the target being addressed when configured as an I2C controller. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetAddress (I2C_Regs *i2c, uint32_t targetAddress) |
| | Set the address of the target being addressed when configured as an I2C controller. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_ADDRESSING_MODE | DL_I2C_getControllerAddressingMode (I2C_Regs *i2c) |
| | Get controller addressing mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setControllerAddressingMode (I2C_Regs *i2c, DL_I2C_CONTROLLER_ADDRESSING_MODE mode) |
| | Set controller addressing mode between 7-bit and 10-bit mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerACKOverride (I2C_Regs *i2c) |
| | Disable controller ACK override. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerACKOverrideEnabled (I2C_Regs *i2c) |
| | Checks if controller ACK override is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerACKOverride (I2C_Regs *i2c) |
| | Enable controller ACK override. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerReadOnTXEmpty (I2C_Regs *i2c) |
| | Disable controller read on TX empty. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerReadOnTXEmptyEnabled (I2C_Regs *i2c) |
| | Checks if controller read on TX empty is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerReadOnTXEmpty (I2C_Regs *i2c) |
| | Enable controller read on TX empty. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getControllerPECCountValue (I2C_Regs *i2c) |
| | Get the SMBus/PMBus Packet Error Checking (PEC) count value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setControllerPECCountValue (I2C_Regs *i2c, uint32_t count) |
| | Set the SMBus/PMBus Packet Error Checking (PEC) count value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerPEC (I2C_Regs *i2c) |
| | Disable controller SMBus/PMBus Packet Error Checking (PEC) More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerPECEnabled (I2C_Regs *i2c) |
| | Checks if controller SMBus/PMBus Packet Error Checking (PEC) is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerPEC (I2C_Regs *i2c) |
| | Enable controller SMBus/PMBus Packet Error Checking (PEC) More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getControllerCurrentPECCount (I2C_Regs *i2c) |
| | Get the current SMBus/PMBus PEC byte count of the controller state machine. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_PEC_STATUS | DL_I2C_getControllerPECCheckedStatus (I2C_Regs *i2c) |
| | If controller SMBus/PMBus PEC was checked in last transaction. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_PEC_CHECK_ERROR | DL_I2C_getControllerPECCheckError (I2C_Regs *i2c) |
| | Get the status of the controller SMBus/PMBus PEC Check error. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerBurst (I2C_Regs *i2c) |
| | Disable I2C controller burst mode. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerBurstEnabled (I2C_Regs *i2c) |
| | Checks if I2C controller burst mode is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerBurst (I2C_Regs *i2c) |
| | Enable I2C controller burst mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableStartCondition (I2C_Regs *i2c) |
| | Disable I2C START generation. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isStartConditionEnabled (I2C_Regs *i2c) |
| | Checks if I2C START generation is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableStartCondition (I2C_Regs *i2c) |
| | Enable I2C START generation. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableStopCondition (I2C_Regs *i2c) |
| | Disable I2C STOP generation. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isStopConditionEnabled (I2C_Regs *i2c) |
| | Checks if I2C STOP generation is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableStopCondition (I2C_Regs *i2c) |
| | Enable I2C STOP generation. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerACK (I2C_Regs *i2c) |
| | Disable I2C controller data acknowledge (ACK or NACK) More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerACKEnabled (I2C_Regs *i2c) |
| | Checks if I2C controller data acknowledge (ACK or NACK) is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerACK (I2C_Regs *i2c) |
| | Enable I2C controller data acknowledge (ACK or NACK) More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTransactionLength (I2C_Regs *i2c) |
| | Get transaction length in bytes. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTransactionLength (I2C_Regs *i2c, uint32_t length) |
| | Set transaction length in bytes. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getControllerStatus (I2C_Regs *i2c) |
| | Get status of I2C bus controller for controller. More...
|
| |
| __STATIC_INLINE uint16_t | DL_I2C_getTransactionCount (I2C_Regs *i2c) |
| | Get transaction count in bytes. More...
|
| |
| __STATIC_INLINE uint8_t | DL_I2C_receiveControllerData (I2C_Regs *i2c) |
| | Get byte of data from I2C controller. More...
|
| |
| __STATIC_INLINE void | DL_I2C_transmitControllerData (I2C_Regs *i2c, uint8_t data) |
| | Set next byte to be transferred during the next transaction. More...
|
| |
| __STATIC_INLINE uint8_t | DL_I2C_getTimerPeriod (I2C_Regs *i2c) |
| | Get timer period This field is used in the equation to configure SCL_PERIOD: More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTimerPeriod (I2C_Regs *i2c, uint8_t period) |
| | Set timer period This field is used in the equation to configure SCL_PERIOD: More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableLoopbackMode (I2C_Regs *i2c) |
| | Disable loopback mode. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isLoopbackModeEnabled (I2C_Regs *i2c) |
| | Checks if loopback mode is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableLoopbackMode (I2C_Regs *i2c) |
| | Enable loopback mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableMultiControllerMode (I2C_Regs *i2c) |
| | Disable multicontroller mode. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isMultiControllerModeEnabled (I2C_Regs *i2c) |
| | Checks if multicontroller mode is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableMultiControllerMode (I2C_Regs *i2c) |
| | Enable multicontroller mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableController (I2C_Regs *i2c) |
| | Disable controller. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerEnabled (I2C_Regs *i2c) |
| | Checks if controller is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableController (I2C_Regs *i2c) |
| | Enable controller. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableControllerClockStretching (I2C_Regs *i2c) |
| | Disable controller clock stretching. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerClockStretchingEnabled (I2C_Regs *i2c) |
| | Checks if controller clock stretching is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableControllerClockStretching (I2C_Regs *i2c) |
| | Enable controller clock stretching. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_SCL | DL_I2C_getSCLStatus (I2C_Regs *i2c) |
| | Get SCL signal status. More...
|
| |
| __STATIC_INLINE DL_I2C_CONTROLLER_SDA | DL_I2C_getSDAStatus (I2C_Regs *i2c) |
| | Get SDA signal status. More...
|
| |
| __STATIC_INLINE DL_I2C_TX_FIFO_LEVEL | DL_I2C_getControllerTXFIFOThreshold (I2C_Regs *i2c) |
| | Get controller TX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setControllerTXFIFOThreshold (I2C_Regs *i2c, DL_I2C_TX_FIFO_LEVEL level) |
| | Set controller TX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_stopFlushControllerTXFIFO (I2C_Regs *i2c) |
| | Stop controller TX FIFO flush. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startFlushControllerTXFIFO (I2C_Regs *i2c) |
| | Start controller TX FIFO flush. More...
|
| |
| __STATIC_INLINE DL_I2C_RX_FIFO_LEVEL | DL_I2C_getControllerRXFIFOThreshold (I2C_Regs *i2c) |
| | Get controller RX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setControllerRXFIFOThreshold (I2C_Regs *i2c, DL_I2C_RX_FIFO_LEVEL level) |
| | Set controller RX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_stopFlushControllerRXFIFO (I2C_Regs *i2c) |
| | Stop controller RX FIFO flush. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startFlushControllerRXFIFO (I2C_Regs *i2c) |
| | Start controller RX FIFO flush. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getControllerRXFIFOCounter (I2C_Regs *i2c) |
| | Get number of bytes which can be read from RX FIFO. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getControllerTXFIFOCounter (I2C_Regs *i2c) |
| | Get number of bytes which can be put into TX FIFO. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerRXFIFOFlushActive (I2C_Regs *i2c) |
| | Checks if controller RX FIFO flush is active. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isControllerTXFIFOFlushActive (I2C_Regs *i2c) |
| | Checks if controller TX FIFO flush is active. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetOwnAddress (I2C_Regs *i2c, uint32_t addr) |
| | Set target own address. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetOwnAddress (I2C_Regs *i2c) |
| | Get target own address. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetOwnAddress (I2C_Regs *i2c) |
| | Enable target own address. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetOwnAddress (I2C_Regs *i2c) |
| | Disable target own address. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetOwnAddressEnabled (I2C_Regs *i2c) |
| | Checks if target own address is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetAddressingMode (I2C_Regs *i2c, DL_I2C_TARGET_ADDRESSING_MODE mode) |
| | Set target addressing mode. More...
|
| |
| __STATIC_INLINE DL_I2C_TARGET_ADDRESSING_MODE | DL_I2C_getTargetAddressingMode (I2C_Regs *i2c) |
| | Get target addressing mode. More...
|
| |
| __STATIC_INLINE uint32_t | I2C_getTargetOwnAddressAlternate (I2C_Regs *i2c) |
| | Get target own address alternate. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetOwnAddressAlternate (I2C_Regs *i2c, uint32_t addr) |
| | Set target own address alternate. More...
|
| |
| __STATIC_INLINE uint32_t | I2C_getTargetOwnAddressAlternateMask (I2C_Regs *i2c) |
| | Get target own address alternate mask. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetOwnAddressAlternateMask (I2C_Regs *i2c, uint32_t addressMask) |
| | Set target own address alternate mask. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetOwnAddressAlternate (I2C_Regs *i2c) |
| | Disable usage of target own address alternate. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetOwnAddressAlternateEnabled (I2C_Regs *i2c) |
| | Checks if target own address alternate is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetOwnAddressAlternate (I2C_Regs *i2c) |
| | Enable usage of target own address alternate. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetAddressMatch (I2C_Regs *i2c) |
| | Get the address for which address match happened. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetClockStretching (I2C_Regs *i2c) |
| | Disable target clock stretching. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetClockStretchingEnabled (I2C_Regs *i2c) |
| | Checks if target clock stretching is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetClockStretching (I2C_Regs *i2c) |
| | Enable target clock stretching. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetTXEmptyOnTXRequest (I2C_Regs *i2c) |
| | Disable target TX empty interrupt on transmit request. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXEmptyOnTXRequestEnabled (I2C_Regs *i2c) |
| | Checks if target TX empty interrupt on transmit request is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetTXEmptyOnTXRequest (I2C_Regs *i2c) |
| | Enable target TX empty interrupt on transmit request. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetTXTriggerInTXMode (I2C_Regs *i2c) |
| | Disable target TX trigger in TX mode. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXTriggerInTXModeEnabled (I2C_Regs *i2c) |
| | Checks if target TX trigger in TX mode is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetTXTriggerInTXMode (I2C_Regs *i2c) |
| | Enable TX trigger when target is in TX mode. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetTXWaitWhenTXFIFOStale (I2C_Regs *i2c) |
| | Disable target TX transfer waits when stale data in TX FIFO. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXWaitWhenTXFIFOStaleEnabled (I2C_Regs *i2c) |
| | Checks if target TX transfer waits when stale data in TX FIFO is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetTXWaitWhenTXFIFOStale (I2C_Regs *i2c) |
| | Enable target TX transfer waits when stale data in TX FIFO. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetRXFullOnRXRequest (I2C_Regs *i2c) |
| | Disable target RX full interrupt on receive request. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetRXFullOnRXRequestEnabled (I2C_Regs *i2c) |
| | Checks if target RX full interrupt on receive request is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetRXFullOnRXRequest (I2C_Regs *i2c) |
| | Enable target RX full interrupt on receive request. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableDefaultHostAddress (I2C_Regs *i2c) |
| | Disable SMBus/PMBus default host address of 000 1000b. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isDefaultHostAddressEnabled (I2C_Regs *i2c) |
| | Checks if SMBus/PMBus default host address of 000 1000b is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableDefaultHostAddress (I2C_Regs *i2c) |
| | Enable SMBus/PMBus default host address of 000 1000b. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableAlertResponseAddress (I2C_Regs *i2c) |
| | Disable SMBus/PMBus Alert response address (ARA) of 000 1100b. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isAlertResponseAddressEnabled (I2C_Regs *i2c) |
| | Checks if SMBus/PMBus Alert response address (ARA) of 000 1100b is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableAlertResponseAddress (I2C_Regs *i2c) |
| | Enable SMBus/PMBus Alert response address (ARA) of 000 1100b. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableDefaultDeviceAddress (I2C_Regs *i2c) |
| | Disable SMBus/PMBus default device address of 110 0001b. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isDefaultDeviceAddressEnabled (I2C_Regs *i2c) |
| | Checks SMBus/PMBus default device address of 110 0001b is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableDefaultDeviceAddress (I2C_Regs *i2c) |
| | Enable SMBus/PMBus default device address of 110 0001b. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetWakeup (I2C_Regs *i2c) |
| | Disable target wakeup. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetWakeupEnabled (I2C_Regs *i2c) |
| | Checks if target wakeup is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetWakeup (I2C_Regs *i2c) |
| | Enable target wakeup. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTarget (I2C_Regs *i2c) |
| | Disable target functionality. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetEnabled (I2C_Regs *i2c) |
| | Checks if target functionality is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTarget (I2C_Regs *i2c) |
| | Enable usage of target functionality. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableGeneralCall (I2C_Regs *i2c) |
| | Disable general call address of 000 0000b. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isGeneralCallEnabled (I2C_Regs *i2c) |
| | Checks if general call address of 000 0000b is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableGeneralCall (I2C_Regs *i2c) |
| | Enable usage of general call address of 000 0000b. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetStatus (I2C_Regs *i2c) |
| | Get status of I2C bus controller for target. More...
|
| |
| __STATIC_INLINE uint8_t | DL_I2C_receiveTargetData (I2C_Regs *i2c) |
| | Get byte of data from I2C target. More...
|
| |
| __STATIC_INLINE void | DL_I2C_transmitTargetData (I2C_Regs *i2c, uint8_t data) |
| | Set next byte to be transferred during the next transaction. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetACKOverride (I2C_Regs *i2c) |
| | Disable target ACK override. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetACKOverrideEnabled (I2C_Regs *i2c) |
| | Checks if target ACK override is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetACKOverride (I2C_Regs *i2c) |
| | Enable target ACK override. More...
|
| |
| __STATIC_INLINE DL_I2C_TARGET_RESPONSE_OVERRIDE_VALUE | DL_I2C_getTargetACKOverrideValue (I2C_Regs *i2c) |
| | Get target acknowledge override value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetACKOverrideValue (I2C_Regs *i2c, DL_I2C_TARGET_RESPONSE_OVERRIDE_VALUE value) |
| | Set target acknowledge override value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableACKOverrideOnStart (I2C_Regs *i2c) |
| | Disable target ACK override on Start Condition. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isACKOverrideOnStartEnabled (I2C_Regs *i2c) |
| | Checks if target ACK override on Start condition is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableACKOverrideOnStart (I2C_Regs *i2c) |
| | Enable target ACK override on Start condition. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableACKOverrideOnPECNext (I2C_Regs *i2c) |
| | Disable target ACK override when SMBus/PMBus PEC is next byte. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isACKOverrideOnPECNextEnabled (I2C_Regs *i2c) |
| | Checks if target ACK override when SMBus/PMBus PEC is next byte is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableACKOverrideOnPECNext (I2C_Regs *i2c) |
| | Enable target ACK override when SMBus/PMBus PEC is next byte. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableACKOverrideOnPECDone (I2C_Regs *i2c) |
| | Disable target ACK override when SMBus/PMBus PEC is next byte. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isACKOverrideOnPECDoneEnabled (I2C_Regs *i2c) |
| | Checks if target ACK override when SMBus/PMBus PEC is next byte is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableACKOverrideOnPECDone (I2C_Regs *i2c) |
| | Enable target ACK override when SMBus/PMBus PEC is done. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetPECCountValue (I2C_Regs *i2c) |
| | Get the target SMBus/PMBus Packet Error Checking (PEC) count value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetPECCountValue (I2C_Regs *i2c, uint32_t count) |
| | Set the target SMBus/PMBus Packet Error Checking (PEC) count value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTargetPEC (I2C_Regs *i2c) |
| | Disable target SMBus/PMBus Packet Error Checking (PEC) More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetPECEnabled (I2C_Regs *i2c) |
| | Checks if target SMBus/PMBus Packet Error Checking (PEC) is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTargetPEC (I2C_Regs *i2c) |
| | Enable target SMBus/PMBus Packet Error Checking (PEC) More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetCurrentPECCount (I2C_Regs *i2c) |
| | Get the current SMBus/PMBus PEC byte count of the Target state machine. More...
|
| |
| __STATIC_INLINE DL_I2C_TARGET_PEC_STATUS | DL_I2C_getTargetPECCheckedStatus (I2C_Regs *i2c) |
| | Get status if SMBus/PMBus target PEC was checked in last transaction. More...
|
| |
| __STATIC_INLINE DL_I2C_TARGET_PEC_CHECK_ERROR | DL_I2C_getTargetPECCheckError (I2C_Regs *i2c) |
| | Get status if SMBus/PMBus target PEC had an error. More...
|
| |
| __STATIC_INLINE DL_I2C_TX_FIFO_LEVEL | DL_I2C_getTargetTXFIFOThreshold (I2C_Regs *i2c) |
| | Get target TX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetTXFIFOThreshold (I2C_Regs *i2c, DL_I2C_TX_FIFO_LEVEL level) |
| | Set target TX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_stopFlushTargetTXFIFO (I2C_Regs *i2c) |
| | Stop target TX FIFO flush. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startFlushTargetTXFIFO (I2C_Regs *i2c) |
| | Start target TX FIFO flush. More...
|
| |
| __STATIC_INLINE void | DL_I2C_stopFlushTargetRXFIFO (I2C_Regs *i2c) |
| | Stop target RX FIFO flush. More...
|
| |
| __STATIC_INLINE void | DL_I2C_startFlushTargetRXFIFO (I2C_Regs *i2c) |
| | Start target RX FIFO flush. More...
|
| |
| __STATIC_INLINE DL_I2C_RX_FIFO_LEVEL | DL_I2C_getTargetRXFIFOThreshold (I2C_Regs *i2c) |
| | Get target RX FIFO threshold level. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTargetRXFIFOThreshold (I2C_Regs *i2c, DL_I2C_RX_FIFO_LEVEL level) |
| | Set target RX FIFO threshold level. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetRXFIFOCounter (I2C_Regs *i2c) |
| | Get number of bytes which can be read from RX FIFO. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTargetTXFIFOCounter (I2C_Regs *i2c) |
| | Get number of bytes which can be put into TX FIFO. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetRXFIFOFlushActive (I2C_Regs *i2c) |
| | Checks if target RX FIFO flush is active. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTargetTXFIFOFlushActive (I2C_Regs *i2c) |
| | Checks if target TX FIFO flush is active. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableInterrupt (I2C_Regs *i2c, uint32_t interruptMask) |
| | Enable I2C interrupts. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableInterrupt (I2C_Regs *i2c, uint32_t interruptMask) |
| | Disable I2C interrupts. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getEnabledInterrupts (I2C_Regs *i2c, uint32_t interruptMask) |
| | Check which I2C interrupts are enabled. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getEnabledInterruptStatus (I2C_Regs *i2c, uint32_t interruptMask) |
| | Check interrupt flag of enabled I2C interrupts. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getRawInterruptStatus (I2C_Regs *i2c, uint32_t interruptMask) |
| | Check interrupt flag of any I2C interrupt. More...
|
| |
| __STATIC_INLINE DL_I2C_IIDX | DL_I2C_getPendingInterrupt (I2C_Regs *i2c) |
| | Get highest priority pending I2C interrupt. More...
|
| |
| __STATIC_INLINE void | DL_I2C_clearInterruptStatus (I2C_Regs *i2c, uint32_t interruptMask) |
| | Clear pending I2C interrupts. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableDMAEvent (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interrupt) |
| | Enables I2C interrupt for triggering DMA events. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableDMAEvent (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interrupt) |
| | Disables I2C interrupt from triggering DMA events. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getEnabledDMAEvents (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interruptMask) |
| | Check which I2C interrupt for DMA receive events is enabled. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getEnabledDMAEventStatus (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interruptMask) |
| | Check interrupt flag of enabled I2C interrupt for DMA event. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getRawDMAEventStatus (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interruptMask) |
| | Check interrupt flag of any I2C interrupt for DMA event. More...
|
| |
| __STATIC_INLINE DL_I2C_DMA_IIDX | DL_I2C_getPendingDMAEvent (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index) |
| | Get highest priority pending I2C interrupt for DMA event. More...
|
| |
| __STATIC_INLINE void | DL_I2C_clearDMAEvent (I2C_Regs *i2c, DL_I2C_EVENT_ROUTE index, uint32_t interrupt) |
| | Clear pending SPI interrupts for DMA events. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableGlitchFilterChaining (I2C_Regs *i2c) |
| | Disable analog and digital glitch filter chaining. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isGlitchFilterChainingEnabled (I2C_Regs *i2c) |
| | Checks if analog and digital glitch filter chaining is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableGlitchFilterChaining (I2C_Regs *i2c) |
| | Enable analog and digitial glitch filter chaining. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTimeoutACount (I2C_Regs *i2c) |
| | Get the Timeout Counter A value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTimeoutACount (I2C_Regs *i2c, uint32_t count) |
| | Set the Timeout Counter A value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTimeoutA (I2C_Regs *i2c) |
| | Disable Timeout Counter A. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTimeoutAEnabled (I2C_Regs *i2c) |
| | Checks if Timeout Counter A is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTimeoutA (I2C_Regs *i2c) |
| | Enable Timeout Counter A. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getCurrentTimeoutACounter (I2C_Regs *i2c) |
| | Get the current Timer Counter A value. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getTimeoutBCount (I2C_Regs *i2c) |
| | Get the Timeout Counter B value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_setTimeoutBCount (I2C_Regs *i2c, uint32_t count) |
| | Set the Timeout Counter B value. More...
|
| |
| __STATIC_INLINE void | DL_I2C_disableTimeoutB (I2C_Regs *i2c) |
| | Disable Timeout Counter B. More...
|
| |
| __STATIC_INLINE bool | DL_I2C_isTimeoutBEnabled (I2C_Regs *i2c) |
| | Checks if Timeout Counter B is enabled. More...
|
| |
| __STATIC_INLINE void | DL_I2C_enableTimeoutB (I2C_Regs *i2c) |
| | Enable Timeout Counter B. More...
|
| |
| __STATIC_INLINE uint32_t | DL_I2C_getCurrentTimeoutBCounter (I2C_Regs *i2c) |
| | Get the current Timer Counter B value. More...
|
| |