MSPM0L11XX_L13XX TI-Driver Library
2.01.00.03
|
I2CTarget driver implementation for a MSPM0 device I2C target.
#include <stdint.h>
#include <stdbool.h>
#include <ti/driverlib/dl_i2c.h>
#include <ti/drivers/I2CTarget.h>
Go to the source code of this file.
Data Structures | |
struct | I2CTargetMSPM0_HWAttrs |
I2CTargetMSPM0 Hardware attributes. More... | |
struct | I2CTargetMSPM0_Object |
I2CTargetMSPM0 Object. More... | |
Functions | |
static bool | I2CBaseValid (I2C_Regs *i2c) |
Checks an I2C base address. This function determines if a I2C port base address is valid. More... | |