![]() |
![]() |
MSPM0G1X0X_G3X0X TI-Driver Library
2.00.01.00
|
SPI driver implementation for MSPM0 SPI controller using the DMA controller.
#include <stdint.h>
#include <ti/drivers/SPI.h>
#include <ti/drivers/dma/DMAMSPM0.h>
#include <ti/drivers/gpio/GPIOMSPM0.h>
#include <ti/driverlib/dl_spi.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
Go to the source code of this file.
Data Structures | |
struct | SPIMSPM0_HWAttrs |
SPIMSPM0 Hardware attributes. More... | |
struct | SPIMSPM0_Object |
SPIMSPM0 Object. More... | |
Macros | |
#define | SPIMSPM0_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) |
Command used by SPI_control() to enable partial return. More... | |
#define | SPIMSPM0_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) |
Command used by SPI_control() to disable partial return. More... | |
#define | SPIMSPM0_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) |
Command used by SPI_control() to re-configure chip select pin. More... | |
#define | SPIMSPM0_CMD_CLEAR_CSN_PIN (SPI_CMD_RESERVED + 3) |
Command used by SPI_control() to clear the chip select pin. More... | |
#define | SPIMSPM0_CMD_SET_MANUAL (SPI_CMD_RESERVED + 4) |
Command used by SPI_control() to enable manual start mode. More... | |
#define | SPIMSPM0_CMD_CLR_MANUAL (SPI_CMD_RESERVED + 5) |
Command used by SPI_control() to disable manual start mode. More... | |
#define | SPIMSPM0_CMD_MANUAL_START (SPI_CMD_RESERVED + 6) |
Command used by SPI_control() to enable manual start mode. More... | |
#define | SPIMSPM0_CMD_SET_SAMPLE_DELAY (SPI_CMD_RESERVED + 7) |
Command used by SPI_control() to set the sample delay in controller mode. More... | |
Enumerations | |
enum | SPIMSPM0_FrameSize { SPIMSPM0_8bit = 0, SPIMSPM0_16bit = 1 } |
SPIMSPM0 data frame size is used to determine how to configure the DMA data transfers. This field is to be only used internally. More... | |
enum | SPIMSPM0_ReturnPartial { SPIMSPM0_retPartDisabled = 0, SPIMSPM0_retPartEnabledIntNotSet = 1, SPIMSPM0_retPartEnabledIntSet = 2 } |
SPIMSPM0 return partial field indicates the status of the return partial mode and the associated pin interrupt. This field is for internal use only. More... | |
Variables | |
const SPI_FxnTable | SPIMSPM0_fxnTable |
SPI function table pointer. | |