MSPM0L11XX_L13XX TI-Driver Library
2.00.00.03
|
I2C Driver.
Go to the source code of this file.
Data Structures | |
struct | I2C_Transaction |
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout(). More... | |
struct | I2C_Params |
I2C parameters used with I2C_open(). More... | |
struct | I2C_Config_ |
I2C driver's configuration structure. More... | |
Macros | |
#define | I2C_STATUS_QUEUED (1) |
I2C transaction is queued but has not started. | |
#define | I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API. | |
#define | I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API. | |
#define | I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes. | |
#define | I2C_STATUS_TIMEOUT (-3) |
I2C operation timed-out. | |
#define | I2C_STATUS_CLOCK_TIMEOUT (-4) |
I2C serial clock line timeout. | |
#define | I2C_STATUS_ADDR_NACK (-5) |
I2C target address not acknowledged. | |
#define | I2C_STATUS_DATA_NACK (-6) |
I2C data byte not acknowledged. | |
#define | I2C_STATUS_ARB_LOST (-7) |
I2C multi-controller arbitration lost. | |
#define | I2C_STATUS_INCOMPLETE (-8) |
I2C transaction is in progress or returned without completing. | |
#define | I2C_STATUS_BUS_BUSY (-9) |
I2C bus already in use by another controller. The I2C transaction. was therefore unable to start. | |
#define | I2C_STATUS_CANCEL (-10) |
I2C transaction canceled by I2C_cancel(). | |
#define | I2C_STATUS_INVALID_TRANS (-11) |
I2C transaction is invalid. More... | |
#define | I2C_WAIT_FOREVER (~(0U)) |
Wait forever define used to specify timeouts. | |
Typedefs | |
typedef struct I2C_Config_ * | I2C_Handle |
A handle that is returned from an I2C_open() call. | |
typedef void(* | I2C_CallbackFxn) (I2C_Handle handle, I2C_Transaction *transaction, bool transferStatus) |
The definition of a callback function. More... | |
typedef struct I2C_Config_ | I2C_Config |
I2C driver's configuration structure. More... | |
Enumerations | |
enum | I2C_TransferMode { I2C_MODE_BLOCKING, I2C_MODE_CALLBACK } |
Return behavior of I2C_Transfer() specified in the I2C_Params. More... | |
enum | I2C_BitRate { I2C_100kHz = 0, I2C_400kHz = 1, I2C_1000kHz = 2 } |
Bit rate for an I2C driver instance specified in the I2C_Params. More... | |
Functions | |
void | I2C_cancel (I2C_Handle handle) |
Cancels all I2C transfers. More... | |
void | I2C_close (I2C_Handle handle) |
Function to close an I2C driver instance. More... | |
int_fast16_t | I2C_control (I2C_Handle handle, uint_fast16_t cmd, void *controlArg) |
Function performs implementation specific features on a driver instance. More... | |
void | I2C_init (void) |
Function to initialize the I2C driver. More... | |
I2C_Handle | I2C_open (uint_least8_t index, I2C_Params *params) |
Open an I2C driver instance. More... | |
void | I2C_Params_init (I2C_Params *params) |
Initialize an I2C_Params structure to its default values. More... | |
int_fast16_t | I2C_setClockTimeout (I2C_Handle handle, uint32_t timeout) |
Set the I2C SCL clock timeout. More... | |
bool | I2C_transfer (I2C_Handle handle, I2C_Transaction *transaction) |
Perform an I2C transaction with an I2C target peripheral. More... | |
int_fast16_t | I2C_transferTimeout (I2C_Handle handle, I2C_Transaction *transaction, uint32_t timeout) |
Perform an I2C transaction with an I2C target peripheral. More... | |
Variables | |
const I2C_Config | I2C_config [] |
Instance of I2C driver's configuration structure. | |
const uint_least8_t | I2C_count |
Count of I2C instance. | |