![]() |
![]() |
MSPM0L11XX_L13XX TI-Driver Library
1.20.01.06
|
GPIO driver implementation for MSPM0 devices.
#include <ti/drivers/GPIO.h>
Go to the source code of this file.
Macros | |
#define | GPIO_CFG_DRVSTR_MED_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
Medium drive strength is not available on MSPM0 devices. | |
#define | GPIO_CFG_INT_LOW_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
Low value interrupts are not available on MSPM0 devices. | |
#define | GPIO_CFG_INT_HIGH_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
High value interrupts are not available on MSPM0 devices. | |