49 #ifndef ti_drivers_I2CSupport__include 50 #define ti_drivers_I2CSupport__include 56 #include <ti/driverlib/dl_i2c.h> void I2CSupport_powerRelConstraint(void)
Function to release power constraint.
void I2CSupport_powerSetConstraint(void)
Function to set power constraint.
I2C driver's configuration structure.
Definition: I2C.h:688
int_fast16_t I2CSupport_primeTransfer(I2C_Handle handle, I2C_Transaction *transaction)
Function to initialize transfers.
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout().
Definition: I2C.h:423
void I2CSupport_controllerFinish(I2C_HWAttrs const *hwAttrs)
Function to send a finish command to the controller module.