![]() |
![]() |
MSPM0L11XX_L13XX TI-Driver Library
1.20.01.06
|
DMA driver implementation for MSPM0.
#include <stdbool.h>
#include <stdint.h>
#include <ti/driverlib/dl_dma.h>
#include <ti/drivers/dpl/HwiP.h>
Go to the source code of this file.
Data Structures | |
struct | DMAMSPM0_HWAttrs |
DMAMSPM0 Hardware attributes. More... | |
struct | DMAMSPM0_Transfer |
DMAMSPM0 channel based Transfer configuration. More... | |
struct | DMAMSPM0_Object |
DMAMSPM0 object. More... | |
struct | DMAMSPM0_Cfg |
DMAMSPM0 Global configuration. More... | |
Macros | |
#define | NUM_DMA_CHANNELS (DMA_SYS_N_DMA_CHANNEL) |
Number of DMA channels supported by Device. The same can be used to define the number of interrupts. More... | |
Typedefs | |
typedef void(* | DMAMSPM0_IsrFxn) (uintptr_t arg) |
DMA error function pointers. | |
typedef DMAMSPM0_Cfg * | DMAMSPM0_Handle |
A handle that is returned from a DMAMSPM0_open() call. | |
Functions | |
void | DMAMSPM0_close (DMA_Regs *handle, uint8_t channelNum) |
Function to close the DMA channel. More... | |
bool | DMAMSPM0_init (void) |
Function to initialize the MSPM0 DMA driver. More... | |
DMAMSPM0_Handle | DMAMSPM0_open (uint_least8_t index, uint8_t channelNum) |
Function to initialize the MSPM0 DMA peripheral and corresponding interrupt. More... | |
bool | DMAMSPM0_setupTransfer (DMAMSPM0_Transfer *transfer, DL_DMA_Config *DMACfg) |
Function to set up a DMA channel for data transfer. More... | |
DMAMSPM0_Handle | DMA_Init (DMAMSPM0_Transfer *dmaParams, DL_DMA_Config *DMACfg, uint8_t noOfChs) |
One Function that initialize DMA by calling all needed functions in sequence. User may call this function to initialize DMA without calling other needed functions separately. More... | |
void | DMAMSPM0_disableChannel (DMAMSPM0_Handle handle, uint8_t dmaChannel) |
This function will disable the channel and related flags. More... | |
uint16_t | DMAMSPM0_getCurrTransferSize (uint8_t dmaChannel) |
This function will return the DMA transfer size in bytes for given channel. More... | |
void | DMA_Params_init (DMAMSPM0_Transfer *params) |
This function will initialize the default params. More... | |
void | DMAMSPM0_copyDMAParams (DMAMSPM0_Transfer *dmaParams, DL_DMA_Config *dmaConfig) |
This function will extract parameters from DMA Config struct to DMA Transfer struct. More... | |
Variables | |
const DMAMSPM0_Cfg | DMAMSPM0_Config [] |
Instance of a DMA Config structure. | |
const uint_least8_t | DMA_Count |
Number of DMA channels. | |