SensorlessFOCMotorControlLibrary  1.0
Data Structures | Macros | Functions
cirlimit.h File Reference

Detailed Description

Sensorless FOC Motor Control Library Circle limitation Module.


Overview

APIs for circle limitation


#include <ti/devices/msp/msp.h>
#include "ti/iqmath/include/IQmathLib.h"
Include dependency graph for cirlimit.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  CIRLMT_Instance
 Define circle limit structure. More...
 

Macros

#define CIRLMT_DEFAULTS   { 0,0,0,0,0,_IQ(0.866) }
 Default values for the circle limit instance.
 

Functions

__STATIC_INLINE void CIRLIMIT_run (CIRLMT_Instance *handle)
 Limits the Vq and Vd in pu within the circle of set radius. More...
 
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale