MCUSW
Loading...
Searching...
No Matches
Fls User Guide

Table of Contents

Introduction

This document details AUTOSAR BSW Flash module implementation

  • Supported AUTOSAR Release : 4.3.1
  • Supported Configuration Variants : Pre-Compile, Post-Build
  • Vendor ID : FLS_VENDOR_ID (44)
  • Module ID : FLS_MODULE_ID (92)

The Flash Driver provides services for reading, writing, erasing flash memory and Execute-in-Place (XIP) mode for external Flash Device.
The driver supports the following devices:

Device Flash Protocol Boards supported
S28HS512T XSPI AM62X_SK, AM62DX, AM62PX, AM275X

The main tasks of the FLS driver are:

  • Perform storage mode applications:
    • Read from flash.
    • Write to flash.
    • Erase Flash.
    • Compare and Blank Check flash memory location.

Fls Driver Architecture/Design

Please refer the Flash design, which is included as part of CSP.


Functional Description

The Fls Module uses internal OSPI peripheral as the serial bus to transfer data to and from the attached flash device.

Programming of clock source for the flash, is beyond the scope of this document. The Clock programming is taken care by the test application.

1 Fls instance is supported by this driver implementation.

In case of AM275X only 1 OSPI instance is supported at a given point of time.

Back To Top


Configuration

The Fls Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Fls_Cfg.h to be present as (Configuration Folder Structure). Please refer (Build) to specify path to generated configuration. The associated Fls configuration generated files Fls_Cfg.c, and Fls_PBcfg.c to be present as shown (Configuration Folder Structure)

Board Layer for Flash Driver (FLS)

Overview

The Flash (FLS) driver in the MCAL layer interacts with various types of NOR flash memory devices. To maintain modularity and enhance portability across different hardware platforms, the board layer has been introduced.

The board layer resides separately at: mcusw/mcal_drv/mcal/board

Purpose of Board Layer

The board layer for the FLS driver contains hardware-specific implementations, configurations, and command sequences necessary to interact directly with flash memory devices. By isolating board-specific details from the generic FLS driver logic, we achieve:

  • Hardware Abstraction: Generic flash driver code remains hardware-independent, promoting reusability across different boards.
  • Ease of Maintenance: Board-specific changes and adaptations can be performed without affecting the core logic of the flash driver.

Files in Board Layer

The board layer consists of the following important files for flash functionality:

File Name Description
Fls_Brd_Nor_Ospi.c Board-specific implementation for NOR flash using OSPI protocol
Fls_Brd_Nor_Qspi.c NOR flash interactions via QSPI interface
Fls_Brd_Nor_Xspi.c XSPI-based flash access and command sequencing
Fls_Brd_Nor.c SPI command patterns specific to flash operations
nor_spi_patterns.c, nor_spi_phy_tune.c PHY-level tuning and adjustments for stable flash interactions

Responsibilities

The board layer takes care of:

  • Handling protocol-specific sequences (SPI, OSPI, QSPI, XSPI).
  • Performing necessary hardware tuning and PHY adjustments.
  • Abstracting board-dependent initialization and timing parameters.

Custom Flash Device Support (Important Note)

When adding a custom flash device, users may need to modify or extend the board layer code according to the specifications provided in the flash datasheet. This could involve:

  • Adding new flash commands.
  • Adjusting existing command sequences or methods of sending commands.
  • Handling unique flash-specific requirements.

Note: The board layer implementation is not qualified for functional safety.

Flash Protocols Supported

The current driver supports the following protocols for custom flash devices:

  1. OSPI (Octal SPI)
  2. XSPI (Extended SPI)
  3. QSPI (Quad SPI)

Ensure the correct protocol is selected based on the flash device’s capabilities.

Adding and Configuring Custom Flash Support

The FlsMemConfiguration section of the EB Tresos configurator allows the user to define custom flash devices. Key fields and their descriptions for custom flash configuration include:

  1. FlsDeviceType: Specifies the type of flash (e.g., NOR, NAND).
    • Example: FLS_NOR
  2. FlsProtocolMode: Specifies the protocol mode (e.g., OSPI, QSPI, XSPI).
    • Example: FLS_OSPI
    • Note: If the flash device used is S28HS512T(Cypress Flash), user need to select XSPI as protocol mode.
  3. FlsNORBlockSize: Defines the block size of the flash memory in bytes.
    • Example: 67108864 (64KB)
  4. FlsNORUniformSectorSize: Defines the uniform sector size in bytes. This field is only applicable for NOR flash devices with a uniform sector structure, where all sectors have the same size.
    • Example: 4096 (4KB)
  5. FlsNORHybridSectorSize: Defines the size of hybrid sectors if applicable. Some flash devices may have a mixture of large and small sectors.
    • Example: 4096 (4KB) for hybrid sectors.
    • Note: If the flash device does not have hybrid sectors, set this field to FlsNORUniformSectorSize. It will default to FlsNORUniformSectorSize which represents the regular sector size.
  6. FlsNORSize: Total size of the NOR flash in bytes.
    • Example: 0x4000000 (64MB)
  7. FlsNORPageSize: Defines the page size for writes in bytes.
    • Example: 0x100 (256B)
  8. FlsNORErasedData: Specifies the erased data value, typically 0xFF.
  9. FlsNORCmdBulkErase: Defines the command for bulk erase.
    • Example: 0xC7 for supported devices, 0U if unsupported.
  10. FlsNORCmdWrReg: Command to write to the flash configuration register.
    • Example: 0x01 for supported devices, 0U if unsupported.

In addition to the above, other fields are also present in the configuration, such as commands for read, write, and specific flash operations, which are similarly defined for supported and unsupported devices. Above is the description of some key fields.

Ensure all relevant commands are defined according to the flash device’s datasheet.

FLS Sector List

This section explains the purpose and structure of the sectorList[] configuration used in the Flash (FLS) Driver module, following AUTOSAR standards. This configuration is typically set up in EB Tresos and consumed by the FLS driver during runtime to manage flash memory operations.

The sectorList[] is an array of Fls_SectorType structures. Each element describes a block of flash memory with a common configuration, allowing the driver to correctly interpret fl layout and perform operations like read, write, and erase.

Structure Definition
typedef struct {
uint32 sectorStartaddress;
uint32 sectorSize;
uint32 sectorPageSize;
uint32 numberOfSectors;
FLS Module Flashable Sectors and pages.
Definition Fls.h:304
Description of Fields:
Field Name Type Description
sectorStartaddress uint32 Start address (in flash address space) of the first sector in this configuration block. It must be aligned to the corresponding sectorSize.
sectorSize uint32 Size (in bytes) of one sector in this configuration block. It may vary between configurations in case of hybrid sector layout.
sectorPageSize uint32 Page size (in bytes) of the sector. This is the granularity used for programming (writing) operations. This is typically constant for a given flash device.
numberOfSectors uint32 Number of contiguous sectors with identical configuration starting at sectorStartaddress.
EB Tresos Configuration

In EB Tresos, users should:

  1. Navigate to the FLS module configuration.
  2. Under Sector Configuration, define one or more FlsSectorList entries.
  3. For each entry, specify:
    • Start Address
    • Sector Size
    • Page Size
    • Number of Sectors
  4. Ensure configurations are non-overlapping and aligned.

‍Tip: Uniform sectors can be defined with one entry. Hybrid sector layouts (e.g., small boot sectors + large data sectors) require multiple entries.

How It Is Used in Driver

During runtime, the FLS driver uses sectorList[] to:

  • Map addresses to their corresponding sector configurations
  • Validate write/erase boundaries
  • Align operations to page/sector boundaries
  • Optimize performance by avoiding repetitive calculations

The driver internally stores sectorList[] in Fls_DrvObj.sectorList[] and determines the active configuration using Fls_DetermineSectorCfgIndex().


Example
sectorList[0] = {
.sectorStartaddress = 0x67100000U,
.sectorSize = 0x00040000U, /* 256 KB */
.sectorPageSize = 0x00001000U, /* 4 KB */
.numberOfSectors = 4U
};
sectorList[1] = {
.sectorStartaddress = 0x67200000U,
.sectorSize = 0x00020000U, /* 128 KB */
.sectorPageSize = 0x00001000U,
.numberOfSectors = 8U
};

Notes
  • Flash addresses must be within valid memory map of the target SoC.
  • This configuration directly impacts validation and boundary checks within the FLS driver.

The image below illustrates the Custom Flash Configuration in the EB Tresos tool, where the user can define parameters such as the NOR device type, protocol mode, sector sizes, and various command configurations. These fields allow seamless integration and customization of external flash devices by configuring the appropriate values for each field.


Flash Configuration Header Files

The driver uses two primary configuration files:

  • Fls_Cfg.h: Contains the general flash configuration parameters.

Above file is generated based on the configuration fields set in the configurator. Ensure that file is included correctly in the build path to avoid errors.

Handling Different Flash Configurations

Sector Size Configuration In the FLS driver configuration, two key fields help in defining the size of sectors in the flash memory:

  • NOR_UNIFORM_SECTOR_SIZE: This field represents the size of the sectors when the flash uses a regular or uniform sector size throughout the memory. If the flash device has consistent sector sizes across the entire memory, this parameter is used to define the sector size.

    Example:

    #define NOR_UNIFORM_SECTOR_SIZE 64KB

In such cases, the flash memory has uniform sectors of 64KB, and this value will be used for erasing, writing, and reading operations. The system will rely on this parameter alone to manage sector-related operations.

  • NOR_SECTOR_SIZE: This field is used if the flash memory supports hybrid sectors, where a combination of smaller and larger sectors exists in the memory. This is common in flashes that have some portions (e.g., near the beginning or end) that use smaller 4KB sectors for more granular control, while the rest of the flash uses larger uniform sectors. If hybrid sectoring is supported, the NOR_SECTOR_SIZE field must be used alongside the uniform sector size to represent the different sector sizes.

Example

#define NOR_SECTOR_SIZE 4KB

Protocol Configuration

Current FLS driver uses OSPI, XSPI, and QSPI protocol modes and supports the three NOR Flash devices for all devices (MT35XU512ABA1G12, S28HS512T, and MT25QU512ABB).

If variation to the supported features are needed, user will need to take care to modify the driver to accommodate changes.

  1. Configuring other flash protocols
    • All protocols should be able to use existent OSPI files: Fls_Ospi.c and Fls_Ospi.h.
    • The board config files (Fls_Brd_Nor.c) will need slight modification to ensure that Flash Device is configured correctly when using other protocols.
    • Then Fls_Brd_Nor_<new protocol>.c file need to be added to support functions specific to that new flash protocol.
  2. Integrating new Flash Device
    • Configure plugin with required flash memory configuration for new flash device such as device name, device type, protocol mode. This can be done based on the flash device specification.
    • All flash device configured will be generated as an array of structures with all the flash specific commands. User can add multiple flash devices and need to specify the flash specific details as mentioned in the configuration section and generate the file Fls_Cfg.c.
    • Note: Multi-flash support has been added in which user can add multiple flash devices during configuration. The configured Flash devices will be generated as an array of structures in Fls_Cfg.c or Fls_PBcfg.c. Since a single flash device can be used in runtime, driver will detect the flash used during the Fls_init and use that flash configured in the driver. Although detecting the flash device used during the runtime is taken care in the driver, the user needs to ensure the flash commands are configured properly during the configuration.
    • Next, the board configuration files (Fls_Brd_Nor.c, etc.) will need to be modified to work with the new flash device. The APIs in the board configuration files are used to set the flash device settings. They should be carefully modified to ensure that correct commands are being written on the flash device. This can be done based on the flash device specification.
  • Note: Writing incorrect commands can break the flash device and make is obsolete. Proper care should be taken to ensure integration had been done correctly.

As the Fls driver supports different flash protocols, and the configuration differs based on the selected protocol:

  1. FLS_XSPI:
    • The NOR_BLOCK_SIZE parameter is used when configuring devices with the XSPI protocol. The block size value defines the erase unit size for the flash memory.
    • In this mode, the driver utilizes the block size for operations such as erasing and chunking write jobs.
  2. FLS_OSPI / FLS_QSPI
    • For devices using OSPI or QSPI protocols, the NOR_SECTOR_SIZE parameter is utilized. This configuration reflects the sector size used for read, write, and erase operations specific to these protocols.
    • This differentiation allows the driver to handle sector-based memory operations efficiently in these protocols.

(When configuring flash devices using the FlsMemConfiguration field, ensure that the correct protocol is set so that the driver can apply the appropriate block or sector sizes based on the selected flash type.)

  • Note: Please note that the PHY Tune algorithm is not expected to work with other flash devices.

Handling Flash Operations

The driver supports the following operations for custom flash devices:

  1. Erase
    • Erase operations must be aligned to the block or sector size.
    • NOR_UNIFORM_SECTOR_SIZE is applicable to devices with uniform sectors, while NOR_BLOCK_SIZE is used for devices with mixed sector sizes.
    • Example Check:
      if ((TargetAddress % NOR_BLOCK_SIZE) != 0) {
      return E_NOT_OK; /* Address not aligned to block size */
      }
  2. Write:
    • Write operations must be aligned to the page size of the flash.
    • Page size must be configured correctly in FlsNORPageSize.
  3. Read::
    • Read operations can occur at any address but should consider sector boundaries for performance optimization.

Error Handling for Custom Flash Devices

When integrating custom flash devices, pay attention to the following error handling mechanisms:

  1. Command Not Supported Error:
    • If a required command is not supported by the custom flash, set the value to 0U in the configuration to avoid operation failure.
  2. Alignment Errors:
    • Erase, write, and read operations should always be aligned to the sector or block size.
    • For example, if the sector size is 4KB, an erase operation starting at an unaligned address will fail.
  3. Timeouts:
    • Timeout supervision for custom flash devices is not supported in this driver version. Users should manage timeouts externally if required.

Key Considerations

When configuring a custom flash device, ensure the following:

  1. Command Support:
    • Verify that all required commands (e.g., FlsNORCmdPageProg, FlsNORCmdSecErase) are supported by the custom flash. Unsupported commands should be set to 0U.
  2. Sector and Block Alignment:
    • Memory operations should always be aligned to the sector or block size to prevent data corruption.
  3. Erased Data Value:
    • Typically, NOR flash devices use 0xFF for erased data. Ensure the FlsNORErasedData is correctly set.
  4. Page Size Configuration:
    • Write operations are performed in page-sized chunks (e.g., 256B). Ensure FlsNORPageSize is correctly configured.
  5. Uniform Sector and Hybrid Sector Handling:
    • For flash devices with uniform sectors, configure FlsNORUniformSectorSize with the appropriate value.
    • For devices with hybrid sectors, set the FlsNORHybridSectorSize accordingly. If not applicable, set this to 0U, and the driver will fall back on the regular FlsNORUniformSectorSize.

Safety and Validation for Custom Flash Devices

The FLS driver incorporates safety checks to ensure data integrity and proper operation across supported flash devices. These checks include boundary verifications for uniform and hybrid sector sizes, valid address alignment, and command execution correctness. Although the driver is thoroughly tested and verified for the following flash devices:

  • S28HS512T (XSPI, tested on AM62X_SK, AM62PX)

It is important to note that when adding custom flash devices, these safety mechanisms will ensure that the driver performs appropriate validations during read, write, and erase operations. While custom devices can be configured, it is critical to refer to the device's datasheet to ensure proper configuration of commands, sizes, and addressing modes. For any device not listed here, ensure that it adheres to similar specifications to the tested devices to maintain the driver's integrity and safety standards.

Note: For detailed descriptions of all configurable parameters, refer to the design document provided in the CSP package. The document is located at: "$(MCAL_INSTALL_PATH)/mcusw/csp"

The following section details on the unsupported features and additional features added.

Back To Top


Variance / Deviation from the specification


FlsDacEnable

This parameter is the switch between Direct Access Mode (DAC) and Indirect Access Mode (INDAC) used by the OSPI module to communicate with the Flash Device. The Flash will be memory mapped when running in DAC mode, and execution in place will happen directly from flash memory. In INDAC mode, data transfer between system memory and external flash occurs through the internal SRAM.


FlsXipEnable

This parameter is the switch to turn on or off XIP mode. Only XIP Read mode is supported in current driver. XIP mode will only be functional in DAC mode of operation.


FlsOspiClkSpeed

This parameter defines the Clock Speed for the OSPI peripheral. The supported clock speeds are as follows:

  1. 133Mhz (133333333U) - This Clock freq works with all modes of the Flash Driver.
  2. 166Mhz (166666666U) - This Clock freq is fully supported in INDAC mode of operations. In DAC mode, only read operation is supported.

FlsDtrEnable

This parameter is the switch between Double Transfer Rate (DTR) and Single Transfer Rate (STR) for OSPI Flash.


FlsPhyEnable

This parameter is the switch to turn on and off PHY mode.


FlsBlockSize

This parameter defines the Block size for the OSPI peripheral. The parameter shall be obtained as the base-2 logarithm of sectorSize.

For example: if the sectorSize is 262144 then, blockSize = log2(262144) = 18


Features that are not supported:

Following features outlined in Specification are not supported:

  1. Fast vs Normal Mode - devices only has one mode of execution for OSPI Flash. Only normal mode is supported. Relevant features not implemented include:
    1. FlsSetModeAPI
    2. FlsDefaultMode
    3. FlsMaxReadFastMode
    4. FlsMaxWriteFastMode
  2. Access Code Placement - Write and Erase in XIP mode is not supported. Only Read in XIP implemented. Relevant features not implemented include:
    1. FlsAcLoadOnJobStart
    2. FlsAcErase
    3. FlsAcWrite
  3. Timeout Supervision - Relevant features not implemented include:
    1. FlsTimeoutSupervision
    2. FlsCallCycle
  4. FlsSector - Internal Flash Device Info structure used instead of FlsSector
    1. Fls_NorOspiInfo structure is used by driver for flash device information.
  5. DET RunTime Error is not supported. DET Dev Errors and DET Transient Faults are supported.

    Note: For AM275x, FSS data reg 1 is associated with FOTA and OTFA. So there are a bunch of registers that are associated with it. When configuring the RAT we redirect the access from FSS data reg 1 to FSS data reg 3 which is a bypass region. The configuration of RAT entry in SYSCFG tool is shown below is added in ti_dpl_config.c

RAT configuration in SYSCFG tool

Custom Flash Configuration Adaptation

In compliance with project-specific requirements, the FlsSectorList field has been removed from the configurator. Instead, the flash-related information, such as sector size, block size, and page size, is now defined through the fields in FlsMemConfiguration. These fields include:

  • FlsNORBlockSize: Defines the block size for the NOR flash.
  • FlsNORUniformSectorSize: Represents the uniform sector size for flash devices where applicable.
  • FlsNORHybridSectorSize: Represents the hybrid sector size, used when supported by the flash device. If not applicable, the uniform sector size is used.
  • FlsNORPageSize: Specifies the page size for write operations.

This deviation from the AUTOSAR specification ensures a more streamlined and flexible configuration for flash devices. The use of the FlsMemConfiguration fields allows for easier integration of custom flash devices while maintaining necessary safety and validation checks.

By using these parameters, the driver automatically detects the flash used in runtime during the Fls_Init by reading and comparing the Flash device and manufacturer Id. The driver will use the commands specific to that flash instance. This modification allows support for multiple custom flash devices while still adhering to core safety mechanisms, even though it deviates from the strict AUTOSAR spec implementation. Refer section (refer section Configuration) for custom flash addition.


Migration Guide

With the introduction of multi-flash support, existing customers must adjust their configurations to align with the new structure. Follow the steps below to transition smoothly:

Key Changes:

  1. Multiple Flash Configuration:
    • User can add multiple flash devices in the FlsMemConfiguration and add all flash specific commands for each flash devices.
    • All commands, block sizes, sector sizes, and protocol-specific configurations for all configured flash will be generated in Fls_Cfg.c.
  2. Updated Configuration Process:
    • Use the FlsMemConfiguration field in the EB Tresos configurator to define flash parameters such as:
      • Device Type: e.g., NOR
      • Protocol Mode: OSPI, QSPI, or XSPI
      • Block Size, Sector Size, and Page Size
      • Flash Specific Commands
    • The flash specific commands for all configured devices are generated as an array of structure in Fls_Cfg.c. The driver will detect the flash used in the application and use the configured commands specific to that flash in the driver.
  3. Board Layer Updates:
    • Ensure the board-specific configuration files (e.g., Fls_Brd_Nor.c) reference the new flash specific commands and settings.
    • Modify these files to ensure compatibility with your custom flash device, particularly in setting the correct device commands and configurations.
  4. Handling Custom Flash Devices:
    • For custom flash integration, add the required configurations in FlsMemConfiguration within EB Tresos.
    • Use the generated structure in Fls_Cfg.c for any custom commands or configurations.

Migration Steps:

  1. Backup: Save your current configuration files and header files.
  2. Configure in EB Tresos:
    • Add the new flash and all flash specific parameters via the FlsMemConfiguration field.
  3. Generate Configuration Files:
    • Generate the configurations and ensure all flash device parameters are correctly defined in Fls_Cfg.c.
  4. Modify Board Layer:
    • Update the board configuration files to reference flash specific commands.
  5. Validate:
    • Test the configuration with your device to ensure all functionalities work correctly.

Back To Top



Non Standard Service APIs


Ospi_RegisterReadback

As noted from the previous MCAL implementation, some of the critical configuration registers could potentially be corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection

Description Comments
Service Name Ospi_RegisterReadback Can potentially be turned OFF (Refer to Design Document provided in CSP)
Syntax Ospi_RegisterReadback( P2VAR(CSL_ospi_flash_cfgRegs, AUTOMATIC, SPI_APPL_DATA) RegRbPtr) E_OK: Register read back has been done, E_NOT_OK: Register read back failed
Service ID NA
Sync / Async Sync
Reentrancy Reentrant
Parameter in None
Parameters out RegRbPtr Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.
Return Value Std_ReturnType E_OK, E_NOT_OK

Fls_dataOverflowUnderflowIntrEnable

This API Enable Under/Overflow Interrupts of the hardware unit and returns the status.

Description Comments
Service Name Fls_dataOverflowUnderflowIntrEnable Fls_dataOverflowUnderflowIntrEnable Enable Under/Overflow Interrupts of the hardware unit
Syntax Fls_dataOverflowUnderflowIntrEnable(uint32 intrFlag)
Service ID NA
Sync / Async Sync
Reentrancy Reentrant
Parameter in intrFlag Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U
Parameters out NA
Return Value Std_ReturnType E_OK: Interrupt Enabled E_NOT_OK: Interrupt Enable failed

Fls_dataOverflowUnderflowIntrDisable

This API Disable Under/Overflow Interrupts of the hardware unit and returns the status.

Description Comments
Service Name Fls_dataOverflowUnderflowIntrDisable Spi_dataOverflowUnderflowIntrDisable Disable Under/Overflow Interrupts of the hardware unit and returns the status.
Syntax Fls_dataOverflowUnderflowIntrDisable(uint32 intrFlag)
Service ID NA
Sync / Async Sync
Reentrancy Reentrant
Parameter in intrFlag Interrupt Disable flag for Underflow=2U Interrupt Disable flag for Overflow=128U
Parameters out NA
Return Value Std_ReturnType E_OK: Interrupt Disabled E_NOT_OK: Interrupt Disabled failed

Fls_dataOverflowUnderflowIntrGetStatus

This API gets status of Under/Overflow Interrupts of the hardware unit and returns the status.

Description Comments
Service Name Fls_dataOverflowUnderflowIntrGetStatus Fls_dataOverflowUnderflowIntrGetStatus gets status of Under/Overflow Interrupts of the hardware unit
Syntax Fls_dataOverflowUnderflowIntrGetStatus(uint32 intFlags)
Service ID NA
Sync / Async Sync
Reentrancy Reentrant
Parameter in intrFlag Interrupt Enable flag
Parameters out NA
Return Value ospiIrqstatus OSPI_NO_EVENT: No underflow event OSPI_EVENT_PENDING: Underflow Event OSPI_STATUS_READ_FAIL: Status read fail

Fls_dataOverflowUnderflowIntrStatusClear

This API clear Under/Overflow Interrupts of the hardware unit and returns the status.

Description Comments
Service Name Fls_dataOverflowUnderflowIntrStatusClear Fls_dataOverflowUnderflowIntrStatusClear clear Under/Overflow Interrupts of the hardware unit and returns the status.
Syntax Fls_dataOverflowUnderflowIntrStatusClear(uint32 intrFlag)
Service ID NA
Sync / Async Sync
Reentrancy Reentrant
Parameter in intrFlag Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U
Parameters out NA
Return Value Std_ReturnType E_OK: Interrupt status clears E_NOT_OK: Interrupt status clear failed

Back To Top


Constraints

The driver can have unexpected behavior and loss of functionality if unsupported values are passed into configurator or unsupported combinations are used. Below is a list of such constraints.

  • Configurator Input Values Constraints:
    1. maxReadNormalMode and maxWriteNormalMode values should be aligned with (multiples of) the Flash device page size.
    2. sectorList structure should not be changed, as that is specific to Flash Device.
    3. ospiClkSpeed should be either 133333333U or 166666666U.
    4. FlsDeviceType should be either FLS_NOR or FLS_NAND based on flash device type.
    5. FlsProtocolMode should be either FLS_OSPI, FLS_XSPI, or FLS_QSPI based on supported flash protocol mode.
  • Feature Combination Constraints:
    1. When using Interrupt mode, dacEnable should be set to FALSE. Interrupt mode is only available when using INDAC mode.
    2. When using Interrupt mode, maxWriteNormalMode value has to be equal to page size of flash device. Please see Fls_Cfg.c sample configuration file in the examples/Fls/fls_app_intr.
    3. If operating in XIP mode, dacEnable has to be enabled, and Interrupt mode has to be set to STD_OFF.
    4. In Interrupt mode, BlankCheck API and Compare API are not supported and should be disabled.
    5. For XSPI supported devices, write and erase is not functional in DAC mode. Only Read is possible in DAC mode. Please use INDAC mode for writing and erasing flash.
    6. The OSPI PHY enable feature is currently not supported.
    7. SDR mode not supported

Note: Only one OSPI instance (OSPI_0 or OSPI_1) is supported at a time.

Back To Top


Interrupt Configuration

The Driver does not register any interrupt service routine(ISR), it’s expected that consumer of this driver registers the required interrupt handler.

The interrupt number associated with instance of the Fls is detailed in TRM. Please refer FlsApp_InterruptConfig() in fls_app_intr test application for reference.

Please note that interrupt implementation is only available when running with INDAC mode. BlankCheck and Compare APIs are not supported with interrupt mode.

Back To Top


Power-up

The driver doesn't configure the functional clock and power for the Fls modules. It's expected that secondary boot loader(SBL) power-up the required modules. Please refer SBL documentation.

Back To Top


PHY Tune Module Algorithm

AM62AX, AM62X, AM62PX do not have PHY tune as of now.

Note:PHY Algorithm not validated on SMPU

Back To Top


Build and Running the Application

Please follow steps detailed in section (Build) to build library or example. Please note that OSPI Boot mode is not applicable for Fls module.

The below Fls Test Applications are available:

  1. fls_app_dac - Test Application to demo DAC storage mode
  2. fls_app_indac - Test Application to demo INDAC storage mode and general flash usage
  3. fls_app_intr - Testing interrupt mode. Requires clean flash build since different interrupt Fls_Cfg.h needs to be included. Clean build required even if's the same fls protocol

Please refer to Configuration Folder Structure on which of the three configuration folders each Fls Test Apllication uses.

Note: Please do a clean build (make -s allclean) when a different configuration folder is used. Each configuration folder header files have different define values.

Back To Top


Steps to run example application

Please follow steps detailed in section (Build) to build example

Poll Mode - Storage Mode

Test Applications fls_app_dac and fls_app_indac will run as packaged, just build and the executable will be generated.

Interrupt Mode - Storage Mode

Build fls_app_intr and run. Uses different configuration files than Poll Mode, so please build this application on a clean build.

Back To Top


Dependencies on SW Modules


DET

This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.

Back To Top


SchM

This implementation requires one level of exclusive access to guard critical sections. Invokes SchM_Enter_Fls_FLS_EXCLUSIVE_AREA_0 (), SchM_Exit_Fls_FLS_EXCLUSIVE_AREA_0 () to enter critical section and exit.

In the example implementation (Driver File Structure SchM_Fls.c) , all the interrupts on CPU are disabled. However, disabling of the enabled Fls interrupt should suffice.

Back To Top


MemIf

This implementation depends on MemIf module and uses its imported types such as MemIf_JobResultType, MemIf_ModeType and MemIf_StatusType.

Back To Top


Fee

This implementation depends on Fee module for callback notification to notify the module environment about job end and job error.

Back To Top


Driver File Structure

  1. Driver implemented by : Fls.h, Fls_Irq.h, Fls.c, Fls_Brd_Nor_Ospi.c, Fls_Brd_Nor_Xspi.c, Fls_Brd_Nor_Qspi.c, Fls_Irq.c, Fls_Ospi.c, Fls_Ospi.h, Fls_Brd_Nor.c, and Fls_Brd_Nor.h
  2. Flash Devices by : Fls_Cfg.c based on the Flash devices configured in the configurator (m35xu512, mt25qu512abb, s28hs512t or any custom flash added).
  3. Example Application by : FlsApp_Startup.h, FlsApp_Startup.c and FlsApp.c
  4. Phy tune algorithm files: nor_spi_patterns.c, nor_spi_patterns.h, nor_spi_phy_tune.c and nor_spi_phy_tune.h

Back To Top


Configuration Folder Structure

  • There are 3 configuration folders: examples_config/Fls_Demo_Cfg, examples/Fls/QSPI_Cfg, and examples/Fls/fls_app_intr
  • Note: Please do a clean build (make -s allclean) when a different configuration folder is used. Each configuration folder header files have different define values.
    • For example, if fls_app_indac (uses examples_config/Fls_Demo_Cfg) is built, please do a clean build when fls_app_intr (uses examples/Fls/fls_app_intr) is needed.
  • Example Configuration by : Fls_Cfg.h, Fls_Cfg.c, Fls_Cfg_dac.c, Fls_Cfg_indac.c and Fls_PBcfg.c

Fls configuration files in examples_config/Fls_Demo_Cfg folder

  • Used by OSPI0 interface (OSPI/XSPI flash device) build in fls_app_dac and fls_app_indac applications.
  • make -s fls_app_dac fls_app_indac BOARD=... SOC=... will use configuration files in this folder. Since FLS_PROTOCOL is defaulted to ospi, it's optional to specify "FLS_PROTOCOL=ospi".

QSPI Fls configuration in examples/Fls/QSPI_Cfg folder

  • Used by OSPI1 interface (QSPI flash device) build (FLS_PROTOCOL=qspi) in fls_app_dac and fls_app_indac applications.
  • Only used on J721S2 since QSPI flash protocol is only supported on J721S2.
  • make -s fls_app_dac fls_app_indac BOARD=j721s2_evm SOC=j721s2 FLS_PROTOCOL=qspi will use configuration files in this folder. Must specify "FLS_PROTOCOL=qspi".

OSPI and QSPI interrupt configuration in examples/Fls/fls_app_intr folder

  • Used by OSPI0 interface and OSPI1 interface in fls_app_intr application, respectively.
  • make -s fls_app_intr BOARD=j721s2_evm SOC=j721s2 FLS_PROTOCOL=qspi and make -s fls_app_intr BOARD=... SOC=... will use configuration files in this folder.

Back To Top


Error Handling


Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Fls.h) lists the SID.

Back To Top


Error codes

Type of Error Related Error code Value (Hex)
API service called with wrong parameter FLS_E_PARAM_CONFIG 0x01
API service called with wrong parameter FLS_E_PARAM_ADDRESS 0x02
API service called with wrong parameter FLS_E_PARAM_LENGTH 0x03
API service called with wrong parameter FLS_E_PARAM_DATA 0x04
API service used without module initialization FLS_E_UNINIT 0x05
API called when module is busy FLS_E_BUSY 0x06
API called with a Null Pointer FLS_E_PARAM_POINTER 0x0A

Back To Top


Transient Faults Reporting

Transient errors are reported to the DET using the service Det_reportDetTransientFault(). The driver interface (Fls.h) lists the SID.

Back To Top


Fault codes

Type of Error Related Error code Value (Hex)
Flash Erase Failed in HW FLS_E_ERASE_FAILED 0x01
Flash Write Failed in HW FLS_E_WRITE_FAILED 0x02
Flash Read Failed in HW FLS_E_READ_FAILED 0x03
Flash Compare Failed in HW FLS_E_COMPARE_FAILED 0x04
Expected HW ID not matched FLS_E_UNEXPECTED_FLASH_ID 0x05

Back To Top


Fls with DMA Enabled

Introduction

The FLS driver supports DMA-accelerated read transfers in DAC (Direct Access / memory-mapped) mode. When DMA is enabled, flash read operations are offloaded from the CPU to the BCDMA hardware, reducing CPU load and improving throughput.

Key characteristics of FLS DMA support:

  • DMA is used for DAC mode read transfers. Write and erase operations always use CPU-based transfers.
  • The destination buffer for a DMA read must not reside in the R5F Tightly Coupled Memory (ATCM/BTCM). Reads targeting TCM regions automatically fall back to CPU copy.
  • The CDD DMA driver must be initialized before calling Fls_Init(). Refer fls_app_dma for detailed application flow.

Back To Top


EB Tresos Configuration for FLS DMA

To enable DMA support in the FLS driver, the following configuration must be set in the EB Tresos FLS module:

FlsDmaEnable

Configuration Parameter Location in EB Tresos Value
FlsDmaEnable FLS → FlsGeneral → FlsDmaEnable true

Setting FlsDmaEnable to true generates the following in Fls_Cfg.h:

#define FLS_DMA_ENABLE (STD_ON)

And sets the dmaEnable field in the runtime configuration structure in Fls_Cfg.c:

.dmaEnable = TRUE,

Note: DMA reads are triggered in DAC (Direct Access / memory-mapped) mode. Ensure FlsDacEnable is set to true alongside FlsDmaEnable to use DMA-accelerated reads.

Back To Top


CDD DMA Configuration for FLS

The FLS driver uses the CDD DMA module to manage OSPI peripheral DMA transfers. The CDD DMA must be configured with an OSPI peripheral TX channel. The following parameters must be set in the EB Tresos CDD DMA module:

Channel Configuration

CDD DMA Parameter EB Tresos Location Required Value Description
DmaTransType CDD_DMA → CddDmaChannelConfig → DmaTransType CDD_DMA_PERIPH_TX_MODE Peripheral transmit mode — required for OSPI DAC read DMA
DmaPeriphUsed CDD_DMA → CddDmaChannelConfig → DmaPeriphUsed CDD_DMA_PERIPH_OSPI Selects the OSPI peripheral as the DMA peer
DmaInstID CDD_DMA → CddDmaChannelConfig → DmaInstID CDD_DMA_ID_0 BCDMA instance 0
DmaMode CDD_DMA → CddDmaChannelConfig → DmaMode CDD_DMA_MODE_INTERRUPT Interrupt-driven transfer completion
RingElemCount CDD_DMA → CddDmaChannelConfig → DmaRingConfig → RingElemCount 1 One ring element is sufficient for single-channel OSPI DMA

The corresponding generated configuration in Cdd_Dma_Cfg.c should look like:

CONST(Cdd_Dma_ConfigType, CDD_DMA_CONFIG_DATA) Cdd_Dma_Config = {
.netChannels = 1,
.channelCfg = {
[0] = {
.dmaTransType = CDD_DMA_PERIPH_TX_MODE, /* OSPI TX peripheral mode */
.dmaInstID = CDD_DMA_ID_0, /* BCDMA instance 0 */
.dmaMode = CDD_DMA_MODE_INTERRUPT, /* Interrupt mode */
.dmaPeriphUsed = CDD_DMA_PERIPH_OSPI, /* OSPI peripheral */
.dmaRingConfig = {
.ringElemCount = 1U,
},
},
}
};

Why CDD_DMA_PERIPH_TX_MODE?

Even though the FLS operation is a read from flash into system memory, the OSPI controller's DMA interface is configured on the transmit (TX) side. The memory-mapped XIP flash address is the source, and the destination is a system-memory buffer. This is why CDD_DMA_PERIPH_TX_MODE (not RX) is the correct setting for OSPI DAC DMA reads.

Back To Top


Application Initialization Sequence

When DMA is enabled, the application must initialize the CDD DMA module and register the DMA interrupt before calling Fls_Init(). The correct initialization sequence is:

/* 1. Register the CDD DMA channel interrupt handler */
FlsApp_DmaInterruptConfig();
/* 2. Initialize the CDD DMA driver */
Cdd_Dma_Init(NULL_PTR);
/* 3. Initialize the FLS driver — opens the DMA channel internally */
Fls_Init((const Fls_ConfigType *) NULL_PTR);
void Fls_Init(const Fls_ConfigType *ConfigPtr)
Initializes the Flash Driver.
FLS Module Configuration Structure.
Definition Fls.h:346

The FLS driver calls Fls_OspiDmaOpen() internally during Fls_Init() to acquire the CDD DMA channel. Fls_OspiDmaOpen() will fail and DMA will be disabled at runtime if Cdd_Dma_Init() has not been called beforehand.

Refer to FlsApp_DmaInterruptConfig() in mcal/examples/Fls/fls_app_dma/soc/<soc>/<core>/FlsApp_Startup.h for a reference implementation of DMA interrupt registration.

Refer to CDD DMA documentation for information on valid interrupt numbers to be configured for BCDMA mode.

Back To Top


DMA Constraints and Notes

  • DMA is not used for flash write or erase operations. These always use CPU-based transfers.
  • DMA reads require FlsDacEnable = true. DMA is triggered inside the DAC read path (OSPI_dac_xfer_mode_read).
  • The destination buffer supplied to Fls_Read() must be located in cacheable DDR memory. Buffers in R5F ATCM or BTCM are not accessible by the BCDMA hardware and will automatically fall back to CPU copy.
  • Both Polling/Interrupt mode is supported for FLS DMA transfers.
  • The example application for FLS with DMA is located at mcal/examples/Fls/fls_app_dma/.

Back To Top


API Description

The AUTOSAR BSW Flash Driver specification details the APIs required for Flash Driver. Please refer to (Refer to Design Document provided in CSP) for detailed API description.

Refer API Documentation for details

Back To Top


Example Application

The example application demonstrates use of Fls module, the list below identifies key steps performed in the example. The configuration file is present at (Configuration Folder Structure).

Polled Storage Mode (fls_app_dac and fls_app_indac)

  • Initializes “Result Status Flags: Fls_JobDoneSuccess and Fls_JobDoneError”
  • Perform Pinmux configuration needed and initializes Board.
  • Core Application ()
    • Fls_Init() - Takes FlsConfigSet as input and Initializes Flash and OSPI
    • Fls_OSPI_configClk () - Configure the OSPI Clocks
    • Set starting address to base address of flash device, and data size to 1M Bytes
    • Fls_GetVersionInfo() - Prints module version info
    • Fls_GetStatus() - Gets the Module status
    • Fls_Erase() - Submits Erase job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_BlankCheck() - Submits BlankCheck job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Write() - Submits Write job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Read() - Submits Read job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Compare() - Submits Compare job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.

Interrupt Storage Mode (fls_app_intr)

  • Initializes “Result Status Flags: Fls_JobDoneSuccess and Fls_JobDoneError”
  • Perform Pinmux configuration needed and initializes Board.
  • FlsApp_InterruptConfig()
    • Register the Interrupt and ISR
  • Core Application ()
    • Fls_Init() - Takes FlsConfigSet as input and Initializes Flash and OSPI
    • Fls_OSPI_configClk () - Configure the OSPI Clocks
    • Set starting address to base address of flash device, and data size to 1M Bytes
    • Fls_GetVersionInfo() - Prints module version info
    • Fls_GetStatus() - Gets the Module status
    • Fls_Erase() - Submits Erase job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Read() - Submits Read job to manually compare erased data
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Write() - Submits Write job
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Read() - Submits Read job to manually compare written data
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.

DMA Storage Mode (fls_app_dma)

  • Initializes “Result Status Flags: Fls_JobDoneSuccess and Fls_JobDoneError”
  • Perform Pinmux configuration needed and initializes Board.
  • FlsApp_DmaInterruptConfig()
    • Register the DMA interrupt and ISR
  • Core Application ()
    • Cdd_Dma_Init() - Initializes the CDD DMA driver
    • Fls_Init() - Takes FlsConfigSet as input and Initializes Flash and OSPI
    • Fls_OSPI_configClk () - Configure the OSPI Clocks
    • Set starting address to base address of flash device, and data size to 1M Bytes
    • Fls_GetVersionInfo() - Prints module version info
    • Fls_GetStatus() - Gets the Module status
    • Fls_Read() - Submits Read job (uses DMA-accelerated transfer in DAC mode)
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.
    • Fls_Compare() - Submits Compare job to verify read data
    • Fls_MainFunction() - Called in while loop, processes job, and exits when Fls_JobEndNotification/Fls_JobErrorNotification reached.

Performance Measurements

  • You can turn on the performance measurements for the storage mode app by enabling the "PERF_TEST" macro in FlsApp.c. This is enabled by default.

Back To Top


Example Log

fls_app_dac

    FLS_APP_DAC: 
    ------------------FLS Sample Application - STARTS !!! ------------------
    FLS_APP_DAC: 
    Running on J7 ES 
    FLS_APP_DAC: OSPI0 controller will be configured for OSPI/XSPI flash
    FLS_APP_DAC: FLS spi_test Initiating and Starting.
    FLS_APP_DAC: Variant - Pre Compile being used !!!
    FLS_APP_DAC: Configuring Clocks.
    FLS_APP_DAC: Clock Configured at 166666666Hz
    
    FLS MCAL Version Info
    ---------------------
    Vendor ID           : 44
    Module ID           : 92
    SW Major Version    : 10
    SW Minor Version    : 0
    SW Patch Version    : 0
    
    FLS_APP_DAC: DATA SIZE TEST is 0x100000 
    FLS_APP_DAC: Offset is 0x0 
    
    FLS_APP_DAC:
    *****************Writing PHY Tune Data to last sector in memory*****************
    FLS_APP_DAC: Erasing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC: Blank Checking 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC: Writing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    FLS_APP_DAC: 
    Write 1048576 bytes at transfer rate 107557 Kbps 
    
    FLS_APP_DAC: Comparing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC:
    *************************Writing PHY Tune Data complete*************************

    FLS_APP_DAC: Erasing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC: Blank Checking 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC: Writing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    FLS_APP_DAC: 
    Write 1048576 bytes at transfer rate 2533 Kbps 
    
    FLS_APP_DAC: Reading 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    FLS_APP_DAC: 
    Read 1048576 bytes at transfer rate 40725 Kbps 
    
    FLS_APP_DAC: Comparing 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    
    FLS_APP_DAC: Reading 
    FLS_APP_DAC: Job Processing in Progress.
    FLS_APP_DAC: Job Ends: SUCCESS
    FLS_APP_DAC: 
    Read 1048576 bytes at transfer rate 41341 Kbps 
    
    FLS_APP_DAC: All tests have passed! 

fls_app_indac

    FLS_APP_INDAC: 
    ------------------FLS Sample Application - STARTS !!! ------------------
    FLS_APP_INDAC: 
    Running on J7 ES 
    FLS_APP_INDAC: OSPI0 controller will be configured for OSPI/XSPI flash
    FLS_APP_INDAC: FLS spi_test Initiating and Starting.
    FLS_APP_INDAC: Variant - Pre Compile being used !!!
    FLS_APP_INDAC: Configuring Clocks.
    FLS_APP_INDAC: Clock Configured at 166666666Hz
    
    FLS MCAL Version Info
    ---------------------
    Vendor ID           : 44
    Module ID           : 92
    SW Major Version    : 10
    SW Minor Version    : 0
    SW Patch Version    : 0
    
    FLS_APP_INDAC: DATA SIZE TEST is 0x100000 
    FLS_APP_INDAC: Offset is 0x0 

    FLS_APP_INDAC: Erasing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Blank Checking 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Writing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 8912 Kbps 
    
    FLS_APP_INDAC: Cancel while Erasing 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Cancel while Writing 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 53350 Kbps 
    
    FLS_APP_INDAC: Erasing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Comparing.Expected to fail as data is erased. 
    FLS_APP_INDAC: Job Processing in Progress.
    Det Error reported
      Module ID       92
      Instance ID     0
      SID             8
      Error ID        8
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Cancel while Comparing.Expected to fail as data is erased. 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Writing to compare again 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 8911 Kbps 
    
    FLS_APP_INDAC: Comparing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Reading 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 44758 Kbps 
    
    FLS_APP_INDAC: Cancel while Reading 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 53349 Kbps 
    
    FLS_APP_INDAC: 
    .......................Changing mode to DAC....................... 
    FLS_APP_INDAC: Reading 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 20022 Kbps 
    
    FLS_APP_INDAC: Comparing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: 
    ....................Changing mode to INDAC..................... 
    FLS_APP_INDAC: Erasing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Blank Checking 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Writing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 8913 Kbps 
    
    FLS_APP_INDAC: Reading 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 44756 Kbps 
    
    FLS_APP_INDAC: Comparing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Cancel Erase Job
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Blank Checking after erase cancel-----Expect to fail
    FLS_APP_INDAC: Job Processing in Progress.
    Det Error reported
      Module ID       92
      Instance ID     0
      SID             10
      Error ID        7
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Erasing again 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Blank Checking after erase again
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Cancel after Writing 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 53350 Kbps 
    
    FLS_APP_INDAC: Comparing after write cancel---Expect to fail
    FLS_APP_INDAC: Job Processing in Progress.
    Det Error reported
      Module ID       92
      Instance ID     0
      SID             8
      Error ID        8
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Writing again. Will pass
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 8914 Kbps 
    
    FLS_APP_INDAC: Comparing.Expected to pass since write passed. 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Erasing 
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: Writing.
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Write 1048576 bytes at transfer rate 8913 Kbps 
    
    FLS_APP_INDAC: Cancel while Reading 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 53349 Kbps 
    
    FLS_APP_INDAC: Reading again
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    FLS_APP_INDAC: 
    Read 1048576 bytes at transfer rate 44751 Kbps 
    
    FLS_APP_INDAC: Cancel while Comparing 
    FLS_APP_INDAC: Cancel job Processing in Progress.
    FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
    FLS_APP_INDAC: Job Ends: ERROR
    
    FLS_APP_INDAC: Comparing again
    FLS_APP_INDAC: Job Processing in Progress.
    FLS_APP_INDAC: Job Ends: SUCCESS
    
    FLS_APP_INDAC: 
    Changing mode to DAC 
    FLS_APP_INDAC: FLS SPI TEST DONE! 

    FLS_APP_INDAC: Ospi configuration Register Readback values  
    FLS_APP_INDAC: CONFIG_REG                                     : 0x81783881
    FLS_APP_INDAC: DEV_INSTR_RD_CONFIG_REG                  : 0x1e03339d
    FLS_APP_INDAC: DEV_INSTR_WR_CONFIG_REG                  : 0x33082
    FLS_APP_INDAC: DEV_DELAY_REG                              : 0x300000a
    FLS_APP_INDAC: DEV_SIZE_CONFIG_REG                          : 0x111003
    FLS_APP_INDAC: SRAM_PARTITION_CFG_REG                     : 0x3f
    FLS_APP_INDAC: DMA_PERIPH_CONFIG_REG                      : 0x0
    FLS_APP_INDAC: MODE_BIT_CONFIG_REG                          : 0x200
    FLS_APP_INDAC: TX_THRESH_REG                              : 0x1
    FLS_APP_INDAC: RX_THRESH_REG                              : 0x1
    FLS_APP_INDAC: PHY_CONFIGURATION_REG                      : 0x2d0021

    FLS_APP_INDAC: All tests have passed!                                                           

fls_app_intr

    FLS_APP_INTR: 
    ------------------FLS Sample Application - STARTS !!! ------------------
    FLS_APP_INTR: OSPI0 controller will be configured for OSPI/XSPI flash
    FLS_APP_INTR: FLS spi_test Initiating and Starting.
    FLS_APP_INTR: Configuring Interrupt.
    FLS_APP_INTR: Variant - Pre Compile being used !!!
    FLS_APP_INTR: Configuring Clocks.
    FLS_APP_INTR: Clock Configured at 166666666Hz
    
    FLS MCAL Version Info
    ---------------------
    Vendor ID           : 44
    Module ID           : 92
    SW Major Version    : 10
    SW Minor Version    : 0
    SW Patch Version    : 0
    
    FLS_APP_INTR: DATA SIZE TEST is 0x100000 
    FLS_APP_INTR: Offset is 0x0 

    FLS_APP_INTR: Erasing 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    
    FLS_APP_INTR: Manual comparing erased data

    FLS_APP_INTR: Calling Read to manually compare 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    FLS_APP_INTR: 
    Read 1048576 bytes at transfer rate 58417 Kbps 
    
    FLS_APP_INTR: Manual Comparing is Correct

    FLS_APP_INTR: Cancel while Writing 
    FLS_APP_INTR: Cancel job Processing in Progress.
    FLS_APP_INTR: Error is expected as we are cancelling the operation. 
    FLS_APP_INTR: Job Ends: ERROR
    FLS_APP_INTR: 
    Write 1048576 bytes at transfer rate 55448 Kbps 
    
    FLS_APP_INTR: Cancel while Reading 
    FLS_APP_INTR: Cancel job Processing in Progress.
    FLS_APP_INTR: Error is expected as we are cancelling the operation. 
    FLS_APP_INTR: Job Ends: ERROR
    FLS_APP_INTR: 
    Read 1048576 bytes at transfer rate 56766 Kbps 
    
    FLS_APP_INTR: Erasing 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    
    FLS_APP_INTR: Manual comparing erased data

    FLS_APP_INTR: Calling Read to manually compare 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    FLS_APP_INTR: 
    Read 1048576 bytes at transfer rate 58439 Kbps 
    
    FLS_APP_INTR: Manual Comparing is Correct

    FLS_APP_INTR: Writing Again without Cancel
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    FLS_APP_INTR: 
    Write 1048576 bytes at transfer rate 13121 Kbps 
    
    FLS_APP_INTR: Reading without cancel 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    FLS_APP_INTR: 
    Read 1048576 bytes at transfer rate 58452 Kbps 
    
    FLS_APP_INTR: Manual Comparing written data 

    FLS_APP_INTR: Calling Read to manually compare 
    FLS_APP_INTR: Job Processing in Progress.
    FLS_APP_INTR: Job Ends: SUCCESS
    FLS_APP_INTR: 
    Read 1048576 bytes at transfer rate 58433 Kbps 
    
    FLS_APP_INTR: Manual Comparing is Correct

    FLS_APP_INTR: 
    Changing mode to DAC 
    FLS_APP_INTR: FLS SPI TEST DONE! 

    FLS_APP_INTR: Ospi configuration Register Readback values  
    FLS_APP_INTR: CONFIG_REG                                      : 0x81783881
    FLS_APP_INTR: DEV_INSTR_RD_CONFIG_REG                   : 0x1e03339d
    FLS_APP_INTR: DEV_INSTR_WR_CONFIG_REG                   : 0x33082
    FLS_APP_INTR: DEV_DELAY_REG                               : 0x300000a
    FLS_APP_INTR: DEV_SIZE_CONFIG_REG                           : 0x111003
    FLS_APP_INTR: SRAM_PARTITION_CFG_REG                      : 0x3f
    FLS_APP_INTR: DMA_PERIPH_CONFIG_REG                       : 0x0
    FLS_APP_INTR: MODE_BIT_CONFIG_REG                           : 0x200
    FLS_APP_INTR: TX_THRESH_REG                               : 0x1
    FLS_APP_INTR: RX_THRESH_REG                               : 0x1
    FLS_APP_INTR: PHY_CONFIGURATION_REG                       : 0x2d0021

    FLS_APP_INTR: All tests have passed! 

fls_app_xip

    FLS_APP_XIP:
    ------------------FLS Sample Application - STARTS !!! ------------------
    FLS_APP_XIP:
     Running on J7 ES
    FLS_APP_XIP: FLS spi_test Initiating and Starting.
    FLS_APP_XIP: Variant - Pre Compile being used !!!
    FLS_APP_XIP: Configuring Clocks.
    FLS_APP_XIP: Clock Configured at 166666666Hz

    FLS MCAL Version Info
    ---------------------
    Vendor ID           : 44
    Module ID           : 92                                                        
    SW Major Version    : 1                                                         
    SW Minor Version    : 2                                                         
    SW Patch Version    : 1                                                         

    FLS_APP_XIP: DATA SIZE TEST is 0x1000                                           
    FLS_APP_XIP: Offset is 0x0                                                      
    FLS_APP_XIP: Erasing                                                            
    FLS_APP_XIP: Job Processing in Progress.                                        
    FLS_APP_XIP: Job Ends: SUCCESS                                                  
    FLS_APP_XIP: Blank Checking                                                     
    FLS_APP_XIP: Job Processing in Progress.                                        
    FLS_APP_XIP: Job Ends: SUCCESS                                                  
    FLS_APP_XIP: Writing                                                            
    FLS_APP_XIP: Job Processing in Progress.                                        
    FLS_APP_XIP: Job Ends: SUCCESS                                                  
    FLS_APP_XIP: Calling XIP app                                                    
    MCU1_0 running                                                                  
    MCU1_0 reports: All tests have passed                                           
    FLS_APP_XIP: Returning from XIP app, returned value is 0xFEEDFACE               
    FLS_APP_XIP: Reading                                                            
    FLS_APP_XIP: Job Processing in Progress.                                        
    FLS_APP_XIP: Job Ends: SUCCESS                                                  
    FLS_APP_XIP: Comparing                                                          
    FLS_APP_XIP: Job Processing in Progress.                                        
    FLS_APP_XIP: Job Ends: SUCCESS                                                  
    FLS_APP_XIP: DONE!    

Log for AM275x device

fls_app_dac

  FLS_APP_DAC: 
  ------------------FLS Sample Application - STARTS !!! ------------------
  FLS_APP_DAC: 
  Running on AM275X
  FLS_APP_DAC: OSPI0 controller will be configured for OSPI/XSPI flash
  FLS_APP_DAC: FLS spi_test Initiating and Starting.
  FLS_APP_DAC: Variant - Pre Compile being used !!!
  FLS_APP_DAC: Configuring Clocks.
  MCU Initialized!
  Module clock frequency set. Module = 75 , Freq = 166666666 !!!
  FLS_APP_DAC: Clock Configured at 166666666Hz
  
  FLS MCAL Version Info
  ---------------------
  Vendor ID           : 44
  Module ID           : 92
  SW Major Version    : 10
  SW Minor Version    : 1
  SW Patch Version    : 0
  
  FLS_APP_DAC: DATA SIZE TEST is 0x100000 
  FLS_APP_DAC: Offset is 0x0 
  
  FLS_APP_DAC: Reading 
  FLS_APP_DAC: Job Processing in Progress.
  FLS_APP_DAC: Job Ends: SUCCESS
  
  FLS_APP_DAC: Reading 
  FLS_APP_DAC: Job Processing in Progress.
  FLS_APP_DAC: Job Ends: SUCCESS
  
  FLS_APP_DAC: All tests have passed! 

fls_app_indac

  FLS_APP_INDAC: 
  ------------------FLS Sample Application - STARTS !!! ------------------
  FLS_APP_INDAC: 
  Running on AM275X
  FLS_APP_INDAC: OSPI0 controller will be configured for OSPI/XSPI flash
  FLS_APP_INDAC: FLS spi_test Initiating and Starting.
  FLS_APP_INDAC: Variant - Pre Compile being used !!!
  FLS_APP_INDAC: Configuring Clocks.
  MCU Initialized!
  Module clock frequency set. Module = 75 , Freq = 166666666 !!!
  FLS_APP_INDAC: Clock Configured at 166666666Hz
  
  FLS MCAL Version Info
  ---------------------
  Vendor ID           : 44
  Module ID           : 92
  SW Major Version    : 10
  SW Minor Version    : 1
  SW Patch Version    : 0
  
  FLS_APP_INDAC: DATA SIZE TEST is 0x100000 
  FLS_APP_INDAC: Offset is 0x0 

  FLS_APP_INDAC: Erasing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Blank Checking 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Writing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel while Erasing 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Cancel while Writing 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Erasing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Comparing.Expected to fail as data is erased. 
  FLS_APP_INDAC: Job Processing in Progress.
  Det Error reported
    Module ID       92
    Instance ID     0
    SID             8
    Error ID        8
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Cancel while Comparing.Expected to fail as data is erased. 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Writing to compare again 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Comparing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Reading 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel while Reading 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: 
  .......................Changing mode to DAC....................... 
  FLS_APP_INDAC: Reading 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Comparing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: 
  ....................Changing mode to INDAC..................... 
  FLS_APP_INDAC: Erasing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Blank Checking 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Writing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Reading 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Comparing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel Erase Job
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Blank Checking after erase cancel-----Expect to fail
  FLS_APP_INDAC: Job Processing in Progress.
  Det Error reported
    Module ID       92
    Instance ID     0
    SID             10
    Error ID        7
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Erasing again 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Blank Checking after erase again
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel after Writing 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Comparing after write cancel---Expect to fail
  FLS_APP_INDAC: Job Processing in Progress.
  Det Error reported
    Module ID       92
    Instance ID     0
    SID             8
    Error ID        8
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Writing again. Will pass
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Comparing.Expected to pass since write passed. 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Erasing 
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Writing.
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel while Reading 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Reading again
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: Cancel while Comparing 
  FLS_APP_INDAC: Cancel job Processing in Progress.
  FLS_APP_INDAC: Error is expected as we are cancelling the operation. 
  FLS_APP_INDAC: Job Ends: ERROR
  
  FLS_APP_INDAC: Comparing again
  FLS_APP_INDAC: Job Processing in Progress.
  FLS_APP_INDAC: Job Ends: SUCCESS
  
  FLS_APP_INDAC: 
  Changing mode to DAC 
  FLS_APP_INDAC: FLS SPI TEST DONE! 

  FLS_APP_INDAC: Ospi configuration Register Readback values  
  FLS_APP_INDAC: CONFIG_REG                                     : 0xc1083881
  FLS_APP_INDAC: DEV_INSTR_RD_CONFIG_REG                  : 0x190333ee
  FLS_APP_INDAC: DEV_INSTR_WR_CONFIG_REG                  : 0x33012
  FLS_APP_INDAC: DEV_DELAY_REG                              : 0x300000a
  FLS_APP_INDAC: DEV_SIZE_CONFIG_REG                          : 0x121003
  FLS_APP_INDAC: SRAM_PARTITION_CFG_REG                     : 0x3f
  FLS_APP_INDAC: DMA_PERIPH_CONFIG_REG                      : 0x0
  FLS_APP_INDAC: MODE_BIT_CONFIG_REG                          : 0x0
  FLS_APP_INDAC: TX_THRESH_REG                              : 0x1
  FLS_APP_INDAC: RX_THRESH_REG                              : 0x1
  FLS_APP_INDAC: PHY_CONFIGURATION_REG                      : 0x0

  FLS_APP_INDAC: All tests have passed! 

fls_app_intr

  FLS_APP_INTR: 
  ------------------FLS Sample Application - STARTS !!! ------------------
  FLS_APP_INTR: OSPI0 controller will be configured for OSPI/XSPI flash
  FLS_APP_INTR: FLS spi_test Initiating and Starting.
  FLS_APP_INTR: Configuring Interrupt.
  FLS_APP_INTR: Variant - Pre Compile being used !!!
  FLS_APP_INTR: Configuring Clocks.
  FLS_APP_INTR: Clock Configured at 166666666Hz
  
  FLS MCAL Version Info
  ---------------------
  Vendor ID           : 44
  Module ID           : 92
  SW Major Version    : 10
  SW Minor Version    : 1
  SW Patch Version    : 0
  
  FLS_APP_INTR: DATA SIZE TEST is 0x100000 
  FLS_APP_INTR: Offset is 0x0 

  FLS_APP_INTR: Erasing 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual comparing erased data

  FLS_APP_INTR: Calling Read to manually compare 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual Comparing is Correct

  FLS_APP_INTR: Cancel while Writing 
  FLS_APP_INTR: Cancel job Processing in Progress.
  FLS_APP_INTR: Error is expected as we are cancelling the operation. 
  FLS_APP_INTR: Job Ends: ERROR
  
  FLS_APP_INTR: Cancel while Reading 
  FLS_APP_INTR: Cancel job Processing in Progress.
  FLS_APP_INTR: Error is expected as we are cancelling the operation. 
  FLS_APP_INTR: Job Ends: ERROR
  
  FLS_APP_INTR: Erasing 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual comparing erased data

  FLS_APP_INTR: Calling Read to manually compare 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual Comparing is Correct

  FLS_APP_INTR: Writing Again without Cancel
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Reading without cancel 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual Comparing written data 

  FLS_APP_INTR: Calling Read to manually compare 
  FLS_APP_INTR: Job Processing in Progress.
  FLS_APP_INTR: Job Ends: SUCCESS
  
  FLS_APP_INTR: Manual Comparing is Correct

  FLS_APP_INTR: 
  Changing mode to DAC 
  FLS_APP_INTR: FLS SPI TEST DONE! 

  FLS_APP_INTR: Ospi configuration Register Readback values  
  FLS_APP_INTR: CONFIG_REG                                      : 0xc1083881
  FLS_APP_INTR: DEV_INSTR_RD_CONFIG_REG                   : 0x190333ee
  FLS_APP_INTR: DEV_INSTR_WR_CONFIG_REG                   : 0x33012
  FLS_APP_INTR: DEV_DELAY_REG                               : 0x300000a
  FLS_APP_INTR: DEV_SIZE_CONFIG_REG                           : 0x121003
  FLS_APP_INTR: SRAM_PARTITION_CFG_REG                      : 0x3f
  FLS_APP_INTR: DMA_PERIPH_CONFIG_REG                       : 0x0
  FLS_APP_INTR: MODE_BIT_CONFIG_REG                           : 0x0
  FLS_APP_INTR: TX_THRESH_REG                               : 0x1
  FLS_APP_INTR: RX_THRESH_REG                               : 0x1
  FLS_APP_INTR: PHY_CONFIGURATION_REG                       : 0x0

  FLS_APP_INTR: All tests have passed! 

Back To Top


References

Back To Top