![]() |
MCUSW
|
This component provides services for initialization and control of the ICU unit. The ICU module captures and measures signals. signal period time.
Sub Modules | |
| ICU Configuration | |
| ICU Driver Interrupt Handlers | |
ICU Driver ID Info | |
| #define | ICU_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. | |
| #define | ICU_MODULE_ID ((uint16) 122U) |
| ICU Driver Module ID. | |
| #define | ICU_INSTANCE_ID ((uint8) 0U) |
| ICU Driver Instance ID. | |
ICU Driver Module SW Version Info | |
Defines for ICU Driver version used for compatibility checks | |
| #define | ICU_SW_MAJOR_VERSION (9U) |
| Driver Implementation Major Version. | |
| #define | ICU_SW_MINOR_VERSION (1U) |
| Driver Implementation Minor Version. | |
| #define | ICU_SW_PATCH_VERSION (2U) |
| Driver Implementation Patch Version. | |
ICU Driver Module AUTOSAR Version Info | |
Defines for ICU Driver AUTOSAR version used for compatibility checks | |
| #define | ICU_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by ICU Driver. | |
| #define | ICU_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by ICU Driver. | |
| #define | ICU_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by ICU Driver. | |
ICU Service IDs | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | ICU_INIT_ID ((uint8) 0x00U) |
| Icu_Init() API Service ID. | |
| #define | ICU_DEINIT_ID ((uint8) 0x01U) |
| Icu_DeInit() API Service ID. | |
| #define | ICU_SETMODE_ID ((uint8) 0x02U) |
| Icu_SetMode() API Service ID. | |
| #define | ICU_SETACTIVATIONCONDITION_ID ((uint8) 0x05U) |
| Icu_SetActivationCondition() API Service ID. | |
| #define | ICU_DISABLENOTIFICATION_ID ((uint8) 0x06U) |
| Icu_DisableNotification() API Service ID. | |
| #define | ICU_ENABLENOTIFICATION_ID ((uint8) 0x07U) |
| Icu_EnableNotification() API Service ID. | |
| #define | ICU_GETINPUTSTATE_ID ((uint8) 0x08U) |
| Icu_GetInputState() API Service ID. | |
| #define | ICU_STARTTIMESTAMP_ID ((uint8) 0x09U) |
| Icu_StartTimestamp() API Service ID. | |
| #define | ICU_STOPTIMESTAMP_ID ((uint8) 0x0AU) |
| Icu_StopTimestamp() API Service ID. | |
| #define | ICU_GETTIMESTAMPINDEX_ID ((uint8) 0x0BU) |
| Icu_GetTimeStampIndex() API Service ID. | |
| #define | ICU_RESETEDGECOUNT_ID ((uint8) 0x0CU) |
| Icu_ResetEdgeCount() API Service ID. | |
| #define | ICU_ENABLEEDGECOUNT_ID ((uint8) 0x0DU) |
| Icu_EnableEdgeCount() API Service ID. | |
| #define | ICU_ENABLEEDGEDETECTION_ID ((uint8) 0x16U) |
| Icu_EnableEdgeDetection() API Service ID. | |
| #define | ICU_DISABLEEDGEDETECTION_ID ((uint8) 0x17U) |
| Icu_DisableEdgeDetection() API Service ID. | |
| #define | ICU_DISABLEEDGECOUNT_ID ((uint8) 0x0EU) |
| Icu_DisableEdgeCount() API Service ID. | |
| #define | ICU_GETEDGENUMBERS_ID ((uint8) 0x0FU) |
| Icu_GetEdgeNumbers() API Service ID. | |
| #define | ICU_STARTSIGNALMEASUREMENT_ID ((uint8) 0x13U) |
| Icu_StartSignalMeasurement() API Service ID. | |
| #define | ICU_STOPSIGNALMEASUREMENT_ID ((uint8) 0x14U) |
| Icu_StopSignalMeasurement() API Service ID. | |
| #define | ICU_GETTIMEELAPSED_ID ((uint8) 0x10U) |
| Icu_GetTimeElapsed() API Service ID. | |
| #define | ICU_GETDUTYCYCLEVALUES_ID ((uint8) 0x11U) |
| Icu_GetDutyCycleValues() API Service ID. | |
| #define | ICU_GETVERSIONINFO_ID ((uint8) 0x12U) |
| Icu_GetVersionInfo() API Service ID. | |
| #define | ICU_SID_REGISTER_READBACK ((uint8) 0x18U) |
| Icu_Regesterreadback() API Serviece ID. | |
ICU Error Codes | |
Error codes returned by ICU functions | |
| #define | ICU_E_PARAM_POINTER ((uint8) 0x0AU) |
| API service called with invalid pointer. | |
| #define | ICU_E_PARAM_CHANNEL ((uint8) 0x0BU) |
| API service called with invalid channel identifier or channel not configured. | |
| #define | ICU_E_PARAM_ACTIVATION ((uint8) 0x0CU) |
| API service calleed with an invalid or not feasible activation. | |
| #define | ICU_E_INIT_FAILED ((uint8) 0x0DU) |
| Init Function Failed. | |
| #define | ICU_E_PARAM_BUFFER_SIZE ((uint8) 0x0EU) |
| API service used with invalid Buffer size. | |
| #define | ICU_E_PARAM_MODE ((uint8) 0x0FU) |
| API service called with invalid mode. | |
| #define | ICU_E_UNINIT ((uint8) 0x14U) |
| API service calleed without module initialisation. | |
| #define | ICU_E_NOT_STARTED ((uint8) 0x16U) |
| Icu_StopTimestamp called on channel not started or already stopped. | |
| #define | ICU_E_BUSY_OPERATION ((uint8) 0x16U) |
| API service called while a running operation. | |
| #define | ICU_E_ALREADY_INITIALIZED ((uint8) 0x17U) |
| API service Icu_Init called when module already initialized. | |
| #define | ICU_E_PARAM_NOTIFY_INTERVAL ((uint8) 0x18U) |
| API service called when notify interval is invalid. | |
| #define | ICU_E_PARAM_VINFO ((uint8) 0x19U) |
| API service Icu_GetVersionInfo called and parameter is invalid. | |
ICU Driver State Values | |
The ICU Driver State Values | |
| #define | ICU_STATUS_UNINIT ((uint8)(0U)) |
| ICU driver Status uninitialized. | |
| #define | ICU_STATUS_INIT ((uint8)(1U)) |
| ICU driver Status Initialized. | |
Macros to define Rising and Falling edge config for capture registers | |
| #define | ICU_FALLING ((uint8)(0U)) |
| Capture regsiter configuration for FALLING edge | |
| #define | ICU_RISING ((uint8)(1U)) |
| Capture regsiter configuration for RISING edge | |
| enum | Icu_ModeType { ICU_MODE_NORMAL , ICU_MODE_SLEEP } |
| This type defines a range of mode type. More... | |
| enum | Icu_InputStateType { ICU_ACTIVE , ICU_IDLE } |
| This type defines a input state of ICU driver. More... | |
| enum | Icu_ActivationType { ICU_RISING_EDGE , ICU_FALLING_EDGE , ICU_BOTH_EDGES } |
| This type defines Activation range. More... | |
| enum | Icu_MeasurementModeType { ICU_MODE_SIGNAL_EDGE_DETECT , ICU_MODE_SIGNAL_MEASUREMENT , ICU_MODE_TIMESTAMP , ICU_MODE_EDGE_COUNTER } |
| This type defines available measurement modes. More... | |
| enum | Icu_SignalMeasurementPropertyType { ICU_LOW_TIME , ICU_HIGH_TIME , ICU_PERIOD_TIME , ICU_DUTY_CYCLE } |
| This type defines Signal Measurement Property range. More... | |
| enum | Icu_TimestampBufferType { ICU_LINEAR_BUFFER , ICU_CIRCULAR_BUFFER } |
| This type defines TimeStamp Property range. More... | |
| typedef uint32 | Icu_ValueType |
| This type defines Value type. | |
| typedef uint32 | Icu_IndexType |
| This type defines return value Icu_GetTimeStampIndex. | |
| typedef uint32 | Icu_EdgeNumberType |
| This type defines return value of Icu-Icu_GetEdgeNumbers. | |
| typedef void(* | Icu_NotifyFuncType) (void) |
| Notification callback function pointer | |
| typedef uint8 | Icu_ChannelType |
| This type defines Channel type. | |
| typedef uint32 | Icu_ChannelPrescalerType |
| This type defines Prescaler type. | |
| void | Icu_Init (const Icu_ConfigType *ConfigPtr) |
| Service for ICU initialization. | |
| void | Icu_DeInit (void) |
| Service for ICU de-initialization. | |
| void | Icu_SetActivationCondition (Icu_ChannelType Channel, Icu_ActivationType Activation) |
| Service for setting Activation Condition. | |
| void | Icu_DisableNotification (Icu_ChannelType Channel) |
| Service for disabling notification. | |
| void | Icu_EnableNotification (Icu_ChannelType Channel) |
| Service for enabling notification. | |
| Icu_InputStateType | Icu_GetInputState (Icu_ChannelType Channel) |
| Service for getting the ICU input status. | |
| void | Icu_StartTimestamp (Icu_ChannelType Channel, Icu_ValueType *BufferPtr, uint16 BufferSize, uint16 NotifyInterval) |
| Service for starts the captuing of timer values on the edges. | |
| void | Icu_StopTimestamp (Icu_ChannelType Channel) |
| Service for stopping the timestamp measurement. | |
| Icu_IndexType | Icu_GetTimestampIndex (Icu_ChannelType Channel) |
| Service for reading the timestamp index of a givem channel. | |
| void | Icu_ResetEdgeCount (Icu_ChannelType Channel) |
| Service for resets the value of the counted edges to zero. | |
| void | Icu_EnableEdgeCount (Icu_ChannelType Channel) |
| Service enabling the counting of edges of a given channel. | |
| void | Icu_DisableEdgeCount (Icu_ChannelType Channel) |
| Service for disabling the couting of edges of the given channel. | |
| Icu_EdgeNumberType | Icu_GetEdgeNumbers (Icu_ChannelType Channel) |
| Service for reading the number of counted edges. | |
| void | Icu_EnableEdgeDetection (Icu_ChannelType Channel) |
| Service for enabling/re-enabling the detection of edges of the given channel. | |
| void | Icu_DisableEdgeDetection (Icu_ChannelType Channel) |
| Service for disabling the detection of edges of the given channel. | |
| void | Icu_StartSignalMeasurement (Icu_ChannelType Channel) |
| Service for starting the measurement of signals. | |
| void | Icu_StopSignalMeasurement (Icu_ChannelType Channel) |
| Service for stopping the measurement of signals. | |
| Icu_ValueType | Icu_GetTimeElapsed (Icu_ChannelType Channel) |
| Service for reading the elasped time for the given channel. | |
| void | Icu_GetDutyCycleValues (Icu_ChannelType Channel, Icu_DutyCycleType *DutyCycleValues) |
| Service for reading the coherent active time and period time of given channel. | |
| void | Icu_CheckWakeup (EcuM_WakeupSourceType WakeupSource) |
| This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event. | |
| void | Icu_DisableWakeup (Icu_ChannelType Channel) |
| This function disables the wakeup capability of a single ICU channel. | |
| void | Icu_EnableWakeup (Icu_ChannelType Channel) |
| This function (re-)enables the wakeup capability of the given ICU channel. | |
| void | Icu_SetMode (Icu_ModeType Mode) |
| This function sets the ICU mode. | |
| Std_ReturnType | Icu_RegisterReadback (Icu_ChannelType IcuChannel, Icu_RegisterReadbackType *RegRbPtr) |
| Icu_IndexType | Icu_GetTimeStampIndex (Icu_ChannelType Channel) |
| #define ICU_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID.
| #define ICU_MODULE_ID ((uint16) 122U) |
ICU Driver Module ID.
| #define ICU_INSTANCE_ID ((uint8) 0U) |
ICU Driver Instance ID.
| #define ICU_SW_MAJOR_VERSION (9U) |
Driver Implementation Major Version.
| #define ICU_SW_MINOR_VERSION (1U) |
Driver Implementation Minor Version.
| #define ICU_SW_PATCH_VERSION (2U) |
Driver Implementation Patch Version.
| #define ICU_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by ICU Driver.
| #define ICU_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by ICU Driver.
| #define ICU_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by ICU Driver.
| #define ICU_INIT_ID ((uint8) 0x00U) |
Icu_Init() API Service ID.
| #define ICU_DEINIT_ID ((uint8) 0x01U) |
Icu_DeInit() API Service ID.
| #define ICU_SETMODE_ID ((uint8) 0x02U) |
Icu_SetMode() API Service ID.
| #define ICU_SETACTIVATIONCONDITION_ID ((uint8) 0x05U) |
Icu_SetActivationCondition() API Service ID.
| #define ICU_DISABLENOTIFICATION_ID ((uint8) 0x06U) |
Icu_DisableNotification() API Service ID.
| #define ICU_ENABLENOTIFICATION_ID ((uint8) 0x07U) |
Icu_EnableNotification() API Service ID.
| #define ICU_GETINPUTSTATE_ID ((uint8) 0x08U) |
Icu_GetInputState() API Service ID.
| #define ICU_STARTTIMESTAMP_ID ((uint8) 0x09U) |
Icu_StartTimestamp() API Service ID.
| #define ICU_STOPTIMESTAMP_ID ((uint8) 0x0AU) |
Icu_StopTimestamp() API Service ID.
| #define ICU_GETTIMESTAMPINDEX_ID ((uint8) 0x0BU) |
Icu_GetTimeStampIndex() API Service ID.
| #define ICU_RESETEDGECOUNT_ID ((uint8) 0x0CU) |
Icu_ResetEdgeCount() API Service ID.
| #define ICU_ENABLEEDGECOUNT_ID ((uint8) 0x0DU) |
Icu_EnableEdgeCount() API Service ID.
| #define ICU_ENABLEEDGEDETECTION_ID ((uint8) 0x16U) |
Icu_EnableEdgeDetection() API Service ID.
| #define ICU_DISABLEEDGEDETECTION_ID ((uint8) 0x17U) |
Icu_DisableEdgeDetection() API Service ID.
| #define ICU_DISABLEEDGECOUNT_ID ((uint8) 0x0EU) |
Icu_DisableEdgeCount() API Service ID.
| #define ICU_GETEDGENUMBERS_ID ((uint8) 0x0FU) |
Icu_GetEdgeNumbers() API Service ID.
| #define ICU_STARTSIGNALMEASUREMENT_ID ((uint8) 0x13U) |
Icu_StartSignalMeasurement() API Service ID.
| #define ICU_STOPSIGNALMEASUREMENT_ID ((uint8) 0x14U) |
Icu_StopSignalMeasurement() API Service ID.
| #define ICU_GETTIMEELAPSED_ID ((uint8) 0x10U) |
Icu_GetTimeElapsed() API Service ID.
| #define ICU_GETDUTYCYCLEVALUES_ID ((uint8) 0x11U) |
Icu_GetDutyCycleValues() API Service ID.
| #define ICU_GETVERSIONINFO_ID ((uint8) 0x12U) |
Icu_GetVersionInfo() API Service ID.
| #define ICU_SID_REGISTER_READBACK ((uint8) 0x18U) |
Icu_Regesterreadback() API Serviece ID.
| #define ICU_E_PARAM_POINTER ((uint8) 0x0AU) |
API service called with invalid pointer.
| #define ICU_E_PARAM_CHANNEL ((uint8) 0x0BU) |
API service called with invalid channel identifier or channel not configured.
| #define ICU_E_PARAM_ACTIVATION ((uint8) 0x0CU) |
API service calleed with an invalid or not feasible activation.
| #define ICU_E_INIT_FAILED ((uint8) 0x0DU) |
Init Function Failed.
| #define ICU_E_PARAM_BUFFER_SIZE ((uint8) 0x0EU) |
API service used with invalid Buffer size.
| #define ICU_E_PARAM_MODE ((uint8) 0x0FU) |
API service called with invalid mode.
| #define ICU_E_UNINIT ((uint8) 0x14U) |
API service calleed without module initialisation.
| #define ICU_E_NOT_STARTED ((uint8) 0x16U) |
Icu_StopTimestamp called on channel not started or already stopped.
| #define ICU_E_BUSY_OPERATION ((uint8) 0x16U) |
API service called while a running operation.
| #define ICU_E_ALREADY_INITIALIZED ((uint8) 0x17U) |
API service Icu_Init called when module already initialized.
| #define ICU_E_PARAM_NOTIFY_INTERVAL ((uint8) 0x18U) |
API service called when notify interval is invalid.
| #define ICU_E_PARAM_VINFO ((uint8) 0x19U) |
API service Icu_GetVersionInfo called and parameter is invalid.
| #define ICU_STATUS_UNINIT ((uint8)(0U)) |
ICU driver Status uninitialized.
| #define ICU_STATUS_INIT ((uint8)(1U)) |
ICU driver Status Initialized.
| #define ICU_FALLING ((uint8)(0U)) |
Capture regsiter configuration for FALLING edge
| #define ICU_RISING ((uint8)(1U)) |
Capture regsiter configuration for RISING edge
| typedef uint32 Icu_ValueType |
This type defines Value type.
| typedef uint32 Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex.
| typedef uint32 Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers.
| typedef void(* Icu_NotifyFuncType) (void) |
Notification callback function pointer
| typedef uint8 Icu_ChannelType |
This type defines Channel type.
| typedef uint32 Icu_ChannelPrescalerType |
This type defines Prescaler type.
| enum Icu_ModeType |
| enum Icu_InputStateType |
| enum Icu_ActivationType |
| void Icu_Init | ( | const Icu_ConfigType * | ConfigPtr | ) |
Service for ICU initialization.
* Service name : Icu_Init * Syntax : Icu_Init(const Icu_ConfigType* ConfigPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Pointer to the configuration * Parameters (out) : None * Return value : void * Description : Initializes internal variables * and the ECAP unit of the micro controller. * The function can be called on task level. *
| void Icu_DeInit | ( | void | ) |
Service for ICU de-initialization.
* Service name : Icu_DeInit * Syntax : Icu_DeInit(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (out) : None * Return value : void * Description : DeInit ECAP module *
| void Icu_SetActivationCondition | ( | Icu_ChannelType | Channel, |
| Icu_ActivationType | Activation ) |
Service for setting Activation Condition.
* Service name : Icu_SetActivationCondition * Syntax : Icu_SetActivationCondition(Icu_ChannelType Channel, * Icu_ActivationType Activation) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : Icu_ActivationType Activation * Parameters (out) : None * Return value : void * Description : This service sets the Activation edge for channel * Type of activation (if supported by hardware) * ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES *
| void Icu_DisableNotification | ( | Icu_ChannelType | Channel | ) |
Service for disabling notification.
* Service name : Icu_DisableNotification * Syntax : Icu_DisableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the notificaiton of a channel *
| void Icu_EnableNotification | ( | Icu_ChannelType | Channel | ) |
Service for enabling notification.
* Service name : Icu_EnableNotification * Syntax : Icu_EnableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the notificaiton of a channel *
| Icu_InputStateType Icu_GetInputState | ( | Icu_ChannelType | Channel | ) |
Service for getting the ICU input status.
* Service name : Icu_GetInputState * Syntax : Icu_GetInputState(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service returns the status of the ICU input *
| void Icu_StartTimestamp | ( | Icu_ChannelType | Channel, |
| Icu_ValueType * | BufferPtr, | ||
| uint16 | BufferSize, | ||
| uint16 | NotifyInterval ) |
Service for starts the captuing of timer values on the edges.
* Service name : Icu_StartTimestamp * Syntax : Icu_StartTimestamp(Icu_ChannelType Channel, * Icu_ValueType* BufferPtr, * uint16 BufferSize, * uint16 NotifyInterval) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x09 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : uint16 BufferSize * Parameters (in) : uint16 NotifyInterval * Parameters (out) : Icu_ValueType* BufferPtr * Return value : void * Description : This service starts the capturing of timer values on the edges *
| void Icu_StopTimestamp | ( | Icu_ChannelType | Channel | ) |
Service for stopping the timestamp measurement.
* Service name : Icu_StopTimestamp * Syntax : Icu_StopTimestamp(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops timestamp measurement of the given channel. *
| Icu_IndexType Icu_GetTimestampIndex | ( | Icu_ChannelType | Channel | ) |
Service for reading the timestamp index of a givem channel.
* Service name : Icu_GetTimestampIndex * Syntax : Icu_GetTimestampIndex(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0B * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the timestamp index of a given channel. *
| void Icu_ResetEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for resets the value of the counted edges to zero.
* Service name : Icu_ResetEdgeCount * Syntax : Icu_ResetEdgeCount(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0C * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service resets the value of the counted edges to zero. *
| void Icu_EnableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service enabling the counting of edges of a given channel.
* Service name : Icu_EnableEdgeCount * Syntax : Icu_EnableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0D * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the couting of edges of the given channel. *
| void Icu_DisableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for disabling the couting of edges of the given channel.
* Service name : Icu_DisableEdgeCount * Syntax : Icu_DisableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0E * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the couting of edges of a given channel. *
| Icu_EdgeNumberType Icu_GetEdgeNumbers | ( | Icu_ChannelType | Channel | ) |
Service for reading the number of counted edges.
* Service name : Icu_GetEdgeNumbers * Syntax : Icu_GetEdgeNumbers(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0F * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the number of counted edges. *
| void Icu_EnableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for enabling/re-enabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x16 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables/re-enables the detection of edges of a channel. *
| void Icu_DisableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for disabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x17 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the detection of edges of a channel. *
| void Icu_StartSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for starting the measurement of signals.
* Service name : Icu_StartSignalMeasurement * Syntax : Icu_StartSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x13 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service starts the measurement of signals of a given channel. *
| void Icu_StopSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for stopping the measurement of signals.
* Service name : Icu_StopSignalMeasurement * Syntax : Icu_StopSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x14 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops the measurement of signals of a given channel. *
| Icu_ValueType Icu_GetTimeElapsed | ( | Icu_ChannelType | Channel | ) |
Service for reading the elasped time for the given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads elasped time for a given channel. *
| void Icu_GetDutyCycleValues | ( | Icu_ChannelType | Channel, |
| Icu_DutyCycleType * | DutyCycleValues ) |
Service for reading the coherent active time and period time of given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel, * Icu_DutyCycleType* DutyCycleValues) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x11 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : Icu_DutyCycleType* DutyCycleValues * Return value : void * Description : This service reads active time and period of given channel. *
| void Icu_CheckWakeup | ( | EcuM_WakeupSourceType | WakeupSource | ) |
This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event.
* Service name : Icu_CheckWakeup
* Syntax : void Icu_CheckWakeup(EcuM_WakeupSourceType WakeupSource)
* Service ID[hex] : 0x19
* Sync/Async : Synchronous
* Reentrancy : Reentrant(limited according to ICU050)
* Parameters (in) : WakeupSource
* Informatin on wakeup source to be checked.
The associated ICU channel can be determined from configuration data
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Checks if a wakeup capable ICU channel is the source for a wakeup event and
* calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU
* channel wakeup event.
*
| void Icu_DisableWakeup | ( | Icu_ChannelType | Channel | ) |
This function disables the wakeup capability of a single ICU channel.
* Service name : Icu_DisableWakeup * Syntax : void Icu_DisableWakeup(Icu_ChannelType Channel) * Service ID[hex] : 0x20 * Sync/Async : Synchronous * Reentrancy : Reentrant(limited according to ICU050) * Parameters (in) : Channel * Numeric identifier of the ICU channel * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function disables the wakeup capability of a single ICU channel. *
| void Icu_EnableWakeup | ( | Icu_ChannelType | Channel | ) |
This function (re-)enables the wakeup capability of the given ICU channel.
* Service name : Icu_EnableWakeup * Syntax : void Icu_EnableWakeup(Icu_ChannelType Channel) * Service ID[hex] : 0x21 * Sync/Async : Synchronous * Reentrancy : Reentrant(limited according to ICU050) * Parameters (in) : Channel * Numeric identifier of the ICU channel * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function (re-)enables the wakeup capability of the given ICU channel. *
| void Icu_SetMode | ( | Icu_ModeType | Mode | ) |
This function sets the ICU mode.
* Service name : Icu_SetMode * Syntax : void Icu_SetMode(Icu_ModeType Mode) * Service ID[hex] : 0x22 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Mode * ICU_MODE_NORMAL: Normal operation, all used interrupts are enabled * according to the notification requests. * ICU_MODE_SLEEP: Reduced power mode. In sleep mode only those * notifications are available which are configured as wakeup capable. * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function sets the ICU mode. *
| Std_ReturnType Icu_RegisterReadback | ( | Icu_ChannelType | IcuChannel, |
| Icu_RegisterReadbackType * | RegRbPtr ) |
| Icu_IndexType Icu_GetTimeStampIndex | ( | Icu_ChannelType | Channel | ) |